Post Go back to editing

FPGA Reference Design

Thread Summary

The user is facing issues routing custom CW generator DMA data to the DAC output in the ADRV9364-Z7020 reference design. The final answer suggests adding a 0x4000 offset to the DAC regmap and clarifies that reading 0xDEADDEAD from registers indicates an undefined register space. The correct configuration sequence for routing DMA data to the DAC is not explicitly provided.
AI Generated Content
Category: Hardware

 Hi ,
For my earlier thread,
https://ez.analog.com/fpga/f/q-a/601964/issue-connecting-custom-cw-generator-to-dac-fifo-in-adrv9364z7020-reference-design

Based on the guidance provided there, I attempted to change the DAC_DDS_SEL mux setting to route DMA data to the DAC output. However, I am facing some issues and would appreciate your support.

From the Address Editor, the base address for the DAC core (axi_ad9361) is:

  • Base Address: 0x7902_0000

To control the DAC_DDS_SEL mux for Channel-0, I used the following calculation:

  • IP Base Address: 0x7902_0000

  • Register Offset (CHAN_CNTRLn_7): 0x0418

  • Final Address: 0x7902_0418

For the remaining channels, I used the formula:

address = 0x79020000 + 0x418 + (n * 0x40)

Using this formula, I calculated the addresses for all channels and wrote the value 0x2 (to select DMA input data) using devmem in order to route DMA data to the DAC.

However, I am still unable to observe my custom CW signal (implemented in HDL) at the DAC output. Additionally, from around the third channel onward, it seems that register writes are not taking effect. When I read back the register values for those channels, the value returned is 0xDEADDEAD (screenshot attached).

I have the following questions:

  1. What is the correct configuration sequence to route DMA data to the DAC?

  2. Why am I seeing 0xDEADDEAD when reading some channel register addresses?
    Does this indicate an invalid or unmapped address region,?

Could you please help clarify the correct configuration procedure and the reason for this behavior?


Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.