Post Go back to editing

Change Hdl design clk rates

Thread Summary

The user wants to change the clock rates of util_dac, util_adc, tx2_dma, and rx2_dma to 15.26 MHz in the ADRV9001-ZCU102 project. The final answer suggests that the clock rate is determined by the sampling rate and interface configuration, which can be adjusted by uploading a new profile. The user is advised to refer to the AXI ADRV9001 documentation for more details on interface clock frequencies and to ensure that changing the clock rates does not cause timing issues.
AI Generated Content
Category: Software
Product Number: ADRV9002
Software Version: Vivado 2022.1

Hello Everyone ,

Actually i have a doubt in adrv9001_zcu102 project

i want to set util_dac , util_adc , tx2_dma , rx2_dma clock rates for my convenience so that i can work according with my pl and work at the rate which i required

how can i change it in root directory in zcu102 or any where in the hdl block design 

please reply if anyone knows about it 

Thread Notes

Parents Reply Children
No Data