Post Go back to editing

Porting Reference Design to VCK190

Thread Summary

The user attempted to port the ADRV9009 reference design from the ZCU102 to the VCK190 but encountered issues. The final answer indicates that the VCK190 does not support the ADRV9009 due to voltage incompatibility, with the ADRV9009 requiring a minimum of 1.7V and the VCK190 providing a maximum of 1.5V. Alternative examples for the VCK190 using the AD9081 and AD9084 transceivers are suggested.
AI Generated Content
Category: Hardware
Product Number: ADRV9009

I want to take the example design for the ZCU102 for the ADRV9009 and port it over to the VCK190. I attempted to do this however am running into trouble with how to reconfigure the files. I am following this guide on how to port reference designs to other boards but am running into lots of issues (https://analogdevicesinc.github.io/hdl/user_guide/porting_project.html). Can attach my current project code if needed. 

Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.