Post Go back to editing

ZCU102 Rev D1: SPI1 Clock Divider Failure Affecting ALL FMC Cards (ADRV9009, FMCOMMS4)

Thread Summary

The user is experiencing a SPI1 clock configuration failure on a ZCU102 Rev D1 board, preventing ADRV9009-W/PCBZ and FMCOMMS4 (AD9364) FMC cards from working. The error occurs at boot time and is related to the PMU firmware rejecting the clock divider setup. The final answer suggests verifying the FMC connector used (ADRV9009 should use HPC1, FMCOMMS4 uses HPC0) and checking for any damage to the FMC pins. The accompanying answers note that the VADJ voltage should be checked and that this issue has not been reported before.
AI Generated Content
Category: Hardware
Product Number: ADRV9009

I am experiencing a **SPI1 clock configuration failure** on my ZCU102 Rev D1 board that prevents **all** FMC cards from working. Both ADRV9009-W/PCBZ and FMCOMMS4 (AD9364) fail with SPI communication errors. The root cause appears to be: ``` zynqmp_clk_divider_set_rate() set divider failed for spi1_ref_div1, ret = -13 ``` This error occurs at boot time before any device-specific driver loads, causing SPI1 to malfunction while SPI0 (QSPI flash) works perfectly. --- ## Hardware Configuration - **Carrier Board:** Xilinx ZCU102 Rev D1 - **FMC Cards Tested:** - ADRV9009-W/PCBZ (on HPC0) - FMCOMMS4 / AD9364 (on HPC0) - **Software:** ADI Kuiper Linux (tested 2021 and latest images) - **Boot Mode:** SD Card --- ## The Problem ### Error Message (appears on EVERY boot): ``` [ 3.645235] zynqmp_clk_divider_set_rate() set divider failed for spi1_ref_div1, ret = -13 ``` Error -13 is `EACCES` (Permission denied), indicating the PMU firmware is rejecting the clock divider configuration request. ### Result with ADRV9009: ``` [ 12.199560] iio iio:device1: SPI Read Verify failed (0xFFFFFF) [ 12.205424] ad9528 spi1.0: Dropping the link to regulator.0 [ 12.211068] ad9528: probe of spi1.0 failed with error -5 ``` ### Result with FMCOMMS4 (AD9364): ``` [ 7.941805] ad9361 spi1.0: ad9361_probe : Unsupported PRODUCT_ID 0xFF ``` Both cards return **0xFF/0xFFFFFF** on SPI reads, indicating the MISO line is stuck high (no response from devices). --- ## Key Finding: SPI0 Works, SPI1 Fails | Interface | Device | Result | |-----------|--------|--------| | SPI0 | QSPI Flash (m25p80) | White check mark **Works perfectly** | | SPI1 | ADRV9009 AD9528 | X Returns 0xFFFFFF | | SPI1 | FMCOMMS4 AD9364 | X Returns 0xFF | | I2C | FMC EEPROM | White check mark Works | | I2C | AD7291 (ADRV9009) | White check mark Works | **This proves the FMC connector and cards are fine - only SPI1 is broken.** --- ## Testing Performed ### 1. Multiple FMC Cards - ADRV9009-W/PCBZ → SPI1 fails - FMCOMMS4 → SPI1 fails - Both cards' I2C devices work fine ### 2. Multiple BOOT.BIN Files - ADRV9009 BOOT.BIN (15.3 MB) → Same SPI1 clock error - FMCOMMS4 BOOT.BIN (9.9 MB) → Same SPI1 clock error ### 3. Multiple Kuiper Linux Versions - 2021 Kuiper image → SPI1 clock error - Latest Kuiper image → SPI1 clock error ### 4. ZCU102 Rev D1 VADJ Fix - Applied I2C commands to enable VADJ 1.8V - VADJ confirmed at 1798mV - DS15 LED is GREEN - **SPI1 still fails** --- ## Clock Status Analysis ```bash root@analog:~# cat /sys/kernel/debug/clk/clk_summary | grep -i spi spi1_ref_mux 0 0 0 <-- enable_count = 0 (NOT ENABLED) spi1_ref_div1 0 0 0 spi1_ref 0 0 0 qspi_ref_mux 1 1 1 <-- enable_count = 1 (ENABLED) qspi_ref_div1 1 1 1 qspi_ref 1 1 1 ``` The **qspi_ref** clock (SPI0) has enable_count = 1 and works. The **spi1_ref** clock has enable_count = 0 - it never got enabled due to the divider failure! --- ## PMU Firmware Version ``` zynqmp_firmware_probe Platform Management API v1.1 ``` From BOOT.BIN strings: ``` v2.0(release):xilinx-v2019.2 ``` --- ## Board Details - **ZCU102 Revision:** Rev D1 (older board, unused for extended period) - **Known Rev D1 Issue:** VADJ defaults to 0V (already worked around via I2C) - **Suspected Issue:** PMU firmware incompatibility or corruption --- ## What I've Ruled Out | Potential Cause | Status | |-----------------|--------| | ADRV9009 card defective | X Ruled out - FMCOMMS4 also fails | | FMCOMMS4 card defective | X Ruled out - ADRV9009 also fails | | FMC connector issue | X Ruled out - I2C works on both cards | | Wrong BOOT.BIN | X Ruled out - Multiple tested, same error | | Wrong Kuiper image | X Ruled out - Multiple versions tested | | VADJ power issue | X Ruled out - 1.8V verified | | Software/driver issue | X Ruled out - Clock error is in PMU/kernel | --- ## Questions for ADI/Xilinx Community 1. **Is this a known ZCU102 Rev D1 issue?** Similar to the VADJ bug that requires I2C workaround? 2. **Can the SPI1 clock be enabled manually?** Is there a workaround like the VADJ fix? 3. **Does the ZCU102 need a PMU firmware update?** If so, what is the procedure for updating the onboard QSPI firmware? 4. **Is error -13 (EACCES) from PMU normal?** What would cause the PMU to reject a clock divider request? 5. **Has anyone else experienced this?** Especially with older ZCU102 boards that sat unused? --- ## Technical Details ### GPIO Status (Reset lines are correct): ``` gpio-137: AD9528 reset - direction: out, value: 1 (de-asserted) ``` ### FMC EEPROM Readable (proves FMC connection is good): ``` root@analog:~# cat /sys/bus/i2c/devices/16-0050/eeprom | hexdump -C | head -5 00000000 01 00 00 01 00 0e 00 f0 01 0d 19 e5 e7 da 8b a1 ... ``` ### SPI Devices Present: ``` root@analog:~# ls /sys/bus/spi/devices/ spi0.0 spi1.0 spi1.1 ``` --- ## Summary This is **not an FMC card issue** - it's a **ZCU102 SPI1 clock configuration failure** that affects all FMC cards. The PMU firmware (error -13) is rejecting the SPI1 clock divider setup, causing SPI1 to be non-functional while SPI0 works fine. I suspect this may be related to: - Old/incompatible PMU firmware on the ZCU102's onboard QSPI - A ZCU102 Rev D1 specific bug (like the VADJ issue) - Possible corruption from the board sitting unused Any guidance on updating the ZCU102's onboard firmware or working around this SPI1 clock issue would be greatly appreciated. ---

Thread Notes

Parents
  •  I don't remember customers reporting this issue earlier.

    Can you please check if you are able to get the interface voltage (VADJ )?

    Are you using the correct HPC slot in the FMC connector while connecting to ZCU102 and also can you check if there is any damage to the FMC Pins connector in ZCU102 /daughter card?

    Will move to FPGA reference designs forum for further comments .

  • Hi,

    The Interface VADJ is set to 1.8V and is on HPC0.

    I suspect that the Rev D1 of the ZCU102 i am using could be the culprit here. Please let me know if there's an ADI image available specifically for this Rev of the ZCU102?

  • Hello  ,

    We discussed this internally and we don't have specific boot files for this revision of ZCU102. The one we have for testing is Rev 1.1, but we don't know what differences might be between these revisions. We advise you to contact Xilinx on this matter.

    Kind regards,

    Stanca

Reply Children
  • Hi Stanca,

    Thank you for checking internally. I understand ADI tests on Rev 1.1 and doesn't have Rev D1 hardware available.

    Before I go to Xilinx, I'd like to clarify a few things on the ADI side since the boot files (BOOT.BIN, devicetree.dtb) are generated from ADI's HDL and build system:

    1. Are there any plans to produce ADI boot files that support ZCU102 Rev D1? Even if Rev 1.1 is the primary test platform, Rev D1 boards are still in circulation and this would help anyone else hitting this issue.

    2. Is it possible to take the existing Rev 1.1 boot files and modify them to work on Rev D1? Specifically, the SPI1 clock failure (spi1_ref_div1 ret=-13) suggests the PMU firmware or device tree in the current BOOT.BIN has clock permission settings that don't match Rev D1 silicon. If the difference is isolated to PMU configuration or device tree clock phandles, a targeted fix might be straightforward.

    3. If modification is possible, what exactly would need to change? For example:
       - Does the PMU firmware need to be rebuilt with different clock access permissions for Rev D1?
       - Are there device tree clock index or phandle differences between Rev D1 and Rev 1.1 that I could patch manually?
       - Is it a matter of swapping just the PMU firmware ELF inside BOOT.BIN while keeping the FSBL and bitstream the same?

    I want to make sure I'm not duplicating effort, if ADI can point me to what's Rev-specific in the build, I can likely make the modifications myself. Otherwise I'll take this to Xilinx, but they won't have context on the ADI HDL/driver side.

    Thanks.

  • Hello  ,

    Thank you for your interest and patience on this matter.

    1. We do not have the resources to research and support older version of zcu102.
    2. We don't not know the cause of the issues in the first place, so we cannot say. You should be able to build all the files from scratch. I would go that way instead of trying to decompile /reverse built files. The PMU firmware is built with the FSBL.
      wiki-scripts/zynqmp_boot_bin/build_zynqmp_boot_bin.sh at main · analogdevicesinc/wiki-scripts
    3. You can build the FSBL and check if there are things to change.

    The u-boot is built from this repo: History for configs - analogdevicesinc/u-boot-xlnx

    Kind regards,

    Stanca

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.