Post Go back to editing

Reg usage of AD9467-FMC-250EBZ with VC707 FPGA

Thread Summary

The user is facing difficulties generating a bitstream to connect the VC707 FPGA with the AD9467-FMC-250EBZ evaluation board. The final answer provides HDL design and documentation links for the AD9467-FMC, noting that VC707 support is no longer available in the main branch. The user is advised to follow the documentation for building the HDL design in Vivado 2023.2 and porting the project to the VC707. The user is also encouraged to provide specific issues encountered for further assistance.
AI Generated Content
Category: Hardware
Product Number: AD9467

I am planning to use the VC707 FPGA with the AD9467-FMC-250EBZ evaluation board. However, the support of connecting the two, i.e., generating the bitstream is facing difficulties. Can anyone help out as to the sequence of operation and confirm if I should be using Vivado or ISE Xilinx Design Suite