I also posted this issue here: ADI HDL Github
Describe the bug
Using the axi_dmac in Vivado, I am able to transfer FIFO input data from peripheral to DDR only once using Autorun mode. But doing a software request to the same address sets the destination data to zero.
To Reproduce
- Setup Vivado project with
axi_dmacIP Block, setSourceto FIFO width 32-bit,Destinationto AXI3 64-bit wide, enableAutorunwithDestination address0x10000000. Connectfifo_wr_din[31:0]to a 32-bit constant block with0xaabbccdd(test data), andfifo_wr_ento a single bit constant of1. - Build a Vitis project with any of these sets of sources:
- no-os-driver-src.zip
- register-access-only-src.zip (uncomment line defining DMA_TEST_BUFFER1 to 0x10000000 if needed)
- Connect to Zynq PS7 UART port with baud 115200 or add breakpoint on the last line of the
whileloop. - Start debug session to flash bitfile and program elf.
- See that:
- Initial data on DMA_TEST_BUFFER1 (0x10000000) is the FIFO test data.
- Data is zeroed by
memsetat the start of thewhileloop. - DMA transaction completes and interrupt is obtained, but data on DMA_TEST_BUFFER1 (0x10000000) is still zero.
Expected behavior
Data on destination (0x10000000) should be test data (0xaabbccdd) after each DMA transaction has been completed
Desktop
- Project name: adaq23878_eval
- Carrier board: Omdazz XC7Z020 Zedboard-compatible with FMC
- Used Software: No-OS
- Tool version: Vivado 2020.2
- HDL Release version: git commit a22fce4
- No-OS Software Release version: git commit b75d62f
Additional context
Also, if I connect the DMA block to the ADC IP block, even after enabling Cyclic mode in the AXI_DMAC IP Block and setting the Autorun Flags to 0x1 (CYCLIC) or 0x7 (CYCLIC, TLAST,PARTIAL_REPORTING_EN), I only observe one DMA transfer. If I disable TESTPAT, I still see the same data on the destination buffer (0x330fc), it does not change if the ADC data changes (there is an ILA block and I can see that the ADC data is changing). Expected behavior is that the data on DDR destination would change as the ADC data changes.
Vivado block diagram with ADC block connected: design_1_adc_connected.pdf
Edit Notes
Fixed typo[edited by: bleudoutremer at 7:57 PM (GMT -4) on 10 Sep 2025]