Post Go back to editing

ADV7511 on custom board not working

Category: Software
Product Number: ADV7511
Software Version: ADI Linux 2021_R1

Hi, I am  working to  use ADV7511 hdmi output on a custom Zynq 7100 board. Have you solved the problem regarding the output of the adv7511? I'm currently encountering an issue with the abnormal output of the adv7511. I'm using the ADI HDL reference project for the zc706 and have made some modifications, mainly changing the pin definitions and removing the spdif_tx part because the spdif part of my adv7511 is not connected to the PL. I used ADI's 2021_R1 Linux and compiled the uImage. The system seems to start successfully, and there are no obvious errors in the log, but the HDMI output is a white screen. I've noticed a strange phenomenon: the interrupt count of the axi-i2c connected to the adv7511 keeps increasing, but the interrupt count of the HDMI_DMA remains at 0, as if no DMA transmission is taking place.

Does anyone have any suggestions?

Thanks!

root@analog:/proc/device-tree/fpga-axi@0/axi_hdmi@70e00000# dmesg
[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 5.10.0 (fang@fang) (arm-xilinx-linux-gnueabi-gcc.real (GCC) 10.2.0, GNU ld (GNU Binutils) 2.35.0.20200730) #1 SMP PREEMPT Wed Jan 15 13:40:15 CST 2025
[    0.000000] CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] OF: fdt: Machine model: Xilinx Zynq RK_Z7100
[    0.000000] earlycon: cdns0 at MMIO 0xe0000000 (options '115200n8')
[    0.000000] printk: bootconsole [cdns0] enabled
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] cma: Reserved 128 MiB at 0x38000000
[    0.000000] Zone ranges:
[    0.000000]   Normal   [mem 0x0000000000000000-0x000000002fffffff]
[    0.000000]   HighMem  [mem 0x0000000030000000-0x000000003fffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000000000000-0x000000003fffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000000000000-0x000000003fffffff]
[    0.000000] On node 0 totalpages: 262144
[    0.000000]   Normal zone: 1536 pages used for memmap
[    0.000000]   Normal zone: 0 pages reserved
[    0.000000]   Normal zone: 196608 pages, LIFO batch:63
[    0.000000]   HighMem zone: 65536 pages, LIFO batch:15
[    0.000000] percpu: Embedded 15 pages/cpu s29900 r8192 d23348 u61440
[    0.000000] pcpu-alloc: s29900 r8192 d23348 u61440 alloc=15*4096
[    0.000000] pcpu-alloc: [0] 0 [0] 1
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 260608
[    0.000000] Kernel command line: consolve=ttyPS0,115200 earlycon root=/dev/mmcblk0p2 rw rootwait
[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear)
[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] Memory: 886016K/1048576K available (11264K kernel code, 802K rwdata, 7488K rodata, 1024K init, 490K bss, 31488K reserved, 131072K cma-reserved, 131072K highmem)
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[    0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[    0.000000] efuse mapped to (ptrval)
[    0.000000] slcr mapped to (ptrval)
[    0.000000] L2C: platform modifies aux control register: 0x72360000 -> 0x72760000
[    0.000000] L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000
[    0.000000] L2C-310 erratum 769419 enabled
[    0.000000] L2C-310 enabling early BRESP for Cortex-A9
[    0.000000] L2C-310 full line of zeros enabled for Cortex-A9
[    0.000000] L2C-310 ID prefetch enabled, offset 1 lines
[    0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled
[    0.000000] L2C-310 cache controller enabled, 8 ways, 512 kB
[    0.000000] L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001
[    0.000000] random: get_random_bytes called from start_kernel+0x33c/0x4e0 with crng_init=0
[    0.000000] zynq_clock_init: clkc starts at (ptrval)
[    0.000000] Zynq clock init
[    0.000008] sched_clock: 64 bits at 399MHz, resolution 2ns, wraps every 4398046511103ns
[    0.005032] clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x5c4093a7d1, max_idle_ns: 440795210635 ns
[    0.014671] Switching to timer-based delay loop, resolution 2ns
[    0.019281] clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 447945978 ns
[    0.026981] timer #0 at (ptrval), irq=25
[    0.030026] Console: colour dummy device 80x30
[    0.032633] printk: console [tty0] enabled
[    0.035382] printk: bootconsole [cdns0] disabled
[    0.038669] Calibrating delay loop (skipped), value calculated using timer frequency.. 799.99 BogoMIPS (lpj=3999999)
[    0.038696] pid_max: default: 32768 minimum: 301
[    0.038870] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
[    0.038892] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
[    0.039460] CPU: Testing write buffer coherency: ok
[    0.039498] CPU0: Spectre v2: using BPIALL workaround
[    0.039676] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.040120] Setting up static identity map for 0x100000 - 0x100060
[    0.040244] rcu: Hierarchical SRCU implementation.
[    0.040495] smp: Bringing up secondary CPUs ...
[    0.041179] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.041187] CPU1: Spectre v2: using BPIALL workaround
[    0.041321] smp: Brought up 1 node, 2 CPUs
[    0.041338] SMP: Total of 2 processors activated (1599.99 BogoMIPS).
[    0.041351] CPU: All CPU(s) started in SVC mode.
[    0.041828] devtmpfs: initialized
[    0.045805] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    0.046130] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.046160] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[    0.051490] pinctrl core: initialized pinctrl subsystem
[    0.052165] NET: Registered protocol family 16
[    0.053928] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.054771] thermal_sys: Registered thermal governor 'step_wise'
[    0.055010] cpuidle: using governor ladder
[    0.070870] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.070894] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.071027] zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0x(ptrval)
[    0.071600] e0000000.serial: ttyPS0 at MMIO 0xe0000000 (irq = 34, base_baud = 3125000) is a xuartps
[    0.461318] printk: console [ttyPS0] enabled
[    0.474176] SCSI subsystem initialized
[    0.476813] usbcore: registered new interface driver usbfs
[    0.480996] usbcore: registered new interface driver hub
[    0.485073] usbcore: registered new device driver usb
[    0.489074] mc: Linux media interface: v0.10
[    0.492098] videodev: Linux video capture interface: v2.00
[    0.496635] jesd204: found 0 devices and 0 topologies
[    0.500452] FPGA manager framework
[    0.502760] Advanced Linux Sound Architecture Driver Initialized.
[    0.508441] clocksource: Switched to clocksource arm_global_timer
[    0.520083] NET: Registered protocol family 2
[    0.523632] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear)
[    0.530741] TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear)
[    0.537254] TCP bind hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.543226] TCP: Hash tables configured (established 8192 bind 8192)
[    0.548364] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
[    0.553754] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
[    0.559703] NET: Registered protocol family 1
[    0.563177] RPC: Registered named UNIX socket transport module.
[    0.567802] RPC: Registered udp transport module.
[    0.571220] RPC: Registered tcp transport module.
[    0.574618] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.580128] hw perfevents: no interrupt-affinity property for /pmu@f8891000, guessing.
[    0.586916] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[    0.594746] workingset: timestamp_bits=30 max_order=18 bucket_order=0
[    0.600654] NFS: Registering the id_resolver key type
[    0.604424] Key type id_resolver registered
[    0.607297] Key type id_legacy registered
[    0.610051] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.615609] fuse: init (API version 7.32)
[    0.618584] bounce: pool size: 64 pages
[    0.621128] io scheduler mq-deadline registered
[    0.624355] io scheduler kyber registered
[    0.627338] zynq-pinctrl 700.pinctrl: zynq pinctrl initialized
[    0.635249] dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330
[    0.640686] dma-pl330 f8003000.dmac:         DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
[    0.655286] brd: module loaded
[    0.663677] loop: module loaded
[    0.665765] Registered mathworks_ip class
[    0.670834] spi-nor spi1.0: failed to read ear reg
[    0.674357] spi-nor spi1.0: w25q256 (65536 Kbytes)
[    0.677879] 4 fixed-partitions partitions found on MTD device spi1.0
[    0.682962] Creating 4 MTD partitions on "spi1.0":
[    0.686460] 0x000000000000-0x000000500000 : "boot"
[    0.699126] 0x000000500000-0x000000520000 : "bootenv"
[    0.709091] 0x000000520000-0x000000fa0000 : "kernel"
[    0.719088] 0x000000fa0000-0x000004000000 : "spare"
[    0.729232] MACsec IEEE 802.1AE
[    0.731615] libphy: Fixed MDIO Bus: probed
[    0.734726] tun: Universal TUN/TAP device driver, 1.6
[    0.742925] libphy: MACB_mii_bus: probed
[    0.745588] macb e000b000.ethernet eth0: Cadence GEM rev 0x00020118 at 0xe000b000 irq 37 (00:0a:35:00:1e:53)
[    0.754499] usbcore: registered new interface driver asix
[    0.758678] usbcore: registered new interface driver ax88179_178a
[    0.763501] usbcore: registered new interface driver cdc_ether
[    0.768054] usbcore: registered new interface driver net1080
[    0.772453] usbcore: registered new interface driver cdc_subset
[    0.777103] usbcore: registered new interface driver zaurus
[    0.781423] usbcore: registered new interface driver cdc_ncm
[    0.786480] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    0.792146] usbcore: registered new interface driver uas
[    0.796194] usbcore: registered new interface driver usb-storage
[    0.800995] usbcore: registered new interface driver usbserial_generic
[    0.806239] usbserial: USB Serial support registered for generic
[    0.810980] usbcore: registered new interface driver ftdi_sio
[    0.815437] usbserial: USB Serial support registered for FTDI USB Serial Device
[    0.821481] usbcore: registered new interface driver upd78f0730
[    0.826119] usbserial: USB Serial support registered for upd78f0730
[    0.831805] ULPI transceiver vendor/product ID 0x0424/0x0007
[    0.836170] Found SMSC USB3320 ULPI transceiver.
[    0.839510] ULPI integrity check: passed.
[    0.842231] ci_hdrc ci_hdrc.0: EHCI Host Controller
[    0.845818] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[    0.878457] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[    0.882681] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[    0.889675] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    0.895592] usb usb1: Product: EHCI Host Controller
[    0.899181] usb usb1: Manufacturer: Linux 5.10.0 ehci_hcd
[    0.903270] usb usb1: SerialNumber: ci_hdrc.0
[    0.906777] hub 1-0:1.0: USB hub found
[    0.909274] hub 1-0:1.0: 1 port detected
[    0.913611] i2c /dev entries driver
[    0.916924] at24 0-0050: supply vcc not found, using dummy regulator
[    0.922828] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 32 bytes/write
[    0.928583] cdns-i2c e0004000.i2c: 100 kHz mmio e0004000 irq 31
[    0.934281] at24 1-0050: supply vcc not found, using dummy regulator
[    0.940071] at24 1-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write
[    0.946216] adv7511 2-0039: supply avdd not found, using dummy regulator
[    0.951780] adv7511 2-0039: supply dvdd not found, using dummy regulator
[    0.957228] adv7511 2-0039: supply pvdd not found, using dummy regulator
[    0.962689] adv7511 2-0039: supply bgvdd not found, using dummy regulator
[    0.968221] adv7511 2-0039: supply dvdd-3v not found, using dummy regulator
[    0.981623] usbcore: registered new interface driver uvcvideo
[    0.986073] USB Video Class driver (1.1.1)
[    0.988883] gspca_main: v2.14.0 registered
[    0.993637] cdns-wdt f8005000.watchdog: Xilinx Watchdog Timer with timeout 10s
[    0.999821] Xilinx Zynq CpuIdle Driver started
[    1.003303] sdhci: Secure Digital Host Controller Interface driver
[    1.008178] sdhci: Copyright(c) Pierre Ossman
[    1.011168] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.017186] ledtrig-cpu: registered to indicate activity on CPUs
[    1.022738] hid: raw HID events driver (C) Jiri Kosina
[    1.028520] usbcore: registered new interface driver usbhid
[    1.032787] usbhid: USB HID core driver
[    1.039209] ad9361 spi0.0: ad9361_probe : enter (ad9361)
[    1.041004] mmc0: SDHCI controller on e0100000.mmc [e0100000.mmc] using ADMA
[    1.043253] mmc1: SDHCI controller on e0101000.mmc [e0101000.mmc] using ADMA
[    1.050147] ad9361 spi0.0: No GPIOs defined for ext band ctrl
[    1.066187] random: fast init done
[    1.093236] mmc0: new high speed SDHC card at address 0001
[    1.097927] mmcblk0: mmc0:0001 SD 29.5 GiB
[    1.102603]  mmcblk0: p1 p2 p3
[    1.184221] mmc1: new high speed MMC card at address 0001
[    1.188866] mmcblk1: mmc1:0001 8GTF4R 7.28 GiB
[    1.192355] mmcblk1boot0: mmc1:0001 8GTF4R partition 1 4.00 MiB
[    1.197240] mmcblk1boot1: mmc1:0001 8GTF4R partition 2 4.00 MiB
[    1.202067] mmcblk1rpmb: mmc1:0001 8GTF4R partition 3 512 KiB, chardev (245:0)
[    1.209417]  mmcblk1: p1
[    1.293890] ad9361 spi0.0: ad9361_probe : AD936x Rev 0 successfully initialized
[    1.329190] cf_axi_dds 79024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x79024000 mapped to 0x(ptrval), probed DDS AD9361
[    1.344266] fpga_manager fpga0: Xilinx Zynq FPGA Manager registered
[    1.349945] usbcore: registered new interface driver snd-usb-audio
[    1.356874] NET: Registered protocol family 10
[    1.360852] Segment Routing with IPv6
[    1.363199] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    1.368332] NET: Registered protocol family 17
[    1.371733] NET: Registered protocol family 36
[    1.374894] Key type dns_resolver registered
[    1.378017] Registering SWP/SWPB emulation handler
[    1.389867] of-fpga-region fpga-full: FPGA Region probed
[    1.394668] [drm] Initialized axi_hdmi_drm 1.0.0 20120930 for 70e00000.axi_hdmi on minor 0
[    1.588145] Console: switching to colour frame buffer device 240x67
[    1.618654] axi-hdmi 70e00000.axi_hdmi: [drm] fb0: axi_hdmi_drmdrm frame buffer device
[    3.020752] cf_axi_adc 79020000.cf-ad9361-lpc: ADI AIM (10.01.b) at 0x79020000 mapped to 0x(ptrval), probed ADC AD9361 as MASTER
[    3.031520] of_cfs_init
[    3.032713] of_cfs_init: OK
[    3.034532] ALSA device list:
[    3.036235]   No soundcards found.
[    3.052694] EXT4-fs (mmcblk0p2): recovery complete
[    3.056280] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    3.063264] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    3.076047] devtmpfs: mounted
[    3.079080] Freeing unused kernel memory: 1024K
[    3.098936] Run /sbin/init as init process
[    3.101791]   with arguments:
[    3.101796]     /sbin/init
[    3.101800]   with environment:
[    3.101804]     HOME=/
[    3.101808]     TERM=linux
[    3.101812]     consolve=ttyPS0,115200
[    3.665836] systemd[1]: System time before build time, advancing clock.
[    3.721797] systemd[1]: systemd 247.3-7+rpi1 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +ZSTD +SECCOMP +BLKID +ELFUTILS +KMOD +IDN2 -IDN +PCRE2 default-hierarchy=unified)
[    3.744133] systemd[1]: Detected architecture arm.
[    3.799604] systemd[1]: Set hostname to <analog>.
[    5.670544] systemd[1]: /lib/systemd/system/plymouth-start.service:16: Unit configured to use KillMode=none. This is unsafe, as it disables systemd's process lifecycle management for the service. Please update your service to use a safer KillMode=, such as 'mixed' or 'control-group'. Support for KillMode=none is deprecated and will eventually be removed.
[    5.958370] systemd[1]: Queued start job for default target Graphical Interface.
[    5.966514] random: systemd: uninitialized urandom read (16 bytes read)
[    5.972270] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[    5.983576] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[    5.991912] systemd[1]: Created slice system-getty.slice.
[    6.038679] random: systemd: uninitialized urandom read (16 bytes read)
[    6.044847] systemd[1]: Created slice system-modprobe.slice.
[    6.088647] random: systemd: uninitialized urandom read (16 bytes read)
[    6.094795] systemd[1]: Created slice system-serial\x2dgetty.slice.
[    6.129356] systemd[1]: Created slice system-systemd\x2dfsck.slice.
[    6.179082] systemd[1]: Created slice User and Session Slice.
[    6.229052] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[    6.278942] systemd[1]: Condition check resulted in Arbitrary Executable File Formats File System Automount Point being skipped.
[    6.297527] systemd[1]: Reached target Slices.
[    6.328778] systemd[1]: Reached target Swap.
[    6.379853] systemd[1]: Listening on Syslog Socket.
[    6.429258] systemd[1]: Listening on fsck to fsckd communication Socket.
[    6.478968] systemd[1]: Listening on initctl Compatibility Named Pipe.
[    6.551782] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[    6.566503] systemd[1]: Listening on Journal Socket (/dev/log).
[    6.619490] systemd[1]: Listening on Journal Socket.
[    6.677101] systemd[1]: Listening on udev Control Socket.
[    6.719257] systemd[1]: Listening on udev Kernel Socket.
[    6.769484] systemd[1]: Condition check resulted in Huge Pages File System being skipped.
[    6.783982] systemd[1]: Condition check resulted in POSIX Message Queue File System being skipped.
[    6.801750] systemd[1]: Mounting RPC Pipe File System...
[    6.841588] systemd[1]: Mounting Kernel Debug File System...
[    6.889116] systemd[1]: Condition check resulted in Kernel Trace File System being skipped.
[    6.903737] systemd[1]: Condition check resulted in Kernel Module supporting RPCSEC_GSS being skipped.
[    6.923690] systemd[1]: Starting Restore / save the current clock...
[    6.983006] systemd[1]: Starting Set the console keyboard layout...
[    7.028812] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped.
[    7.050156] systemd[1]: Starting Load Kernel Module configfs...
[    7.092100] systemd[1]: Starting Load Kernel Module drm...
[    7.141807] systemd[1]: Starting Load Kernel Module fuse...
[    7.202112] systemd[1]: Condition check resulted in Set Up Additional Binary Formats being skipped.
[    7.217383] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[    7.235394] systemd[1]: Starting Journal Service...
[    7.294215] systemd[1]: Starting Load Kernel Modules...
[    7.331700] systemd[1]: Starting Remount Root and Kernel File Systems...
[    7.402303] systemd[1]: Starting Coldplug All udev Devices...
[    7.510756] systemd[1]: Mounted RPC Pipe File System.
[    7.569286] systemd[1]: Mounted Kernel Debug File System.
[    7.613910] random: crng init done
[    7.622720] random: 7 urandom warning(s) missed due to ratelimiting
[    7.649352] systemd[1]: Finished Restore / save the current clock.
[    7.774082] systemd[1]: Started Journal Service.
[    7.966867] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[    8.193603] systemd-journald[102]: Received client request to flush runtime journal.
[   14.972730] macb e000b000.ethernet eth0: PHY [e000b000.ethernet-ffffffff:00] driver [Generic PHY] (irq=POLL)
[   14.972753] macb e000b000.ethernet eth0: configuring for phy/rgmii-id link mode

root@analog:/proc/device-tree/fpga-axi@0/axi_hdmi@70e00000# cat /proc/interrupts
           CPU0       CPU1
 24:          1          0     GIC-0  27 Edge      gt
 25:          0          0     GIC-0  43 Level     ttc_clockevent
 26:     469087     538361     GIC-0  29 Edge      twd
 27:          0          0     GIC-0  37 Level     arm-pmu
 28:          0          0     GIC-0  38 Level     arm-pmu
 29:         43          0     GIC-0  39 Level     f8007100.adc
 31:       2818          0     GIC-0  57 Level     cdns-i2c
 33:          0          0     GIC-0  35 Level     f800c000.ocmc
 34:       1838          0     GIC-0  59 Level     xuartps
 35:       3819          0     GIC-0  58 Level     e0006000.spi
 36:      18233          0     GIC-0  51 Level     e000d000.spi
 37:          0          0     GIC-0  54 Level     eth0
 38:     264106          0     GIC-0  56 Level     mmc0
 39:        563          0     GIC-0  79 Level     mmc1
 40:          0          0     GIC-0  45 Level     f8003000.dmac
 41:          0          0     GIC-0  46 Level     f8003000.dmac
 42:          0          0     GIC-0  47 Level     f8003000.dmac
 43:          0          0     GIC-0  48 Level     f8003000.dmac
 44:          0          0     GIC-0  49 Level     f8003000.dmac
 45:          0          0     GIC-0  72 Level     f8003000.dmac
 46:          0          0     GIC-0  73 Level     f8003000.dmac
 47:          0          0     GIC-0  74 Level     f8003000.dmac
 48:          0          0     GIC-0  75 Level     f8003000.dmac
 49:          0          0     GIC-0  40 Level     f8007000.devcfg
 55:          0          0     GIC-0  53 Level     e0002000.usb
 56:          0          0     GIC-0  41 Edge      f8005000.watchdog
 57:         24          0     GIC-0  87 Level     41620000.i2c
 58:          0          0     GIC-0  89 Level     7c400000.dma
 59:          0          0     GIC-0  88 Level     7c420000.dma
 60:      60187          0     GIC-0  90 Level     41600000.i2c
 61:          0          0     GIC-0  91 Level     43000000.dma
IPI0:          0          0  CPU wakeup interrupts
IPI1:          0          0  Timer broadcast interrupts
IPI2:     498399     583768  Rescheduling interrupts
IPI3:      21801      29288  Function call interrupts
IPI4:          0          0  CPU stop interrupts
IPI5:          0          0  IRQ work interrupts
IPI6:          0          0  completion interrupts
Err:          0

Thread Notes

Parents Reply Children
  • Hi, 

     Strangely enough, but I made some minor modifications to the device tree, or re-generated the bitstream file to synthesize BOOT.BIN. After the initial loading, I would encounter the phenomenon of a white screen on the HDMI output. However, when I restarted the Zynq Linux system after a day, without any modification in the process, it would turn into a gray screen phenomenon. Meanwhile, just now when I started the system, I found that the output was unstable as well, and it would flash a green screen. The specific output is shown in the video.

  • Regarding the configuration of the registers for the adv7511 in i2c, it should have been done by the Linux driver. When I scanned the i2c bus connected to the adv7511, all of them were occupied.

    root@analog:~# i2cdetect -y 2
         0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
    00:                         -- -- -- -- -- -- -- --
    10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
    20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
    30: -- -- -- -- -- -- -- -- UU UU -- -- UU -- -- UU
    40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
    50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
    60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
    70: -- -- -- -- -- -- -- --
    root@analog:~# cat /proc/interrupts
               CPU0       CPU1
     24:          1          0     GIC-0  27 Edge      gt
     25:          0          0     GIC-0  43 Level     ttc_clockevent
     26:     129971     149295     GIC-0  29 Edge      twd
     27:          0          0     GIC-0  37 Level     arm-pmu
     28:          0          0     GIC-0  38 Level     arm-pmu
     29:         43          0     GIC-0  39 Level     f8007100.adc
     31:       2818          0     GIC-0  57 Level     cdns-i2c
     33:          0          0     GIC-0  35 Level     f800c000.ocmc
     34:        701          0     GIC-0  59 Level     xuartps
     35:       3839          0     GIC-0  58 Level     e0006000.spi
     36:      18233          0     GIC-0  51 Level     e000d000.spi
     37:          0          0     GIC-0  54 Level     eth0
     38:      82220          0     GIC-0  56 Level     mmc0
     39:        643          0     GIC-0  79 Level     mmc1
     40:          0          0     GIC-0  45 Level     f8003000.dmac
     41:          0          0     GIC-0  46 Level     f8003000.dmac
     42:          0          0     GIC-0  47 Level     f8003000.dmac
     43:          0          0     GIC-0  48 Level     f8003000.dmac
     44:          0          0     GIC-0  49 Level     f8003000.dmac
     45:          0          0     GIC-0  72 Level     f8003000.dmac
     46:          0          0     GIC-0  73 Level     f8003000.dmac
     47:          0          0     GIC-0  74 Level     f8003000.dmac
     48:          0          0     GIC-0  75 Level     f8003000.dmac
     49:          0          0     GIC-0  40 Level     f8007000.devcfg
     55:          0          0     GIC-0  53 Level     e0002000.usb
     56:          0          0     GIC-0  41 Edge      f8005000.watchdog
     57:         24          0     GIC-0  87 Level     41620000.i2c
     58:          0          0     GIC-0  89 Level     7c400000.dma
     59:          0          0     GIC-0  88 Level     7c420000.dma
     60:      16651          0     GIC-0  90 Level     41600000.i2c
     61:          0          0     GIC-0  91 Level     43000000.dma
    IPI0:          0          0  CPU wakeup interrupts
    IPI1:          0          0  Timer broadcast interrupts
    IPI2:     137982     179305  Rescheduling interrupts
    IPI3:       5847       8061  Function call interrupts
    IPI4:          0          0  CPU stop interrupts
    IPI5:          0          0  IRQ work interrupts
    IPI6:          0          0  completion interrupts
    Err:          0
    

  • Hi,actually I refer the link https://wiki.analog.com/resources/tools-software/linux-build/generic/zynq.

    I used the linux kernel from the 2021_R1 branch on GitHub. It is supposed to include the linux driver for the adv7511.

  • In fact, I deleted the SPDIF-related content of adv7511. I removed the SPDIF_TX related IP cores from the HDL project, and only retained the HDMI_TX part. That is, I only need the video output of HDMI and do not need the sound output. Will this affect the configuration of the Linux driver? Meanwhile, I found in the Linux system that HDMI_DMA was not enabled, and the interrupt count remained 0 all the time. I suspect whether it is because some registers need to be configured before enabling DMA, and some register configurations failed. Because I saw that the interrupt count of I2C was constantly increasing.

  • This is the schematic diagram of the part related to adv7511 in the development board.

  • Then this is the entire content of the dts file that I obtained by decompiling the dtb file.

    /dts-v1/;
    
    / {
    	#address-cells = <0x01>;
    	#size-cells = <0x01>;
    	compatible = "xlnx,zynq-7000";
    	model = "Xilinx Zynq RK_Z7100";
    
    	cpus {
    		#address-cells = <0x01>;
    		#size-cells = <0x00>;
    
    		cpu@0 {
    			compatible = "arm,cortex-a9";
    			device_type = "cpu";
    			reg = <0x00>;
    			clocks = <0x01 0x03>;
    			clock-latency = <0x3e8>;
    			cpu0-supply = <0x02>;
    			operating-points = <0xc3500 0xf4240 0x61a80 0xf4240 0x30d40 0xf4240>;
    			phandle = <0x11>;
    		};
    
    		cpu@1 {
    			compatible = "arm,cortex-a9";
    			device_type = "cpu";
    			reg = <0x01>;
    			clocks = <0x01 0x03>;
    			phandle = <0x13>;
    		};
    	};
    
    	fpga-full {
    		compatible = "fpga-region";
    		fpga-mgr = <0x03>;
    		#address-cells = <0x01>;
    		#size-cells = <0x01>;
    		ranges;
    		phandle = <0x1d>;
    	};
    
    	pmu@f8891000 {
    		compatible = "arm,cortex-a9-pmu";
    		interrupts = <0x00 0x05 0x04 0x00 0x06 0x04>;
    		interrupt-parent = <0x04>;
    		reg = <0xf8891000 0x1000 0xf8893000 0x1000>;
    	};
    
    	fixedregulator {
    		compatible = "regulator-fixed";
    		regulator-name = "VCCPINT";
    		regulator-min-microvolt = <0xf4240>;
    		regulator-max-microvolt = <0xf4240>;
    		regulator-boot-on;
    		regulator-always-on;
    		phandle = <0x02>;
    	};
    
    	replicator {
    		compatible = "arm,coresight-static-replicator";
    		clocks = <0x01 0x1b 0x01 0x2e 0x01 0x2f>;
    		clock-names = "apb_pclk\0dbg_trc\0dbg_apb";
    
    		out-ports {
    			#address-cells = <0x01>;
    			#size-cells = <0x00>;
    
    			port@0 {
    				reg = <0x00>;
    
    				endpoint {
    					remote-endpoint = <0x05>;
    					phandle = <0x0d>;
    				};
    			};
    
    			port@1 {
    				reg = <0x01>;
    
    				endpoint {
    					remote-endpoint = <0x06>;
    					phandle = <0x0c>;
    				};
    			};
    		};
    
    		in-ports {
    
    			port {
    
    				endpoint {
    					remote-endpoint = <0x07>;
    					phandle = <0x0e>;
    				};
    			};
    		};
    	};
    
    	axi {
    		u-boot,dm-pre-reloc;
    		compatible = "simple-bus";
    		#address-cells = <0x01>;
    		#size-cells = <0x01>;
    		interrupt-parent = <0x04>;
    		ranges;
    		phandle = <0x1e>;
    
    		adc@f8007100 {
    			compatible = "xlnx,zynq-xadc-1.00.a";
    			reg = <0xf8007100 0x20>;
    			interrupts = <0x00 0x07 0x04>;
    			interrupt-parent = <0x04>;
    			clocks = <0x01 0x0c>;
    			phandle = <0x1f>;
    		};
    
    		can@e0008000 {
    			compatible = "xlnx,zynq-can-1.0";
    			status = "disabled";
    			clocks = <0x01 0x13 0x01 0x24>;
    			clock-names = "can_clk\0pclk";
    			reg = <0xe0008000 0x1000>;
    			interrupts = <0x00 0x1c 0x04>;
    			interrupt-parent = <0x04>;
    			tx-fifo-depth = <0x40>;
    			rx-fifo-depth = <0x40>;
    			phandle = <0x20>;
    		};
    
    		can@e0009000 {
    			compatible = "xlnx,zynq-can-1.0";
    			status = "disabled";
    			clocks = <0x01 0x14 0x01 0x25>;
    			clock-names = "can_clk\0pclk";
    			reg = <0xe0009000 0x1000>;
    			interrupts = <0x00 0x33 0x04>;
    			interrupt-parent = <0x04>;
    			tx-fifo-depth = <0x40>;
    			rx-fifo-depth = <0x40>;
    			phandle = <0x21>;
    		};
    
    		gpio@e000a000 {
    			compatible = "xlnx,zynq-gpio-1.0";
    			#gpio-cells = <0x02>;
    			clocks = <0x01 0x2a>;
    			gpio-controller;
    			interrupt-controller;
    			#interrupt-cells = <0x02>;
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x14 0x04>;
    			reg = <0xe000a000 0x1000>;
    			emio-gpio-width = <0x40>;
    			gpio-mask-high = <0x00>;
    			gpio-mask-low = <0x5600>;
    			phandle = <0x09>;
    		};
    
    		i2c@e0004000 {
    			compatible = "cdns,i2c-r1p10";
    			status = "okay";
    			clocks = <0x01 0x26>;
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x19 0x04>;
    			reg = <0xe0004000 0x1000>;
    			#address-cells = <0x01>;
    			#size-cells = <0x00>;
    			clock-frequency = <0x186a0>;
    			phandle = <0x22>;
    
    			eeprom1@50 {
    				compatible = "atmel,24c256";
    				reg = <0x50>;
    				pagesize = <0x20>;
    			};
    		};
    
    		i2c@e0005000 {
    			compatible = "cdns,i2c-r1p10";
    			status = "disabled";
    			clocks = <0x01 0x27>;
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x30 0x04>;
    			reg = <0xe0005000 0x1000>;
    			#address-cells = <0x01>;
    			#size-cells = <0x00>;
    			phandle = <0x23>;
    		};
    
    		interrupt-controller@f8f01000 {
    			compatible = "arm,cortex-a9-gic";
    			#interrupt-cells = <0x03>;
    			interrupt-controller;
    			reg = <0xf8f01000 0x1000 0xf8f00100 0x100>;
    			num_cpus = <0x02>;
    			num_interrupts = <0x60>;
    			phandle = <0x04>;
    		};
    
    		cache-controller@f8f02000 {
    			compatible = "arm,pl310-cache";
    			reg = <0xf8f02000 0x1000>;
    			interrupts = <0x00 0x02 0x04>;
    			arm,data-latency = <0x03 0x02 0x02>;
    			arm,tag-latency = <0x02 0x02 0x02>;
    			cache-unified;
    			cache-level = <0x02>;
    			phandle = <0x24>;
    		};
    
    		memory-controller@f8006000 {
    			compatible = "xlnx,zynq-ddrc-a05";
    			reg = <0xf8006000 0x1000>;
    			phandle = <0x25>;
    		};
    
    		ocmc@f800c000 {
    			compatible = "xlnx,zynq-ocmc-1.0";
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x03 0x04>;
    			reg = <0xf800c000 0x1000>;
    			phandle = <0x26>;
    		};
    
    		serial@e0000000 {
    			compatible = "xlnx,xuartps\0cdns,uart-r1p8";
    			status = "okay";
    			clocks = <0x01 0x17 0x01 0x28>;
    			clock-names = "uart_clk\0pclk";
    			reg = <0xe0000000 0x1000>;
    			interrupts = <0x00 0x1b 0x04>;
    			cts-override;
    			device_type = "serial";
    			port-number = <0x00>;
    			phandle = <0x27>;
    		};
    
    		serial@e0001000 {
    			compatible = "xlnx,xuartps\0cdns,uart-r1p8";
    			status = "disabled";
    			clocks = <0x01 0x18 0x01 0x29>;
    			clock-names = "uart_clk\0pclk";
    			reg = <0xe0001000 0x1000>;
    			interrupts = <0x00 0x32 0x04>;
    			phandle = <0x28>;
    		};
    
    		spi@e0006000 {
    			compatible = "xlnx,zynq-spi-r1p6";
    			reg = <0xe0006000 0x1000>;
    			status = "okay";
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x1a 0x04>;
    			clocks = <0x01 0x19 0x01 0x22>;
    			clock-names = "ref_clk\0pclk";
    			#address-cells = <0x01>;
    			#size-cells = <0x00>;
    			is-decoded-cs = <0x00>;
    			num-cs = <0x03>;
    			phandle = <0x29>;
    
    			ad9361-phy@0 {
    				compatible = "adi,ad9361";
    				reg = <0x00>;
    				spi-cpha;
    				spi-max-frequency = <0x989680>;
    				clocks = <0x08 0x00>;
    				clock-names = "ad9361_ext_refclk";
    				clock-output-names = "rx_sampl_clk\0tx_sampl_clk";
    				#clock-cells = <0x01>;
    				adi,digital-interface-tune-skip-mode = <0x00>;
    				adi,pp-tx-swap-enable;
    				adi,pp-rx-swap-enable;
    				adi,rx-frame-pulse-mode-enable;
    				adi,lvds-mode-enable;
    				adi,lvds-bias-mV = <0x96>;
    				adi,lvds-rx-onchip-termination-enable;
    				adi,rx-data-delay = <0x04>;
    				adi,tx-fb-clock-delay = <0x07>;
    				adi,dcxo-coarse-and-fine-tune = <0x08 0x1720>;
    				adi,2rx-2tx-mode-enable;
    				adi,frequency-division-duplex-mode-enable;
    				adi,rx-rf-port-input-select = <0x00>;
    				adi,tx-rf-port-input-select = <0x00>;
    				adi,tx-attenuation-mdB = <0x2710>;
    				adi,tx-lo-powerdown-managed-enable;
    				adi,rf-rx-bandwidth-hz = <0x112a880>;
    				adi,rf-tx-bandwidth-hz = <0x112a880>;
    				adi,rx-synthesizer-frequency-hz = <0x00 0x8f0d1800>;
    				adi,tx-synthesizer-frequency-hz = <0x00 0x92080880>;
    				adi,rx-path-clock-frequencies = <0x3a980000 0xea60000 0x7530000 0x3a98000 0x1d4c000 0x1d4c000>;
    				adi,tx-path-clock-frequencies = <0x3a980000 0x7530000 0x7530000 0x3a98000 0x1d4c000 0x1d4c000>;
    				adi,gc-rx1-mode = <0x02>;
    				adi,gc-rx2-mode = <0x02>;
    				adi,gc-adc-ovr-sample-size = <0x04>;
    				adi,gc-adc-small-overload-thresh = <0x2f>;
    				adi,gc-adc-large-overload-thresh = <0x3a>;
    				adi,gc-lmt-overload-high-thresh = <0x320>;
    				adi,gc-lmt-overload-low-thresh = <0x2c0>;
    				adi,gc-dec-pow-measurement-duration = <0x2000>;
    				adi,gc-low-power-thresh = <0x18>;
    				adi,mgc-inc-gain-step = <0x02>;
    				adi,mgc-dec-gain-step = <0x02>;
    				adi,mgc-split-table-ctrl-inp-gain-mode = <0x00>;
    				adi,agc-attack-delay-extra-margin-us = <0x01>;
    				adi,agc-outer-thresh-high = <0x05>;
    				adi,agc-outer-thresh-high-dec-steps = <0x02>;
    				adi,agc-inner-thresh-high = <0x0a>;
    				adi,agc-inner-thresh-high-dec-steps = <0x01>;
    				adi,agc-inner-thresh-low = <0x0c>;
    				adi,agc-inner-thresh-low-inc-steps = <0x01>;
    				adi,agc-outer-thresh-low = <0x12>;
    				adi,agc-outer-thresh-low-inc-steps = <0x02>;
    				adi,agc-adc-small-overload-exceed-counter = <0x0a>;
    				adi,agc-adc-large-overload-exceed-counter = <0x0a>;
    				adi,agc-adc-large-overload-inc-steps = <0x02>;
    				adi,agc-lmt-overload-large-exceed-counter = <0x0a>;
    				adi,agc-lmt-overload-small-exceed-counter = <0x0a>;
    				adi,agc-lmt-overload-large-inc-steps = <0x02>;
    				adi,agc-gain-update-interval-us = <0x3e8>;
    				adi,fagc-dec-pow-measurement-duration = <0x40>;
    				adi,fagc-lp-thresh-increment-steps = <0x01>;
    				adi,fagc-lp-thresh-increment-time = <0x05>;
    				adi,fagc-energy-lost-stronger-sig-gain-lock-exit-cnt = <0x08>;
    				adi,fagc-final-overrange-count = <0x03>;
    				adi,fagc-gain-index-type-after-exit-rx-mode = <0x00>;
    				adi,fagc-lmt-final-settling-steps = <0x01>;
    				adi,fagc-lock-level = <0x0a>;
    				adi,fagc-lock-level-gain-increase-upper-limit = <0x05>;
    				adi,fagc-lock-level-lmt-gain-increase-enable;
    				adi,fagc-lpf-final-settling-steps = <0x01>;
    				adi,fagc-optimized-gain-offset = <0x05>;
    				adi,fagc-power-measurement-duration-in-state5 = <0x40>;
    				adi,fagc-rst-gla-engergy-lost-goto-optim-gain-enable;
    				adi,fagc-rst-gla-engergy-lost-sig-thresh-below-ll = <0x0a>;
    				adi,fagc-rst-gla-engergy-lost-sig-thresh-exceeded-enable;
    				adi,fagc-rst-gla-if-en-agc-pulled-high-mode = <0x00>;
    				adi,fagc-rst-gla-large-adc-overload-enable;
    				adi,fagc-rst-gla-large-lmt-overload-enable;
    				adi,fagc-rst-gla-stronger-sig-thresh-above-ll = <0x0a>;
    				adi,fagc-rst-gla-stronger-sig-thresh-exceeded-enable;
    				adi,fagc-state-wait-time-ns = <0x104>;
    				adi,fagc-use-last-lock-level-for-set-gain-enable;
    				adi,rssi-restart-mode = <0x03>;
    				adi,rssi-delay = <0x01>;
    				adi,rssi-wait = <0x01>;
    				adi,rssi-duration = <0x3e8>;
    				adi,ctrl-outs-index = <0x00>;
    				adi,ctrl-outs-enable-mask = <0xff>;
    				adi,temp-sense-measurement-interval-ms = <0x3e8>;
    				adi,temp-sense-offset-signed = <0xce>;
    				adi,temp-sense-periodic-measurement-enable;
    				adi,aux-dac-manual-mode-enable;
    				adi,aux-dac1-default-value-mV = <0x00>;
    				adi,aux-dac1-rx-delay-us = <0x00>;
    				adi,aux-dac1-tx-delay-us = <0x00>;
    				adi,aux-dac2-default-value-mV = <0x00>;
    				adi,aux-dac2-rx-delay-us = <0x00>;
    				adi,aux-dac2-tx-delay-us = <0x00>;
    				en_agc-gpios = <0x09 0x62 0x00>;
    				sync-gpios = <0x09 0x63 0x00>;
    				reset-gpios = <0x09 0x64 0x00>;
    				enable-gpios = <0x09 0x65 0x00>;
    				txnrx-gpios = <0x09 0x66 0x00>;
    				phandle = <0x16>;
    			};
    		};
    
    		spi@e0007000 {
    			compatible = "xlnx,zynq-spi-r1p6";
    			reg = <0xe0007000 0x1000>;
    			status = "disabled";
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x31 0x04>;
    			clocks = <0x01 0x1a 0x01 0x23>;
    			clock-names = "ref_clk\0pclk";
    			#address-cells = <0x01>;
    			#size-cells = <0x00>;
    			phandle = <0x2a>;
    		};
    
    		spi@e000d000 {
    			clock-names = "ref_clk\0pclk";
    			clocks = <0x01 0x0a 0x01 0x2b>;
    			compatible = "xlnx,zynq-qspi-1.0";
    			status = "okay";
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x13 0x04>;
    			reg = <0xe000d000 0x1000>;
    			#address-cells = <0x01>;
    			#size-cells = <0x00>;
    			is-dual = <0x01>;
    			num-cs = <0x02>;
    			spi-rx-bus-width = <0x08>;
    			spi-tx-bus-width = <0x08>;
    			phandle = <0x2b>;
    
    			flash@0 {
    				phandle = <0x2c>;
    				reg = <0x00>;
    				#address-cells = <0x01>;
    				#size-cells = <0x01>;
    				compatible = "w25q256\0jedec,spi-nor";
    				spi-tx-bus-width = <0x01>;
    				spi-rx-bus-width = <0x04>;
    				spi-max-frequency = <0x2faf080>;
    				parallel-memories = <0x00 0x2000000 0x00 0x2000000>;
    
    				partition@0 {
    					label = "boot";
    					reg = <0x00 0x500000>;
    				};
    
    				partition@1 {
    					label = "bootenv";
    					reg = <0x500000 0x20000>;
    				};
    
    				partition@2 {
    					label = "kernel";
    					reg = <0x520000 0xa80000>;
    				};
    
    				partition@3 {
    					label = "spare";
    					reg = <0xfa0000 0x00>;
    				};
    			};
    		};
    
    		memory-controller@e000e000 {
    			#address-cells = <0x01>;
    			#size-cells = <0x01>;
    			status = "disabled";
    			clock-names = "memclk\0apb_pclk";
    			clocks = <0x01 0x0b 0x01 0x2c>;
    			compatible = "arm,pl353-smc-r2p1\0arm,primecell";
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x12 0x04>;
    			ranges;
    			reg = <0xe000e000 0x1000>;
    			phandle = <0x2d>;
    
    			flash@e1000000 {
    				status = "disabled";
    				compatible = "arm,pl353-nand-r2p1";
    				reg = <0xe1000000 0x1000000>;
    				#address-cells = <0x01>;
    				#size-cells = <0x01>;
    				phandle = <0x2e>;
    			};
    
    			flash@e2000000 {
    				status = "disabled";
    				compatible = "cfi-flash";
    				reg = <0xe2000000 0x2000000>;
    				#address-cells = <0x01>;
    				#size-cells = <0x01>;
    				phandle = <0x2f>;
    			};
    		};
    
    		ethernet@e000b000 {
    			compatible = "cdns,zynq-gem\0cdns,gem";
    			reg = <0xe000b000 0x1000>;
    			status = "okay";
    			interrupts = <0x00 0x16 0x04>;
    			clocks = <0x01 0x1e 0x01 0x1e 0x01 0x0d>;
    			clock-names = "pclk\0hclk\0tx_clk";
    			#address-cells = <0x01>;
    			#size-cells = <0x00>;
    			phy-mode = "rgmii-id";
    			xlnx,ptp-enet-clock = <0x7f28150>;
    			local-mac-address = [00 0a 35 00 1e 53];
    			phandle = <0x30>;
    		};
    
    		ethernet@e000c000 {
    			compatible = "cdns,zynq-gem\0cdns,gem";
    			reg = <0xe000c000 0x1000>;
    			status = "disabled";
    			interrupts = <0x00 0x2d 0x04>;
    			clocks = <0x01 0x1f 0x01 0x1f 0x01 0x0e>;
    			clock-names = "pclk\0hclk\0tx_clk";
    			#address-cells = <0x01>;
    			#size-cells = <0x00>;
    			phandle = <0x31>;
    		};
    
    		mmc@e0100000 {
    			compatible = "arasan,sdhci-8.9a";
    			status = "okay";
    			clock-names = "clk_xin\0clk_ahb";
    			clocks = <0x01 0x15 0x01 0x20>;
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x18 0x04>;
    			reg = <0xe0100000 0x1000>;
    			xlnx,has-cd = <0x00>;
    			xlnx,has-power = <0x00>;
    			xlnx,has-wp = <0x00>;
    			phandle = <0x32>;
    		};
    
    		mmc@e0101000 {
    			compatible = "arasan,sdhci-8.9a";
    			status = "okay";
    			clock-names = "clk_xin\0clk_ahb";
    			clocks = <0x01 0x16 0x01 0x21>;
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x2f 0x04>;
    			reg = <0xe0101000 0x1000>;
    			xlnx,has-cd = <0x00>;
    			xlnx,has-power = <0x00>;
    			xlnx,has-wp = <0x00>;
    			phandle = <0x33>;
    		};
    
    		slcr@f8000000 {
    			u-boot,dm-pre-reloc;
    			#address-cells = <0x01>;
    			#size-cells = <0x01>;
    			compatible = "xlnx,zynq-slcr\0syscon\0simple-mfd";
    			reg = <0xf8000000 0x1000>;
    			ranges;
    			phandle = <0x0a>;
    
    			clkc@100 {
    				u-boot,dm-pre-reloc;
    				#clock-cells = <0x01>;
    				compatible = "xlnx,ps7-clkc";
    				fclk-enable = <0x03>;
    				clock-output-names = "armpll\0ddrpll\0iopll\0cpu_6or4x\0cpu_3or2x\0cpu_2x\0cpu_1x\0ddr2x\0ddr3x\0dci\0lqspi\0smc\0pcap\0gem0\0gem1\0fclk0\0fclk1\0fclk2\0fclk3\0can0\0can1\0sdio0\0sdio1\0uart0\0uart1\0spi0\0spi1\0dma\0usb0_aper\0usb1_aper\0gem0_aper\0gem1_aper\0sdio0_aper\0sdio1_aper\0spi0_aper\0spi1_aper\0can0_aper\0can1_aper\0i2c0_aper\0i2c1_aper\0uart0_aper\0uart1_aper\0gpio_aper\0lqspi_aper\0smc_aper\0swdt\0dbg_trc\0dbg_apb";
    				reg = <0x100 0x100>;
    				ps-clk-frequency = <0x1fca055>;
    				phandle = <0x01>;
    			};
    
    			rstc@200 {
    				compatible = "xlnx,zynq-reset";
    				reg = <0x200 0x48>;
    				#reset-cells = <0x01>;
    				syscon = <0x0a>;
    				phandle = <0x34>;
    			};
    
    			pinctrl@700 {
    				compatible = "xlnx,pinctrl-zynq";
    				reg = <0x700 0x200>;
    				syscon = <0x0a>;
    				phandle = <0x35>;
    			};
    		};
    
    		dmac@f8003000 {
    			compatible = "arm,pl330\0arm,primecell";
    			reg = <0xf8003000 0x1000>;
    			interrupt-parent = <0x04>;
    			interrupt-names = "abort\0dma0\0dma1\0dma2\0dma3\0dma4\0dma5\0dma6\0dma7";
    			interrupts = <0x00 0x0d 0x04 0x00 0x0e 0x04 0x00 0x0f 0x04 0x00 0x10 0x04 0x00 0x11 0x04 0x00 0x28 0x04 0x00 0x29 0x04 0x00 0x2a 0x04 0x00 0x2b 0x04>;
    			#dma-cells = <0x01>;
    			#dma-channels = <0x08>;
    			#dma-requests = <0x04>;
    			clocks = <0x01 0x1b>;
    			clock-names = "apb_pclk";
    			phandle = <0x36>;
    		};
    
    		devcfg@f8007000 {
    			compatible = "xlnx,zynq-devcfg-1.0";
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x08 0x04>;
    			reg = <0xf8007000 0x100>;
    			clocks = <0x01 0x0c 0x01 0x0f 0x01 0x10 0x01 0x11 0x01 0x12>;
    			clock-names = "ref_clk\0fclk0\0fclk1\0fclk2\0fclk3";
    			syscon = <0x0a>;
    			phandle = <0x03>;
    		};
    
    		efuse@f800d000 {
    			compatible = "xlnx,zynq-efuse";
    			reg = <0xf800d000 0x20>;
    			phandle = <0x37>;
    		};
    
    		timer@f8f00200 {
    			compatible = "arm,cortex-a9-global-timer";
    			reg = <0xf8f00200 0x20>;
    			interrupts = <0x01 0x0b 0x301>;
    			interrupt-parent = <0x04>;
    			clocks = <0x01 0x04>;
    			phandle = <0x38>;
    		};
    
    		timer@f8001000 {
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x0a 0x04 0x00 0x0b 0x04 0x00 0x0c 0x04>;
    			compatible = "cdns,ttc";
    			clocks = <0x01 0x06>;
    			reg = <0xf8001000 0x1000>;
    			phandle = <0x39>;
    		};
    
    		timer@f8002000 {
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x25 0x04 0x00 0x26 0x04 0x00 0x27 0x04>;
    			compatible = "cdns,ttc";
    			clocks = <0x01 0x06>;
    			reg = <0xf8002000 0x1000>;
    			phandle = <0x3a>;
    		};
    
    		timer@f8f00600 {
    			interrupt-parent = <0x04>;
    			interrupts = <0x01 0x0d 0x301>;
    			compatible = "arm,cortex-a9-twd-timer";
    			reg = <0xf8f00600 0x20>;
    			clocks = <0x01 0x04>;
    			phandle = <0x3b>;
    		};
    
    		usb@e0002000 {
    			compatible = "xlnx,zynq-usb-2.20a\0chipidea,usb2";
    			status = "okay";
    			clocks = <0x01 0x1c>;
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x15 0x04>;
    			reg = <0xe0002000 0x1000>;
    			#address-cells = <0x01>;
    			#size-cells = <0x01>;
    			phandle = <0x3c>;
    			phy_type = "ulpi";
    			usb-reset = <0x09 0x07 0x00>;
    			dr_mode = "host";
    
    			usb_phy {
    				compatible = "ulpi-phy";
    				#phy-cells = <0x00>;
    				reg = <0xe0002000 0x1000>;
    				view-port = <0x170>;
    				drv-vbus;
    			};
    		};
    
    		usb@e0003000 {
    			compatible = "xlnx,zynq-usb-2.20a\0chipidea,usb2";
    			status = "disabled";
    			clocks = <0x01 0x1d>;
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x2c 0x04>;
    			reg = <0xe0003000 0x1000>;
    			phy_type = "ulpi";
    			phandle = <0x3d>;
    		};
    
    		watchdog@f8005000 {
    			clocks = <0x01 0x2d>;
    			compatible = "cdns,wdt-r1p2";
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x09 0x01>;
    			reg = <0xf8005000 0x1000>;
    			timeout-sec = <0x0a>;
    			phandle = <0x3e>;
    		};
    
    		etb@f8801000 {
    			compatible = "arm,coresight-etb10\0arm,primecell";
    			reg = <0xf8801000 0x1000>;
    			clocks = <0x01 0x1b 0x01 0x2e 0x01 0x2f>;
    			clock-names = "apb_pclk\0dbg_trc\0dbg_apb";
    
    			in-ports {
    
    				port {
    
    					endpoint {
    						remote-endpoint = <0x0c>;
    						phandle = <0x06>;
    					};
    				};
    			};
    		};
    
    		tpiu@f8803000 {
    			compatible = "arm,coresight-tpiu\0arm,primecell";
    			reg = <0xf8803000 0x1000>;
    			clocks = <0x01 0x1b 0x01 0x2e 0x01 0x2f>;
    			clock-names = "apb_pclk\0dbg_trc\0dbg_apb";
    
    			in-ports {
    
    				port {
    
    					endpoint {
    						remote-endpoint = <0x0d>;
    						phandle = <0x05>;
    					};
    				};
    			};
    		};
    
    		funnel@f8804000 {
    			compatible = "arm,coresight-static-funnel\0arm,primecell";
    			reg = <0xf8804000 0x1000>;
    			clocks = <0x01 0x1b 0x01 0x2e 0x01 0x2f>;
    			clock-names = "apb_pclk\0dbg_trc\0dbg_apb";
    
    			out-ports {
    
    				port {
    
    					endpoint {
    						remote-endpoint = <0x0e>;
    						phandle = <0x07>;
    					};
    				};
    			};
    
    			in-ports {
    				#address-cells = <0x01>;
    				#size-cells = <0x00>;
    
    				port@0 {
    					reg = <0x00>;
    
    					endpoint {
    						remote-endpoint = <0x0f>;
    						phandle = <0x12>;
    					};
    				};
    
    				port@1 {
    					reg = <0x01>;
    
    					endpoint {
    						remote-endpoint = <0x10>;
    						phandle = <0x14>;
    					};
    				};
    
    				port@2 {
    					reg = <0x02>;
    
    					endpoint {
    						phandle = <0x3f>;
    					};
    				};
    			};
    		};
    
    		ptm@f889c000 {
    			compatible = "arm,coresight-etm3x\0arm,primecell";
    			reg = <0xf889c000 0x1000>;
    			clocks = <0x01 0x1b 0x01 0x2e 0x01 0x2f>;
    			clock-names = "apb_pclk\0dbg_trc\0dbg_apb";
    			cpu = <0x11>;
    
    			out-ports {
    
    				port {
    
    					endpoint {
    						remote-endpoint = <0x12>;
    						phandle = <0x0f>;
    					};
    				};
    			};
    		};
    
    		ptm@f889d000 {
    			compatible = "arm,coresight-etm3x\0arm,primecell";
    			reg = <0xf889d000 0x1000>;
    			clocks = <0x01 0x1b 0x01 0x2e 0x01 0x2f>;
    			clock-names = "apb_pclk\0dbg_trc\0dbg_apb";
    			cpu = <0x13>;
    
    			out-ports {
    
    				port {
    
    					endpoint {
    						remote-endpoint = <0x14>;
    						phandle = <0x10>;
    					};
    				};
    			};
    		};
    	};
    
    	chosen {
    		bootargs = "console=ttyPS0,115200 earlycon root=/dev/mmcblk0p2 rw rootwait";
    		stdout-path = "serial0:115200n8";
    	};
    
    	aliases {
    		ethernet0 = "/axi/ethernet@e000b000";
    		serial0 = "/axi/serial@e0000000";
    	};
    
    	memory {
    		device_type = "memory";
    		reg = <0x00 0x40000000>;
    	};
    
    	leds {
    		compatible = "gpio-leds";
    
    		led0 {
    			label = "pl_led1";
    			gpios = <0x09 0x36 0x00>;
    			default-state = "on";
    		};
    
    		led1 {
    			label = "pl_led2";
    			gpios = <0x09 0x37 0x00>;
    			default-state = "on";
    		};
    
    		led2 {
    			label = "pl_led3";
    			gpios = <0x09 0x38 0x00>;
    			default-state = "on";
    		};
    
    		led3 {
    			label = "pl_led4";
    			gpios = <0x09 0x39 0x00>;
    			default-state = "on";
    		};
    
    		led4 {
    			label = "pl_led5";
    			gpios = <0x09 0x3a 0x00>;
    			linux,default-trigger = "heartbeat";
    		};
    
    		led5 {
    			label = "pl_led6";
    			gpios = <0x09 0x3b 0x00>;
    			linux,default-trigger = "timer";
    		};
    	};
    
    	fpga-axi@0 {
    		compatible = "simple-bus";
    		interrupt-parent = <0x04>;
    		#address-cells = <0x01>;
    		#size-cells = <0x01>;
    		ranges;
    		phandle = <0x40>;
    
    		i2c@41620000 {
    			compatible = "xlnx,axi-iic-1.01.b\0xlnx,xps-iic-2.00.a";
    			reg = <0x41620000 0x10000>;
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x37 0x04>;
    			clocks = <0x01 0x0f>;
    			clock-names = "pclk";
    			#size-cells = <0x00>;
    			#address-cells = <0x01>;
    			phandle = <0x41>;
    			clock-frequency = <100000>;
    			
    			ad7291@2f {
    				compatible = "adi,ad7291";
    				reg = <0x2f>;
    			};
    
    			eeprom@50 {
    				compatible = "at24,24c02";
    				reg = <0x50>;
    			};
    		};
    
    		dma@7c400000 {
    			compatible = "adi,axi-dmac-1.00.a";
    			reg = <0x7c400000 0x10000>;
    			#dma-cells = <0x01>;
    			interrupts = <0x00 0x39 0x04>;
    			clocks = <0x01 0x10>;
    			phandle = <0x15>;
    
    			adi,channels {
    				#size-cells = <0x00>;
    				#address-cells = <0x01>;
    
    				dma-channel@0 {
    					reg = <0x00>;
    					adi,source-bus-width = <0x40>;
    					adi,source-bus-type = <0x02>;
    					adi,destination-bus-width = <0x40>;
    					adi,destination-bus-type = <0x00>;
    				};
    			};
    		};
    
    		dma@7c420000 {
    			compatible = "adi,axi-dmac-1.00.a";
    			reg = <0x7c420000 0x10000>;
    			#dma-cells = <0x01>;
    			interrupts = <0x00 0x38 0x04>;
    			clocks = <0x01 0x10>;
    			phandle = <0x17>;
    
    			adi,channels {
    				#size-cells = <0x00>;
    				#address-cells = <0x01>;
    
    				dma-channel@0 {
    					reg = <0x00>;
    					adi,source-bus-width = <0x40>;
    					adi,source-bus-type = <0x00>;
    					adi,destination-bus-width = <0x40>;
    					adi,destination-bus-type = <0x02>;
    				};
    			};
    		};
    
    		cf-ad9361-lpc@79020000 {
    			compatible = "adi,axi-ad9361-6.00.a";
    			reg = <0x79020000 0x6000>;
    			dmas = <0x15 0x00>;
    			dma-names = "rx";
    			spibus-connected = <0x16>;
    			phandle = <0x42>;
    		};
    
    		cf-ad9361-dds-core-lpc@79024000 {
    			compatible = "adi,axi-ad9361-dds-6.00.a";
    			reg = <0x79024000 0x1000>;
    			clocks = <0x16 0x0d>;
    			clock-names = "sampl_clk";
    			dmas = <0x17 0x00>;
    			dma-names = "tx";
    			phandle = <0x43>;
    		};
    
    		i2c@41600000 {
    			compatible = "xlnx,axi-iic-1.01.b\0xlnx,xps-iic-2.00.a";
    			reg = <0x41600000 0x10000>;
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x3a 0x04>;
    			clocks = <0x01 0x0f>;
    			clock-names = "pclk";
    			#size-cells = <0x00>;
    			#address-cells = <0x01>;
    			clock-frequency = <100000>;
    
    			adv7511@39 {
    				compatible = "adi,adv7511";
    				reg = <0x39>;
    				reg-names = "main";
    				adi,input-depth = <0x08>;
    				adi,input-colorspace = "rgb";
    				adi,input-clock = "1x";
    				adi,clock-delay = <0x00>;
    				phandle = <0x44>;
    
    				ports {
    					#address-cells = <0x01>;
    					#size-cells = <0x00>;
    
    					port@0 {
    						reg = <0x00>;
    
    						endpoint {
    							remote-endpoint = <0x18>;
    							phandle = <0x1b>;
    						};
    					};
    
    					port@1 {
    						reg = <0x01>;
    					};
    				};
    			};
    		};
    
    		dma@43000000 {
    			compatible = "adi,axi-dmac-1.00.a";
    			reg = <0x43000000 0x10000>;
    			#dma-cells = <0x01>;
    			interrupts = <0x00 0x3b 0x04>;
    			clocks = <0x01 0x10>;
    			phandle = <0x19>;
    
    			adi,channels {
    				#size-cells = <0x00>;
    				#address-cells = <0x01>;
    
    				dma-channel@0 {
    					reg = <0x00>;
    					adi,source-bus-width = <0x40>;
    					adi,source-bus-type = <0x00>;
    					adi,destination-bus-width = <0x40>;
    					adi,destination-bus-type = <0x01>;
    				};
    			};
    		};
    
    		axi-clkgen@79000000 {
    			compatible = "adi,axi-clkgen-2.00.a";
    			reg = <0x79000000 0x10000>;
    			#clock-cells = <0x00>;
    			clocks = <0x01 0x0f 0x01 0x10>;
    			clock-names = "s_axi_aclk\0clkin1";
    			phandle = <0x1a>;
    		};
    
    		axi_hdmi@70e00000 {
    			compatible = "adi,axi-hdmi-tx-1.00.a";
    			reg = <0x70e00000 0x10000>;
    			dmas = <0x19 0x00>;
    			dma-names = "video";
    			clocks = <0x1a>;
    			adi,is-rgb;
    
    			port {
    
    				endpoint {
    					remote-endpoint = <0x1b>;
    					phandle = <0x18>;
    				};
    			};
    		};
    
    		axi-pwmgen@43c00000 {
    			compatible = "adi,axi-pwmgen";
    			reg = <0x43c00000 0x10000>;
    			#pwm-cells = <0x02>;
    			clocks = <0x01 0x0f>;
    			phandle = <0x1c>;
    		};
    	};
    
    	pwm-fan {
    		compatible = "pwm-fan";
    		status = "okay";
    		pwms = <0x1c 0x00 0xc350 0x00>;
    		#cooling-cells = <0x02>;
    		cooling-levels = <0x00 0x66 0xaa 0xc8>;
    		interrupt-parent = <0x09>;
    		interrupts = <0x41 0x02>;
    		pulses-per-revolution = <0x02>;
    	};
    
    	clocks {
    
    		clock@0 {
    			compatible = "fixed-clock";
    			clock-frequency = <0x2625a00>;
    			clock-output-names = "ad9361_ext_refclk";
    			#clock-cells = <0x00>;
    			phandle = <0x08>;
    		};
    	};
    
    	__symbols__ {
    		cpu0 = "/cpus/cpu@0";
    		cpu1 = "/cpus/cpu@1";
    		fpga_full = "/fpga-full";
    		regulator_vccpint = "/fixedregulator";
    		replicator_out_port0 = "/replicator/out-ports/port@0/endpoint";
    		replicator_out_port1 = "/replicator/out-ports/port@1/endpoint";
    		replicator_in_port0 = "/replicator/in-ports/port/endpoint";
    		amba = "/axi";
    		adc = "/axi/adc@f8007100";
    		can0 = "/axi/can@e0008000";
    		can1 = "/axi/can@e0009000";
    		gpio0 = "/axi/gpio@e000a000";
    		i2c0 = "/axi/i2c@e0004000";
    		i2c1 = "/axi/i2c@e0005000";
    		intc = "/axi/interrupt-controller@f8f01000";
    		L2 = "/axi/cache-controller@f8f02000";
    		mc = "/axi/memory-controller@f8006000";
    		ocmc = "/axi/ocmc@f800c000";
    		uart0 = "/axi/serial@e0000000";
    		uart1 = "/axi/serial@e0001000";
    		spi0 = "/axi/spi@e0006000";
    		adc0_ad9361 = "/axi/spi@e0006000/ad9361-phy@0";
    		spi1 = "/axi/spi@e0007000";
    		qspi = "/axi/spi@e000d000";
    		flash0 = "/axi/spi@e000d000/flash@0";
    		smcc = "/axi/memory-controller@e000e000";
    		nand0 = "/axi/memory-controller@e000e000/flash@e1000000";
    		nor0 = "/axi/memory-controller@e000e000/flash@e2000000";
    		gem0 = "/axi/ethernet@e000b000";
    		gem1 = "/axi/ethernet@e000c000";
    		sdhci0 = "/axi/mmc@e0100000";
    		sdhci1 = "/axi/mmc@e0101000";
    		slcr = "/axi/slcr@f8000000";
    		clkc = "/axi/slcr@f8000000/clkc@100";
    		rstc = "/axi/slcr@f8000000/rstc@200";
    		pinctrl0 = "/axi/slcr@f8000000/pinctrl@700";
    		dmac_s = "/axi/dmac@f8003000";
    		devcfg = "/axi/devcfg@f8007000";
    		efuse = "/axi/efuse@f800d000";
    		global_timer = "/axi/timer@f8f00200";
    		ttc0 = "/axi/timer@f8001000";
    		ttc1 = "/axi/timer@f8002000";
    		scutimer = "/axi/timer@f8f00600";
    		usb0 = "/axi/usb@e0002000";
    		usb1 = "/axi/usb@e0003000";
    		watchdog0 = "/axi/watchdog@f8005000";
    		etb_in_port = "/axi/etb@f8801000/in-ports/port/endpoint";
    		tpiu_in_port = "/axi/tpiu@f8803000/in-ports/port/endpoint";
    		funnel_out_port = "/axi/funnel@f8804000/out-ports/port/endpoint";
    		funnel0_in_port0 = "/axi/funnel@f8804000/in-ports/port@0/endpoint";
    		funnel0_in_port1 = "/axi/funnel@f8804000/in-ports/port@1/endpoint";
    		funnel0_in_port2 = "/axi/funnel@f8804000/in-ports/port@2/endpoint";
    		ptm0_out_port = "/axi/ptm@f889c000/out-ports/port/endpoint";
    		ptm1_out_port = "/axi/ptm@f889d000/out-ports/port/endpoint";
    		fpga_axi = "/fpga-axi@0";
    		fmc_i2c = "/fpga-axi@0/i2c@41620000";
    		rx_dma = "/fpga-axi@0/dma@7c400000";
    		tx_dma = "/fpga-axi@0/dma@7c420000";
    		cf_ad9361_adc_core_0 = "/fpga-axi@0/cf-ad9361-lpc@79020000";
    		cf_ad9361_dac_core_0 = "/fpga-axi@0/cf-ad9361-dds-core-lpc@79024000";
    		adv7511 = "/fpga-axi@0/i2c@41600000/adv7511@39";
    		adv7511_in = "/fpga-axi@0/i2c@41600000/adv7511@39/ports/port@0/endpoint";
    		hdmi_dma = "/fpga-axi@0/dma@43000000";
    		hdmi_clock = "/fpga-axi@0/axi-clkgen@79000000";
    		axi_hdmi_out = "/fpga-axi@0/axi_hdmi@70e00000/port/endpoint";
    		pwm = "/fpga-axi@0/axi-pwmgen@44b00000";
    		ad9361_clkin = "/clocks/clock@0";
    	};
    };

  • And here is the vivado block design and reg map.

  • root@analog:/sys/bus/platform/devices/70e00000.axi_hdmi# ls
    dma:video  driver_override  graphics  of_node  subsystem
    driver     drm              modalias  power    uevent
    root@analog:/sys/bus/platform/devices/70e00000.axi_hdmi# cd dma:video
    root@analog:/sys/bus/platform/devices/70e00000.axi_hdmi/dma:video# ls -ll
    total 0
    -r--r--r-- 1 root root 4096 Aug  5 03:55 bytes_transferred
    lrwxrwxrwx 1 root root    0 Aug  5 03:55 device -> ../../../43000000.dma
    -r--r--r-- 1 root root 4096 Aug  5 03:55 in_use
    -r--r--r-- 1 root root 4096 Aug  5 03:55 memcpy_count
    drwxr-xr-x 2 root root    0 Aug  5 03:54 power
    lrwxrwxrwx 1 root root    0 Aug  5 03:55 slave -> ../../../70e00000.axi_hdmi
    lrwxrwxrwx 1 root root    0 Aug  5 03:53 subsystem -> ../../../../../../class/dma
    -rw-r--r-- 1 root root 4096 Aug  5 03:53 uevent                                s
    root@analog:/sys/class# tform/devices/70e00000.axi_hdmi/dma:video# cd /sys/class
    root@analog:/sys/class#
    root@analog:/sys/class#
    root@analog:/sys/class# ls -ll
    total 0
    drwxr-xr-x 2 root root 0 Aug  5 03:53 arvo
    drwxr-xr-x 2 root root 0 Aug  5 03:53 backlight
    drwxr-xr-x 2 root root 0 Aug  5 03:53 bdi
    drwxr-xr-x 2 root root 0 Aug  5 03:53 block
    drwxr-xr-x 2 root root 0 Aug  5 03:53 devlink
    drwxr-xr-x 2 root root 0 Aug  5 03:53 dma
    drwxr-xr-x 2 root root 0 Aug  5 03:53 drm
    drwxr-xr-x 2 root root 0 Aug  5 03:53 dvb
    drwxr-xr-x 2 root root 0 Aug  5 03:53 extcon
    drwxr-xr-x 2 root root 0 Aug  5 03:53 fpga_bridge
    drwxr-xr-x 2 root root 0 Aug  5 03:53 fpga_manager
    drwxr-xr-x 2 root root 0 Aug  5 03:53 fpga_region
    drwxrwxr-x 2 root gpio 0 Aug  5 03:54 gpio
    drwxr-xr-x 2 root root 0 Aug  5 03:53 graphics
    drwxr-xr-x 2 root root 0 Aug  5 03:53 hidraw
    drwxr-xr-x 2 root root 0 Aug  5 03:53 hwmon
    drwxr-xr-x 2 root root 0 Aug  5 03:53 i2c-adapter
    drwxr-xr-x 2 root root 0 Aug  5 03:53 i2c-dev
    drwxr-xr-x 2 root root 0 Aug  5 03:53 ieee802154
    drwxr-xr-x 2 root root 0 Aug  5 03:53 input
    drwxr-xr-x 2 root root 0 Aug  5 03:53 isku
    drwxr-xr-x 2 root root 0 Aug  5 03:53 kone
    drwxr-xr-x 2 root root 0 Aug  5 03:53 koneplus
    drwxr-xr-x 2 root root 0 Aug  5 03:53 konepure
    drwxr-xr-x 2 root root 0 Aug  5 03:53 kovaplus
    drwxr-xr-x 2 root root 0 Aug  5 03:53 leds
    drwxr-xr-x 2 root root 0 Aug  5 03:53 mathworks_ip
    drwxr-xr-x 2 root root 0 Aug  5 03:53 mdio_bus
    drwxr-xr-x 2 root root 0 Aug  5 03:53 mem
    drwxr-xr-x 2 root root 0 Mar 27 06:42 misc
    drwxr-xr-x 2 root root 0 Aug  5 03:53 mmc_host
    drwxr-xr-x 2 root root 0 Aug  5 03:53 mtd
    drwxr-xr-x 2 root root 0 Aug  5 03:53 mux
    drwxr-xr-x 2 root root 0 Aug  5 03:53 net
    drwxr-xr-x 2 root root 0 Aug  5 03:53 power_supply
    drwxr-xr-x 2 root root 0 Aug  5 03:53 pwm
    drwxr-xr-x 2 root root 0 Aug  5 03:53 pyra
    drwxr-xr-x 2 root root 0 Aug  5 03:53 regulator
    drwxr-xr-x 2 root root 0 Aug  5 03:53 rtc
    drwxr-xr-x 2 root root 0 Aug  5 03:53 ryos
    drwxr-xr-x 2 root root 0 Aug  5 03:53 savu
    drwxr-xr-x 2 root root 0 Aug  5 03:53 scsi_device
    drwxr-xr-x 2 root root 0 Aug  5 03:53 scsi_disk
    drwxr-xr-x 2 root root 0 Aug  5 03:53 scsi_generic
    drwxr-xr-x 2 root root 0 Aug  5 03:53 scsi_host
    drwxr-xr-x 2 root root 0 Aug  5 03:53 sound
    drwxr-xr-x 2 root root 0 Aug  5 03:53 spidev
    drwxr-xr-x 2 root root 0 Aug  5 03:53 spi_master
    drwxr-xr-x 2 root root 0 Aug  5 03:53 thermal
    drwxr-xr-x 2 root root 0 Mar 27 06:42 tty
    drwxr-xr-x 2 root root 0 Aug  5 03:53 typec
    drwxr-xr-x 2 root root 0 Aug  5 03:53 typec_mux
    drwxr-xr-x 2 root root 0 Aug  5 03:53 udc
    drwxr-xr-x 2 root root 0 Aug  5 03:53 uio
    drwxr-xr-x 2 root root 0 Aug  5 03:53 usb_role
    drwxr-xr-x 2 root root 0 Aug  5 03:53 vc
    drwxr-xr-x 2 root root 0 Aug  5 03:53 video4linux
    drwxr-xr-x 2 root root 0 Aug  5 03:53 vtconsole
    drwxr-xr-x 2 root root 0 Aug  5 03:53 wakeup
    drwxr-xr-x 2 root root 0 Aug  5 03:53 watchdog
    root@analog:/sys/class# cd dma
    root@analog:/sys/class/dma# ls
    dma0chan0  dma2chan0  dma3chan1  dma3chan3  dma3chan5  dma3chan7
    dma1chan0  dma3chan0  dma3chan2  dma3chan4  dma3chan6
    root@analog:/sys/class/dma# cd dma2chan0
    root@analog:/sys/class/dma/dma2chan0# ls
    bytes_transferred  in_use        power  subsystem
    device             memcpy_count  slave  uevent
    root@analog:/sys/class/dma/dma2chan0# cat in_use
    1
    root@analog:/sys/class/dma/dma2chan0# ll
    -bash: ll: command not found
    root@analog:/sys/class/dma/dma2chan0# ls
    bytes_transferred  in_use        power  subsystem
    device             memcpy_count  slave  uevent
    root@analog:/sys/class/dma/dma2chan0# cat slave
    cat: slave: Is a directory
    root@analog:/sys/class/dma/dma2chan0# ll
    -bash: ll: command not found
    root@analog:/sys/class/dma/dma2chan0# ls -ll
    total 0
    -r--r--r-- 1 root root 4096 Aug  5 03:55 bytes_transferred
    lrwxrwxrwx 1 root root    0 Aug  5 03:55 device -> ../../../43000000.dma
    -r--r--r-- 1 root root 4096 Aug  5 03:55 in_use
    -r--r--r-- 1 root root 4096 Aug  5 03:55 memcpy_count
    drwxr-xr-x 2 root root    0 Aug  5 03:54 power
    lrwxrwxrwx 1 root root    0 Aug  5 03:55 slave -> ../../../70e00000.axi_hdmi
    lrwxrwxrwx 1 root root    0 Aug  5 03:53 subsystem -> ../../../../../../class/dma
    -rw-r--r-- 1 root root 4096 Aug  5 03:53 uevent
    root@analog:/sys/class/dma/dma2chan0# cat bytes_transferred
    0
    root@analog:/sys/class/dma/dma2chan0# cat memcpy_count
    0
    root@analog:/sys/class/dma/dma2chan0# cd /sys/class/graphics/fb0/
    root@analog:/sys/class/graphics/fb0# ls -ll
    total 0
    -rw-r--r-- 1 root root 4096 Aug  5 03:59 bits_per_pixel
    -rw-r--r-- 1 root root 4096 Aug  5 03:59 blank
    -rw-r--r-- 1 root root 4096 Aug  5 03:59 bl_curve
    -rw-r--r-- 1 root root 4096 Aug  5 03:59 console
    -rw-r--r-- 1 root root 4096 Aug  5 03:59 cursor
    -r--r--r-- 1 root root 4096 Aug  5 03:59 dev
    lrwxrwxrwx 1 root root    0 Aug  5 03:59 device -> ../../../70e00000.axi_hdmi
    -rw-r--r-- 1 root root 4096 Aug  5 03:59 mode
    -rw-r--r-- 1 root root 4096 Aug  5 03:59 modes
    -r--r--r-- 1 root root 4096 Aug  5 03:54 name
    -rw-r--r-- 1 root root 4096 Aug  5 03:59 pan
    drwxr-xr-x 2 root root    0 Aug  5 03:54 power
    -rw-r--r-- 1 root root 4096 Aug  5 03:59 rotate
    -rw-r--r-- 1 root root 4096 Aug  5 03:59 state
    -r--r--r-- 1 root root 4096 Aug  5 03:59 stride
    lrwxrwxrwx 1 root root    0 Aug  5 03:53 subsystem -> ../../../../../../class/graphics
    -rw-r--r-- 1 root root 4096 Aug  5 03:53 uevent
    -rw-r--r-- 1 root root 4096 Aug  5 03:59 virtual_size

  • Hi RunfengFang, 

    Based on the contents of this post and your other posts, it seems this post should be located in the FPGA Reference Designs forum:
    https://ez.analog.com/fpga/

    -Matt

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.