KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
MAX96724
Recommended for New Designs
The MAX96724/F/R deserializer converts four GMSL2/1 inputs to 1, 2, or 4 MIPI D-PHY or C-PHY outputs. The device allows simultaneous transmit bidirectional...
Datasheet
MAX96724 on Analog.com
brief:
I am having problems to evaluate the max96724 deserialzer with c1 moduel as recommended by the wiki and followed the steps AMD Kria User Guide [Analog Devices Wiki]. The media node fails to get registered, as i2c-subdev serializer is not responding.
I am using only one c1 camera module and also using the correct device-tree for 1cam, which is shared in the new sd-image.
As debug I tried the following,
1- swapping with new coax cables for the camera module,
2- ensuring the switch settings on the adapter, ensuring the correct or default jumper settings from evk-user guide, connecting the camera module to the J7 connector (INA)
3- the wiki is missing instructions to insert the 12V baller jack power supply to the eval kit and turn on the ON switch.
4- I followed the EVK with GMSL GUI to read and write a couple of register as described in the ser-des userguide under the section "I2c braodcasting GMSL2 programming examples"