MAX96724
Recommended for New Designs
The MAX96724/F/R deserializer converts four GMSL2/1 inputs to 1, 2, or 4 MIPI D-PHY or C-PHY outputs. The device allows simultaneous transmit bidirectional...
Datasheet
MAX96724 on Analog.com
brief:
I am having problems to evaluate the max96724 deserialzer with c1 moduel as recommended by the wiki and followed the steps AMD Kria User Guide [Analog Devices Wiki]. The media node fails to get registered, as i2c-subdev serializer is not responding.
I am using only one c1 camera module and also using the correct device-tree for 1cam, which is shared in the new sd-image.
As debug I tried the following,
1- swapping with new coax cables for the camera module,
2- ensuring the switch settings on the adapter, ensuring the correct or default jumper settings from evk-user guide, connecting the camera module to the J7 connector (INA)
3- the wiki is missing instructions to insert the 12V baller jack power supply to the eval kit and turn on the ON switch.
4- I followed the EVK with GMSL GUI to read and write a couple of register as described in the ser-des userguide under the section "I2c braodcasting GMSL2 programming examples"


Hi Yuba,
If it is not working with GMSL GUI then I think is a configuration problem.
Can you please connect the deserializer eval kit to GMSL GUI and check the CFG pins?
You should find them in GMSL GUI -> tab Tools -> Set CFG Pin Levels
Should both be set to 0 for COAX GMSL2.
I am able to capture frames from the sensor.
I am able to capture frames from the sensor.