Post Go back to editing

evaluating max96724 eval kit with kria som

Thread Summary

The user encountered issues with the MAX96724 deserializer and C1 camera module on the AMD Kria platform, where the media node failed to register due to a non-responding I2C subdev serializer. The problem was resolved by setting the CFG pins to 0x00, which allowed the media node to register and the user to capture frames from the sensor.
AI Generated Content
Category: Software
Product Number: max96724-bak-evk
Software Version: linux

brief: 

I am having problems to evaluate the max96724 deserialzer with c1 moduel as recommended by the wiki and followed the steps AMD Kria User Guide [Analog Devices Wiki]. The media node fails to get registered, as i2c-subdev serializer is not responding.

I am using only one c1 camera module and also using the correct device-tree for 1cam, which is shared in the new sd-image. 

As debug I tried the following,

1- swapping with new coax cables for the camera module, 

2- ensuring the switch settings on the adapter, ensuring the correct or default jumper settings from evk-user guide, connecting the camera module to the J7 connector (INA) 

3- the wiki is missing instructions to insert the 12V baller jack power supply to the eval kit and turn on the ON switch. 

4- I followed the EVK with GMSL GUI to read and write a couple of register as described in the ser-des userguide under the section "I2c braodcasting GMSL2 programming examples"

the first instruction to enable Link A goes through, while the second instruction to change the device address for serializer fails with a NACK operation. 
Here are the commands which also reflect in the max MAX9295D UG as well.
0x4E,0x0003,0xFE
0x80,0x0000,0x82
5- I replaced the c1 camera module with a known good camera module with the same SER device (LI-VENUS-OX03F10-9295-075H), faild to get any response from the serializer. 
Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.