To create our multi-channel magnetic field meter project, we purchased the set of AD9656 Evaluation Board and HSC-ADC-EVALEZ FPGA Based Data Capture Kit. However, the capabilities of the firmware provided with this kit were insufficient for the implementation of our project.
To create our own firmware with the required functionality, we were provided with the firmware source code for ad9656 + evalez board. The source code was dated 6 Jan 2020 and provided as an ISE project for version 14.7 and implemented for the Xilinx Virtex-6 FPGA.
Unfortunately, in the provided sample project was missing several files, namely:
jesd204_v2_2_1l.ngc
jesd204_v2_2_1l.v
jesd204_v2_2_2l.ngc
jesd204_v2_2_2l.v
jesd204_v2_2_4l.ngc
jesd204_v2_2_4l.v
Please tell me where I can get these missing files?