Post Go back to editing

AD9081 Petalinux 2022.2 ad9081 spi1.0: PLL not locked Error

Category: Software
Product Number: AD9081
Software Version: Petalinıx 2022.2

Hello everyone,

I am developing a Linux based application using AD9081 and ZCU102. I compiled a kernel using the xsa file I received with the reference HDL design (dafault). Everything is as it should be but I am getting an error in ad9081 spi1.0. dmseg messages are as follows;

ad9081 spi1.0: supply vdd not found, using dummy regulator
ad9081 spi1.0:PLL not locked, "pll_lock" in adi_ad9081_device_clk_pll_div_set(...), line 402 in drivers/iio/adc/ad9081/adi_ad9081_device.c
ad9081 spi1.0:Failed to initialize: -21
ad9081: probe of spi1.0 failed with error -21

Because this is the case, ad9081 does not appear as a device under iio.

The dtsi files I used are as follows. 

https://github.com/analogdevicesinc/linux/blob/main/arch/arm/boot/dts/adi-ad9081-fmc-ebz.dtsi

https://github.com/analogdevicesinc/linux/blob/main/arch/arm64/boot/dts/xilinx/zynqmp-zcu102-rev10-ad9081-default.dtsi

I couldn't understand what the problem was. In addition the output of the " iio_attr -D hmc7044 status " message is as follows.

- - - PLL1 - - -
Status : Locked
Using : CLKIN0 @ 100000000 Hz
PFD: 1000 kHz

- - - PLL2 - - -
Status : Unlocked(Synchronized)
Frequency : 300000000 Hz(Autocal cap bank value:16)
SYSREF Status: Invalid
SYNC Status : Unsynchronized
Lock Status: Unlocked

system-user.dtsi file

// SPDX-License-Identifier: GPL-2.0
/*
 * Analog Devices AD9081-FMC-EBZ
 * https://wiki.analog.com/resources/tools-software/linux-drivers/iio-mxfe/ad9081
 * https://wiki.analog.com/resources/eval/user-guides/ad9081_fmca_ebz/ad9081_fmca_ebz_hdl
 *
 * Copyright (C) 2019-2020 Analog Devices Inc.
 */

#include <dt-bindings/interrupt-controller/irq.h>
#include <dt-bindings/iio/adc/adi,ad9081.h>
#include <dt-bindings/jesd204/adxcvr.h>

&i2c1 {
	i2c-mux@75 {
		i2c@0 { /* HPC0 */
			#address-cells = <1>;
			#size-cells = <0>;
			reg = <0>;
			/* HPC0_IIC */
			eeprom@50 {
				compatible = "at24,24c02";
				reg = <0x50>;
			};
		};
	};
};

@qspi 
{
	flash@0
	{
		compatible = "m25p80", "jedec,spi-nor";
		reg = <0>;
		spi-tx-bus-width = <1>;
		spi-rx-bus-width = <4>;
		spi-max-freqency = <20000000>;
	}
}

/ {
	fpga_axi: fpga-axi@0 {
		interrupt-parent = <&gic>;
		compatible = "simple-bus";
		#address-cells = <0x1>;
		#size-cells = <0x1>;
		ranges = <0 0 0 0xffffffff>;

		rx_dma: dma@9c420000 {
			compatible = "adi,axi-dmac-1.00.a";
			reg = <0x9c420000 0x10000>;
			#dma-cells = <1>;
			#clock-cells = <0>;
			interrupts = <0 109 IRQ_TYPE_LEVEL_HIGH>;
			clocks = <&zynqmp_clk 73>;
		};

		tx_dma: dma@9c430000  {
			compatible = "adi,axi-dmac-1.00.a";
			reg = <0x9c430000 0x10000>;
			#dma-cells = <1>;
			#clock-cells = <0>;
			interrupts = <0 108 IRQ_TYPE_LEVEL_HIGH>;
			clocks = <&zynqmp_clk 73>;
		};

		axi_ad9081_core_rx: axi-ad9081-rx-hpc@84a10000 {
			compatible = "adi,axi-ad9081-rx-1.0";
			reg = <0x84a10000 0x8000>;
			dmas = <&rx_dma 0>;
			dma-names = "rx";
			spibus-connected = <&trx0_ad9081>;

			jesd204-device;
			#jesd204-cells = <2>;
			jesd204-inputs = <&axi_ad9081_rx_jesd 0 FRAMER_LINK0_RX>;
		};

		axi_ad9081_core_tx: axi-ad9081-tx-hpc@84b10000 {
			compatible = "adi,axi-ad9081-tx-1.0";
			reg = <0x84b10000 0x4000>;
			dmas = <&tx_dma 0>;
			dma-names = "tx";
			clocks = <&trx0_ad9081 1>;
			clock-names = "sampl_clk";
			spibus-connected = <&trx0_ad9081>;
			//adi,axi-pl-fifo-enable;
			adi,axi-data-offload-connected = <&axi_data_offload_tx>;

			jesd204-device;
			#jesd204-cells = <2>;
			jesd204-inputs = <&axi_ad9081_tx_jesd 0 DEFRAMER_LINK0_TX>;
		};

		axi_ad9081_rx_jesd: axi-jesd204-rx@84a90000 {
			compatible = "adi,axi-jesd204-rx-1.0";
			reg = <0x84a90000 0x1000>;

			interrupts = <0 107 IRQ_TYPE_LEVEL_HIGH>;

			clocks = <&zynqmp_clk 71>, <&hmc7044 10>, <&axi_ad9081_adxcvr_rx 0>;
			clock-names = "s_axi_aclk", "device_clk", "lane_clk";

			#clock-cells = <0>;
			clock-output-names = "jesd_rx_lane_clk";

			jesd204-device;
			#jesd204-cells = <2>;
			jesd204-inputs = <&axi_ad9081_adxcvr_rx 0 FRAMER_LINK0_RX>;
		};

		axi_ad9081_tx_jesd: axi-jesd204-tx@84b90000 {
			compatible = "adi,axi-jesd204-tx-1.0";
			reg = <0x84b90000 0x1000>;

			interrupts = <0 106 IRQ_TYPE_LEVEL_HIGH>;

			clocks = <&zynqmp_clk 71>, <&hmc7044 6>, <&axi_ad9081_adxcvr_tx 0>;
			clock-names = "s_axi_aclk", "device_clk", "lane_clk";

			#clock-cells = <0>;
			clock-output-names = "jesd_tx_lane_clk";

			jesd204-device;
			#jesd204-cells = <2>;
			jesd204-inputs = <&axi_ad9081_adxcvr_tx 0 DEFRAMER_LINK0_TX>;
		};

		axi_ad9081_adxcvr_rx: axi-adxcvr-rx@84a60000 {
			#address-cells = <1>;
			#size-cells = <0>;
			compatible = "adi,axi-adxcvr-1.0";
			reg = <0x84a60000 0x1000>;

			clocks = <&hmc7044 12>;
			clock-names = "conv";

			#clock-cells = <1>;
			clock-output-names = "rx_gt_clk", "rx_out_clk";

			adi,sys-clk-select = <XCVR_QPLL>;
			adi,out-clk-select = <XCVR_REFCLK_DIV2>;
			adi,use-lpm-enable;

			jesd204-device;
			#jesd204-cells = <2>;
			jesd204-inputs =  <&hmc7044 0 FRAMER_LINK0_RX>;
		};

		axi_ad9081_adxcvr_tx: axi-adxcvr-tx@84b60000 {
			#address-cells = <1>;
			#size-cells = <0>;
			compatible = "adi,axi-adxcvr-1.0";
			reg = <0x84b60000 0x1000>;

			clocks = <&hmc7044 12>;
			clock-names = "conv";

			#clock-cells = <1>;
			clock-output-names = "tx_gt_clk", "tx_out_clk";

			adi,sys-clk-select = <XCVR_QPLL>;
			adi,out-clk-select = <XCVR_REFCLK_DIV2>;

			jesd204-device;
			#jesd204-cells = <2>;
			jesd204-inputs =  <&hmc7044 0 DEFRAMER_LINK0_TX>;
		};

		axi_sysid_0: axi-sysid-0@85000000 {
			compatible = "adi,axi-sysid-1.00.a";
			reg = <0x85000000 0x10000>;
		};

		axi_data_offload_tx: axi-data-offload-0@9c440000 {
			compatible = "adi,axi-data-offload-1.0.a";
			reg = <0x9c440000 0x10000>;
			// adi,bringup;
			// adi,oneshot;
			// adi,bypass;
			// adi,sync-config = <2>;
			// adi,transfer-length = /bits/ 64 <0x10000>; // 2**16 bytes
		};

		axi_data_offload_rx: axi-data-offload-1@9c450000 {
			compatible = "adi,axi-data-offload-1.0.a";
			reg = <0x9c450000 0x10000>;
		};
	};
};

&spi0 {
	status = "okay";
};

#define fmc_spi spi0

#include "ad9081-device.dtsi"

// ad_iobuf #(.DATA_WIDTH(12)) i_iobuf (
//	.dio_t (gpio_t[43:32]),
//	.dio_i (gpio_o[43:32]),
//	.dio_o (gpio_i[43:32]),
//	dio_p ({hmc_gpio1,       // 43 121
//	gpio[10:0]}));   // 42-32
//
// assign gpio_i[44] = agc0[0];
// assign gpio_i[45] = agc0[1];
// assign gpio_i[46] = agc1[0];
// assign gpio_i[47] = agc1[1];
// assign gpio_i[48] = agc2[0];
// assign gpio_i[49] = agc2[1];
// assign gpio_i[50] = agc3[0];
// assign gpio_i[51] = agc3[1];
// assign gpio_i[52] = irqb[0];
// assign gpio_i[53] = irqb[1];
//
// assign hmc_sync         = gpio_o[54];
// assign rstb             = gpio_o[55]; 133
// assign rxen[0]          = gpio_o[56]; 134
// assign rxen[1]          = gpio_o[57]; 135
// assign txen[0]          = gpio_o[58]; 136
// assign txen[1]          = gpio_o[59]; 137

&fmc_spi {

	trx0_ad9081: ad9081@0 {
		#address-cells = <1>;
		#size-cells = <0>;

		reset-gpios = <&gpio 133 0>;
		sysref-req-gpios = <&gpio 121 0>;
		rx2-enable-gpios = <&gpio 135 0>;
		rx1-enable-gpios = <&gpio 134 0>;
		tx2-enable-gpios = <&gpio 137 0>;
		tx1-enable-gpios = <&gpio 136 0>;

	};
};

ad9081-device.dtsi file

// SPDX-License-Identifier: GPL-2.0
/*
 * Analog Devices AD9081-FMC-EBZ on Xilinx ZynqMP ZCU102 Rev 1.0
 * https://wiki.analog.com/resources/tools-software/linux-drivers/iio-mxfe/ad9081
 * https://wiki.analog.com/resources/eval/user-guides/ad9081_fmca_ebz/ad9081_fmca_ebz_hdl
 *
 * Copyright (C) 2019-2020 Analog Devices Inc.
 */

#include <dt-bindings/iio/frequency/hmc7044.h>
#include <dt-bindings/iio/adc/adi,ad9081.h>

/delete-node/ &axi_mxfe_rx_dma;
/delete-node/ &axi_mxfe_rx_jesd_rx_axi;
/delete-node/ &misc_clk_0;
/delete-node/ &axi_mxfe_rx_xcvr;
/delete-node/ &axi_mxfe_tx_dma;
/delete-node/ &axi_mxfe_tx_jesd_tx_axi;
/delete-node/ &axi_mxfe_tx_xcvr;
/delete-node/ &axi_sysid_0;
/delete-node/ &mxfe_rx_data_offload_i_data_offload;
/delete-node/ &mxfe_tx_data_offload_i_data_offload;
/delete-node/ &rx_mxfe_tpl_core_adc_tpl_core;
/delete-node/ &tx_mxfe_tpl_core_dac_tpl_core;

/*
 *	VCXO = 122.880 MHz, XO = 122.880 MHz (AD9081-FMC-EBZ)
 */

&spi1 {
	status = "okay";

	hmc7044: hmc7044@0 {
		#address-cells = <1>;
		#size-cells = <0>;
		#clock-cells = <1>;
		compatible = "adi,hmc7044";
		reg = <0>;
		spi-max-frequency = <1000000>;

		jesd204-device;
		#jesd204-cells = <2>;
		jesd204-sysref-provider;

		adi,jesd204-max-sysref-frequency-hz = <2000000>; /* 2 MHz */

		/*
		* There are different versions of the AD9081-FMCA-EBZ & AD9082-FMCA-EBZ
		* VCXO = 122.880 MHz, XO = 122.880MHz (AD9081-FMC-EBZ & AD9082-FMC-EBZ)
		* VCXO = 100.000 MHz, XO = 100.000MHz (AD9081-FMC-EBZ-A2 & AD9082-FMC-EBZ-A2)
		* To determine which board is which, read the freqency printed on the VCXO
		* or use the fru-dump utility:
		* #fru-dump -b /sys/bus/i2c/devices/15-0050/eeprom
		*/

		//adi,pll1-clkin-frequencies = <122880000 30720000 0 0>;
		//adi,vcxo-frequency = <122880000>;

		adi,pll1-clkin-frequencies = <100000000 10000000 0 0>;
		adi,vcxo-frequency = <100000000>;

		adi,pll1-loop-bandwidth-hz = <200>;
		adi,pll1-charge-pump-current-ua = <720>;
		adi,pfd1-maximum-limit-frequency-hz = <1000000>; /* 1 MHz */

		adi,pll2-output-frequency = <3000000000>;

		adi,sysref-timer-divider = <1024>;
		adi,pulse-generator-mode = <0>;

		adi,clkin0-buffer-mode  = <0x07>;
		adi,clkin1-buffer-mode  = <0x07>;
		adi,oscin-buffer-mode = <0x15>;

		adi,gpi-controls = <0x00 0x00 0x00 0x00>;
		adi,gpo-controls = <0x37 0x33 0x00 0x00>;

		clock-output-names =
				"hmc7044_out0", "hmc7044_out1", "hmc7044_out2",
				"hmc7044_out3", "hmc7044_out4", "hmc7044_out5",
				"hmc7044_out6", "hmc7044_out7", "hmc7044_out8",
				"hmc7044_out9", "hmc7044_out10", "hmc7044_out11",
				"hmc7044_out12", "hmc7044_out13";

		hmc7044_c0: channel@0 {
			reg = <0>;
			adi,extended-name = "CORE_CLK_RX";
			adi,divider = <12>;	// 250
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS

		};
		hmc7044_c2: channel@2 {
			reg = <2>;
			adi,extended-name = "DEV_REFCLK";
			adi,divider = <12>;	// 250
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
		};
		hmc7044_c3: channel@3 {
			reg = <3>;
			adi,extended-name = "DEV_SYSREF";
			adi,divider = <1536>;	// 1.953125
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
			adi,jesd204-sysref-chan;
		};

		hmc7044_c6: channel@6 {
			reg = <6>;
			adi,extended-name = "CORE_CLK_TX";
			adi,divider = <12>;	// 250
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
		};

		hmc7044_c8: channel@8 {
			reg = <8>;
			adi,extended-name = "FPGA_REFCLK1";
			adi,divider = <12>;	// 250
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
		};
		hmc7044_c10: channel@10 {
			reg = <10>;
			adi,extended-name = "CORE_CLK_RX_ALT";
			adi,divider = <12>;	// 250
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
		};
		hmc7044_c12: channel@12 {
			reg = <12>;
			adi,extended-name = "FPGA_REFCLK2";
			adi,divider = <12>;	// 250
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
		};
		hmc7044_c13: channel@13 {
			reg = <13>;
			adi,extended-name = "FPGA_SYSREF";
			adi,divider = <1536>;	// 1.953125
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;	// LVDS
			adi,jesd204-sysref-chan;
		};
	};
};

&fmc_spi {

	trx0_ad9081: ad9081@0 {
		#address-cells = <1>;
		#size-cells = <0>;
		compatible = "adi,ad9081";
		reg = <0>;
		spi-max-frequency = <5000000>;

		/* Clocks */
		clocks = <&hmc7044 2>;
		clock-names = "dev_clk";

		clock-output-names = "rx_sampl_clk", "tx_sampl_clk";
		#clock-cells = <1>;

		jesd204-device;
		#jesd204-cells = <2>;
		jesd204-top-device = <0>; /* This is the TOP device */
		jesd204-link-ids = <FRAMER_LINK0_RX DEFRAMER_LINK0_TX>;

		jesd204-inputs =
			<&axi_ad9081_core_rx 0 FRAMER_LINK0_RX>,
			<&axi_ad9081_core_tx 0 DEFRAMER_LINK0_TX>;

		adi,tx-dacs {
			#size-cells = <0>;
			#address-cells = <1>;

			adi,dac-frequency-hz = /bits/ 64 <12000000000>;

			adi,main-data-paths {
				#address-cells = <1>;
				#size-cells = <0>;

				adi,interpolation = <6>;

				ad9081_dac0: dac@0 {
					reg = <0>;
					adi,crossbar-select = <&ad9081_tx_fddc_chan0>;
					adi,nco-frequency-shift-hz = /bits/ 64 <1000000000>; /* 1000 MHz */
				};
				ad9081_dac1: dac@1 {
					reg = <1>;
					adi,crossbar-select = <&ad9081_tx_fddc_chan1>;
					adi,nco-frequency-shift-hz = /bits/ 64 <1100000000>; /* 1100 MHz */
				};
				ad9081_dac2: dac@2 {
					reg = <2>;
					adi,crossbar-select = <&ad9081_tx_fddc_chan2>; /* All 4 channels @ dac2 */
					adi,nco-frequency-shift-hz = /bits/ 64 <1200000000>;  /* 1200 MHz */
				};
				ad9081_dac3: dac@3 {
					reg = <3>;
					adi,crossbar-select = <&ad9081_tx_fddc_chan3>; /* All 4 channels @ dac2 */
					adi,nco-frequency-shift-hz = /bits/ 64 <1300000000>; /* 1300 MHz */
				};
			};

			adi,channelizer-paths {
				#address-cells = <1>;
				#size-cells = <0>;
				adi,interpolation = <8>;

				ad9081_tx_fddc_chan0: channel@0 {
					reg = <0>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

				};
				ad9081_tx_fddc_chan1: channel@1 {
					reg = <1>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

				};
				ad9081_tx_fddc_chan2: channel@2 {
					reg = <2>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

				};
				ad9081_tx_fddc_chan3: channel@3 {
					reg = <3>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

				};
			};

			adi,jesd-links {
				#size-cells = <0>;
				#address-cells = <1>;

				ad9081_tx_jesd_l0: link@0 {
					#address-cells = <1>;
					#size-cells = <0>;
					reg = <0>;

					adi,logical-lane-mapping = /bits/ 8 <0 2 7 6 1 5 4 3>;

					adi,link-mode = <9>;			/* JESD Quick Configuration Mode */
					adi,subclass = <1>;			/* JESD SUBCLASS 0,1,2 */
					adi,version = <1>;			/* JESD VERSION 0=204A,1=204B,2=204C */
					adi,dual-link = <0>;			/* JESD Dual Link Mode */

					adi,converters-per-device = <8>;	/* JESD M */
					adi,octets-per-frame = <4>;		/* JESD F */

					adi,frames-per-multiframe = <32>;	/* JESD K */
					adi,converter-resolution = <16>;	/* JESD N */
					adi,bits-per-sample = <16>;		/* JESD NP' */
					adi,control-bits-per-sample = <0>;	/* JESD CS */
					adi,lanes-per-device = <4>;		/* JESD L */
					adi,samples-per-converter-per-frame = <1>; /* JESD S */
					adi,high-density = <0>;			/* JESD HD */
				};
			};
		};

		adi,rx-adcs {
			#size-cells = <0>;
			#address-cells = <1>;

			adi,adc-frequency-hz = /bits/ 64 <4000000000>;

			adi,main-data-paths {
				#address-cells = <1>;
				#size-cells = <0>;


				ad9081_adc0: adc@0 {
					reg = <0>;
					adi,decimation = <4>;
					adi,nco-frequency-shift-hz =  /bits/ 64 <400000000>;
					adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
				};
				ad9081_adc1: adc@1 {
					reg = <1>;
					adi,decimation = <4>;
					adi,nco-frequency-shift-hz =  /bits/ 64 <(-400000000)>;
					adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
				};
				ad9081_adc2: adc@2 {
					reg = <2>;
					adi,decimation = <4>;
					adi,nco-frequency-shift-hz =  /bits/ 64 <100000000>;
					adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
				};
				ad9081_adc3: adc@3 {
					reg = <3>;
					adi,decimation = <4>;
					adi,nco-frequency-shift-hz =  /bits/ 64 <100000000>;
					adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
				};
			};

			adi,channelizer-paths {
				#address-cells = <1>;
				#size-cells = <0>;


				ad9081_rx_fddc_chan0: channel@0 {
					reg = <0>;
					adi,decimation = <4>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

				};
				ad9081_rx_fddc_chan1: channel@1 {
					reg = <1>;
					adi,decimation = <4>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

				};
				ad9081_rx_fddc_chan4: channel@4 {
					reg = <4>;
					adi,decimation = <4>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

				};
				ad9081_rx_fddc_chan5: channel@5 {
					reg = <5>;
					adi,decimation = <4>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

				};
			};

			adi,jesd-links {
				#size-cells = <0>;
				#address-cells = <1>;

				ad9081_rx_jesd_l0: link@0 {
					reg = <0>;
					adi,converter-select =
						<&ad9081_rx_fddc_chan0 FDDC_I>, <&ad9081_rx_fddc_chan0 FDDC_Q>,
						<&ad9081_rx_fddc_chan1 FDDC_I>, <&ad9081_rx_fddc_chan1 FDDC_Q>,
						<&ad9081_rx_fddc_chan4 FDDC_I>, <&ad9081_rx_fddc_chan4 FDDC_Q>,
						<&ad9081_rx_fddc_chan5 FDDC_I>, <&ad9081_rx_fddc_chan5 FDDC_Q>;

					adi,logical-lane-mapping = /bits/ 8 <2 0 7 6 5 4 3 1>;

					adi,link-mode = <10>;			/* JESD Quick Configuration Mode */
					adi,subclass = <1>;			/* JESD SUBCLASS 0,1,2 */
					adi,version = <1>;			/* JESD VERSION 0=204A,1=204B,2=204C */
					adi,dual-link = <0>;			/* JESD Dual Link Mode */

					adi,converters-per-device = <8>;	/* JESD M */
					adi,octets-per-frame = <4>;		/* JESD F */

					adi,frames-per-multiframe = <32>;	/* JESD K */
					adi,converter-resolution = <16>;	/* JESD N */
					adi,bits-per-sample = <16>;		/* JESD NP' */
					adi,control-bits-per-sample = <0>;	/* JESD CS */
					adi,lanes-per-device = <4>;		/* JESD L */
					adi,samples-per-converter-per-frame = <1>; /* JESD S */
					adi,high-density = <0>;			/* JESD HD */
				};
			};
		};
	};
};

Note: Additionally, when I try with non-OS I get the same error code.

Sincelery



No-Os result
[edited by: FarukS at 5:44 PM (GMT -5) on 4 Nov 2024]

Thread Notes

Parents
  • Hi,

    Could you tell me from what branch did you take the HDL source code?

     , do you have any thoughts on the Petalinux side?

    Best regards,
    Iulia

  • Hi  

    Thansk for reply. HDL branch is R2022_2.

    I had another eval board for AD9081. The crash problem during product testing has been eliminated.

    It's said that probe messages can be found on the AD9081 spi line. However, the device still does not appear under sys/bus/iio/devices  

    current "iio_attr -D hmc7044" status message:


    --- PLL1 ---
    Status:	Locked
    Using:	CLKIN0 @ 100000000 Hz
    PFD:	1000 kHz
    --- PLL2 ---
    Status:	Locked (Synchronized)
    Frequency:	3000000000 Hz (Autocal cap bank value: 14)
    SYSREF Status:	Valid & Locked
    SYNC Status:	Synchronized
    Lock Status:	PLL1 & PLL2 Locked


    current "dmesg" output for AD9081 spi1.0:

    [    6.415831] ad9081 spi1.0: supply vdd not found, using dummy regulator
    [    8.313972] ad9081 spi1.0: AD9081 Rev. 3 Grade 10 (API 1.6.0) probed



    I have a few questions regarding the latest updates.
    1. In my kernel build the libio version is 0.23. But looking at meta-adi-xilinx, it is 0.25. Should I increase this to 0.25?
    2. Should jesd-status and fru-tools definitely be installed? Or is it necessary to provide some ease of access to the device?
    3. When I look at the meta-adi-xilinx content, I see a patch plugin "syvinitscript.patch" along with libiio-v0.25. I guess this is very very important?

    Sincelery

    
    
  • Hi,

    In my kernel build the libio version is 0.23. But looking at meta-adi-xilinx, it is 0.25. Should I increase this to 0.25?

    if you can I would do so, it's always a good thing on be on the latest stable release

    Should jesd-status and fru-tools definitely be installed? Or is it necessary to provide some ease of access to the device?

    Don't think they are mandatory but jesd-satus is a nice tool to display the status of the data interface.

    I guess this is very very important?

    That should only matter if you're using old sysv init system. If you have systemd, it should not be needed.

    - Nuno Sá

  • Hello  

    Thanks for reply. The possible problem is in the device tree creation. When I compile the meta-adi-xilinx repo as is, there is no problem. But when I configure the device tree as above, the AD9081 probes the SPI line and the installation does not occur.

    I compared the system.dtb files created for two different compilations and I observed that some parameters were different. I'm not sure yet what causes these differences.

    I will examine it a little more. Do you have a suggestion?

    Is overlay.dtsi used for zynqmp?

    Sincelery

Reply
  • Hello  

    Thanks for reply. The possible problem is in the device tree creation. When I compile the meta-adi-xilinx repo as is, there is no problem. But when I configure the device tree as above, the AD9081 probes the SPI line and the installation does not occur.

    I compared the system.dtb files created for two different compilations and I observed that some parameters were different. I'm not sure yet what causes these differences.

    I will examine it a little more. Do you have a suggestion?

    Is overlay.dtsi used for zynqmp?

    Sincelery

Children