Post Go back to editing

the bandwith wrong with adrv9002

Category: Software
Product Number: adrv9002
Software Version: 2022_R2

Hi

    I'm using zcu102+adrv9002 platform, generated a profile with 30.72Msps sampling rate and 15.36MHz bandwidth. Under this configuration, the max frequency of cw tone should not over ±7.68MHz,but actually the cw tone can up to ±15.36MHz, it seems wrong.

   when I trying to send an 9.36MHz bandwidth ofdm signal with dac_data_in mode, the acutally bandwith is also 18.72MHz.

the relationship between dac_data_in and dac1_clk/dac1_valid are below. sampling one data when dac1_valid high.

Is there any mistake of my configuration?

Thanks