AD7988-5
Production
The AD7988-1/AD7988-5 are 16-bit, successive approximation,
analog-to-digital converters (ADC) that operate from a single
power supply, VDD. The AD7988...
Datasheet
AD7988-5 on Analog.com
AD7988-1
Production
The AD7988-1/AD7988-5 are 16-bit, successive approximation,
analog-to-digital converters (ADC) that operate from a single
power supply, VDD. The AD7988...
Datasheet
AD7988-1 on Analog.com
AD7984
Production
The AD7984 is an 18-bit, successive approximation, analog-to-digital converter (ADC) that operates from a single power supply, VDD. It contains a low power...
Datasheet
AD7984 on Analog.com
AD7983
Production
The AD7983 is a 16-bit, successive approximation, analog-to-digital converter (ADC) that operates from a single power supply, VDD. It contains a low power...
Datasheet
AD7983 on Analog.com
AD7982
Production
The AD7982 is an 18-bit, successive approximation, analog-to-digital converter (ADC) that operates from a single power supply, VDD. The AD7982 contains...
Datasheet
AD7982 on Analog.com
AD7980
Production
The AD7980 is a 16-bit, successive approximation, analog-to-digital converter (ADC) that operates from a single power supply, VDD. It contains a low power...
Datasheet
AD7980 on Analog.com
AD7949
Production
The AD7949 is an 8-channel, 14-bit, charge redistribution successive approximation register (SAR) analog-to-digital converter (ADC) that operates from...
Datasheet
AD7949 on Analog.com
AD7946
Production
The AD7946 is a 14-bit, 500 kSPS, charge redistribution successive-approximation Analog-to-Digital Converter which operates from a single 5V power supply...
Datasheet
AD7946 on Analog.com
AD7942
Production
The AD7942 is a 14-bit, charge redistribution, successive approximation PulSAR® ADC that operates from a single power supply, VDD, between 2.3 V to 5...
Datasheet
AD7942 on Analog.com
AD7699
Production
The AD7699 is an 8-channel, 16-bit, charge redistribution successive approximation register (SAR) analog-to-digital
converter (ADC) that operates from...
Datasheet
AD7699 on Analog.com
AD7693
Production
The AD7693 is a 16-bit, successive approximation analog-to-digital converter (ADC) that operates from a single power supply, VDD. It contains a low power...
Datasheet
AD7693 on Analog.com
AD7691
Production
The AD7691 is an 18-bit, charge redistribution, successive approximation, analog-to-digital converter (ADC) that operates from a single power supply, VDD...
Datasheet
AD7691 on Analog.com
AD7690
Production
The AD7690 is an 18-bit, successive approximation, analog-to-digital converter (ADC) that operates from a single power supply, VDD. It contains a low power...
Datasheet
AD7690 on Analog.com
AD7689
Production
The AD7682/AD7689 are 4-channel/8-channel, 16-bit, charge redistribution successive approximation register (SAR) analog-to-digital converters (ADCs) that...
Datasheet
AD7689 on Analog.com
AD7688
Production
The AD7688 is a 16-bit, 500 kSPS, charge redistribution successive-approximation Analog-to-Digital Converter which operates from a single 5V power supply...
Datasheet
AD7688 on Analog.com
AD7687
Production
The AD76871 is a 16-bit, charge redistribution, successive approximation, analog-to-digital converter (ADC) that operates from a single power supply, VDD...
Datasheet
AD7687 on Analog.com
AD7686
Production
The AD7686 is a 16-bit, charge redistribution, successive approximation, analog-to-digital converter (ADC) that operates from a single 5 V power supply...
Datasheet
AD7686 on Analog.com
AD7685
Production
The AD7685 is a 16-bit, charge redistribution successive approximation, analog-to-digital converter (ADC) that operates from a single power supply, VDD...
Datasheet
AD7685 on Analog.com
AD7682
Production
The AD7682/AD7689 are 4-channel/8-channel, 16-bit, charge
redistribution successive approximation register (SAR) analog-to-digital
converters (ADCs) that...
Datasheet
AD7682 on Analog.com
AD7124-4
Recommended for New Designs
The AD7124-4 is a low power, low noise, completely integrated analog front end for high precision measurement applications. The device contains a low noise...
Datasheet
AD7124-4 on Analog.com
AD7124-8
Recommended for New Designs
The AD7124-8 is a low power, low noise, completely integrated
analog front end for high precision measurement applications. The
AD7124-8 W grade is AEC...
Datasheet
AD7124-8 on Analog.com
AD7192
Production
The AD7192 is a low noise, complete analog front end for high precision measurement applications. It contains a low noise, 24-bit sigma-delta (Σ-Δ) analog...
Datasheet
AD7192 on Analog.com
AD7190
Production
The AD7190 is a low noise, complete analog front end for high precision measurement applications. It contains a low noise, 24-bit sigma-delta (Σ-Δ) analog...
Datasheet
AD7190 on Analog.com
AD7193
Production
The AD7193 is a low noise, complete analog front end for high precision measurement applications. It contains a low noise, 24-bit sigma-delta (Σ-Δ) analog...
Datasheet
AD7193 on Analog.com
AD7195
Recommended for New Designs
The AD7195 is a low noise, complete analog front end for high precision measurement applications. It contains a low noise, 24-bit sigma-delta (Σ-Δ) analog...
Datasheet
AD7195 on Analog.com
AD9467
Recommended for New Designs
The AD9467 is a 16-bit, monolithic, IF sampling analog-to-digital converter (ADC). It is optimized for high performance over wide bandwidths and ease of...
Datasheet
AD9467 on Analog.com
AD9643
Recommended for New Designs
The AD9643 is a dual, 14-bit analog-to-digital converter (ADC) with sampling speeds of up to 250 MSPS. The AD9643 is designed to support communications...
Datasheet
AD9643 on Analog.com
AD9250
Recommended for New Designs
The AD9250 is a dual, 14-bit ADC with sampling speeds of up to 250 MSPS. The AD9250 is designed to support communications applications where low cost,...
Datasheet
AD9250 on Analog.com
AD9265
Production
The AD9265 is a 16-bit, 125 MSPS analog-to-digital converter (ADC). The AD9265 is designed to support communications applications where high performance...
Datasheet
AD9265 on Analog.com
AD9683
Recommended for New Designs
The AD9683 is a 14-bit ADC with sampling speeds of up to
250 MSPS. The AD9683 supports communications applications
where low cost, small size, wide bandwidth...
Datasheet
AD9683 on Analog.com
AD9434
Recommended for New Designs
The AD9434 is a 12-bit monolithic sampling analog-to-digital converter (ADC) optimized for high performance, low power, and ease of use. The part operates...
Datasheet
AD9434 on Analog.com
AD9625
Recommended for New Designs
The AD9625 is a 12-bit monolithic sampling analog-to-digital converter (ADC) that operates at conversion rates of up to 2.6 giga samples per second (GSPS...
Datasheet
AD9625 on Analog.com
ad9652
Recommended for New Designs
The AD9652 is a dual, 16-bit analog-to-digital converter (ADC) with sampling speeds of up to 310 MSPS. It is designed to support demanding, high speed...
Datasheet
ad9652 on Analog.com
AD9649
Production
The AD9649 is a monolithic, single channel 1.8 V supply, 14-bit, 20/40/65/80 MSPS analog-to-digital converter (ADC). It features a high performance sample...
Datasheet
AD9649 on Analog.com
ADAR3000
Recommended for New Designs
ADAR3000 on Analog.com
ADAR3001
Recommended for New Designs
ADAR3001 on Analog.com
ADAR3002
Recommended for New Designs
The ADAR3002 is a 17.7 GHz to 21.2 GHz receive, 2-beam and
4-dual polarized elements, beamforming chip for polarized phased
arrays. Each of the 16 RF paths...
Datasheet
ADAR3002 on Analog.com
AD9783
Production
The AD9780 / AD9781 / AD9783 include pin-compatible, high dynamic range, dual digital-to-analog converters (DACs) with 12-/14-/16-bit resolutions, and...
Datasheet
AD9783 on Analog.com
AD9780
Production
The AD9780 / AD9781 / AD9783 include pin-compatible, high dynamic range, dual digital-to-analog converters (DACs) with 12-/14-/16-bit resolutions, and...
Datasheet
AD9780 on Analog.com
AD9781
Production
The AD9780Â / AD9781 / AD9783Â include pin-compatible, high dynamic range, dual digital-to-analog converters (DACs) with 12-/14-/16-bit resolutions, and...
Datasheet
AD9781 on Analog.com
ADIS16475
Recommended for New Designs
The ADIS16475 is a precision, miniature MEMS inertial measurement unit (IMU) that includes a triaxial gyroscope and a triaxial accelerometer. Each inertial...
Datasheet
ADIS16475 on Analog.com
ADIS16470
Recommended for New Designs
The ADIS16470 is a miniature MEMS inertial measurement unit (IMU) that includes a triaxial gyroscope and a triaxial accelerometer. Each inertial sensor...
Datasheet
ADIS16470 on Analog.com
ADIS16500
Recommended for New Designs
The ADIS16500 is a precision, miniature microelectromechanical system (MEMS) inertial measurement unit (IMU) that includes a triaxial gyroscope and a triaxial...
Datasheet
ADIS16500 on Analog.com
ADIS16505-1
Recommended for New Designs
ADIS16505-1 on Analog.com
ADIS16505-2
Recommended for New Designs
ADIS16505-2 on Analog.com
ADIS16505-3
Recommended for New Designs
ADIS16505-3 on Analog.com
AD9208
Recommended for New Designs
The AD9208 is a dual, 14-bit, 3 GSPS analog-to-digital converter (ADC). The device has an on-chip buffer and a sample-and-
hold circuit designed for low...
Datasheet
AD9208 on Analog.com
AD9695
Recommended for New Designs
The AD9695 is a dual, 14-bit, 1300 MSPS/625 MSPS analog-to-digital converter (ADC). The device has an on-chip buffer and a sample-and-hold circuit designed...
Datasheet
AD9695 on Analog.com
AD9689
Recommended for New Designs
The AD9689 is a dual, 14-bit, 2.0 GSPS/2.6 GSPS analog-to-digital converter (ADC). The device has an on-chip buffer and a sample-and-hold circuit designed...
Datasheet
AD9689 on Analog.com
Im using the GT wizard instructions here https://wiki.analog.com/resources/fpga/docs/xgt_wizard to modify the the trancievers of the ad9695_fmc project to use with the -625 speed grade board. the parsing script spits generates the GTHE4_cfng.txt as the instructions say. this is were the instructions leave off. the tcl lines 71 through 100 https://github.com/analogdevicesinc/hdl/blob/main/projects/ad9695_fmc/common/ad9695_fmc_bd.tcl need to be modified according to the text file. the two do not exactly match up. can I simply replace the parameters in the tcl script with the one from the txt file and match the syntax? I have tried to overwite values from the txt to the tcl and rebuild the project. this does not seem to work. here is my boot, generated text file as well as my modified tcl script as well as my device tree
Zynq MP First Stage Boot Loader
Release 2023.2 Oct 12 2023 - 15:51:06
NOTICE: BL31: Non secure code at 0x8000000
NOTICE: BL31: v2.8(release):xlnx_rebase_v2.8_2023.2_ksb_aug
NOTICE: BL31: Built : 12:21:43, Aug 31 2023
U-Boot 2023.01 (Sep 21 2023 - 11:02:37 +0000)
CPU: ZynqMP
Silicon: v3
Chip: zu9eg
Model: ZynqMP ZCU102 Rev1.0
Board: Xilinx ZynqMP
DRAM: 2 GiB (effective 4 GiB)
PMUFW: v1.1
PMUFW: No permission to change config object
Xilinx I2C Legacy format at nvmem0:
Board name: zcu102
Board rev: 1.0
Board SN: 1030078312236-7370
Ethernet mac: 00:0a:35:07:bc:f6
EL Level: EL2
Secure Boot: not authenticated, not encrypted
Core: 80 devices, 30 uclasses, devicetree: board
NAND: 0 MiB
MMC: mmc@ff170000: 0
Loading Environment from FAT... *** Error - No Valid Environment Area found
*** Warning - bad env area, using default environment
In: serial
Out: serial
Err: serial
Bootmode: LVL_SHFT_SD_MODE1
Reset reason: EXTERNAL
Net:
ZYNQ GEM: ff0e0000, mdio bus ff0e0000, phyaddr 12, interface rgmii-id
eth0: ethernet@ff0e0000
scanning bus for devices...
SATA link 0 timeout.
SATA link 1 timeout.
AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst
starting USB...
Bus usb@fe200000: Register 2000440 NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus usb@fe200000 for devices... 1 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found
Hit any key to stop autoboot: 0
ZynqMP> mmc rescan
ZynqMP> mmc part
Partition Map for MMC device 0 -- Partition Type: DOS
Part Start Sector Num Sectors UUID Type
1 24576 4194304 e66bf917-01 0c
2 4218880 120516608 e66bf917-02 83
3 8192 16384 e66bf917-03 a2
ZynqMP> fatload mmc 0:1 0x100000 BOOT.BIN
11130128 bytes read in 768 ms (13.8 MiB/s)
ZynqMP> fatload mmc 0:1 0x2A00000 system.dtb
Unknown command 'fatload' - try 'help'
ZynqMP> fatload mmc 0:1 0x3000000 Image
34955776 bytes read in 2360 ms (14.1 MiB/s)
ZynqMP> setenv bootargs 'console=ttyPS0,115200 root=/dev/mmcblk0p2 rw ea'
ZynqMP> fatload mmc 0:1 0x100000 BOOT.BIN
11130128 bytes read in 768 ms (13.8 MiB/s)
ZynqMP> fatload mmc 0:1 0x2A00000 system.dtb
59167 bytes read in 31 ms (1.8 MiB/s)
ZynqMP> setenv bootargs 'console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait clk_ignore_unused cpuidle.off=1'
ZynqMP> booti 0x3000000 - 0x2A00000
## Flattened Device Tree blob at 02a00000
Booting using the fdt blob at 0x2a00000
Working FDT set to 2a00000
Host not halted after 16000 microseconds.
Loading Device Tree to 000000007bde0000, end 000000007bdf171e ... OK
Working FDT set to 7bde0000
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.15.36-182044-g85078536473b (jenkins@romlxbuild1) (aarch64-xilinx-linux-gcc.real (GCC) 11.2.0, GNU ld (GNU Binutils) 2.37.20210721) #1140 SMP Wed Apr 3 07:20:38 EEST 2024
[ 0.000000] Machine model: ZynqMP ZCU102 Rev1.0
[ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
[ 0.000000] printk: bootconsole [cdns0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000000000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x000000087fffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000000000000-0x000000007fffffff]
[ 0.000000] node 0: [mem 0x0000000800000000-0x000000087fffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000000000000-0x000000087fffffff]
[ 0.000000] cma: Reserved 256 MiB at 0x000000006bc00000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 18 pages/cpu s34008 r8192 d31528 u73728
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1034240
[ 0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait clk_ignore_unused cpuidle.off=1
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: mapped [mem 0x000000007c000000-0x0000000080000000] (64MB)
[ 0.000000] Memory: 3758736K/4194304K available (16704K kernel code, 1688K rwdata, 13024K rodata, 2624K init, 639K bss, 173424K reserved, 262144K cma-reserved)
[ 0.000000] rcu: Hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] random: get_random_bytes called from start_kernel+0x470/0x6fc with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 100.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171024e7e0, max_idle_ns: 440795205315 ns
[ 0.000000] sched_clock: 56 bits at 100MHz, resolution 10ns, wraps every 4398046511100ns
[ 0.008489] Console: colour dummy device 80x25
[ 0.012557] Calibrating delay loop (skipped), value calculated using timer frequency.. 200.00 BogoMIPS (lpj=400000)
[ 0.022971] pid_max: default: 32768 minimum: 301
[ 0.027723] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.034987] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.043720] rcu: Hierarchical SRCU implementation.
[ 0.047826] EFI services will not be available.
[ 0.052241] smp: Bringing up secondary CPUs ...
[ 0.056999] Detected VIPT I-cache on CPU1
[ 0.057038] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.057411] Detected VIPT I-cache on CPU2
[ 0.057436] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.057789] Detected VIPT I-cache on CPU3
[ 0.057812] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.057855] smp: Brought up 1 node, 4 CPUs
[ 0.092308] SMP: Total of 4 processors activated.
[ 0.097007] CPU features: detected: 32-bit EL0 Support
[ 0.102141] CPU features: detected: CRC32 instructions
[ 0.107313] CPU: All CPU(s) started at EL2
[ 0.111375] alternatives: patching kernel code
[ 0.116721] devtmpfs: initialized
[ 0.124743] Registered cp15_barrier emulation handler
[ 0.124794] Registered setend emulation handler
[ 0.128781] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.138432] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.151322] pinctrl core: initialized pinctrl subsystem
[ 0.152092] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.157898] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[ 0.163976] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.171763] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.179580] audit: initializing netlink subsys (disabled)
[ 0.185011] audit: type=2000 audit(0.116:1): state=initialized audit_enabled=0 res=1
[ 0.185360] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.199522] ASID allocator initialised with 65536 entries
[ 0.224738] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.225819] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.232516] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.239210] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 1.329980] DRBG: Continuing without Jitter RNG
[ 1.430721] raid6: neonx8 gen() 2139 MB/s
[ 1.498773] raid6: neonx8 xor() 1586 MB/s
[ 1.566840] raid6: neonx4 gen() 2177 MB/s
[ 1.634890] raid6: neonx4 xor() 1555 MB/s
[ 1.702955] raid6: neonx2 gen() 2065 MB/s
[ 1.771010] raid6: neonx2 xor() 1423 MB/s
[ 1.839079] raid6: neonx1 gen() 1764 MB/s
[ 1.907132] raid6: neonx1 xor() 1208 MB/s
[ 1.975199] raid6: int64x8 gen() 1366 MB/s
[ 2.043252] raid6: int64x8 xor() 773 MB/s
[ 2.111309] raid6: int64x4 gen() 1597 MB/s
[ 2.179369] raid6: int64x4 xor() 846 MB/s
[ 2.247448] raid6: int64x2 gen() 1397 MB/s
[ 2.315488] raid6: int64x2 xor() 747 MB/s
[ 2.383572] raid6: int64x1 gen() 1032 MB/s
[ 2.451609] raid6: int64x1 xor() 517 MB/s
[ 2.451648] raid6: using algorithm neonx4 gen() 2177 MB/s
[ 2.455629] raid6: .... xor() 1555 MB/s, rmw enabled
[ 2.460589] raid6: using neon recovery algorithm
[ 2.465625] iommu: Default domain type: Translated
[ 2.470074] iommu: DMA domain TLB invalidation policy: strict mode
[ 2.476539] SCSI subsystem initialized
[ 2.480224] usbcore: registered new interface driver usbfs
[ 2.485588] usbcore: registered new interface driver hub
[ 2.490885] usbcore: registered new device driver usb
[ 2.496042] mc: Linux media interface: v0.10
[ 2.500191] videodev: Linux video capture interface: v2.00
[ 2.505708] pps_core: LinuxPPS API ver. 1 registered
[ 2.510614] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 2.519759] PTP clock support registered
[ 2.523683] EDAC MC: Ver: 3.0.0
[ 2.527079] zynqmp-ipi-mbox mailbox@ff9905c0: Registered ZynqMP IPI mbox with TX/RX channels.
[ 2.535699] jesd204: found 0 devices and 0 topologies
[ 2.540399] FPGA manager framework
[ 2.543890] Advanced Linux Sound Architecture Driver Initialized.
[ 2.550260] Bluetooth: Core ver 2.22
[ 2.553428] NET: Registered PF_BLUETOOTH protocol family
[ 2.558726] Bluetooth: HCI device and connection manager initialized
[ 2.565079] Bluetooth: HCI socket layer initialized
[ 2.569949] Bluetooth: L2CAP socket layer initialized
[ 2.575001] Bluetooth: SCO socket layer initialized
[ 2.580270] clocksource: Switched to clocksource arch_sys_counter
[ 2.586077] VFS: Disk quotas dquot_6.6.0
[ 2.589910] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 2.601130] NET: Registered PF_INET protocol family
[ 2.601732] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 2.610559] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[ 2.617577] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 2.625654] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
[ 2.633159] TCP: Hash tables configured (established 32768 bind 32768)
[ 2.639359] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 2.646056] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 2.653255] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 2.659088] RPC: Registered named UNIX socket transport module.
[ 2.664699] RPC: Registered udp transport module.
[ 2.669392] RPC: Registered tcp transport module.
[ 2.674087] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 2.681117] PCI: CLS 0 bytes, default 64
[ 2.684947] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 2.693053] Initialise system trusted keyrings
[ 2.696698] workingset: timestamp_bits=62 max_order=20 bucket_order=0
[ 2.703640] NFS: Registering the id_resolver key type
[ 2.708117] Key type id_resolver registered
[ 2.712281] Key type id_legacy registered
[ 2.716296] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 2.722982] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 2.730388] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 2.737591] fuse: init (API version 7.34)
[ 2.776886] NET: Registered PF_ALG protocol family
[ 2.776937] xor: measuring software checksum speed
[ 2.784987] 8regs : 2363 MB/sec
[ 2.788680] 32regs : 2799 MB/sec
[ 2.793780] arm64_neon : 2307 MB/sec
[ 2.793864] xor: using function: 32regs (2799 MB/sec)
[ 2.798916] Key type asymmetric registered
[ 2.803003] Asymmetric key parser 'x509' registered
[ 2.807906] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[ 2.815272] io scheduler mq-deadline registered
[ 2.819794] io scheduler kyber registered
[ 2.849889] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[ 2.857148] brd: module loaded
[ 2.860531] loop: module loaded
[ 2.860875] Registered mathworks_ip class
[ 2.865164] tun: Universal TUN/TAP device driver, 1.6
[ 2.867145] CAN device driver interface
[ 2.871672] SPI driver wl1271_spi has no spi_device_id for ti,wl1271
[ 2.877252] SPI driver wl1271_spi has no spi_device_id for ti,wl1273
[ 2.883601] SPI driver wl1271_spi has no spi_device_id for ti,wl1281
[ 2.889951] SPI driver wl1271_spi has no spi_device_id for ti,wl1283
[ 2.896302] SPI driver wl1271_spi has no spi_device_id for ti,wl1285
[ 2.902653] SPI driver wl1271_spi has no spi_device_id for ti,wl1801
[ 2.909003] SPI driver wl1271_spi has no spi_device_id for ti,wl1805
[ 2.915355] SPI driver wl1271_spi has no spi_device_id for ti,wl1807
[ 2.921706] SPI driver wl1271_spi has no spi_device_id for ti,wl1831
[ 2.928056] SPI driver wl1271_spi has no spi_device_id for ti,wl1835
[ 2.934407] SPI driver wl1271_spi has no spi_device_id for ti,wl1837
[ 2.940855] usbcore: registered new interface driver asix
[ 2.946195] usbcore: registered new interface driver ax88179_178a
[ 2.952272] usbcore: registered new interface driver cdc_ether
[ 2.958090] usbcore: registered new interface driver net1080
[ 2.963747] usbcore: registered new interface driver cdc_subset
[ 2.969665] usbcore: registered new interface driver zaurus
[ 2.975240] usbcore: registered new interface driver cdc_ncm
[ 2.981515] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.987395] ehci-pci: EHCI PCI platform driver
[ 2.992225] usbcore: registered new interface driver uas
[ 2.997170] usbcore: registered new interface driver usb-storage
[ 3.003187] usbcore: registered new interface driver usbserial_generic
[ 3.009677] usbserial: USB Serial support registered for generic
[ 3.015684] usbcore: registered new interface driver ftdi_sio
[ 3.021422] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 3.028735] usbcore: registered new interface driver upd78f0730
[ 3.034646] usbserial: USB Serial support registered for upd78f0730
[ 3.041876] SPI driver ads7846 has no spi_device_id for ti,tsc2046
[ 3.047076] SPI driver ads7846 has no spi_device_id for ti,ads7843
[ 3.053252] SPI driver ads7846 has no spi_device_id for ti,ads7845
[ 3.059428] SPI driver ads7846 has no spi_device_id for ti,ads7873
[ 3.066097] rtc_zynqmp ffa60000.rtc: registered as rtc0
[ 3.070836] rtc_zynqmp ffa60000.rtc: setting system clock to 2024-07-30T20:31:29 UTC (1722371489)
[ 3.079760] i2c_dev: i2c /dev entries driver
[ 3.085775] usbcore: registered new interface driver uvcvideo
[ 3.091148] Bluetooth: HCI UART driver ver 2.3
[ 3.094147] Bluetooth: HCI UART protocol H4 registered
[ 3.099275] Bluetooth: HCI UART protocol BCSP registered
[ 3.104594] Bluetooth: HCI UART protocol LL registered
[ 3.109713] Bluetooth: HCI UART protocol ATH3K registered
[ 3.115123] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 3.121408] Bluetooth: HCI UART protocol Intel registered
[ 3.126777] Bluetooth: HCI UART protocol QCA registered
[ 3.132011] usbcore: registered new interface driver bcm203x
[ 3.137663] usbcore: registered new interface driver bpa10x
[ 3.143229] usbcore: registered new interface driver bfusb
[ 3.148713] usbcore: registered new interface driver btusb
[ 3.154205] usbcore: registered new interface driver ath3k
[ 3.159722] EDAC MC: ECC not enabled
[ 3.163372] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
[ 3.175771] sdhci: Secure Digital Host Controller Interface driver
[ 3.181576] sdhci: Copyright(c) Pierre Ossman
[ 3.185926] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.191999] ledtrig-cpu: registered to indicate activity on CPUs
[ 3.197736] SMCCC: SOC_ID: ID = jep106:0049:0000 Revision = 0x24738093
[ 3.204176] zynqmp_firmware_probe Platform Management API v1.1
[ 3.209941] zynqmp_firmware_probe Trustzone version v1.0
[ 3.245042] usbcore: registered new interface driver usbhid
[ 3.245100] usbhid: USB HID core driver
[ 3.248994] SPI driver fb_seps525 has no spi_device_id for syncoam,seps525
[ 3.256348] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7988-5
[ 3.262906] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7988-1
[ 3.270125] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7984
[ 3.277172] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7983
[ 3.284219] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7982
[ 3.291266] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7980
[ 3.298313] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7949
[ 3.305360] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7946
[ 3.312407] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7942
[ 3.319454] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7699
[ 3.326501] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7693
[ 3.333548] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7691
[ 3.340595] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7690
[ 3.347642] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7689
[ 3.354689] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7688
[ 3.361739] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7687
[ 3.368784] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7686
[ 3.375830] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7685
[ 3.382877] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7682
[ 3.390038] SPI driver ad7124 has no spi_device_id for adi,ad7124-4
[ 3.396189] SPI driver ad7124 has no spi_device_id for adi,ad7124-8
[ 3.402466] SPI driver ad7192 has no spi_device_id for adi,ad7190
[ 3.408542] SPI driver ad7192 has no spi_device_id for adi,ad7193
[ 3.414631] SPI driver ad7192 has no spi_device_id for adi,ad7195
[ 3.421521] SPI driver ad9467 has no spi_device_id for adi,ad9643
[ 3.426814] SPI driver ad9467 has no spi_device_id for adi,ad9250
[ 3.432902] SPI driver ad9467 has no spi_device_id for adi,ad9250_2
[ 3.439165] SPI driver ad9467 has no spi_device_id for adi,ad9265
[ 3.445255] SPI driver ad9467 has no spi_device_id for adi,ad9683
[ 3.451345] SPI driver ad9467 has no spi_device_id for adi,ad9434
[ 3.457435] SPI driver ad9467 has no spi_device_id for adi,ad9625
[ 3.463525] SPI driver ad9467 has no spi_device_id for adi,ad9652
[ 3.469615] SPI driver ad9467 has no spi_device_id for adi,ad9649
[ 3.476669] ams ffa50000.ams: invalid resource
[ 3.480137] ams: probe of ffa50000.ams failed with error -22
[ 3.486081] SPI driver adar3000 has no spi_device_id for adi,adar3001
[ 3.492238] SPI driver adar3000 has no spi_device_id for adi,adar3002
[ 3.499870] SPI driver ad9783 has no spi_device_id for adi,ad9780
[ 3.504766] SPI driver ad9783 has no spi_device_id for adi,ad9781
[ 3.511035] SPI driver adis16475 has no spi_device_id for adi,adis16470
[ 3.517467] SPI driver adis16475 has no spi_device_id for adi,adis16475-1
[ 3.524252] SPI driver adis16475 has no spi_device_id for adi,adis16475-2
[ 3.531038] SPI driver adis16475 has no spi_device_id for adi,adis16475-3
[ 3.537823] SPI driver adis16475 has no spi_device_id for adi,adis16477-1
[ 3.544610] SPI driver adis16475 has no spi_device_id for adi,adis16477-2
[ 3.551395] SPI driver adis16475 has no spi_device_id for adi,adis16477-3
[ 3.558181] SPI driver adis16475 has no spi_device_id for adi,adis16465-1
[ 3.564967] SPI driver adis16475 has no spi_device_id for adi,adis16465-2
[ 3.571755] SPI driver adis16475 has no spi_device_id for adi,adis16465-3
[ 3.578539] SPI driver adis16475 has no spi_device_id for adi,adis16467-1
[ 3.585325] SPI driver adis16475 has no spi_device_id for adi,adis16467-2
[ 3.592111] SPI driver adis16475 has no spi_device_id for adi,adis16467-3
[ 3.598897] SPI driver adis16475 has no spi_device_id for adi,adis16500
[ 3.605509] SPI driver adis16475 has no spi_device_id for adi,adis16505-1
[ 3.612299] SPI driver adis16475 has no spi_device_id for adi,adis16505-2
[ 3.619082] SPI driver adis16475 has no spi_device_id for adi,adis16505-3
[ 3.625867] SPI driver adis16475 has no spi_device_id for adi,adis16507-1
[ 3.632653] SPI driver adis16475 has no spi_device_id for adi,adis16507-2
[ 3.639439] SPI driver adis16475 has no spi_device_id for adi,adis16507-3
[ 3.647693] axi_adxcvr 84a60000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.05.a) using QPLL on GTH4 at 0x84A60000. Number of lanes: 4.
[ 3.658096] axi-jesd204-rx 84aa0000.axi-jesd204-rx: AXI-JESD204-RX (1.07.a) at 0x84AA0000. Encoder 8b10b, width 4/4, lanes 4.
[ 3.669632] axi_sysid 85000000.axi-sysid-0: AXI System ID core version (1.01.a) found
[ 3.676770] axi_sysid 85000000.axi-sysid-0: [ad9695_fmc] [RX:L=4 M=2 S=1] on [zcu102] git branch <main> git <ae9605bd224fee266b226413ba3a0e0076ed3c68> dirty [2024-07-30 19:21:01] UTC
[ 3.693438] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
[ 3.699757] usbcore: registered new interface driver snd-usb-audio
[ 3.707257] pktgen: Packet Generator for packet performance testing. Version: 2.75
[ 3.713444] Initializing XFRM netlink socket
[ 3.717384] NET: Registered PF_INET6 protocol family
[ 3.722715] Segment Routing with IPv6
[ 3.725936] In-situ OAM (IOAM) with IPv6
[ 3.729879] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 3.736081] NET: Registered PF_PACKET protocol family
[ 3.740810] NET: Registered PF_KEY protocol family
[ 3.745653] can: controller area network core
[ 3.749958] NET: Registered PF_CAN protocol family
[ 3.754717] can: raw protocol
[ 3.757674] can: broadcast manager protocol
[ 3.761856] can: netlink gateway - max_hops=1
[ 3.766271] Bluetooth: RFCOMM TTY layer initialized
[ 3.771079] Bluetooth: RFCOMM socket layer initialized
[ 3.776218] Bluetooth: RFCOMM ver 1.11
[ 3.779950] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 3.785252] Bluetooth: BNEP filters: protocol multicast
[ 3.790474] Bluetooth: BNEP socket layer initialized
[ 3.795431] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 3.801349] Bluetooth: HIDP socket layer initialized
[ 3.806428] 9pnet: Installing 9P2000 support
[ 3.810581] NET: Registered PF_IEEE802154 protocol family
[ 3.815980] Key type dns_resolver registered
[ 3.820447] registered taskstats version 1
[ 3.824318] Loading compiled-in X.509 certificates
[ 3.829590] Btrfs loaded, crc32c=crc32c-generic, zoned=no, fsverity=no
[ 3.844574] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 48, base_baud = 6249999) is a xuartps
[ 3.853657] printk: console [ttyPS0] enabled
[ 3.853657] printk: console [ttyPS0] enabled
[ 3.857963] printk: bootconsole [cdns0] disabled
[ 3.857963] printk: bootconsole [cdns0] disabled
[ 3.867515] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 49, base_baud = 6249999) is a xuartps
[ 3.880694] of-fpga-region fpga-full: FPGA Region probed
[ 3.887255] nwl-pcie fd0e0000.pcie: host bridge /axi/pcie@fd0e0000 ranges:
[ 3.894154] nwl-pcie fd0e0000.pcie: MEM 0x00e0000000..0x00efffffff -> 0x00e0000000
[ 3.902158] nwl-pcie fd0e0000.pcie: MEM 0x0600000000..0x07ffffffff -> 0x0600000000
[ 3.910233] nwl-pcie fd0e0000.pcie: Link is DOWN
[ 3.914999] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00
[ 3.921180] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 3.926669] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff]
[ 3.933538] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref]
[ 3.941047] pci 0000:00:00.0: [10ee:d021] type 01 class 0x060400
[ 3.947110] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot
[ 3.957305] pci 0000:00:00.0: PCI bridge to [bus 01-0c]
[ 3.963051] xilinx-zynqmp-dma fd500000.dma-controller: ZynqMP DMA driver Probe success
[ 3.971143] xilinx-zynqmp-dma fd510000.dma-controller: ZynqMP DMA driver Probe success
[ 3.979217] xilinx-zynqmp-dma fd520000.dma-controller: ZynqMP DMA driver Probe success
[ 3.987314] xilinx-zynqmp-dma fd530000.dma-controller: ZynqMP DMA driver Probe success
[ 3.995392] xilinx-zynqmp-dma fd540000.dma-controller: ZynqMP DMA driver Probe success
[ 4.003480] xilinx-zynqmp-dma fd550000.dma-controller: ZynqMP DMA driver Probe success
[ 4.011550] xilinx-zynqmp-dma fd560000.dma-controller: ZynqMP DMA driver Probe success
[ 4.019633] xilinx-zynqmp-dma fd570000.dma-controller: ZynqMP DMA driver Probe success
[ 4.027932] xilinx-zynqmp-dpdma fd4c0000.dma-controller: Xilinx DPDMA engine is probed
[ 4.042613] ad9208 spi1.0: Failed to set input clk config (-22)
[ 4.048533] ad9208 spi1.0: Failed to initialize: -22
[ 4.053494] ad9208: probe of spi1.0 failed with error -22
[ 4.059659] spi-nor spi0.0: SPI-NOR-UniqueID 5c9e0b000b07001a00b9cb68e9f7
[ 4.066452] spi-nor spi0.0: found mt25qu512a, expected m25p80
[ 4.072645] spi-nor spi0.0: mt25qu512a (131072 Kbytes)
[ 4.077806] 4 fixed-partitions partitions found on MTD device spi0.0
[ 4.084152] Creating 4 MTD partitions on "spi0.0":
[ 4.088934] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
[ 4.095507] 0x000000100000-0x000000600000 : "qspi-linux"
[ 4.101506] 0x000000600000-0x000000620000 : "qspi-device-tree"
[ 4.108023] 0x000000620000-0x000000c00000 : "qspi-rootfs"
[ 4.115007] xilinx_can ff070000.can can0: TDC Offset value not in range
[ 4.123244] macb ff0e0000.ethernet: Not enabling partial store and forward
[ 4.153224] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
[ 4.159750] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM
[ 4.166231] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM
[ 4.172705] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM
[ 4.180095] pca953x 0-0020: supply vcc not found, using dummy regulator
[ 4.186790] pca953x 0-0020: using no AI
[ 4.191274] gpio-318 (sel0): hogged as output/low
[ 4.196178] gpio-319 (sel1): hogged as output/high
[ 4.201176] gpio-320 (sel2): hogged as output/high
[ 4.206163] gpio-321 (sel3): hogged as output/high
[ 4.211330] pca953x 0-0021: supply vcc not found, using dummy regulator
[ 4.218001] pca953x 0-0021: using no AI
[ 4.223463] ina2xx 2-0040: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.230451] ina2xx 2-0041: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.237446] ina2xx 2-0042: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.244438] ina2xx 2-0043: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.251437] ina2xx 2-0044: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.258431] ina2xx 2-0045: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.265429] ina2xx 2-0046: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.272424] ina2xx 2-0047: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.279428] ina2xx 2-004a: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.286420] ina2xx 2-004b: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.292827] i2c i2c-0: Added multiplexed i2c bus 2
[ 4.298373] ina2xx 3-0040: power monitor ina226 (Rshunt = 2000 uOhm)
[ 4.305367] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.312358] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.319350] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.326341] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.333331] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.340332] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.347324] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.353730] i2c i2c-0: Added multiplexed i2c bus 3
[ 4.368763] random: fast init done
[ 4.412514] i2c i2c-0: Added multiplexed i2c bus 4
[ 4.417468] i2c i2c-0: Added multiplexed i2c bus 5
[ 4.422261] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544
[ 4.429633] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 32
[ 4.437062] at24 6-0054: supply vcc not found, using dummy regulator
[ 4.443946] at24 6-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write
[ 4.450704] i2c i2c-1: Added multiplexed i2c bus 6
[ 4.456063] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[ 4.463369] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[ 4.470674] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[ 4.477973] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[ 4.485273] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[ 4.492574] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[ 4.499873] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[ 4.507172] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[ 4.515584] si5341 7-0036: Chip: 5341 Grade: 1 Rev: 3
[ 4.554103] i2c i2c-1: Added multiplexed i2c bus 7
[ 4.561749] si570 8-005d: registered, current frequency 300000000 Hz
[ 4.568154] i2c i2c-1: Added multiplexed i2c bus 8
[ 4.587922] si570 9-005d: registered, current frequency 148500000 Hz
[ 4.594324] i2c i2c-1: Added multiplexed i2c bus 9
[ 4.599346] si5324 10-0069: si5328 probed
[ 4.664582] si5324 10-0069: si5328 probe successful
[ 4.669510] i2c i2c-1: Added multiplexed i2c bus 10
[ 4.674558] i2c i2c-1: Added multiplexed i2c bus 11
[ 4.679586] i2c i2c-1: Added multiplexed i2c bus 12
[ 4.684625] i2c i2c-1: Added multiplexed i2c bus 13
[ 4.689501] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548
[ 4.697574] at24 14-0050: supply vcc not found, using dummy regulator
[ 4.730439] i2c i2c-1: Added multiplexed i2c bus 14
[ 4.735503] i2c i2c-1: Added multiplexed i2c bus 15
[ 4.740570] i2c i2c-1: Added multiplexed i2c bus 16
[ 4.745609] i2c i2c-1: Added multiplexed i2c bus 17
[ 4.750659] i2c i2c-1: Added multiplexed i2c bus 18
[ 4.755700] i2c i2c-1: Added multiplexed i2c bus 19
[ 4.760746] i2c i2c-1: Added multiplexed i2c bus 20
[ 4.765795] i2c i2c-1: Added multiplexed i2c bus 21
[ 4.770677] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548
[ 4.778295] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 33
[ 4.787697] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer with timeout 60s
[ 4.799629] zynqmp-display fd4a0000.display: vtc bridge property not present
[ 4.807788] zynqmp_clk_divider_set_rate() set divider failed for spi1_ref_div1, ret = -13
[ 4.817582] xilinx-dp-snd-codec fd4a0000.display:zynqmp-dp-snd-codec0: Failed to get required clock freq
[ 4.827074] xilinx-dp-snd-codec: probe of fd4a0000.display:zynqmp-dp-snd-codec0 failed with error -22
[ 4.828281] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit
[ 4.836565] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed
[ 4.852011] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed
[ 4.860224] OF: graph: no port node found in /axi/display@fd4a0000
[ 4.866722] xlnx-drm xlnx-drm.0: bound fd4a0000.display (ops 0xffffffc009123620)
[ 4.881411] mmc0: new high speed SDXC card at address aaaa
[ 4.887240] mmcblk0: mmc0:aaaa SC64G 59.5 GiB
[ 4.894017] mmcblk0: p1 p2 p3
[ 5.952315] zynqmp-display fd4a0000.display: [drm] Cannot find any crtc or sizes
[ 5.959952] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.display on minor 0
[ 5.967458] zynqmp-display fd4a0000.display: ZynqMP DisplayPort Subsystem driver probed
[ 5.975725] ahci-ceva fd0c0000.ahci: supply ahci not found, using dummy regulator
[ 5.983282] ahci-ceva fd0c0000.ahci: supply phy not found, using dummy regulator
[ 5.990747] ahci-ceva fd0c0000.ahci: supply target not found, using dummy regulator
[ 5.998586] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode
[ 6.007547] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
[ 6.018001] scsi host0: ahci-ceva
[ 6.021584] scsi host1: ahci-ceva
[ 6.025007] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 45
[ 6.032918] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 45
[ 6.042462] macb ff0e0000.ethernet: Not enabling partial store and forward
[ 6.051288] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 30 (00:0a:35:07:bc:f6)
[ 6.084169] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 6.089664] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
[ 6.097406] xhci-hcd xhci-hcd.1.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x0000000002010810
[ 6.106821] xhci-hcd xhci-hcd.1.auto: irq 56, io mem 0xfe200000
[ 6.112939] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.15
[ 6.121211] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 6.128433] usb usb1: Product: xHCI Host Controller
[ 6.133300] usb usb1: Manufacturer: Linux 5.15.36-182044-g85078536473b xhci-hcd
[ 6.140599] usb usb1: SerialNumber: xhci-hcd.1.auto
[ 6.145772] hub 1-0:1.0: USB hub found
[ 6.149537] hub 1-0:1.0: 1 port detected
[ 6.153650] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 6.159140] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
[ 6.166792] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[ 6.173425] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.15
[ 6.181688] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 6.188911] usb usb2: Product: xHCI Host Controller
[ 6.193784] usb usb2: Manufacturer: Linux 5.15.36-182044-g85078536473b xhci-hcd
[ 6.201083] usb usb2: SerialNumber: xhci-hcd.1.auto
[ 6.206226] hub 2-0:1.0: USB hub found
[ 6.209998] hub 2-0:1.0: 1 port detected
[ 6.223598] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[ 6.230663] of_cfs_init
[ 6.233134] of_cfs_init: OK
[ 6.236086] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 6.354521] ata2: SATA link down (SStatus 0 SControl 330)
[ 6.359954] ata1: SATA link down (SStatus 0 SControl 330)
[ 6.373490] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 6.380018] clk: Not disabling unused clocks
[ 6.384559] ALSA device list:
[ 6.387515] No soundcards found.
[ 6.391171] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 6.399785] cfg80211: failed to load regulatory.db
[ 6.667840] EXT4-fs (mmcblk0p2): recovery complete
[ 6.673579] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null). Quota mode: none.
[ 6.683358] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 6.696499] devtmpfs: mounted
[ 6.700234] Freeing unused kernel memory: 2624K
[ 6.704900] Run /sbin/init as init process
[ 7.040309] zynqmp-display fd4a0000.display: [drm] Cannot find any crtc or sizes
[ 7.232953] systemd[1]: systemd 247.3-7+rpi1+deb11u5 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +ZSTD +SECCOMP +BLKID +ELFUTILS +KMOD +IDN2 -IDN +PCRE2 default-hierarchy=unified)
[ 7.256887] systemd[1]: Detected architecture arm64.
Welcome to Raspbian GNU/Linux 11 (bullseye)!
[ 7.289191] systemd[1]: Set hostname to <analog>.
[ 8.558930] systemd[1]: /lib/systemd/system/plymouth-start.service:16: Unit configured to use KillMode=none. This is unsafe, as it disables systemd's process lifecycle management for the service. Please update your service to use a safer KillMode=, such as 'mixed' or 'control-group'. Support for KillMode=none is deprecated and will eventually be removed.
[ 8.762605] systemd[1]: Queued start job for default target Graphical Interface.
[ 8.771252] random: systemd: uninitialized urandom read (16 bytes read)
[ 8.778062] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 8.790411] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 8.799485] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 8.820414] random: systemd: uninitialized urandom read (16 bytes read)
[ 8.827419] systemd[1]: Created slice system-modprobe.slice.
[ OK ] Created slice system-modprobe.slice.
[ 8.848345] random: systemd: uninitialized urandom read (16 bytes read)
[ 8.855297] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 8.876673] systemd[1]: Created slice system-systemd\x2dfsck.slice.
[ OK ] Created slice system-systemd\x2dfsck.slice.
[ 8.900567] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 8.920635] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ 8.944635] systemd[1]: Condition check resulted in Arbitrary Executable File Formats File System Automount Point being skipped.
[ 8.957109] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 8.972489] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 8.989230] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 9.004711] systemd[1]: Listening on fsck to fsckd communication Socket.
[ OK ] Listening on fsck to fsckd communication Socket.
[ 9.028575] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 9.053029] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 9.072696] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 9.096783] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 9.112855] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 9.132698] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 9.154296] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 9.170158] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 9.193942] systemd[1]: Mounting RPC Pipe File System...
Mounting RPC Pipe File System...
[ 9.210223] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 9.228797] systemd[1]: Condition check resulted in Kernel Trace File System being skipped.
[ 9.237570] systemd[1]: Condition check resulted in Kernel Module supporting RPCSEC_GSS being skipped.
[ 9.250156] systemd[1]: Starting Restore / save the current clock...
Starting Restore / save the current clock...
[ 9.280865] systemd[1]: Starting Set the console keyboard layout...
Starting Set the console keyboard layout...
[ 9.305229] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped.
[ 9.318803] systemd[1]: Starting Load Kernel Module configfs...
Starting Load Kernel Module configfs...
[ 9.338603] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 9.358860] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 9.378980] systemd[1]: Condition check resulted in Set Up Additional Binary Formats being skipped.
[ 9.388310] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 9.399308] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 9.420222] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 9.438440] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 9.462457] systemd[1]: Starting Coldplug All udev Devices...
Starting Coldplug All udev Devices...
[ 9.485985] systemd[1]: Mounted Huge Pages File System.
[ OK ] Mounted Huge Pages File System.
[ 9.514382] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 9.548924] systemd[1]: Mounted RPC Pipe File System.
[ OK ] Mounted RPC Pipe File System.
[ 9.564950] systemd[1]: Mounted Kernel Debug File System.
[ OK ] Mounted Kernel Debug File System.
[ 9.589239] systemd[1]: Finished Restore / save the current clock.
[ OK ] Finished Restore / save the current clock.
[ 9.613418] systemd[1]: Finished Set the console keyboard layout.
[ OK ] Finished Set the console keyboard layout.
[ 9.636990] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
Mounting FUSE Control File System...
Mounting Kernel Configuration File System...
Starting Apply Kernel Variables...
[ OK ] Mounted FUSE Control File System[ 9.795984] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null). Quota mode: none.
.
[ OK ] Finished Remount Root and Kernel File Systems.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Finished Apply Kernel Variables.
Starting Flush Journal to Persistent Storage...
Starting Load/Save Random Seed...
Starting Create System Users...
[ OK ] Finished Create System Users.
Starting Create Static Device Nodes in /dev...
[ OK ] Finished Coldplug All udev Devices.
Starting Helper to synchronize boot up for ifupdown...
Starting Wait for udev To …plete Device Initialization...
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Finished Helper to synchronize boot up for ifupdown.
[ OK ] Reached target Local File Systems (Pre).
Starting Rule-based Manage…for Device Events and Files...
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Started Rule-based Manager for Device Events and Files.
Starting Show Plymouth Boot Screen...
[ OK ] Started Show Plymouth Boot Screen.
[ OK ] Started Forward Password R…s to Plymouth Directory Watch.
[ OK ] Reached target Local Encrypted Volumes.
[ OK ] Found device /dev/ttyPS0.
[ OK ] Finished Load/Save Random Seed.
[ OK ] Found device /dev/disk/by-partuuid/e66bf917-01.
[ OK ] Found device /dev/ttyS0.
[ OK ] Finished Wait for udev To Complete Device Initialization.
[ OK ] Listening on Load/Save RF …itch Status /dev/rfkill Watch.
Starting File System Check…isk/by-partuuid/e66bf917-01...
[ OK ] Started File System Check Daemon to report status.
[ OK ] Finished File System Check…/disk/by-partuuid/e66bf917-01.
Mounting /boot...
[ OK ] Mounted /boot.
[ OK ] Reached target Local File Systems.
Starting Set console font and keymap...
Starting Raise network interfaces...
Starting Preprocess NFS configuration...
Starting Tell Plymouth To Write Out Runtime Data...
Starting Create Volatile Files and Directories...
[ OK ] Finished Set console font and keymap.
[ OK ] Finished Preprocess NFS configuration.
[ OK ] Reached target NFS client services.
[ OK ] Reached target Remote File Systems (Pre).
[ OK ] Reached target Remote File Systems.
[ OK ] Finished Tell Plymouth To Write Out Runtime Data.
[ OK ] Finished Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Finished Update UTMP about System Boot/Shutdown.
Starting Load Kernel Modules...
[ OK ] Finished Raise network interfaces.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ OK ] Started CUPS Scheduler.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Paths.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Daily apt download activities.
[ OK ] Started Daily apt upgrade and clean activities.
[ OK ] Started Periodic ext4 Onli…ata Check for All Filesystems.
[ OK ] Started Discard unused blocks once a week.
[ OK ] Started Daily rotation of log files.
[ OK ] Started Daily man-db regeneration.
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on CUPS Scheduler.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on Erlang Port Mapper Daemon Activation Socket.
[ OK ] Listening on GPS (Global P…ioning System) Daemon Sockets.
[ OK ] Listening on triggerhappy.socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
Starting Analog Devices power up/down sequence...
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Regular background program processing daemon.
[ OK ] Started D-Bus System Message Bus.
Starting dphys-swapfile - …unt, and delete a swap file...
Starting Remove Stale Onli…t4 Metadata Check Snapshots...
Starting Creating IIOD Context Attributes......
Starting Authorization Manager...
Starting DHCP Client Daemon...
Starting LSB: Switch to on…nless shift key is pressed)...
Starting LSB: rng-tools (Debian variant)...
Starting System Logging Service...
Starting User Login Management...
Starting triggerhappy global hotkey daemon...
Starting Disk Manager...
Starting WPA supplicant...
[ OK ] Finished Remove Stale Onli…ext4 Metadata Check Snapshots.
[ OK ] Started triggerhappy global hotkey daemon.
[ OK ] Started DHCP Client Daemon.
[ OK ] Started LSB: rng-tools (Debian variant).
[ OK ] Started System Logging Service.
[ OK ] Finished dphys-swapfile - …mount, and delete a swap file.
[ OK ] Started User Login Management.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started WPA supplicant.
[ OK ] Reached target Network.
[ OK ] Reached target Network is Online.
Starting CUPS Scheduler...
[ OK ] Started Erlang Port Mapper Daemon.
Starting HTTP based time synchronization tool...
Starting Internet superserver...
Starting /etc/rc.local Compatibility...
Starting OpenBSD Secure Shell server...
Starting Permit User Sessions...
[ OK ] Started Unattended Upgrades Shutdown.
[ OK ] Started /etc/rc.local Compatibility.
[ OK ] Finished Permit User Sessions.
Starting Light Display Manager...
Starting Hold until boot process finishes up...
[ OK ] Started Authorization Manager.
Starting Modem Manager...
[ OK ] Started HTTP based time synchronization tool.
[ OK ] Started Internet superserver.
[ OK ] Finished Creating IIOD Context Attributes....
[ OK ] Started IIO Daemon.
[ OK ] Started OpenBSD Secure Shell server.
Raspbian GNU/Linux 11 analog ttyPS0
analog login:
========================================================================
Unique configuration/attribute values
The following attribute/value pairs are unique for one or more configuration
========================================================================
$VAR1 = 'GTHE4_QPLL0_6_25_156';
$VAR2 = {
'channel' => {},
'common' => {},
'pll_dividers' => {}
};
========================================================================
Common configuration/attribute values
The following attribute/value pairs are the same for each configuration
========================================================================
$VAR1 = 'gt_global';
$VAR2 = {
'common' => {
'QPLL1_CFG1' => '0xD038',
'POR_CFG' => '0x0',
'QPLL0_CP' => '0xFF',
'QPLL1_CFG2' => '0xFC3',
'QPLL1_CFG3' => '0x120',
'QPLL0_CFG1' => '0xD038',
'QPLL1_CP' => '0xFF',
'QPLL0_CFG3' => '0x120',
'QPLL0_CFG2' => '0xFC3',
'QPLL1_CFG4' => '0x3',
'QPLL1_CP_G3' => '0x7F',
'PPF0_CFG' => '0x800',
'QPLL0_CFG4' => '0x4',
'QPLL0_CP_G3' => '0xF',
'QPLL0_CFG1_G3' => '0xD038',
'PPF1_CFG' => '0x600',
'QPLL0_CFG2_G3' => '0xFC3',
'QPLL1_LPF' => '0x21F',
'QPLL1_CFG1_G3' => '0xD038',
'QPLL0_LPF' => '0x21F',
'QPLL1_CFG2_G3' => '0xFC3',
'QPLL0_CFG0' => '0x331C',
'QPLL1_CFG0' => '0x331C'
},
'channel' => {
'TXBUF_EN' => '"TRUE"',
'RXCDR_CFG3_GEN4' => '0x12',
'CPLL_CFG3' => '0x0',
'CPLL_CFG2' => '0x2',
'CH_HSPMUX' => '0x4444',
'CPLL_CFG1' => '0x23',
'PREIQ_FREQ_BST' => '0x1',
'RXDFE_PWR_SAVING' => '0x1',
'GEARBOX_MODE' => '0x0',
'A_TXDIFFCTRL' => '0xC',
'RXBUF_EN' => '"TRUE"',
'RXCDR_CFG3_GEN3' => '0x12',
'DEC_MCOMMA_DETECT' => '"TRUE"',
'RXPI_CFG1' => '0x0',
'RXCDR_CFG2' => '0x255',
'RXCDR_CFG3_GEN2' => '0x12',
'ALIGN_COMMA_ENABLE' => '0x3FF',
'RXCDR_CFG0' => '0x3',
'RX_WIDEMODE_CDR' => '0x0',
'ALIGN_MCOMMA_DET' => '"TRUE"',
'ALIGN_PCOMMA_DET' => '"TRUE"',
'RXCDR_CFG2_GEN4' => '0x164',
'RXGEARBOX_EN' => '"FALSE"',
'CBCC_DATA_SOURCE_SEL' => '"DECODED"',
'DEC_PCOMMA_DETECT' => '"TRUE"',
'TX_DATA_WIDTH' => '40',
'CPLL_CFG0' => '0x1FA',
'TXPH_CFG' => '0x723',
'TXGEARBOX_EN' => '"FALSE"',
'RXCDR_CFG2_GEN3' => '0x255',
'RXBUF_THRESH_UNDFLW' => '3',
'RXGBOX_FIFO_INIT_RD_ADDR' => '4',
'RXCDR_CFG3' => '0x12',
'RX_DATA_WIDTH' => '40',
'RXPI_CFG0' => '0x2004',
'RXCDR_CFG2_GEN2' => '0x255'
},
'pll_dividers' => {
'QPLL0_FBDIV' => '80',
'QPLL1_FBDIV' => '66',
'QPLL0_FBDIV_G3' => '160',
'QPLL1CLKOUT_RATE' => '"HALF"',
'TX_CLK25_DIV' => '7',
'QPLL0CLKOUT_RATE' => '"HALF"',
'RXOUT_DIV' => '2',
'QPLL1_FBDIV_G3' => '80',
'CPLL_FBDIV_45' => '5',
'CPLL_FBDIV' => '2',
'RX_CLK25_DIV' => '7',
'QPLL1_REFCLK_DIV' => '1',
'CPLL_REFCLK_DIV' => '1',
'QPLL0_REFCLK_DIV' => '1',
'TXOUT_DIV' => '2'
}
};
// SPDX-License-Identifier: GPL-2.0
/*
* Analog Devices AD9695 / AD9689 ANALOG-TO-DIGITAL CONVERTER
* https://wiki.analog.com/resources/eval/ad9208-3000ebz
* https://wiki.analog.com/resources/tools-software/linux-drivers/iio-adc/ad9208
*
* hdl_project: <ad9695_fmc/zcu102>
* board_revision: <>
*
* Copyright (C) 2019-2022 Analog Devices Inc.
*/
#include "zynqmp-zcu102-rev1.0.dts"
#include <dt-bindings/interrupt-controller/irq.h>
#include <dt-bindings/iio/adc/adi,ad9208.h>
#include <dt-bindings/jesd204/adxcvr.h>
&i2c1 {
i2c-mux@75 {
i2c@0 {
#address-cells = <1>;
#size-cells = <0>;
reg = <0>;
eeprom@50 {
compatible = "at24,24c02";
reg = <0x50>;
};
};
};
};
/ {
clocks {
ad9695_clkin: clock@0 {
#clock-cells = <0>;
compatible = "adjustable-clock";
clock-frequency = <6250000000>;
clock-accuracy = <1000000000>;
clock-output-names = "ad9695_clk";
};
device_clk: clock@1 {
#clock-cells = <0>;
compatible = "adjustable-clock";
clock-frequency = <156250000>;
clock-accuracy = <1000000000>;
clock-output-names = "dev_clk";
};
sysref: clock@2 {
#clock-cells = <0>;
compatible = "adjustable-clock";
clock-frequency = <9765725>;
clock-accuracy = <1000000000>;
clock-output-names = "adc_sysref";
};
};
fpga_axi: fpga-axi@0 {
interrupt-parent = <&gic>;
compatible = "simple-bus";
#address-cells = <0x1>;
#size-cells = <0x1>;
ranges = <0 0 0 0xffffffff>;
rx_dma: rx-dmac@9c400000 {
#dma-cells = <1>;
compatible = "adi,axi-dmac-1.00.a";
reg = <0x9c400000 0x1000>;
interrupts = <0 109 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&zynqmp_clk 71>;
adi,channels {
#size-cells = <0>;
#address-cells = <1>;
dma-channel@0 {
reg = <0>;
adi,source-bus-width = <128>;
adi,source-bus-type = <1>;
adi,destination-bus-width = <128>;
adi,destination-bus-type = <0>;
};
};
};
axi_ad9695_core: axi-ad9695-hpc@84a00000 {
compatible = "adi,axi-ad9208-1.0";
reg = <0x84a00000 0x2000>;
dmas = <&rx_dma 0>;
dma-names = "rx";
spibus-connected = <&adc0_ad9695>;
};
axi_ad9695_jesd: axi-jesd204-rx@84aa0000 {
compatible = "adi,axi-jesd204-rx-1.0";
reg = <0x84aa0000 0x4000>;
interrupts = <0 108 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&zynqmp_clk 71>, <&device_clk>, <&axi_ad9695_adxcvr 0>;
clock-names = "s_axi_aclk", "device_clk", "lane_clk";
adi,octets-per-frame = <1>;
adi,frames-per-multiframe = <32>;
adi,subclass = <0>; #<1>;
#clock-cells = <0>;
clock-output-names = "jesd_adc_lane_clk";
};
axi_ad9695_adxcvr: axi-adxcvr-rx@84a60000 {
compatible = "adi,axi-adxcvr-1.0";
reg = <0x84a60000 0x10000>;
clocks = <&device_clk>, <&device_clk>;
clock-names = "conv", "div40";
adi,sys-clk-select = <XCVR_QPLL>;
adi,out-clk-select = <XCVR_REFCLK>;
adi,use-lpm-enable;
#clock-cells = <1>;
clock-output-names = "adc_gt_clk", "rx_out_clk";
};
axi_sysid_0: axi-sysid-0@85000000 {
compatible = "adi,axi-sysid-1.00.a";
reg = <0x85000000 0x2000>;
};
};
};
&spi0 {
status = "okay";
adc0_ad9695: ad9695@0 {
compatible = "adi,ad9695";
powerdown-gpios = <&gpio 116 0>;
fastdetect-a-gpios = <&gpio 113 0>;
fastdetect-b-gpios = <&gpio 114 0>;
spi-cpol;
spi-cpha;
spi-max-frequency = <5000000>;
reg = <0>;
clocks = <&axi_ad9695_jesd>, <&ad9695_clkin>, <&sysref>;
clock-names = "jesd_adc_clk", "adc_clk", "adc_sysref";
adi,powerdown-mode = <AD9208_PDN_MODE_POWERDOWN>;
adi,sampling-frequency = /bits/ 64 <6250000000>;
adi,input-clock-divider-ratio = <1>;
adi,duty-cycle-stabilizer-enable;
adi,analog-input-neg-buffer-current = <AD9208_BUFF_CURR_600_UA>;
adi,analog-input-pos-buffer-current = <AD9208_BUFF_CURR_600_UA>;
adi,sysref-lmfc-offset = <0>;
adi,sysref-pos-window-skew = <0>;
adi,sysref-neg-window-skew = <0>;
adi,sysref-mode = <AD9208_SYSREF_CONT>;
adi,sysref-nshot-ignore-count = <0>;
/* JESD204 parameters */
adi,octets-per-frame = <1>;
adi,frames-per-multiframe = <32>;
adi,converter-resolution = <16>;
adi,bits-per-sample = <16>;
adi,converters-per-device = <2>;
adi,control-bits-per-sample = <0>;
adi,lanes-per-device = <4>;
adi,subclass = <1>;
#address-cells = <1>;
#size-cells = <0>;
};
};
###############################################################################
## Copyright (C) 2022-2024 Analog Devices, Inc. All rights reserved.
### SPDX short identifier: ADIBSD
###############################################################################
# RX parameters
set RX_NUM_OF_LANES $ad_project_params(RX_JESD_L) ; # L
set RX_NUM_OF_CONVERTERS $ad_project_params(RX_JESD_M) ; # M
set RX_SAMPLES_PER_FRAME $ad_project_params(RX_JESD_S) ; # S
set RX_SAMPLE_WIDTH 16 ; # N/NP
set RX_SAMPLES_PER_CHANNEL [expr $RX_NUM_OF_LANES * 32 / ($RX_NUM_OF_CONVERTERS * $RX_SAMPLE_WIDTH)]
set adc_data_width [expr $RX_SAMPLE_WIDTH * $RX_NUM_OF_CONVERTERS * $RX_SAMPLES_PER_CHANNEL]
set adc_dma_data_width [expr $RX_SAMPLE_WIDTH * $RX_NUM_OF_CONVERTERS * $RX_SAMPLES_PER_CHANNEL]
# These are max values specific to the board
set MAX_RX_NUM_OF_LANES 4
source $ad_hdl_dir/library/jesd204/scripts/jesd204.tcl
# adc peripherals
ad_ip_instance axi_adxcvr axi_ad9695_rx_xcvr [list \
NUM_OF_LANES $RX_NUM_OF_LANES \
QPLL_ENABLE 1 \
TX_OR_RX_N 0 \
SYS_CLK_SEL 3 \
OUT_CLK_SEL 3 \
]
adi_axi_jesd204_rx_create axi_ad9695_rx_jesd $RX_NUM_OF_LANES
ad_ip_parameter axi_ad9695_rx_jesd/rx CONFIG.SYSREF_IOB false
ad_ip_instance util_cpack2 util_ad9695_rx_cpack [list \
NUM_OF_CHANNELS $RX_NUM_OF_CONVERTERS \
SAMPLES_PER_CHANNEL $RX_SAMPLES_PER_CHANNEL \
SAMPLE_DATA_WIDTH $RX_SAMPLE_WIDTH \
]
adi_tpl_jesd204_rx_create rx_ad9695_tpl_core $RX_NUM_OF_LANES \
$RX_NUM_OF_CONVERTERS \
$RX_SAMPLES_PER_FRAME \
$RX_SAMPLE_WIDTH
ad_ip_instance clk_wiz dma_clk_wiz
ad_ip_parameter dma_clk_wiz CONFIG.PRIMITIVE MMCM
ad_ip_parameter dma_clk_wiz CONFIG.RESET_TYPE ACTIVE_LOW
ad_ip_parameter dma_clk_wiz CONFIG.USE_LOCKED false
ad_ip_parameter dma_clk_wiz CONFIG.CLKOUT1_REQUESTED_OUT_FREQ 332.9
ad_ip_parameter dma_clk_wiz CONFIG.PRIM_SOURCE No_buffer
ad_ip_instance axi_dmac axi_ad9695_rx_dma [list \
DMA_TYPE_SRC 2 \
DMA_TYPE_DEST 0 \
CYCLIC 0 \
SYNC_TRANSFER_START 1 \
DMA_2D_TRANSFER 0 \
FIFO_SIZE 32 \
MAX_BYTES_PER_BURST 2048 \
AXI_SLICE_DEST 1 \
AXI_SLICE_SRC 1 \
DMA_LENGTH_WIDTH 24 \
DMA_DATA_WIDTH_DEST 128 \
DMA_DATA_WIDTH_SRC $adc_dma_data_width \
]
# common cores
# fPLLClkin = 325 MHz => RX_CLK25_DIV = 13
# fPLLClkout = 13000 MHz - qpll0
ad_ip_instance util_adxcvr util_ad9695_xcvr [list \
RX_NUM_OF_LANES $MAX_RX_NUM_OF_LANES \
TX_NUM_OF_LANES 0 \
QPLL_FBDIV 40 \
QPLL_REFCLK_DIV 1 \
RX_OUT_DIV 1 \
RX_CLK25_DIV 13 \
POR_CFG 0x0 \
QPLL_CFG0 0x331c \
QPLL_CFG1 0xd038 \
QPLL_CFG1_G3 0xd038 \
QPLL_CFG2 0xfc3 \
QPLL_CFG2_G3 0xfc1 \
QPLL_CFG3 0x120 \
QPLL_CFG4 0x3 \
QPLL_CP 0xff \
QPLL_CP_G3 0xf \
QPLL_LPF 0x21f \
CH_HSPMUX 0x4444 \
PREIQ_FREQ_BST 1 \
RXPI_CFG0 0x104 \
RXPI_CFG1 0x0 \
RXCDR_CFG0 0x3 \
RXCDR_CFG2_GEN2 0x255 \
RXCDR_CFG2_GEN4 0x164 \
RXCDR_CFG3 0x11 \
RXCDR_CFG3_GEN2 0x12 \
RXCDR_CFG3_GEN3 0x12 \
RXCDR_CFG3_GEN4 0x12 \
]
# xcvr interfaces
set rx_ref_clk rx_ref_clk_0
create_bd_port -dir I $rx_ref_clk
create_bd_port -dir I rx_core_clk_0
ad_connect $sys_cpu_resetn util_ad9695_xcvr/up_rstn
ad_connect $sys_cpu_clk util_ad9695_xcvr/up_clk
# Rx
ad_connect ad9695_rx_device_clk rx_core_clk_0
ad_xcvrcon util_ad9695_xcvr axi_ad9695_rx_xcvr axi_ad9695_rx_jesd {} ad9695_rx_device_clk {} $MAX_RX_NUM_OF_LANES
ad_xcvrpll $rx_ref_clk util_ad9695_xcvr/qpll_ref_clk_0
for {set i 0} {$i < $MAX_RX_NUM_OF_LANES} {incr i} {
set ch [expr $i]
ad_xcvrpll $rx_ref_clk util_ad9695_xcvr/cpll_ref_clk_$ch
ad_xcvrpll axi_ad9695_rx_xcvr/up_pll_rst util_ad9695_xcvr/up_cpll_rst_$ch
}
ad_xcvrpll axi_ad9695_rx_xcvr/up_pll_rst util_ad9695_xcvr/up_qpll_rst_*
# connections (adc)
ad_connect $sys_cpu_resetn axi_ad9695_rx_dma/m_dest_axi_aresetn
ad_connect dma_clk_wiz/clk_out1 axi_ad9695_rx_dma/m_dest_axi_aclk
ad_connect util_ad9695_rx_cpack/packed_fifo_wr axi_ad9695_rx_dma/fifo_wr
ad_connect util_ad9695_rx_cpack/packed_sync axi_ad9695_rx_dma/sync
ad_connect $sys_cpu_clk dma_clk_wiz/clk_in1
ad_connect $sys_cpu_resetn dma_clk_wiz/resetn
ad_connect ad9695_rx_device_clk rx_ad9695_tpl_core/link_clk
ad_connect ad9695_rx_device_clk util_ad9695_rx_cpack/clk
ad_connect ad9695_rx_device_clk axi_ad9695_rx_dma/fifo_wr_clk
ad_connect ad9695_rx_device_clk_rstgen/peripheral_reset util_ad9695_rx_cpack/reset
ad_connect axi_ad9695_rx_jesd/rx_sof rx_ad9695_tpl_core/link_sof
ad_connect axi_ad9695_rx_jesd/rx_data_tdata rx_ad9695_tpl_core/link_data
ad_connect axi_ad9695_rx_jesd/rx_data_tvalid rx_ad9695_tpl_core/link_valid
ad_connect rx_ad9695_tpl_core/adc_valid_0 util_ad9695_rx_cpack/fifo_wr_en
ad_connect rx_ad9695_tpl_core/adc_dovf util_ad9695_rx_cpack/fifo_wr_overflow
for {set i 0} {$i < $RX_NUM_OF_CONVERTERS} {incr i} {
ad_connect rx_ad9695_tpl_core/adc_enable_$i util_ad9695_rx_cpack/enable_$i
ad_connect rx_ad9695_tpl_core/adc_data_$i util_ad9695_rx_cpack/fifo_wr_data_$i
}
# interconnect (cpu)
ad_cpu_interconnect 0x44A00000 rx_ad9695_tpl_core
ad_cpu_interconnect 0x44A60000 axi_ad9695_rx_xcvr
ad_cpu_interconnect 0x44AA0000 axi_ad9695_rx_jesd
ad_cpu_interconnect 0x7c400000 axi_ad9695_rx_dma
ad_mem_hp0_interconnect $sys_cpu_clk sys_ps8/S_AXI_HP0
ad_mem_hp0_interconnect $sys_cpu_clk axi_ad9695_rx_xcvr/m_axi
# interconnect (mem/dac)
ad_mem_hp2_interconnect dma_clk_wiz/clk_out1 sys_ps7/S_AXI_HP1
ad_mem_hp2_interconnect dma_clk_wiz/clk_out1 axi_ad9695_rx_dma/m_dest_axi
# interrupts
ad_cpu_interrupt ps-12 mb-13 axi_ad9695_rx_jesd/irq
ad_cpu_interrupt ps-13 mb-12 axi_ad9695_rx_dma/irq
looks like i have an error in my device tree ref clock. here is the original https://github.com/analogdevicesinc/linux/blob/main/arch/arm64/boot/dts/xilinx/zynqmp-zcu102-rev10-ad9695.dts
when I get done with this Im going to post a bring up procedure for posterity...
Hi,
Apologies for the delay! And for the missed thread AD9695_fmc/ZCU102 modify the util_ad9695_xcvr for the the -625 speed grade
the two do not exactly match up. can I simply replace the parameters in the tcl script with the one from the txt file and match the syntax?
Yes, but my guess is that since your project was built successfully, the problem relies in another part... Did you make changes in the dts?
Best regards,
Iulia