Post Go back to editing

Interfacing AD9361 with digilent zedboard using hdl/fmcomms2 and no-OS/ad9361 (1)

Category: Hardware
Product Number: AD9361

Hi,

Background: I am using the Vivado HDL design given by ADI to get the hardware description and the No-OS code given by ADI to send and receive data. My eventual goal is to design 2 IPs :

  1. Baseband Processor

  2. Control block for AD9361

A few additional details are mentioned below:

  1. Development Board – Zedboard

  2. SDR – AD-FMCOMMS2-EBZ

  3. Vivado and Vitis version – 2019.2, 2022.1, 2023.2 (Have multiple installations and have used all three for this development)

  4. HDL project – projects/fmcomms2/zed

  5. No-OS project - projects/ad9361

I have many queries regarding this and hope to get individual replies. I have posted 3 separate queries on the forum to make a differentiation between 3 separate themes. I have gone through the ez forum and have gotten partial answers (not enough). I have put the questions in order of priority. I am relatively new to this. Thank you in advance for your help.

HDL

  1. Pin mapping for the SPI interface.

While using the HDL project on vivado, I was not able to locate the following pin assignments. These are ports that should somehow connect to the AD9361 board-

  • spi0_clk_o

  • spi0_sdo_o

  • spi0_csn_0_o

  • spi0_csn_1_o

  • spi0_csn_2_o

  • spi1_clk_o

  • spi1_sdo_o

  • spi1_csn_0_o

  • spi1_csn_1_o

  • spi1_csn_2_o

  • spi0_clk_i

  • spi0_sdo_i

  • spi0_sdi_i

  • spi0_csn_1

  • spi1_clk_i

  • spi0_sdo_i

  • spi0_sdi_i

  • spi0_csn_1

These ports are directly connected to the processor. Are these ports not meant to be connected to physical pins? If they are meant to be connected, how?

  1. How to use the SPI engine IP? What is its application?

    Do we need the SPI engine and its peripherals for our custom block?

  2. I have gone through the SDR pin mapping and found that there are only 4 “SPI pins” on the FMC connector.

    The document is linked here on the website under the “Design and Integration File” header. The pins are -

  • SPI_ENB

  • SPI_CLK

  • SPI_DO

  • SPI_DI

  1. I want to introduce a BBP in the hardware description. How and where do I place this IP block in vivado?

This custom IP is supposed to act as a BBP that converts the data stream into I/Q values. I suspect that this block will be just before the “axi_ad9361” block. (That is between axi_ad9361_dac_fifo and axi_ad9361) The logic of converting data streams into I/Q values is a separate topic, and it is not in the scope of this question.

  1. Many IP blocks that do not modify the data.

    There are many IP blocks, like HDMI, audio blocks, etc., that are not used at all by the software (No-OS). Am I safe to remove these blocks? Or are these used in some internal data processing?

  2. Can someone please explain how the "physical pins" on the zedboard be mapped to the "ports" in vivado?

    I know we use the constraints file (.xdc) for this. This question arose because there are many ports that don't have any physical package pin mapping.

  3. Why are there 2 constraint files in the vivado project?

    The files are namely -

  • system_constr.xdc

  • zed_system_constr.xdc

I think “system_constr.xdc” has the AD9361 system-specific pin assignments, and the “zed_system_constr.xdc” has other assignments. Additionally, I want to ask whether the “zed_system_constr.xdc” assignments are system-critical if we wish to make simple Tx and Rx ONLY.

____________________________________

I have tried to state the problem, explain my understanding and provide any necessary links and enumeration required to better communicate the question. Kindly let me know if any additional info is required for any of the questions. I will make necessary edits to the original post, if any. Once again, I have many queries regarding this and hope to get individual replies. Thank you for your patience if reached this far in the post.

Thank You

Pranav Bhaskaran

(Student from India)

Edit Notes

Edited the subject of the post only.
[edited by: pbhereandnow at 5:49 AM (GMT -4) on 30 Jul 2024]

Thread Notes

Parents
  • Thank you  for the detailed support.

    Hi  ,

    I just want to add a few more comments to what my colleague said, because all that was said there is right.

    Vivado and Vitis version – 2019.2, 2022.1, 2023.2 (Have multiple installations and have used all three for this development)

    Mixing them however you like, will result in inconsistencies, because Xilinx made significant updates between versions, and they work best if you choose the same Vitis and Vivado version to work together.

    How to use the SPI engine IP? What is its application?

    Do we need the SPI engine and its peripherals for our custom block?

    This is the SPI Engine IP, but it is not used in this project. Are you referring to something else?

    I want to introduce a BBP in the hardware description. How and where do I place this IP block in vivado?

    https://wiki.analog.com/resources/fpga/docs/hdl/xcomm2ip

    Am I safe to remove these blocks?

    Almost. You have to check how it is used in software to know if it's safe to remove.

    I think “system_constr.xdc” has the AD9361 system-specific pin assignments, and the “zed_system_constr.xdc” has other assignments. Additionally, I want to ask whether the “zed_system_constr.xdc” assignments are system-critical if we wish to make simple Tx and Rx ONLY.

    Yes, system_constr.xdc are eval board-specific: https://analogdevicesinc.github.io/hdl/user_guide/architecture.html#project-files-for-amd-boards 

    zed_system_constr.xdc are specific to Zedboard, to the carrier.

    Best regards,
    Iulia

  • Thank you for your reply,

    Please note that I successfully built and flashed HDL and no-os for the FMCOMMS2 board with Zedboard. This I did without changing anything. Now, I wish to modify the existing code for my use case.

    Mixing them however you like, will result in inconsistencies,

    Also, I am not mixing and matching Vivado, Vitis and No-OS versions. Instead, I have used these versions individually.

    This is the SPI Engine IP,

    Yes, in my question, I was referring to this SPI engine itself. My "custom block" should be able to send and receive spi signals, in that context, do I require this block along with it's peripherals?

    wiki.analog.com/.../quote]

    Yes, I have gone through this blog post. The files I was not able to build and get it in my system. Moreover, if you look closely towards the end of the blog, there are a few headings that don't seem to have any content. As I was to able to build this, I request you to kindly share a screengrab of the final "xcomm2ip" connected to the entire design for my reference.

    Almost

    Noted

    zed_system_constr.xdc are specific to Zedboard, to the carrier.

    Noted

    [/quote]
Reply
  • Thank you for your reply,

    Please note that I successfully built and flashed HDL and no-os for the FMCOMMS2 board with Zedboard. This I did without changing anything. Now, I wish to modify the existing code for my use case.

    Mixing them however you like, will result in inconsistencies,

    Also, I am not mixing and matching Vivado, Vitis and No-OS versions. Instead, I have used these versions individually.

    This is the SPI Engine IP,

    Yes, in my question, I was referring to this SPI engine itself. My "custom block" should be able to send and receive spi signals, in that context, do I require this block along with it's peripherals?

    wiki.analog.com/.../quote]

    Yes, I have gone through this blog post. The files I was not able to build and get it in my system. Moreover, if you look closely towards the end of the blog, there are a few headings that don't seem to have any content. As I was to able to build this, I request you to kindly share a screengrab of the final "xcomm2ip" connected to the entire design for my reference.

    Almost

    Noted

    zed_system_constr.xdc are specific to Zedboard, to the carrier.

    Noted

    [/quote]
Children
No Data