Post Go back to editing

UP_AXI 's address map

Category: Software

Hi , 

I have customize IP which integrated with AXI bus using up_axi.v as memory mapping . It' similar approach like axi_ad961 IP . I have updated address width as 32 bits as below. Actually my design write/read address use 16 bits only . 

I found AD9361 IP Reg Address are 0x0000, 0x0004, 0x0008 etc..

up_raddr <= up_axi_araddr[AW+2:2]; //original axi bus address define from github

up_wdata <= up_axi_wdata; // Updated for my design 

I also used axi_vip IP to verify for AXI bus connection with my design . The simulation results for write / read data is working .

I have Attached simulation picture here. My simulation testbench is using direct address bus mean base address plus my FPGA reg address.  

If our software write / read reg bus address , the address need to be multiple by 4 or can use direct base address plus write_reg address.  I have attached my version of up_axi.v . 

When software try to write address multiple by 4 then , the read back reg bus data is incorrect . Software require to write like 8000_9004 then , can able to read back for 

16 bits data . 8000_0000 is my base address and 9004 is my read reg address. 

 I would like to understand how to adapt up_axi.v to my 16bit write /read reg address bus design . How the software should  write address like need to be 4 bytes align or direct address .

Could you help to take a look for

`timescale 1ns/100ps

module up_axi (

  // reset and clocks

  up_rstn,
  up_clk,

  // axi4 interface

  up_axi_awvalid,
  up_axi_awaddr,
  up_axi_awready,
  /////////////////////////////////////////////////////
  up_axi_wvalid,
  up_axi_wdata,
  up_axi_wstrb,
  up_axi_wready,
  /////////////////////////////////////////////////////
  up_axi_bvalid,
  up_axi_bresp,
  up_axi_bready,
  /////////////////////////////////////////////////////
  up_axi_arvalid,
  up_axi_araddr,
  up_axi_arready,
  /////////////////////////////////////////////////////
  up_axi_rvalid,
  up_axi_rresp,
  up_axi_rdata,
  up_axi_rready,

  // pcore interface

  up_wreq,
  up_waddr,
  up_wdata,
  up_wack,
  up_rreq,
  up_raddr,
  up_rdata,
  up_rack);

  // parameters

  parameter   ADDRESS_WIDTH = 14;
  //parameter   ADDRESS_WIDTH = 16;
  localparam  AW = ADDRESS_WIDTH - 1;

  // reset and clocks

  input           up_rstn;
  input           up_clk;

  // axi4 interface

  input           up_axi_awvalid;
  input   [31:0]  up_axi_awaddr;
  output          up_axi_awready;
  input           up_axi_wvalid;
  input   [31:0]  up_axi_wdata;
  input   [ 3:0]  up_axi_wstrb;
  output          up_axi_wready;
  output          up_axi_bvalid;
  output  [ 1:0]  up_axi_bresp;
  input           up_axi_bready;
  input           up_axi_arvalid;
  input   [31:0]  up_axi_araddr;
  output          up_axi_arready;
  output          up_axi_rvalid;
  output  [ 1:0]  up_axi_rresp;
  output  [31:0]  up_axi_rdata;
  input           up_axi_rready;

  // pcore interface

  output          up_wreq;
  //output  [AW:0]  up_waddr;
  output  [31:0]  up_waddr;
  output  [31:0]  up_wdata;
  input           up_wack;
  output          up_rreq;
  //output  [AW:0]  up_raddr;
  output  [31:0]  up_raddr;
  input   [31:0]  up_rdata;
  input           up_rack;

  // internal registers

  reg             up_axi_awready = 'd0;
  reg             up_axi_wready = 'd0;
  reg             up_axi_bvalid = 'd0;
  reg             up_wsel = 'd0;
  reg             up_wreq = 'd0;
  //reg     [AW:0]  up_waddr = 'd0;
  reg     [31:0]  up_waddr = 'd0;
  reg     [31:0]  up_wdata = 'd0;
  reg     [ 2:0]  up_wcount = 'd0;
  reg             up_wack_int = 'd0;
  reg             up_axi_arready = 'd0;
  reg             up_axi_rvalid = 'd0;
  reg     [31:0]  up_axi_rdata = 'd0;
  reg             up_rsel = 'd0;
  reg             up_rreq = 'd0;
  reg     [31:0]  up_raddr = 'd0;
  //reg     [AW:0]  up_raddr = 'd0;
  reg     [ 3:0]  up_rcount = 'd0;
  reg             up_rack_int = 'd0;
  reg     [31:0]  up_rdata_int = 'd0;
  reg             up_rack_int_d = 'd0;
  reg     [31:0]  up_rdata_int_d = 'd0;

  // write channel interface
 
  assign up_axi_bresp = 2'd0;

  always @(negedge up_rstn or posedge up_clk) begin
    if (up_rstn == 1'b0) begin
      up_axi_awready <= 'd0;
      up_axi_wready <= 'd0;
      up_axi_bvalid <= 'd0;
    end else begin
      if (up_axi_awready == 1'b1) begin
        up_axi_awready <= 1'b0;
      end else if (up_wack_int == 1'b1) begin
        up_axi_awready <= 1'b1;
      end
      if (up_axi_wready == 1'b1) begin
        up_axi_wready <= 1'b0;
      end else if (up_wack_int == 1'b1) begin
        up_axi_wready <= 1'b1;
      end
      if ((up_axi_bready == 1'b1) && (up_axi_bvalid == 1'b1)) begin
        up_axi_bvalid <= 1'b0;
      end else if (up_wack_int == 1'b1) begin
        up_axi_bvalid <= 1'b1;
      end
    end
  end       

  always @(negedge up_rstn or posedge up_clk) begin
    if (up_rstn == 1'b0) begin
      up_wsel <= 'd0;
      up_wreq <= 'd0;
      up_waddr <= 'd0;
      up_wdata <= 'd0;
      up_wcount <= 'd0;
    end else begin
      if (up_wsel == 1'b1) begin
        if ((up_axi_bready == 1'b1) && (up_axi_bvalid == 1'b1)) begin
          up_wsel <= 1'b0;
        end
        up_wreq <= 1'b0;
        up_waddr <= up_waddr;
        up_wdata <= up_wdata;
        up_wcount <= up_wcount + 1'b1;
      end else begin
        up_wsel <= up_axi_awvalid & up_axi_wvalid;
        up_wreq <= up_axi_awvalid & up_axi_wvalid;
        up_waddr <= up_axi_awaddr;
        //up_waddr <= up_axi_awaddr[AW+2:2];
        up_wdata <= up_axi_wdata;
        up_wcount <= 3'd0;
      end
    end
  end

  always @(negedge up_rstn or posedge up_clk) begin
    if (up_rstn == 0) begin
      up_wack_int <= 'd0;
    end else begin
      if ((up_wcount == 3'h7) && (up_wack == 1'b0)) begin
        up_wack_int <= 1'b1;
      end else if (up_wsel == 1'b1) begin
        up_wack_int <= up_wack;
      end
    end
  end

  // read channel interface

  assign up_axi_rresp = 2'd0;

  always @(negedge up_rstn or posedge up_clk) begin
    if (up_rstn == 1'b0) begin
      up_axi_arready <= 'd0;
      up_axi_rvalid <= 'd0;
      up_axi_rdata <= 'd0;
    end else begin
      if (up_axi_arready == 1'b1) begin
        up_axi_arready <= 1'b0;
      end else if (up_rack_int == 1'b1) begin
        up_axi_arready <= 1'b1;
      end
      if ((up_axi_rready == 1'b1) && (up_axi_rvalid == 1'b1)) begin
        up_axi_rvalid <= 1'b0;
        up_axi_rdata <= 32'd0;
      end else if (up_rack_int_d == 1'b1) begin
        up_axi_rvalid <= 1'b1;
        up_axi_rdata <= up_rdata_int_d;
      end
    end
  end       

  always @(negedge up_rstn or posedge up_clk) begin
    if (up_rstn == 1'b0) begin
      up_rsel <= 'd0;
      up_rreq <= 'd0;
      up_raddr <= 'd0;
      up_rcount <= 'd0;
    end else begin
      if (up_rsel == 1'b1) begin
        if ((up_axi_rready == 1'b1) && (up_axi_rvalid == 1'b1)) begin
          up_rsel <= 1'b0;
        end
        up_rreq <= 1'b0;
        up_raddr <= up_raddr;
      end else begin
        up_rsel <= up_axi_arvalid;
        up_rreq <= up_axi_arvalid;
        //up_raddr <= up_axi_araddr[AW+2:2];
        up_raddr <= up_axi_araddr;
      end
      if (up_rack_int == 1'b1) begin
        up_rcount <= 4'd0;
      end else if (up_rcount[3] == 1'b1) begin
        up_rcount <= up_rcount + 1'b1;
      end else if (up_rreq == 1'b1) begin
        up_rcount <= 4'd8;
      end
    end
  end

  always @(negedge up_rstn or posedge up_clk) begin
    if (up_rstn == 0) begin
      up_rack_int <= 'd0;
      up_rdata_int <= 'd0;
      up_rack_int_d <= 'd0;
      up_rdata_int_d <= 'd0;
    end else begin
      if ((up_rcount == 4'hf) && (up_rack == 1'b0)) begin
        up_rack_int <= 1'b1;
        up_rdata_int <= {2{16'hdead}};
      end else begin
        up_rack_int <= up_rack;
        up_rdata_int <= up_rdata;
      end
      up_rack_int_d <= up_rack_int;
      up_rdata_int_d <= up_rdata_int;
    end
  end

endmodule

// ***************************************************************************
// ***************************************************************************
this ? Thank you so much for your help. 

Appreciate for your reply. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.