Post Go back to editing

axi_ad9361 IP testing

Thread Summary

The user inquired about testing the AXI_AD9361 IP core without the FMCOMMS2 or AD9361 hardware board. The final answer indicated that a loopback can be created by connecting clk_out to clk_in, frame_out to frame_in, and data_out to data_in. The user was advised to use the driver (no-OS or Linux) to provide data to the DAC interface and to ensure the testbenches are correctly cloned within the HDL repo. The user encountered issues with waveforms showing '0' values and was advised to add signals to the waveform window and pause the simulation.
AI Generated Content
Category: Software
Product Number: AD9361
Software Version: VIvado 2021.2

Hi,

I would like to know how can I test axi_ad9361 IP alone without Fmcomms OR AD9361 Hardware board. I came across ad9361_bist_loopback, and would appreciate help in the below.

1. Is FIFO required for this test?

2. Could I use this for testing the IP alone.

     If so will I  require IIO oscilloscope along with libiio text files for I,Q data (from github). 

3. Can I test axi_ad9361 IP with ILA. Can I have AD9361 functionalities in the IP without decimator interpolator IP?

Thanks in advance

Jyothi

Thread Notes

Parents Reply
  • Hi,

    Thank you for the support from your side, I am having an idea of what has to be done, although I would really appreciate if you could help me understand a little more. 

    As per my understanding the testbenches have its own project source and does not require any project as reference for carrying out simulation.  I need to give waveforms during simulation or in testbench soucre test_program.sv.

    Is my understanding correct? If so, the steps for cloning clearly states folder structure to be :

    • library
    • projects
    • testbenches

    I have followed the same for cloning the testbenches but it doesnt actually matter cause the testbench is having its own source ?

    I  would really appreciate to get to know about this test code, but I have not been able to find any source for it. Any link or data about this testcode would be of great help.

    Thanks & Regards

                             

Children
  • Yes, the folder structure is correct.

    The testbenches uses the IPs from the HDL repo and are automatically built when you do "make" in a testbench project.

    The Vivado flow copies the IPs source into the created testbench project, that means, vivado will "copy" the IP sources to these paths:

    hdl/testbenches/<TESTBENCH>/runs/cfg*/cfg*.ip_user_files/bd/test_harness/ipshared/*

    hdl/testbenches/<TESTBENCH>/runs/cfg*/cfg*.gen/sources_1/bd/test_harness/ipshared/*

    After the tb project is created, editing the hdl/library/<IP_CORE> sources won't automatically update the test program in execution, you have to either do "make" again (preferred) or patch the folders mentioned above (experienced). The only exception are the test_program.sv files.

    The testbench project may or may not use a hdl/projects/<PROJECT> source code; it really depends on the requirements and on what is being tested.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.