AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
Datasheet
AD9361 on Analog.com
Hi,
I would like to know how can I test axi_ad9361 IP alone without Fmcomms OR AD9361 Hardware board. I came across ad9361_bist_loopback, and would appreciate help in the below.
1. Is FIFO required for this test?
2. Could I use this for testing the IP alone.
If so will I require IIO oscilloscope along with libiio text files for I,Q data (from github).
3. Can I test axi_ad9361 IP with ILA. Can I have AD9361 functionalities in the IP without decimator interpolator IP?
Thanks in advance
Jyothi
srimoyi - Moved from Design Support AD9361/AD9363/AD9364 to FPGA Reference Designs. Post date updated from Thursday, July 4, 2024 10:45 AM UTC to Friday, July 12, 2024 11:52 AM UTC to reflect the move.
I came across ad9361_bist_loopback, and would appreciate help in the below.
You cannot test BIST without actual AD9361 hardware , as BIST generator is internal to the AD9361 chip. Refer to the below block diagram. The AXI_AD9361 IP core interfaces to the AD9361 chip

Refer to the below wiki page for more details:
Hi,
Thanks for the quick response, I have gone through the link mentioned by you multiple times. I want to know how could I test the IP alone?
Testing of IP alone will be phase1 of my project and after searching multiple threads I came across FMCOMMS2 testbench and ILA usage for DAC and ADC.
Though I could not find how exactly could I work with them without hardware board. I have my FPGA board with me, But FMCOMMS2 board is the next phase of my project.
Could you please help, and guide a way to test the IP ?
Thanks & Regards.
Moving to FPGA reference designs forum
Moving to FPGA reference designs forum