Hi,
I have a VPK120, which can output a Vadj of 1V, 1.2V or 1.5V.
I have it attached to an AD9081 board.
As explained here:
AD9081-FMCA-EBZ VADJ
The AD9081/2 has level shifters so it can operate with a multitude of Vadj values.
However when using VPK120 Board UI, "Get FMC1 recommended VADJ setting" from the AD9081 EEPROM, it reads: Min: 1600mV, Max: 2000mV.
So can I use Vadj of 1.5V, with the level shifters mentioned above? Or should it indeed be at least 1.6V?
Many thanks,
EW1