Post Go back to editing

ad9081-fmca-ebz + ZCU102, Measured Link Clock has a wrong value

Category: Hardware
Product Number: zcu102

Dear all, 

I would like to ask for help, first trying to understand the source of the problem and then to solve it.

I'm having a problem with the reported clock value of the JESD204 link frequency value of an ad9081-fmca using a ZCU102 carrier board, running the kuiper linux provided by AD.

I've generated the project with:

make JESD_MODE=8B10B RX_RATE=5 TX_RATE=10 RX_JESD_M=4 RX_JESD_L=4 RX_JESD_S=1 RX_JESD_F=2 RX_JESD_NP=16 TX_JESD_M=4 TX_JESD_L=4 TX_JESD_S=1 TX_JESD_F=2 TX_JESD_NP=16

Before running the make I changed the timing constraints file according to the frequencies resulting of the mode and lane rates, fpga_refclk_in = 500 MHz, rx_device_clk = 125 MHz and tx_device_clk = 250 MHz.

This is the part of the constraint file for the definition of the clocks:

# Primary clock definitions
create_clock -period 2 -name refclk [get_ports fpga_refclk_in_p]

# device clock
create_clock -period 4 -name tx_device_clk [get_ports clkin6_p]
create_clock -period 8 -name rx_device_clk [get_ports clkin10_p]


# Constraint SYSREFs
# Assumption is that REFCLK and SYSREF have similar propagation delay,
# and the SYSREF is a source synchronous Edge-Aligned signal to REFCLK
set_input_delay -clock [get_clocks tx_device_clk] 4 [get_ports sysref2_*]

The frequency values were also updated into the device tree.

This is the output of the jesd_status command:

   

Here it appears the first error/warning, the measured value of the rx link clock is different from the one it should be.

Then, if I search for the reported clocks I see:

cat /sys/kernel/debug/clk/clk_summary

                 enable    prepare    protect                                   duty
clock            count     count      count      rate   accuracy     phase     cycle       nshot
----------------------------------------------------------------------------------------------------
clkin2_0          0        0          0          0          0          0        50000        0
clkin1_0          0        0          0          0          0          0        50000        0
si570_mgt         0        0          0          148499999  0          0        50000        0
si570_user        0        0          0          299999997  0          0        50000        0
hmc7044_out13     0        0          0          1953125    0          0        50000        0
hmc7044_out12     4        4          2          500000000  0          0        50000        0
tx_out_clk        0        0          0          250000000  0          0        50000        0
tx_gt_clk         1        1          1          10000000   0          0        50000        0
rx_out_clk        0        0          0          250000000  0          0        50000        0
rx_gt_clk         1        1          1          5000000    0          0        50000        0
hmc7044_out10     1        1          0          125000000  0          0        50000        0
hmc7044_out6      1        1          0          250000000  0          0        50000        0
hmc7044_out3      0        0          0          1953125    0          0        50000        0
hmc7044_out2      2        2          0          500000000  0          0        50000        0

I couldn't understand if the meaasured link clock os correctly measured or if we are making something wrong here with the parameters we included into the make.

The values were generated with the JESD mode tool.

If I change the PL plclk0 frequency from 100MH to 150 MHz, the reported values are these:

   

Then, making from the clock summary output I see this:

cat /sys/kernel/debug/clk/clk_summary

                                      enable       prepare      protect                                              duty
clock                                 count        count        count          rate        accuracy    phase         cycle    nshot
----------------------------------------------------------------------------------------------------------------------------------
clkin2_0                                0            0              0            0           0             0         50000         0
clkin1_0                                0            0              0            0           0             0         50000         0
si570_mgt                               0            0              0            148499999   0             0         50000         0
si570_user                              0            0              0            299999997   0             0         50000         0
hmc7044_out13                           0            0              0            1953125     0             0         50000         0
hmc7044_out12                           4            4              2            500000000   0             0         50000         0
     tx_out_clk                         0            0              0            250000000   0             0         50000         0
     tx_gt_clk                          1            1              1            10000000    0             0         50000         0
     rx_out_clk                         0            0              0            250000000   0             0         50000         0
     rx_gt_clk                          1            1              1            5000000     0             0         50000         0
hmc7044_out10                           1            1              0            125000000   0             0         50000         0
hmc7044_out6                            1            1              0            250000000   0             0         50000         0
hmc7044_out3                            0            0              0            1953125     0             0         50000         0
hmc7044_out2                            2            2              0            250000000   0             0         50000         0

1_ I would like to understand first, why the reported values are different if I didn't change the frequency values of the HMC7044.

2_ Then, how do I fix this problem?

3_ Is it any guide about how the scripts configure all the internal parameters of the JESD204 interfaces?

4_ Not related to this, but how can I select the internal PBRS generator?

Thank you in advance! 

Parents
  • Can you share with me the changes you did in the dts?

    3_ Is it any guide about how the scripts configure all the internal parameters of the JESD204 interfaces?

    Sadly, we don't have.

    4_ Not related to this, but how can I select the internal PBRS generator?

    Are you referring to this one maybe? https://analogdevicesinc.github.io/hdl/library/axi_adxcvr/index.html#physical-layer-prbs-testing 

  • Sure! I include here only the lines we modified:

    ...
            adi,pll2-output-frequency = <3000000000>;
    ...
            hmc7044_c6: channel@6 {
                reg = <6>;
                adi,extended-name = "CORE_CLK_TX";
                adi,divider = <12>;                                 // 250 MHz (Lane Rate/40)
                adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
            };
            hmc7044_c10: channel@10 {
                reg = <10>;
                adi,extended-name = "CORE_CLK_RX_ALT";
                adi,divider = <24>;                                 // 125 MHz (Lane Rate/40)
                adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
            };
            hmc7044_c12: channel@12 {
                reg = <12>;
                adi,extended-name = "FPGA_REFCLK2";
                adi,divider = <6>;                                  // 500 MHz (Lane Rate/20)
                adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
            };
    ...
                adi,dac-frequency-hz = /bits/ 64 <8000000000>;
    ...
                adi,channelizer-paths {
                    #address-cells = <1>;
                    #size-cells = <0>;
                    adi,interpolation = <2>;
    ...
                adi,jesd-links {
                    #size-cells = <0>;
                    #address-cells = <1>;

                    ad9081_tx_jesd_l0: link@0 {
                        #address-cells = <1>;
                        #size-cells = <0>;
                        reg = <0>;

                        adi,logical-lane-mapping = /bits/ 8 <0 2 7 7 1 7 7 3>;

                        adi,link-mode = <10>;               /* JESD Quick Configuration Mode */
                        adi,subclass = <1>;                 /* JESD SUBCLASS 0,1,2 */
                        adi,version = <1>;                  /* JESD VERSION 0=204A,1=204B,2=204C */
                        adi,dual-link = <0>;                /* JESD Dual Link Mode */

                        adi,converters-per-device = <4>;    /* JESD M */
                        adi,octets-per-frame = <2>;         /* JESD F */

                        adi,frames-per-multiframe = <32>;   /* JESD K */
                        adi,converter-resolution = <16>;    /* JESD N */
                        adi,bits-per-sample = <16>;         /* JESD NP' */
                        adi,control-bits-per-sample = <0>;  /* JESD CS */
                        adi,lanes-per-device = <4>;         /* JESD L */
                        adi,samples-per-converter-per-frame = <1>; /* JESD S */
                        adi,high-density = <0>;             /* JESD HD */
                        adi,tpl-phase-adjust = <3>;
                    };
    ...

                adi,adc-frequency-hz = /bits/ 64 <4000000000>;
                    ad9081_adc0: adc@0 {
                        reg = <0>;
                        adi,decimation = <4>;
                        adi,nco-frequency-shift-hz =  /bits/ 64 <400000000>;
                        adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
                        //adi,crossbar-select = <&ad9081_rx_fddc_chan0>, <&ad9081_rx_fddc_chan2>; /* Static for now */
                    };
                    ad9081_adc1: adc@1 {
                        reg = <1>;
                        adi,decimation = <4>;
                        adi,nco-frequency-shift-hz =  /bits/ 64 <(-400000000)>;
                        adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
                        //adi,crossbar-select = <&ad9081_rx_fddc_chan1>, <&ad9081_rx_fddc_chan3>; /* Static for now */
                    };
                    ad9081_rx_fddc_chan0: channel@0 {
                        reg = <0>;
                        adi,decimation = <4>;
                        adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
                        adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

                    };
                    ad9081_rx_fddc_chan1: channel@1 {
                        reg = <1>;
                        adi,decimation = <4>;
                        adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
                        adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

                    };
    ...
                    ad9081_rx_jesd_l0: link@0 {
                        reg = <0>;
                        adi,converter-select =
                            <&ad9081_rx_fddc_chan0 FDDC_I>, <&ad9081_rx_fddc_chan0 FDDC_Q>,
                            <&ad9081_rx_fddc_chan1 FDDC_I>, <&ad9081_rx_fddc_chan1 FDDC_Q>; // Attention to SEMICOLON
                            // <&ad9081_rx_fddc_chan4 FDDC_I>, <&ad9081_rx_fddc_chan4 FDDC_Q>,
                            // <&ad9081_rx_fddc_chan5 FDDC_I>, <&ad9081_rx_fddc_chan5 FDDC_Q>;

                        adi,logical-lane-mapping = /bits/ 8 <2 0 7 7 7 7 3 1>;

                        adi,link-mode = <11>;               /* JESD Quick Configuration Mode */
                        adi,subclass = <1>;                 /* JESD SUBCLASS 0,1,2 */
                        adi,version = <1>;                  /* JESD VERSION 0=204A,1=204B,2=204C */
                        adi,dual-link = <0>;                /* JESD Dual Link Mode */

                        adi,converters-per-device = <4>;    /* JESD M */
                        adi,octets-per-frame = <2>;         /* JESD F */

                        adi,frames-per-multiframe = <32>;   /* JESD K */
                        adi,converter-resolution = <16>;    /* JESD N */
                        adi,bits-per-sample = <16>;         /* JESD NP' */
                        adi,control-bits-per-sample = <0>;  /* JESD CS */
                        adi,lanes-per-device = <4>;         /* JESD L */
                        adi,samples-per-converter-per-frame = <1>; /* JESD S */
                        adi,high-density = <0>;             /* JESD HD */
                    };
Reply
  • Sure! I include here only the lines we modified:

    ...
            adi,pll2-output-frequency = <3000000000>;
    ...
            hmc7044_c6: channel@6 {
                reg = <6>;
                adi,extended-name = "CORE_CLK_TX";
                adi,divider = <12>;                                 // 250 MHz (Lane Rate/40)
                adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
            };
            hmc7044_c10: channel@10 {
                reg = <10>;
                adi,extended-name = "CORE_CLK_RX_ALT";
                adi,divider = <24>;                                 // 125 MHz (Lane Rate/40)
                adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
            };
            hmc7044_c12: channel@12 {
                reg = <12>;
                adi,extended-name = "FPGA_REFCLK2";
                adi,divider = <6>;                                  // 500 MHz (Lane Rate/20)
                adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
            };
    ...
                adi,dac-frequency-hz = /bits/ 64 <8000000000>;
    ...
                adi,channelizer-paths {
                    #address-cells = <1>;
                    #size-cells = <0>;
                    adi,interpolation = <2>;
    ...
                adi,jesd-links {
                    #size-cells = <0>;
                    #address-cells = <1>;

                    ad9081_tx_jesd_l0: link@0 {
                        #address-cells = <1>;
                        #size-cells = <0>;
                        reg = <0>;

                        adi,logical-lane-mapping = /bits/ 8 <0 2 7 7 1 7 7 3>;

                        adi,link-mode = <10>;               /* JESD Quick Configuration Mode */
                        adi,subclass = <1>;                 /* JESD SUBCLASS 0,1,2 */
                        adi,version = <1>;                  /* JESD VERSION 0=204A,1=204B,2=204C */
                        adi,dual-link = <0>;                /* JESD Dual Link Mode */

                        adi,converters-per-device = <4>;    /* JESD M */
                        adi,octets-per-frame = <2>;         /* JESD F */

                        adi,frames-per-multiframe = <32>;   /* JESD K */
                        adi,converter-resolution = <16>;    /* JESD N */
                        adi,bits-per-sample = <16>;         /* JESD NP' */
                        adi,control-bits-per-sample = <0>;  /* JESD CS */
                        adi,lanes-per-device = <4>;         /* JESD L */
                        adi,samples-per-converter-per-frame = <1>; /* JESD S */
                        adi,high-density = <0>;             /* JESD HD */
                        adi,tpl-phase-adjust = <3>;
                    };
    ...

                adi,adc-frequency-hz = /bits/ 64 <4000000000>;
                    ad9081_adc0: adc@0 {
                        reg = <0>;
                        adi,decimation = <4>;
                        adi,nco-frequency-shift-hz =  /bits/ 64 <400000000>;
                        adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
                        //adi,crossbar-select = <&ad9081_rx_fddc_chan0>, <&ad9081_rx_fddc_chan2>; /* Static for now */
                    };
                    ad9081_adc1: adc@1 {
                        reg = <1>;
                        adi,decimation = <4>;
                        adi,nco-frequency-shift-hz =  /bits/ 64 <(-400000000)>;
                        adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
                        //adi,crossbar-select = <&ad9081_rx_fddc_chan1>, <&ad9081_rx_fddc_chan3>; /* Static for now */
                    };
                    ad9081_rx_fddc_chan0: channel@0 {
                        reg = <0>;
                        adi,decimation = <4>;
                        adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
                        adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

                    };
                    ad9081_rx_fddc_chan1: channel@1 {
                        reg = <1>;
                        adi,decimation = <4>;
                        adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
                        adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

                    };
    ...
                    ad9081_rx_jesd_l0: link@0 {
                        reg = <0>;
                        adi,converter-select =
                            <&ad9081_rx_fddc_chan0 FDDC_I>, <&ad9081_rx_fddc_chan0 FDDC_Q>,
                            <&ad9081_rx_fddc_chan1 FDDC_I>, <&ad9081_rx_fddc_chan1 FDDC_Q>; // Attention to SEMICOLON
                            // <&ad9081_rx_fddc_chan4 FDDC_I>, <&ad9081_rx_fddc_chan4 FDDC_Q>,
                            // <&ad9081_rx_fddc_chan5 FDDC_I>, <&ad9081_rx_fddc_chan5 FDDC_Q>;

                        adi,logical-lane-mapping = /bits/ 8 <2 0 7 7 7 7 3 1>;

                        adi,link-mode = <11>;               /* JESD Quick Configuration Mode */
                        adi,subclass = <1>;                 /* JESD SUBCLASS 0,1,2 */
                        adi,version = <1>;                  /* JESD VERSION 0=204A,1=204B,2=204C */
                        adi,dual-link = <0>;                /* JESD Dual Link Mode */

                        adi,converters-per-device = <4>;    /* JESD M */
                        adi,octets-per-frame = <2>;         /* JESD F */

                        adi,frames-per-multiframe = <32>;   /* JESD K */
                        adi,converter-resolution = <16>;    /* JESD N */
                        adi,bits-per-sample = <16>;         /* JESD NP' */
                        adi,control-bits-per-sample = <0>;  /* JESD CS */
                        adi,lanes-per-device = <4>;         /* JESD L */
                        adi,samples-per-converter-per-frame = <1>; /* JESD S */
                        adi,high-density = <0>;             /* JESD HD */
                    };
Children
No Data