Sl No | Requirement | Query | |
1
|
Single ADC/DAC Port should support upto 400 MHz BandWidth.
Should also support :
2 X 200MHz
4 X 100MHz
|
Does AD9081 have support for this?. | |
If it does support this requirement, could you provide guidance on configuring the JESD204B interface(Xilinx IP)? | |||
Could you share a reference project for implementing this configuration? |
For the 400 MHz bandwidth case, the line rate becomes 19.6608 Gbps, which is not supported by a single JESD204B line. Therefore, we need to use at least 2 JESD lines. This means the JESD stream interface has to operate at a maximum of 245.76 MHz, which implies that we need to send two IQ samples per clock cycle of 245.76 MHz clock or four IQ samples per clock cycle of 122.88 MHz clock.
Could you please provide more information on how the IQ samples are packed and transmitted through the JESD stream interface(FPGA side) in the 400 MHz bandwidth case? It would be very helpful if you could connect with your engineering team and share the details on the data flow and any example projects that demonstrate this implementation. Could you please provide information about how to configure the Xilinx JESD Ip for 400 MHz.