I am using two AD9209, where all x8 Lanes of each data converters shall be used. Logic device is Xilinx FPGA GTY Transceivers
Using a single core to achieve synchronisation is not possible, since a core supports only x8 Lanes.In our case, it is x16 Lanes
To achieve Core Synchronisation. Would you please share the guidelines for both Hardware as well as RTL Perspective
Could you share the Excel for calculating the Variable and Lane Delay of the Link
Do I have to Length Match the Device Clock and SYSREF to the Logic Device and is there any requirement that the Sysref shall be continuous signal not the Single-shot Pulse