Post Go back to editing

Help in building No-OS for Zedboard and FMCOMMS2 using Vitis 2023.2

Category: Software
Product Number: AD9361
Software Version: Vivado 2023.2

Hi.. I am building a transceiver using Zedbaord + FMCOMMS2 (AD9361) board and I am using Vivado and Vitis 2023.2 on windows 11.  My target is to build a no-os or BareMetal with custom modulations blocks. The HDL version provided by analog devices is made to work with 2023.2, but its respective No-OS files are not available. Also, there is no documentation available to add user defined HDL block in the design. If anybody done this kind of setup please help me. 

I am able to build the xsa file for the given HDL files but it is not working with the No-Os files available in the github. HDL code they are recommending  vivado 2023.2 but the no-os files are not compatible for this.

Any leads are appreciated.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.