Post Go back to editing

About the Channel CPACK Utility Core IP output data in the ADRV9009 ZC706 reference design

Category: Software
Product Number: 0
Software Version: 21.2

hello, I have a question about the Channel CPACK Utility Core IP output data in the ADRV9009 ZC706 reference design.I made a testbench about this ip in a new projech,which only contains this ip core.And from the scoped image below(if it's clear enough).I think the output packed_fifo_wr_data seems wrong,unlinke it's wiki introduction,it's seems to be 0000 0000 00000 0000 4444 3333 2222 1111.It is my error?Or it is the right output.My testbench only simply input the data and give a enable signal.

and I also test when 3 channels are enabled.I am not sure it is right or wrong.and it's data is 01030201 02010302 03020103 which every single number means four same numble.

Thanks,

Cai