Hello,
I am using a ZCU102 and AD9081-FMC-EBZA with the reference design provided by ADI (images of version 2022r2). When running iio_info neither axi-ad9081-rx-hpc nor axi-ad9081-tx-hpc.
The build boots with the boot message attached. Running iio_info gives the message attached. The hmc7044 is not locking and I have not provided an external clock.
[ 6.132898] ad9081 spi1.0: 8bit r/w test failed. Write 5a but readback is 00
This message lead me to probe the spi lines on the AD9081 board, I confirmed that 0x5a is being written to the chip and 00 is getting written out. Not sure where to go from here.
Can the issue be rooted in the issue with hmc7044, and would providing an external clock fix the issue?
Can I provide an external clock to the AD9081-FMCA-EBZ and ZCU102 as described in UG-1829 Figure 30? The scheme provided is meant for a setup with ADS9-V2EBZ. If not, how can I provide an external clock with the ZCU102?
Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 5.15.0-175919-g427c94e8faa5 (jenkins@romlxbuild1) ( aarch64-xilinx-linux-gcc.real (GCC) 11.2.0, GNU ld (GNU Binutils) 2.37.20210721) #824 SMP Tue Dec 12 10:32:23 EET 2023 [ 0.000000] Machine model: ZynqMP ZCU102 Rev1.0 [ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8') [ 0.000000] printk: bootconsole [cdns0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000000000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal [mem 0x0000000100000000-0x000000087fffffff] [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000000000000-0x000000007fffffff] [ 0.000000] node 0: [mem 0x0000000800000000-0x000000087fffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000000000000-0x000000087fffffff] [ 0.000000] cma: Reserved 256 MiB at 0x0000000070000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 18 pages/cpu s34008 r8192 d31528 u73728 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1034240 [ 0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait clk_ignore_unused cpuidle.off=1 root=/dev/mmc blk0p2 rw rootwait [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes , linear) [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] software IO TLB: mapped [mem 0x000000006c000000-0x000000007000000 0] (64MB) [ 0.000000] Memory: 3758752K/4194304K available (16640K kernel code, 1690K rw data, 13016K rodata, 2624K init, 634K bss, 173408K reserved, 262144K cma-reserve d) [ 0.000000] rcu: Hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jif fies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000 [ 0.000000] Root IRQ handler: gic_handle_irq [ 0.000000] GIC: Using split EOI/Deactivate mode [ 0.000000] random: get_random_bytes called from start_kernel+0x470/0x6f8 wit h crng_init=0 [ 0.000000] arch_timer: cp15 timer(s) running at 100.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171024e7e0, max_idle_ns: 440795205315 ns [ 0.000000] sched_clock: 56 bits at 100MHz, resolution 10ns, wraps every 4398 046511100ns [ 0.008454] Console: colour dummy device 80x25 [ 0.012485] Calibrating delay loop (skipped), value calculated using timer fr equency.. 200.00 BogoMIPS (lpj=400000) [ 0.022839] pid_max: default: 32768 minimum: 301 [ 0.027534] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, line ar) [ 0.034787] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.043416] rcu: Hierarchical SRCU implementation. [ 0.047568] EFI services will not be available. [ 0.051939] smp: Bringing up secondary CPUs ... [ 0.056658] Detected VIPT I-cache on CPU1 [ 0.056698] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.057072] Detected VIPT I-cache on CPU2 [ 0.057095] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] [ 0.057441] Detected VIPT I-cache on CPU3 [ 0.057464] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] [ 0.057507] smp: Brought up 1 node, 4 CPUs [ 0.091778] SMP: Total of 4 processors activated. [ 0.096450] CPU features: detected: 32-bit EL0 Support [ 0.101554] CPU features: detected: CRC32 instructions [ 0.106695] CPU: All CPU(s) started at EL2 [ 0.110736] alternatives: patching kernel code [ 0.116150] devtmpfs: initialized [ 0.124994] Registered cp15_barrier emulation handler [ 0.125047] Registered setend emulation handler [ 0.129014] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, ma x_idle_ns: 7645041785100000 ns [ 0.138605] futex hash table entries: 1024 (order: 4, 65536 bytes, linear) [ 0.153267] pinctrl core: initialized pinctrl subsystem [ 0.154003] NET: Registered PF_NETLINK/PF_ROUTE protocol family [ 0.159792] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations [ 0.165843] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allo cations [ 0.173590] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic al locations [ 0.181358] audit: initializing netlink subsys (disabled) [ 0.186758] audit: type=2000 audit(0.120:1): state=initialized audit_enabled= 0 res=1 [ 0.187132] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.201184] ASID allocator initialised with 65536 entries [ 0.228008] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages [ 0.229069] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages [ 0.235740] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.242404] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages [ 1.333609] DRBG: Continuing without Jitter RNG [ 1.437857] raid6: neonx8 gen() 2133 MB/s [ 1.505905] raid6: neonx8 xor() 1588 MB/s [ 1.573966] raid6: neonx4 gen() 2182 MB/s [ 1.642025] raid6: neonx4 xor() 1552 MB/s [ 1.710089] raid6: neonx2 gen() 2068 MB/s [ 1.778141] raid6: neonx2 xor() 1429 MB/s [ 1.846202] raid6: neonx1 gen() 1766 MB/s [ 1.914262] raid6: neonx1 xor() 1213 MB/s [ 1.982327] raid6: int64x8 gen() 1356 MB/s [ 2.050389] raid6: int64x8 xor() 773 MB/s [ 2.118454] raid6: int64x4 gen() 1598 MB/s [ 2.186502] raid6: int64x4 xor() 846 MB/s [ 2.254576] raid6: int64x2 gen() 1397 MB/s [ 2.322629] raid6: int64x2 xor() 749 MB/s [ 2.390692] raid6: int64x1 gen() 1032 MB/s [ 2.458747] raid6: int64x1 xor() 517 MB/s [ 2.458785] raid6: using algorithm neonx4 gen() 2182 MB/s [ 2.462739] raid6: .... xor() 1552 MB/s, rmw enabled [ 2.467674] raid6: using neon recovery algorithm [ 2.472699] iommu: Default domain type: Translated [ 2.477105] iommu: DMA domain TLB invalidation policy: strict mode [ 2.483523] SCSI subsystem initialized [ 2.487198] usbcore: registered new interface driver usbfs [ 2.492525] usbcore: registered new interface driver hub [ 2.497799] usbcore: registered new device driver usb [ 2.502931] mc: Linux media interface: v0.10 [ 2.507049] videodev: Linux video capture interface: v2.00 [ 2.512537] pps_core: LinuxPPS API ver. 1 registered [ 2.517413] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giome tti <giometti@linux.it> [ 2.526504] PTP clock support registered [ 2.530406] EDAC MC: Ver: 3.0.0 [ 2.533780] zynqmp-ipi-mbox mailbox@ff990400: Registered ZynqMP IPI mbox with TX/RX channels. [ 2.542398] jesd204: created con: id=0, topo=0, link=0, /axi/spi@ff050000/hmc 7044@0 <-> /fpga-axi@0/axi-adxcvr-tx@84b60000 [ 2.552969] jesd204: created con: id=1, topo=0, link=2, /axi/spi@ff050000/hmc 7044@0 <-> /fpga-axi@0/axi-adxcvr-rx@84a60000 [ 2.563955] jesd204: created con: id=2, topo=0, link=0, /fpga-axi@0/axi-adxcv r-tx@84b60000 <-> /fpga-axi@0/axi-jesd204-tx@84b90000 [ 2.575631] jesd204: created con: id=3, topo=0, link=2, /fpga-axi@0/axi-adxcv r-rx@84a60000 <-> /fpga-axi@0/axi-jesd204-rx@84a90000 [ 2.587335] jesd204: created con: id=4, topo=0, link=0, /fpga-axi@0/axi-jesd2 04-tx@84b90000 <-> /fpga-axi@0/axi-ad9081-tx-hpc@84b10000 [ 2.599331] jesd204: created con: id=5, topo=0, link=2, /fpga-axi@0/axi-jesd2 04-rx@84a90000 <-> /fpga-axi@0/axi-ad9081-rx-hpc@84a10000 [ 2.611378] jesd204: created con: id=6, topo=0, link=2, /fpga-axi@0/axi-ad908 1-rx-hpc@84a10000 <-> /axi/spi@ff040000/ad9081@0 [ 2.622599] jesd204: created con: id=7, topo=0, link=0, /fpga-axi@0/axi-ad908 1-tx-hpc@84b10000 <-> /axi/spi@ff040000/ad9081@0 [ 2.633850] jesd204: /axi/spi@ff040000/ad9081@0: JESD204[0:2] transition unin itialized -> initialized [ 2.643010] jesd204: /axi/spi@ff040000/ad9081@0: JESD204[0:0] transition unin itialized -> initialized [ 2.652180] jesd204: found 8 devices and 1 topologies [ 2.657224] FPGA manager framework [ 2.660701] Advanced Linux Sound Architecture Driver Initialized. [ 2.667032] Bluetooth: Core ver 2.22 [ 2.670181] NET: Registered PF_BLUETOOTH protocol family [ 2.675449] Bluetooth: HCI device and connection manager initialized [ 2.681766] Bluetooth: HCI socket layer initialized [ 2.686608] Bluetooth: L2CAP socket layer initialized [ 2.691629] Bluetooth: SCO socket layer initialized [ 2.696896] clocksource: Switched to clocksource arch_sys_counter [ 2.702634] VFS: Disk quotas dquot_6.6.0 [ 2.706453] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 2.717637] NET: Registered PF_INET protocol family [ 2.718207] IP idents hash table entries: 65536 (order: 7, 524288 bytes, line ar) [ 2.726976] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 3276 8 bytes, linear) [ 2.733962] TCP established hash table entries: 32768 (order: 6, 262144 bytes , linear) [ 2.741994] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linea r) [ 2.749439] TCP: Hash tables configured (established 32768 bind 32768) [ 2.755617] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear) [ 2.762278] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear) [ 2.769458] NET: Registered PF_UNIX/PF_LOCAL protocol family [ 2.775223] RPC: Registered named UNIX socket transport module. [ 2.780811] RPC: Registered udp transport module. [ 2.785480] RPC: Registered tcp transport module. [ 2.790149] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 2.797146] PCI: CLS 0 bytes, default 64 [ 2.800794] armv8-pmu pmu: hw perfevents: no interrupt-affinity property, gue ssing. [ 2.808219] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters av ailable [ 2.816609] Initialise system trusted keyrings [ 2.820242] workingset: timestamp_bits=62 max_order=20 bucket_order=0 [ 2.827129] NFS: Registering the id_resolver key type [ 2.831591] Key type id_resolver registered [ 2.835734] Key type id_legacy registered [ 2.839724] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 2.846374] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering ... [ 2.853737] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. [ 2.860903] fuse: init (API version 7.34) [ 2.900409] NET: Registered PF_ALG protocol family [ 2.900459] xor: measuring software checksum speed [ 2.908486] 8regs : 2363 MB/sec [ 2.912155] 32regs : 2799 MB/sec [ 2.917231] arm64_neon : 2308 MB/sec [ 2.917288] xor: using function: 32regs (2799 MB/sec) [ 2.922311] Key type asymmetric registered [ 2.926375] Asymmetric key parser 'x509' registered [ 2.931250] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 2 46) [ 2.938574] io scheduler mq-deadline registered [ 2.943070] io scheduler kyber registered [ 2.973213] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled [ 2.976149] cacheinfo: Unable to detect cache hierarchy for CPU 0 [ 2.984026] brd: module loaded [ 2.987393] loop: module loaded [ 2.987999] Registered mathworks_ip class [ 2.992156] libphy: Fixed MDIO Bus: probed [ 2.995306] tun: Universal TUN/TAP device driver, 1.6 [ 2.999274] CAN device driver interface [ 3.003856] usbcore: registered new interface driver asix [ 3.008398] usbcore: registered new interface driver ax88179_178a [ 3.014436] usbcore: registered new interface driver cdc_ether [ 3.020238] usbcore: registered new interface driver net1080 [ 3.025854] usbcore: registered new interface driver cdc_subset [ 3.031736] usbcore: registered new interface driver zaurus [ 3.037282] usbcore: registered new interface driver cdc_ncm [ 3.043529] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 3.049364] ehci-pci: EHCI PCI platform driver [ 3.054162] usbcore: registered new interface driver uas [ 3.059081] usbcore: registered new interface driver usb-storage [ 3.065071] usbcore: registered new interface driver usbserial_generic [ 3.071521] usbserial: USB Serial support registered for generic [ 3.077492] usbcore: registered new interface driver ftdi_sio [ 3.083195] usbserial: USB Serial support registered for FTDI USB Serial Devi ce [ 3.090467] usbcore: registered new interface driver upd78f0730 [ 3.096343] usbserial: USB Serial support registered for upd78f0730 [ 3.104019] rtc_zynqmp ffa60000.rtc: registered as rtc0 [ 3.107761] rtc_zynqmp ffa60000.rtc: setting system clock to 1974-05-03T01:27 :23 UTC (136776443) [ 3.116548] i2c_dev: i2c /dev entries driver [ 3.122610] usbcore: registered new interface driver uvcvideo [ 3.127906] Bluetooth: HCI UART driver ver 2.3 [ 3.130851] Bluetooth: HCI UART protocol H4 registered [ 3.135950] Bluetooth: HCI UART protocol BCSP registered [ 3.141241] Bluetooth: HCI UART protocol LL registered [ 3.146328] Bluetooth: HCI UART protocol ATH3K registered [ 3.151703] Bluetooth: HCI UART protocol Three-wire (H5) registered [ 3.157958] Bluetooth: HCI UART protocol Intel registered [ 3.163294] Bluetooth: HCI UART protocol QCA registered [ 3.168495] usbcore: registered new interface driver bcm203x [ 3.174118] usbcore: registered new interface driver bpa10x [ 3.179653] usbcore: registered new interface driver bfusb [ 3.185115] usbcore: registered new interface driver btusb [ 3.190565] usbcore: registered new interface driver ath3k [ 3.196054] EDAC MC: ECC not enabled [ 3.199686] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac control ler zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT) [ 3.212003] sdhci: Secure Digital Host Controller Interface driver [ 3.217778] sdhci: Copyright(c) Pierre Ossman [ 3.222103] sdhci-pltfm: SDHCI platform and OF driver helper [ 3.228150] ledtrig-cpu: registered to indicate activity on CPUs [ 3.233842] SMCCC: SOC_ID: ID = jep106:0049:0000 Revision = 0x24738093 [ 3.240250] zynqmp_firmware_probe Platform Management API v1.1 [ 3.245980] zynqmp_firmware_probe Trustzone version v1.0 [ 3.281432] zynqmp-aes firmware:zynqmp-firmware:zynqmp-aes: will run requests pump with realtime priority [ 3.297057] zynqmp-keccak-384 firmware:zynqmp-firmware:sha384: The zynqmp-sha -deprecated driver shall be deprecated in 2022.2 and removed in 2023.1 release [ 3.305358] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384) [ 3.311624] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa) [ 3.317125] usbcore: registered new interface driver usbhid [ 3.322514] usbhid: USB HID core driver [ 3.333255] axi_sysid 85000000.axi-sysid-0: AXI System ID core version (1.01. a) found [ 3.335615] axi_sysid 85000000.axi-sysid-0: [ad9081_fmca_ebz] on [zcu102] git branch <hdl_2022_r2> git <b31d4fbba87a96f329f858da3118771503c7c6b4> clean [2023 -11-01 14:35:49] UTC [ 3.351763] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered [ 3.358058] usbcore: registered new interface driver snd-usb-audio [ 3.365588] pktgen: Packet Generator for packet performance testing. Version: 2.75 [ 3.371654] Initializing XFRM netlink socket [ 3.375571] NET: Registered PF_INET6 protocol family [ 3.380904] Segment Routing with IPv6 [ 3.384064] In-situ OAM (IOAM) with IPv6 [ 3.387998] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 3.394167] NET: Registered PF_PACKET protocol family [ 3.398858] NET: Registered PF_KEY protocol family [ 3.403693] can: controller area network core [ 3.407961] NET: Registered PF_CAN protocol family [ 3.412691] can: raw protocol [ 3.415630] can: broadcast manager protocol [ 3.419785] can: netlink gateway - max_hops=1 [ 3.424173] Bluetooth: RFCOMM TTY layer initialized [ 3.428958] Bluetooth: RFCOMM socket layer initialized [ 3.434064] Bluetooth: RFCOMM ver 1.11 [ 3.437778] Bluetooth: BNEP (Ethernet Emulation) ver 1.3 [ 3.443050] Bluetooth: BNEP filters: protocol multicast [ 3.448242] Bluetooth: BNEP socket layer initialized [ 3.453170] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 [ 3.459054] Bluetooth: HIDP socket layer initialized [ 3.464111] 9pnet: Installing 9P2000 support [ 3.468233] NET: Registered PF_IEEE802154 protocol family [ 3.473605] Key type dns_resolver registered [ 3.478060] registered taskstats version 1 [ 3.481890] Loading compiled-in X.509 certificates [ 3.487118] Btrfs loaded, crc32c=crc32c-generic, zoned=no, fsverity=no [ 3.501785] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 49, base_baud = 6249999) is a xuartps [ 3.510818] printk: console [ttyPS0] enabled [ 3.510818] printk: console [ttyPS0] enabled [ 3.515113] printk: bootconsole [cdns0] disabled [ 3.515113] printk: bootconsole [cdns0] disabled [ 3.524650] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 50, base_baud = 6249999) is a xuartps [ 3.537851] of-fpga-region fpga-full: FPGA Region probed [ 3.544397] nwl-pcie fd0e0000.pcie: host bridge /axi/pcie@fd0e0000 ranges: [ 3.551299] nwl-pcie fd0e0000.pcie: MEM 0x00e0000000..0x00efffffff -> 0x 00e0000000 [ 3.559312] nwl-pcie fd0e0000.pcie: MEM 0x0600000000..0x07ffffffff -> 0x 0600000000 [ 3.567388] nwl-pcie fd0e0000.pcie: Link is DOWN [ 3.572154] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00 [ 3.578337] pci_bus 0000:00: root bus resource [bus 00-ff] [ 3.583816] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff] [ 3.590683] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff p ref] [ 3.598191] pci 0000:00:00.0: [10ee:d021] type 01 class 0x060400 [ 3.604255] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot [ 3.614890] pci 0000:00:00.0: PCI bridge to [bus 01-0c] [ 3.620791] xilinx-zynqmp-dma fd500000.dma-controller: ZynqMP DMA driver Prob e success [ 3.628869] xilinx-zynqmp-dma fd510000.dma-controller: ZynqMP DMA driver Prob e success [ 3.636972] xilinx-zynqmp-dma fd520000.dma-controller: ZynqMP DMA driver Prob e success [ 3.645048] xilinx-zynqmp-dma fd530000.dma-controller: ZynqMP DMA driver Prob e success [ 3.653132] xilinx-zynqmp-dma fd540000.dma-controller: ZynqMP DMA driver Prob e success [ 3.661209] xilinx-zynqmp-dma fd550000.dma-controller: ZynqMP DMA driver Prob e success [ 3.669295] xilinx-zynqmp-dma fd560000.dma-controller: ZynqMP DMA driver Prob e success [ 3.677370] xilinx-zynqmp-dma fd570000.dma-controller: ZynqMP DMA driver Prob e success [ 3.685683] xilinx-zynqmp-dpdma fd4c0000.dma-controller: Xilinx DPDMA engine is probed [ 3.695924] hmc7044 spi2.0: Read/Write check failed (0x0) [ 3.749509] hmc7044 spi2.0: Probed, SPI read support failed [ 3.755421] jesd204: /axi/spi@ff050000/hmc7044@0,jesd204:1,parent=spi2.0: Usi ng as SYSREF provider [ 3.764935] spi-nor spi0.0: SPI-NOR-UniqueID 364c9200151100290076e3cf9a2f [ 3.771723] spi-nor spi0.0: found mt25qu512a, expected m25p80 [ 3.777851] spi-nor spi0.0: mt25qu512a (131072 Kbytes) [ 3.783014] 4 fixed-partitions partitions found on MTD device spi0.0 [ 3.789362] Creating 4 MTD partitions on "spi0.0": [ 3.794152] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot" [ 3.800734] 0x000000100000-0x000000600000 : "qspi-linux" [ 3.806762] 0x000000600000-0x000000620000 : "qspi-device-tree" [ 3.813299] 0x000000620000-0x000000c00000 : "qspi-rootfs" [ 3.820276] xilinx_can ff070000.can can0: TDC Offset value not in range [ 3.828516] macb ff0e0000.ethernet: Not enabling partial store and forward [ 3.836074] libphy: MACB_mii_bus: probed [ 3.840680] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e 0000 irq 30 (00:0a:35:04:b7:36) [ 3.850796] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM [ 3.857310] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM [ 3.863788] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM [ 3.870262] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM [ 3.877613] pca953x 0-0020: supply vcc not found, using dummy regulator [ 3.884302] pca953x 0-0020: using no AI [ 3.888791] gpio-318 (sel0): hogged as output/low [ 3.893697] gpio-319 (sel1): hogged as output/high [ 3.898683] gpio-320 (sel2): hogged as output/high [ 3.903671] gpio-321 (sel3): hogged as output/high [ 3.908827] pca953x 0-0021: supply vcc not found, using dummy regulator [ 3.915501] pca953x 0-0021: using no AI [ 3.920962] ina2xx 2-0040: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.927950] ina2xx 2-0041: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.934939] ina2xx 2-0042: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.941926] ina2xx 2-0043: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.948923] ina2xx 2-0044: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.955910] ina2xx 2-0045: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.962895] ina2xx 2-0046: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.969887] ina2xx 2-0047: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.976947] ina2xx 2-004a: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.983935] ina2xx 2-004b: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.990343] i2c i2c-0: Added multiplexed i2c bus 2 [ 3.995887] ina2xx 3-0040: power monitor ina226 (Rshunt = 2000 uOhm) [ 4.002874] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm) [ 4.009730] random: fast init done [ 4.013203] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm) [ 4.020198] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm) [ 4.027190] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm) [ 4.034178] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm) [ 4.041167] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm) [ 4.048162] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm) [ 4.054571] i2c i2c-0: Added multiplexed i2c bus 3 [ 4.110347] i2c i2c-0: Added multiplexed i2c bus 4 [ 4.115304] i2c i2c-0: Added multiplexed i2c bus 5 [ 4.120097] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca95 44 [ 4.127474] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 32 [ 4.134885] at24 6-0054: supply vcc not found, using dummy regulator [ 4.141783] at24 6-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write [ 4.148538] i2c i2c-1: Added multiplexed i2c bus 6 [ 4.153896] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for o ut [ 4.161206] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for o ut [ 4.168511] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for o ut [ 4.175810] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for o ut [ 4.183110] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for o ut [ 4.190410] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for o ut [ 4.197710] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for o ut [ 4.205010] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for o ut [ 4.213411] si5341 7-0036: Chip: 5341 Grade: 1 Rev: 1 [ 4.251954] i2c i2c-1: Added multiplexed i2c bus 7 [ 4.259617] si570 8-005d: registered, current frequency 300000000 Hz [ 4.266027] i2c i2c-1: Added multiplexed i2c bus 8 [ 4.285809] si570 9-005d: registered, current frequency 148500000 Hz [ 4.292213] i2c i2c-1: Added multiplexed i2c bus 9 [ 4.297235] si5324 10-0069: si5328 probed [ 4.365304] si5324 10-0069: si5328 probe successful [ 4.370240] i2c i2c-1: Added multiplexed i2c bus 10 [ 4.375281] i2c i2c-1: Added multiplexed i2c bus 11 [ 4.380309] i2c i2c-1: Added multiplexed i2c bus 12 [ 4.385333] i2c i2c-1: Added multiplexed i2c bus 13 [ 4.390210] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pc a9548 [ 4.398291] at24 14-0050: supply vcc not found, using dummy regulator [ 4.431145] i2c i2c-1: Added multiplexed i2c bus 14 [ 4.436220] i2c i2c-1: Added multiplexed i2c bus 15 [ 4.441266] i2c i2c-1: Added multiplexed i2c bus 16 [ 4.446307] i2c i2c-1: Added multiplexed i2c bus 17 [ 4.451354] i2c i2c-1: Added multiplexed i2c bus 18 [ 4.456391] i2c i2c-1: Added multiplexed i2c bus 19 [ 4.461427] i2c i2c-1: Added multiplexed i2c bus 20 [ 4.466468] i2c i2c-1: Added multiplexed i2c bus 21 [ 4.471342] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pc a9548 [ 4.478960] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 33 [ 4.488245] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer with timeout 60 s [ 4.499377] axi_adxcvr 84a60000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.05.a) using CPLL on GTH4 at 0x84A60000. Number of lanes: 4. [ 4.511527] axi_adxcvr 84b60000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.05.a) using QPLL on GTH4 at 0x84B60000. Number of lanes: 4. [ 4.523162] axi-jesd204-rx 84a90000.axi-jesd204-rx: AXI-JESD204-RX (1.07.a) a t 0x84A90000. Encoder 8b10b, width 4/4, lanes 4, jesd204-fsm. [ 4.530072] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit [ 4.535931] axi-jesd204-tx 84b90000.axi-jesd204-tx: AXI-JESD204-TX (1.06.a) a t 0x84B90000. Encoder 8b10b, width 4/4, lanes 4, jesd204-fsm. [ 4.556863] zynqmp-display fd4a0000.display: vtc bridge property not present [ 4.566540] xilinx-dp-snd-codec fd4a0000.display:zynqmp_dp_snd_codec0: Failed to get required clock freq [ 4.576030] xilinx-dp-snd-codec: probe of fd4a0000.display:zynqmp_dp_snd_code c0 failed with error -22 [ 4.585511] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PC M probed [ 4.593586] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PC M probed [ 4.601772] OF: graph: no port node found in /axi/display@fd4a0000 [ 4.608289] xlnx-drm xlnx-drm.0: bound fd4a0000.display (ops 0xffffffc0111124 10) [ 4.650787] mmc0: new high speed SDHC card at address e624 [ 4.656613] mmcblk0: mmc0:e624 SL16G 14.8 GiB [ 4.666390] mmcblk0: p1 p2 p3 [ 5.692919] zynqmp-display fd4a0000.display: [drm] Cannot find any crtc or si zes [ 5.700550] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.display on min or 0 [ 5.708051] zynqmp-display fd4a0000.display: ZynqMP DisplayPort Subsystem dri ver probed [ 5.716309] ahci-ceva fd0c0000.ahci: supply ahci not found, using dummy regul ator [ 5.723861] ahci-ceva fd0c0000.ahci: supply phy not found, using dummy regula tor [ 5.731323] ahci-ceva fd0c0000.ahci: supply target not found, using dummy reg ulator [ 5.739158] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0 x3 impl platform mode [ 5.748115] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fb s pio slum part ccc sds apst [ 5.758544] scsi host0: ahci-ceva [ 5.762131] scsi host1: ahci-ceva [ 5.765546] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x1 00 irq 45 [ 5.773460] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x1 80 irq 45 [ 5.782141] ad9081 spi1.0: supply vdd not found, using dummy regulator [ 6.095159] ata2: SATA link down (SStatus 0 SControl 330) [ 6.100573] ata1: SATA link down (SStatus 0 SControl 330) [ 6.776917] zynqmp-display fd4a0000.display: [drm] Cannot find any crtc or si zes [ 6.945317] ad9081 spi1.0: 8bit r/w test failed. Write 5a but readback is ff. [ 6.952447] ad9081 spi1.0: reset/init failed (-50) [ 6.977832] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 6.983324] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus nu mber 1 [ 6.991069] xhci-hcd xhci-hcd.1.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x0000000002010890 [ 7.000486] xhci-hcd xhci-hcd.1.auto: irq 59, io mem 0xfe200000 [ 7.006497] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 7.011977] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus nu mber 2 [ 7.019632] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed [ 7.026269] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bc dDevice= 5.15 [ 7.034535] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber= 1 [ 7.041754] usb usb1: Product: xHCI Host Controller [ 7.046624] usb usb1: Manufacturer: Linux 5.15.0-175919-g427c94e8faa5 xhci-hc d [ 7.053846] usb usb1: SerialNumber: xhci-hcd.1.auto [ 7.059021] hub 1-0:1.0: USB hub found [ 7.062790] hub 1-0:1.0: 1 port detected [ 7.067001] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bc dDevice= 5.15 [ 7.075262] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber= 1 [ 7.082481] usb usb2: Product: xHCI Host Controller [ 7.087349] usb usb2: Manufacturer: Linux 5.15.0-175919-g427c94e8faa5 xhci-hc d [ 7.094566] usb usb2: SerialNumber: xhci-hcd.1.auto [ 7.099676] hub 2-0:1.0: USB hub found [ 7.103440] hub 2-0:1.0: 1 port detected [ 7.116955] input: gpio-keys as /devices/platform/gpio-keys/input/input0 [ 7.124089] of_cfs_init [ 7.126555] of_cfs_init: OK [ 7.129531] cfg80211: Loading compiled-in X.509 certificates for regulatory d atabase [ 7.266885] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 7.273412] clk: Not disabling unused clocks [ 7.277961] ALSA device list: [ 7.280922] No soundcards found. [ 7.284581] platform regulatory.0: Direct firmware load for regulatory.db fai led with error -2 [ 7.293195] cfg80211: failed to load regulatory.db [ 7.332901] usb 1-1: new high-speed USB device number 2 using xhci-hcd [ 7.485113] usb 1-1: New USB device found, idVendor=1a40, idProduct=0101, bcd Device= 1.11 [ 7.493308] usb 1-1: New USB device strings: Mfr=0, Product=1, SerialNumber=0 [ 7.500446] usb 1-1: Product: USB 2.0 Hub [ 7.538304] hub 1-1:1.0: USB hub found [ 7.542085] hub 1-1:1.0: 4 ports detected [ 7.576345] EXT4-fs (mmcblk0p2): recovery complete [ 7.582188] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. O pts: (null). Quota mode: none. [ 7.591966] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 7.608947] devtmpfs: mounted [ 7.612623] Freeing unused kernel memory: 2624K [ 7.617288] Run /sbin/init as init process [ 7.936917] usb 1-1.1: new low-speed USB device number 3 using xhci-hcd [ 8.075068] systemd[1]: System time before build time, advancing clock. [ 8.127194] systemd[1]: systemd 247.3-7+rpi1+deb11u2 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRY PT +GNUTLS +ACL +XZ +LZ4 +ZSTD +SECCOMP +BLKID +ELFUTILS +KMOD +IDN2 -IDN +PCRE2 default-hierarchy=unified) [ 8.148497] usb 1-1.1: New USB device found, idVendor=04f2, idProduct=0939, b cdDevice= 1.00 [ 8.151169] systemd[1]: Detected architecture arm64. [ 8.158906] usb 1-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber =0 [ 8.171160] usb 1-1.1: Product: USB Optical Mouse [ 8.175858] usb 1-1.1: Manufacturer: PixArt Welcome to Kuiper GNU/Linux 11.2 (bullseye)! [ 8.204359] systemd[1]: Set hostname to <analog>. [ 8.244347] input: PixArt USB Optical Mouse as /devices/platform/axi/ff9d0000 .usb0/fe200000.usb/xhci-hcd.1.auto/usb1/1-1/1-1.1/1-1.1:1.0/0003:04F2:0939.0001/ input/input1 [ 8.259588] hid-generic 0003:04F2:0939.0001: input: USB HID v1.11 Mouse [PixA rt USB Optical Mouse] on usb-xhci-hcd.1.auto-1.1/input0 [ 8.448912] usb 1-1.2: new low-speed USB device number 4 using xhci-hcd [ 8.664557] usb 1-1.2: New USB device found, idVendor=04f2, idProduct=0833, b cdDevice= 2.30 [ 8.672931] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber =0 [ 8.680240] usb 1-1.2: Product: USB Keyboard [ 8.684512] usb 1-1.2: Manufacturer: CHICONY [ 8.758186] input: CHICONY USB Keyboard as /devices/platform/axi/ff9d0000.usb 0/fe200000.usb/xhci-hcd.1.auto/usb1/1-1/1-1.2/1-1.2:1.0/0003:04F2:0833.0002/inpu t/input2 [ 8.833134] hid-generic 0003:04F2:0833.0002: input: USB HID v1.11 Keyboard [C HICONY USB Keyboard] on usb-xhci-hcd.1.auto-1.2/input0 [ 8.852201] input: CHICONY USB Keyboard System Control as /devices/platform/a xi/ff9d0000.usb0/fe200000.usb/xhci-hcd.1.auto/usb1/1-1/1-1.2/1-1.2:1.1/0003:04F2 :0833.0003/input/input3 [ 8.925082] input: CHICONY USB Keyboard Consumer Control as /devices/platform /axi/ff9d0000.usb0/fe200000.usb/xhci-hcd.1.auto/usb1/1-1/1-1.2/1-1.2:1.1/0003:04 F2:0833.0003/input/input4 [ 8.941522] input: CHICONY USB Keyboard as /devices/platform/axi/ff9d0000.usb 0/fe200000.usb/xhci-hcd.1.auto/usb1/1-1/1-1.2/1-1.2:1.1/0003:04F2:0833.0003/inpu t/input5 [ 8.956500] hid-generic 0003:04F2:0833.0003: input,hiddev96: USB HID v1.11 De vice [CHICONY USB Keyboard] on usb-xhci-hcd.1.auto-1.2/input1 [ 9.555036] systemd[1]: /lib/systemd/system/plymouth-start.service:16: Unit c onfigured to use KillMode=none. This is unsafe, as it disables systemd's process lifecycle management for the service. Please update your service to use a safer KillMode=, such as 'mixed' or 'control-group'. Support for KillMode=none is dep recated and will eventually be removed. [ 9.763786] systemd[1]: Queued start job for default target Graphical Interfa ce. [ 9.772400] random: systemd: uninitialized urandom read (16 bytes read) [ 9.779240] systemd[1]: system-getty.slice: unit configures an IP firewall, b ut the local system does not support BPF/cgroup firewalling. [ 9.791603] systemd[1]: (This warning is only shown for the first unit using IP firewalling.) [ 9.800683] systemd[1]: Created slice system-getty.slice. [ OK ] Created slice system-getty.slice. [ 9.821001] random: systemd: uninitialized urandom read (16 bytes read) [ 9.827989] systemd[1]: Created slice system-modprobe.slice. [ OK ] Created slice system-modprobe.slice. [ 9.848985] random: systemd: uninitialized urandom read (16 bytes read) [ 9.855953] systemd[1]: Created slice system-serial\x2dgetty.slice. [ OK ] Created slice system-serial\x2dgetty.slice. [ 9.877291] systemd[1]: Created slice system-systemd\x2dfsck.slice. [ OK ] Created slice system-systemd\x2dfsck.slice. [ 9.901180] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 9.921231] systemd[1]: Started Forward Password Requests to Wall Directory W atch. [ OK ] Started Forward Password R…uests to Wall Directory Watch. [ 9.945225] systemd[1]: Condition check resulted in Arbitrary Executable File Formats File System Automount Point being skipped. [ 9.957705] systemd[1]: Reached target Slices. [ OK ] Reached target Slices. [ 9.973069] systemd[1]: Reached target Swap. [ OK ] Reached target Swap. [ 9.989767] systemd[1]: Listening on Syslog Socket. [ OK ] Listening on Syslog Socket. [ 10.009950] systemd[1]: Listening on fsck to fsckd communication Socket. [ OK ] Listening on fsck to fsckd communication Socket. [ 10.033170] systemd[1]: Listening on initctl Compatibility Named Pipe. [ OK ] Listening on initctl Compatibility Named Pipe. [ 10.057682] systemd[1]: Listening on Journal Audit Socket. [ OK ] Listening on Journal Audit Socket. [ 10.081326] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ 10.105426] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ 10.131312] systemd[1]: Listening on udev Control Socket. [ OK ] Listening on udev Control Socket. [ 10.153334] systemd[1]: Listening on udev Kernel Socket. [ OK ] Listening on udev Kernel Socket. [ 10.174873] systemd[1]: Mounting Huge Pages File System... Mounting Huge Pages File System... [ 10.190747] systemd[1]: Mounting POSIX Message Queue File System... Mounting POSIX Message Queue File System... [ 10.214546] systemd[1]: Mounting RPC Pipe File System... Mounting RPC Pipe File System... [ 10.230850] systemd[1]: Mounting Kernel Debug File System... Mounting Kernel Debug File System... [ 10.245439] systemd[1]: Condition check resulted in Kernel Trace File System being skipped. [ 10.254136] systemd[1]: Condition check resulted in Kernel Module supporting RPCSEC_GSS being skipped. [ 10.269279] systemd[1]: Starting Restore / save the current clock... Starting Restore / save the current clock... [ 10.298438] systemd[1]: Starting Set the console keyboard layout... Starting Set the console keyboard layout... [ 10.322032] systemd[1]: Condition check resulted in Create list of static dev ice nodes for the current kernel being skipped. [ 10.335555] systemd[1]: Starting Load Kernel Module configfs... Starting Load Kernel Module configfs... [ 10.355169] systemd[1]: Starting Load Kernel Module drm... Starting Load Kernel Module drm... [ 10.375172] systemd[1]: Starting Load Kernel Module fuse... Starting Load Kernel Module fuse... [ 10.398111] systemd[1]: Condition check resulted in Set Up Additional Binary Formats being skipped. [ 10.407400] systemd[1]: Condition check resulted in File System Check on Root Device being skipped. [ 10.418423] systemd[1]: Starting Journal Service... Starting Journal Service... [ 10.439519] systemd[1]: Starting Load Kernel Modules... Starting Load Kernel Modules... [ 10.458992] systemd[1]: Starting Remount Root and Kernel File Systems... Starting Remount Root and Kernel File Systems... [ 10.482985] systemd[1]: Starting Coldplug All udev Devices... Starting Coldplug All udev Devices... [ 10.506497] systemd[1]: Mounted Huge Pages File System. [ OK ] Mounted Huge Pages File System. [ 10.530787] systemd[1]: Mounted POSIX Message Queue File System. [ OK ] Mounted POSIX Message Queue File System. [ 10.553485] systemd[1]: Mounted RPC Pipe File System. [ OK ] Mounted RPC Pipe File System. [ 10.569600] systemd[1]: Mounted Kernel Debug File System. [ OK ] Mounted Kernel Debug File System. [ 10.593837] systemd[1]: Finished Restore / save the current clock. [ OK ] Finished Restore / save the current clock. [ 10.618109] systemd[1]: modprobe@configfs.service: Succeeded. [ 10.629560] systemd[1]: Finished Load Kernel Module configfs. [ OK ] Finished Load Kernel Module configfs. [ 10.657639] systemd[1]: Started Journal Service. [ OK ] Started Journal Service. [ OK ] Finished Set the console keyboard layout. [ OK ] Finished Load Kernel Module drm. [ OK ] Finished Load Kernel Module fuse. [FAILED] Failed to start Load Kernel Modules. See 'systemctl status systemd-modules-load.service' for details. [ 10.766479] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null). Quota mode: none. [ OK ] Finished Remount Root and Kernel File Systems. Mounting FUSE Control File System... Mounting Kernel Configuration File System... Starting Flush Journal to Persistent Storage... Starting Load/Save Random Seed... [ 10.876210] systemd-journald[179]: Received client request to flush runtime j ournal. Starting Apply Kernel Variables... Starting Create System Users... [ OK ] Mounted FUSE Control File System. [ 10.941713] systemd-journald[179]: File /var/log/journal/7065f08cb4614e179dbd e7147eb0a762/system.journal corrupted or uncleanly shut down, renaming and repla cing. [ OK ] Mounted Kernel Configuration File System. [ OK ] Finished Apply Kernel Variables. [ OK ] Finished Create System Users. Starting Create Static Device Nodes in /dev... [ OK ] Finished Coldplug All udev Devices. Starting Helper to synchronize boot up for ifupdown... Starting Wait for udev To …plete Device Initialization... [ OK ] Finished Helper to synchronize boot up for ifupdown. [ OK ] Finished Create Static Device Nodes in /dev. [ OK ] Reached target Local File Systems (Pre). Starting Rule-based Manage…for Device Events and Files... [ OK ] Finished Flush Journal to Persistent Storage. [ OK ] Started Rule-based Manager for Device Events and Files. Starting Show Plymouth Boot Screen... [ OK ] Started Show Plymouth Boot Screen. [ OK ] Started Forward Password R…s to Plymouth Directory Watch. [ OK ] Reached target Local Encrypted Volumes. [ OK ] Finished Load/Save Random Seed. [ OK ] Found device /dev/ttyPS0. [ OK ] Found device /dev/disk/by-partuuid/3c47d971-01. [ OK ] Found device /dev/ttyS0. [ OK ] Listening on Load/Save RF …itch Status /dev/rfkill Watch. Starting File System Check…isk/by-partuuid/3c47d971-01... [ OK ] Finished Wait for udev To Complete Device Initialization. [ OK ] Finished File System Check…/disk/by-partuuid/3c47d971-01. Mounting /boot... [ OK ] Started File System Check Daemon to report status. [ OK ] Mounted /boot. [ OK ] Reached target Local File Systems. Starting Set console font and keymap... Starting Raise network interfaces... Starting Preprocess NFS configuration... Starting Tell Plymouth To Write Out Runtime Data... Starting Create Volatile Files and Directories... [ OK ] Finished Set console font and keymap. [ OK ] Finished Preprocess NFS configuration. [ OK ] Reached target NFS client services. [ OK ] Reached target Remote File Systems (Pre). [ OK ] Reached target Remote File Systems. [ OK ] Finished Tell Plymouth To Write Out Runtime Data. [ OK ] Finished Create Volatile Files and Directories. Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Finished Update UTMP about System Boot/Shutdown. Starting Load Kernel Modules... [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Time Set. [ OK ] Reached target System Time Synchronized. [ OK ] Finished Raise network interfaces. [FAILED] Failed to start Load Kernel Modules. See 'systemctl status systemd-modules-load.service' for details. [ OK ] Reached target System Initialization. [ OK ] Started CUPS Scheduler. [ OK ] Started Daily apt download activities. [ OK ] Started Daily apt upgrade and clean activities. [ OK ] Started Periodic ext4 Onli…ata Check for All Filesystems. [ OK ] Started Discard unused blocks once a week. [ OK ] Started Daily rotation of log files. [ OK ] Started Daily man-db regeneration. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target Paths. [ OK ] Reached target Timers. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Listening on CUPS Scheduler. [ OK ] Listening on D-Bus System Message Bus Socket. [ OK ] Listening on Erlang Port Mapper Daemon Activation Socket. [ OK ] Listening on GPS (Global P…ioning System) Daemon Sockets. [ OK ] Listening on triggerhappy.socket. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. Starting Analog Devices power up/down sequence... Starting Avahi mDNS/DNS-SD Stack... [ OK ] Started Regular background program processing daemon. [ OK ] Started D-Bus System Message Bus. Starting dphys-swapfile - …unt, and delete a swap file... Starting Remove Stale Onli…t4 Metadata Check Snapshots... Starting Creating IIOD Context Attributes...... Starting Authorization Manager... Starting DHCP Client Daemon... Starting LSB: Switch to on…nless shift key is pressed)... Starting LSB: rng-tools (Debian variant)... Starting System Logging Service... Starting User Login Management... Starting triggerhappy global hotkey daemon... Starting Disk Manager... Starting WPA supplicant... [ OK ] Finished Remove Stale Onli…ext4 Metadata Check Snapshots. [ OK ] Started triggerhappy global hotkey daemon. [ OK ] Started DHCP Client Daemon. [ OK ] Started LSB: rng-tools (Debian variant). [ OK ] Started System Logging Service. [ OK ] Finished dphys-swapfile - …mount, and delete a swap file. [ OK ] Started User Login Management. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Started WPA supplicant. [ OK ] Reached target Network. [ OK ] Reached target Network is Online. Starting CUPS Scheduler... [ OK ] Started Erlang Port Mapper Daemon. Starting HTTP based time synchronization tool... Starting Internet superserver... Starting /etc/rc.local Compatibility... Starting OpenBSD Secure Shell server... Starting Permit User Sessions... [ OK ] Started Unattended Upgrades Shutdown. [ OK ] Started /etc/rc.local Compatibility. [ OK ] Started Authorization Manager. Starting Modem Manager... [ OK ] Finished Permit User Sessions. Starting Light Display Manager... Starting Hold until boot process finishes up... [ OK ] Started HTTP based time synchronization tool. [ OK ] Started Internet superserver. [ OK ] Finished Creating IIOD Context Attributes.... [ OK ] Started IIO Daemon. [ OK ] Started OpenBSD Secure Shell server. [ OK ] Finished Analog Devices power up/down sequence. [FAILED] Failed to start VNC Server for X11.
root@analog:~# iio_info iio_info version: 0.25 (git tag:8fb78e06) Libiio version: 0.25 (git tag: 8fb78e0) backends: local xml ip usb serial IIO context created with local backend. Backend version: 0.25 (git tag: 8fb78e0) Backend description string: Linux analog 5.15.0-175919-g427c94e8faa5 #824 SMP Tue Dec 12 10:32:23 EET 2023 aarch64 IIO context has 6 attributes: hdl_system_id: [ad9081_fmca_ebz] on [zcu102] git branch [hdl_2022_r2] git [b31d4fbba87a96f329f858da3118771503c7c6b4] clean [2023-11-01 14:35:49] UTC hw_carrier: ZynqMP ZCU102 Rev1.0 unique_id: 364c9200151100290076e3cf9a2f hw_model: AD9081-FMCA-EBZ-A3 on ZynqMP ZCU102 Rev1.0 local,kernel: 5.15.0-175919-g427c94e8faa5 uri: local: IIO context has 23 devices: hwmon0: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 8 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1412500 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 850 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 1665 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon1: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 2 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 287500 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 849 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 328 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon10: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 3 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1218750 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 849 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 1431 2 device-specific attributes found: attr 0: shunt_resistor value: 2000 attr 1: update_interval value: 35 No trigger on this device hwmon11: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 0 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 25000 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 848 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 35 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon12: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 362500 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1798 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 207 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon13: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 0 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 25000 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1200 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 22 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon14: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 0 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 100000 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 3295 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 30 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon15: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 0 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 75000 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1798 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 39 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon16: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 162500 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 900 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 184 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon17: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 2 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 425000 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1199 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 362 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon18: max20751 5 channels found: in2: (input) 8 channel-specific attributes found: attr 0: input value: 900 attr 1: label value: vout1 attr 2: lcrit value: 735 attr 3: lcrit_alarm value: 0 attr 4: max value: 945 attr 5: max_alarm value: 0 attr 6: min value: 855 attr 7: min_alarm value: 0 curr1: (input) 4 channel-specific attributes found: attr 0: input value: 0 attr 1: label value: iout1 attr 2: max value: 511500 attr 3: max_alarm value: 0 in1: (input) 7 channel-specific attributes found: attr 0: alarm value: 0 attr 1: crit value: 15000 attr 2: input value: 11906 attr 3: label value: vin attr 4: lcrit value: 4687 attr 5: max value: 14906 attr 6: min value: 4750 power1: (input) 2 channel-specific attributes found: attr 0: input value: 0 attr 1: label value: pout1 temp1: (input) 7 channel-specific attributes found: attr 0: crit value: 133000 attr 1: crit_alarm value: 0 attr 2: input value: 43000 attr 3: max value: 130000 attr 4: max_alarm value: 0 attr 5: min value: -40000 attr 6: min_alarm value: 0 No trigger on this device hwmon19: max20751 5 channels found: in2: (input) 8 channel-specific attributes found: attr 0: input value: 1200 attr 1: label value: vout1 attr 2: lcrit value: 980 attr 3: lcrit_alarm value: 0 attr 4: max value: 1260 attr 5: max_alarm value: 0 attr 6: min value: 1140 attr 7: min_alarm value: 0 curr1: (input) 4 channel-specific attributes found: attr 0: input value: 0 attr 1: label value: iout1 attr 2: max value: 511500 attr 3: max_alarm value: 0 in1: (input) 7 channel-specific attributes found: attr 0: alarm value: 0 attr 1: crit value: 15000 attr 2: input value: 11968 attr 3: label value: vin attr 4: lcrit value: 4687 attr 5: max value: 14906 attr 6: min value: 4750 power1: (input) 2 channel-specific attributes found: attr 0: input value: 0 attr 1: label value: pout1 temp1: (input) 7 channel-specific attributes found: attr 0: crit value: 133000 attr 1: crit_alarm value: 0 attr 2: input value: 37000 attr 3: max value: 130000 attr 4: max_alarm value: 0 attr 5: min value: -40000 attr 6: min_alarm value: 0 No trigger on this device hwmon2: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 0 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 25000 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1813 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 11 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon3: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 0 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 37500 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1201 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 27 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon4: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 0 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 62500 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 853 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 62 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon5: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 0 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 25000 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1814 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 11 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon6: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 212500 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1191 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 180 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon7: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 0 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 37500 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1794 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 17 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon8: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 0 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 0 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1813 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 1 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device hwmon9: ina226 4 channels found: in0: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 0 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 power1: (input) 3 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 37500 in1: (input) 5 channel-specific attributes found: attr 0: crit value: 0 attr 1: crit_alarm value: 0 attr 2: input value: 1810 attr 3: lcrit value: 0 attr 4: lcrit_alarm value: 0 curr1: (input) 1 channel-specific attributes found: attr 0: input value: 24 2 device-specific attributes found: attr 0: shunt_resistor value: 5000 attr 1: update_interval value: 35 No trigger on this device iio:device0: ams 30 channels found: voltage6: vccpsintfpddr (input) 3 channel-specific attributes found: attr 0: label value: vccpsintfpddr attr 1: raw value: 18428 attr 2: scale value: 0.045776367 voltage18: vccint (input) 3 channel-specific attributes found: attr 0: label value: vccint attr 1: raw value: 18574 attr 2: scale value: 0.045776367 voltage14: vccpsio2 (input) 3 channel-specific attributes found: attr 0: label value: vccpsio2 attr 1: raw value: 19459 attr 2: scale value: 0.091552734 voltage16: psmgtravtt (input) 3 channel-specific attributes found: attr 0: label value: psmgtravtt attr 1: raw value: 39630 attr 2: scale value: 0.045776367 voltage23: vccplintlp (input) 3 channel-specific attributes found: attr 0: label value: vccplintlp attr 1: raw value: 18550 attr 2: scale value: 0.045776367 voltage0: vcc_pspll0 (input) 3 channel-specific attributes found: attr 0: label value: vcc_pspll0 attr 1: raw value: 26211 attr 2: scale value: 0.045776367 voltage8: vccpsintfp (input) 3 channel-specific attributes found: attr 0: label value: vccpsintfp attr 1: raw value: 18456 attr 2: scale value: 0.045776367 voltage22: vccbram (input) 3 channel-specific attributes found: attr 0: label value: vccbram attr 1: raw value: 18528 attr 2: scale value: 0.045776367 voltage26: vccams (input) 3 channel-specific attributes found: attr 0: label value: vccams attr 1: raw value: 39199 attr 2: scale value: 0.015258789 temp1: remote_temp (input) 4 channel-specific attributes found: attr 0: label value: remote_temp attr 1: offset value: -36058 attr 2: raw value: 40508 attr 3: scale value: 7.771514892 voltage9: vccpsaux (input) 3 channel-specific attributes found: attr 0: label value: vccpsaux attr 1: raw value: 39546 attr 2: scale value: 0.045776367 voltage25: vccplaux (input) 3 channel-specific attributes found: attr 0: label value: vccplaux attr 1: raw value: 39564 attr 2: scale value: 0.045776367 voltage15: psmgtravcc (input) 3 channel-specific attributes found: attr 0: label value: psmgtravcc attr 1: raw value: 18552 attr 2: scale value: 0.045776367 temp0: ps_temp (input) 4 channel-specific attributes found: attr 0: label value: ps_temp attr 1: offset value: -36058 attr 2: raw value: 40600 attr 3: scale value: 7.771514892 voltage21: vccvrefn (input) 3 channel-specific attributes found: attr 0: label value: vccvrefn attr 1: raw value: 0 attr 2: scale value: 0.045776367 voltage2: vccint (input) 3 channel-specific attributes found: attr 0: label value: vccint attr 1: raw value: 18539 attr 2: scale value: 0.045776367 voltage5: vcc_psddrpll (input) 3 channel-specific attributes found: attr 0: label value: vcc_psddrpll attr 1: raw value: 39546 attr 2: scale value: 0.045776367 voltage7: vccpsintlp (input) 3 channel-specific attributes found: attr 0: label value: vccpsintlp attr 1: raw value: 18485 attr 2: scale value: 0.045776367 voltage11: vccpsio3 (input) 3 channel-specific attributes found: attr 0: label value: vccpsio3 attr 1: raw value: 19637 attr 2: scale value: 0.091552734 temp2: pl_temp (input) 4 channel-specific attributes found: attr 0: label value: pl_temp attr 1: offset value: -36058 attr 2: raw value: 40302 attr 3: scale value: 7.771514892 voltage13: vccpsio1 (input) 3 channel-specific attributes found: attr 0: label value: vccpsio1 attr 1: raw value: 19434 attr 2: scale value: 0.091552734 voltage3: vccbram (input) 3 channel-specific attributes found: attr 0: label value: vccbram attr 1: raw value: 18462 attr 2: scale value: 0.045776367 voltage4: vccaux (input) 3 channel-specific attributes found: attr 0: label value: vccaux attr 1: raw value: 39228 attr 2: scale value: 0.045776367 voltage12: vccpsio0 (input) 3 channel-specific attributes found: attr 0: label value: vccpsio0 attr 1: raw value: 19442 attr 2: scale value: 0.091552734 voltage24: vccplintfp (input) 3 channel-specific attributes found: attr 0: label value: vccplintfp attr 1: raw value: 18431 attr 2: scale value: 0.045776367 voltage10: vccpsddr (input) 3 channel-specific attributes found: attr 0: label value: vccpsddr attr 1: raw value: 25940 attr 2: scale value: 0.045776367 voltage1: vcc_psbatt (input) 3 channel-specific attributes found: attr 0: label value: vcc_psbatt attr 1: raw value: 27941 attr 2: scale value: 0.045776367 voltage19: vccaux (input) 3 channel-specific attributes found: attr 0: label value: vccaux attr 1: raw value: 39290 attr 2: scale value: 0.045776367 voltage17: vccams (input) 3 channel-specific attributes found: attr 0: label value: vccams attr 1: raw value: 39468 attr 2: scale value: 0.015258789 voltage20: vccvrefp (input) 3 channel-specific attributes found: attr 0: label value: vccvrefp attr 1: raw value: 27315 attr 2: scale value: 0.045776367 1 device-specific attributes found: attr 0: sampling_frequency ERROR: Invalid argument (22) No trigger on this device iio:device1: hmc7044 8 channels found: altvoltage12: FPGA_REFCLK2 (output) 3 channel-specific attributes found: attr 0: frequency value: 500000000 attr 1: label value: FPGA_REFCLK2 attr 2: phase value: 0.000000 altvoltage10: CORE_CLK_RX_ALT (output) 3 channel-specific attributes found: attr 0: frequency value: 250000000 attr 1: label value: CORE_CLK_RX_ALT attr 2: phase value: 0.000000 altvoltage8: FPGA_REFCLK1 (output) 3 channel-specific attributes found: attr 0: frequency value: 500000000 attr 1: label value: FPGA_REFCLK1 attr 2: phase value: 0.000000 altvoltage0: CORE_CLK_RX (output) 3 channel-specific attributes found: attr 0: frequency value: 250000000 attr 1: label value: CORE_CLK_RX attr 2: phase value: 0.000000 altvoltage3: DEV_SYSREF (output) 3 channel-specific attributes found: attr 0: frequency value: 1953125 attr 1: label value: DEV_SYSREF attr 2: phase value: 0.000000 altvoltage13: FPGA_SYSREF (output) 3 channel-specific attributes found: attr 0: frequency value: 1953125 attr 1: label value: FPGA_SYSREF attr 2: phase value: 0.000000 altvoltage6: CORE_CLK_TX (output) 3 channel-specific attributes found: attr 0: frequency value: 250000000 attr 1: label value: CORE_CLK_TX attr 2: phase value: 0.000000 altvoltage2: DEV_REFCLK (output) 3 channel-specific attributes found: attr 0: frequency value: 250000000 attr 1: label value: DEV_REFCLK attr 2: phase value: 0.000000 7 device-specific attributes found: attr 0: mute_request value: 1 attr 1: reseed_request value: 1 attr 2: reset_dividers_request value: 1 attr 3: sleep_request value: 1 attr 4: sync_pin_mode value: sync_else_sysref attr 5: sync_pin_mode_available value: disable sync sysref sync_else_sysref attr 6: sysref_request value: 1 2 debug attributes found: debug attr 0: status ERROR: Input/output error (5) debug attr 1: direct_reg_access value: 0x0 No trigger on this device iio_sysfs_trigger: 0 channels found: 2 device-specific attributes found: attr 0: add_trigger ERROR: Permission denied (13) attr 1: remove_trigger ERROR: Permission denied (13) No trigger on this device