Hello
I am using the ADRV9375-W/PCBZ evaluation board on a ZCU102. I have built the 2022_R2 HDL reference design in Vivado 2022.2. I am using the ADI 2022.2 Petalinux meta layer.
Everything is working for the default 122.88MHz VCXO populated on the ADRV9375 evaluation board.
I have change the VCXO to a 100MHz Crystek part. I used the AD9371 filter wizard to create a new profile for the 100MHz VCXO. The reference frequency provided to the ZCU102 is now 100MHz from the AD9528. I have included the generated profile.
<profile AD9371 version=0 name=Rx 80, IQrate 100.000> <clocks> <deviceClock_kHz=100000> <clkPllVcoFreq_kHz=12000000> <clkPllVcoDiv=3> <clkPllHsDiv=4> </clocks> <rx> <adcDiv=1> <rxFirDecimation=2> <rxDec5Decimation=5> <enHighRejDec5=1> <rhb1Decimation=1> <iqRate_kHz=100000> <rfBandwidth_Hz=80000000> <rxBbf3dBCorner_kHz=80000> <filter FIR gain=-6 num=48> -4 -17 23 41 -53 -95 117 184 -221 -331 389 553 -644 -888 1026 1387 -1608 -2158 2580 3485 -4786 -7622 9629 32372 32372 9629 -7622 -4786 3485 2580 -2158 -1608 1387 1026 -888 -644 553 389 -331 -221 184 117 -95 -53 41 23 -17 -4 </filter> <adc-profile num=16> 660 473 201 98 1280 477 1587 269 1062 82 645 28 48 32 19 190 </adc-profile> </rx> <obs> <adcDiv=1> <rxFirDecimation=1> <rxDec5Decimation=5> <enHighRejDec5=1> <rhb1Decimation=1> <iqRate_kHz=200000> <rfBandwidth_Hz=160000000> <rxBbf3dBCorner_kHz=80000> <filter FIR gain=6 num=24> -119 284 -28 34 149 -287 390 -296 -517 1496 -3974 22853 -3974 1496 -517 -296 390 -287 149 34 -28 284 -119 0 </filter> <adc-profile num=16> 558 443 201 98 1280 711 1679 818 1198 573 682 21 43 30 20 204 </adc-profile> <lpbk-adc-profile num=16> 702 453 201 98 1280 281 1539 143 1073 45 657 35 48 32 19 192 </lpbk-adc-profile> </obs> <sniffer> <adcDiv=1> <rxFirDecimation=4> <rxDec5Decimation=5> <enHighRejDec5=1> <rhb1Decimation=2> <iqRate_kHz=25000> <rfBandwidth_Hz=16000000> <rxBbf3dBCorner_kHz=20000> <filter FIR gain=-6 num=72> 0 2 3 2 -4 -13 -17 -9 17 49 63 30 -51 -143 -174 -82 126 345 409 193 -268 -736 -864 -417 519 1464 1744 887 -975 -2974 -3786 -2264 1885 7761 13502 17045 17045 13502 7761 1885 -2264 -3786 -2974 -975 887 1744 1464 519 -417 -864 -736 -268 193 409 345 126 -82 -174 -143 -51 30 63 49 17 -9 -17 -13 -4 2 3 2 0 </filter> <adc-profile num=16> 737 439 201 98 1280 112 1505 53 1081 17 667 40 48 33 19 194 </adc-profile> </sniffer> <tx> <dacDiv=2.5> <txFirInterpolation=1> <thb1Interpolation=2> <thb2Interpolation=1> <txInputHbInterpolation=1> <iqRate_kHz=200000> <primarySigBandwidth_Hz=60000000> <rfBandwidth_Hz=160000000> <txDac3dBCorner_kHz=160000> <txBbf3dBCorner_kHz=80000> <filter FIR gain=6 num=16> -42 -216 222 -215 -3 889 -3094 20982 -3094 889 -3 -215 222 -216 -42 0 </filter> </tx> </profile>
During boot up, the JESD device driver is complaining of a QPLL TX buffer underflow error and a QPLL TX buffer overflow error:
Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 5.15.36-xilinx-v2022.2 (oe-user@oe-host) (aarch64-xilinx-linux-gcc (GCC) 11.2.0, GNU ld (GNU Binutils) 2.37.20210721) #1 SMP Thu Jan 18 15:59:49 UTC 2024 [ 0.000000] Machine model: xlnx,zynqmp [ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8') [ 0.000000] printk: bootconsole [cdns0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000000000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal [mem 0x0000000100000000-0x000000087fffffff] [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000000000000-0x000000003ecfffff] [ 0.000000] node 0: [mem 0x000000003ed00000-0x000000003ee47fff] [ 0.000000] node 0: [mem 0x000000003ee48000-0x000000007fefffff] [ 0.000000] node 0: [mem 0x0000000800000000-0x000000087fffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000000000000-0x000000087fffffff] [ 0.000000] On node 0, zone Normal: 256 pages in unavailable ranges [ 0.000000] cma: Reserved 256 MiB at 0x0000000067000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 18 pages/cpu s35800 r8192 d29736 u73728 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1031940 [ 0.000000] Kernel command line: earlycon console=ttyPS0,115200 clk_ignore_unused cpuidle.off=1 uio_pdrv_genirq.of_id="generic-uio" [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear) [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] software IO TLB: mapped [mem 0x000000007bf00000-0x000000007ff00000] (64MB) [ 0.000000] Memory: 3673140K/4193280K available (17152K kernel code, 1740K rwdata, 13116K rodata, 2624K init, 650K bss, 257996K reserved, 262144K cma-reserved) [ 0.000000] rcu: Hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000 [ 0.000000] Root IRQ handler: gic_handle_irq [ 0.000000] GIC: Using split EOI/Deactivate mode [ 0.000000] random: get_random_bytes called from start_kernel+0x470/0x6d4 with crng_init=0 [ 0.000000] arch_timer: cp15 timer(s) running at 100.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171024e7e0, max_idle_ns: 440795205315 ns [ 0.000000] sched_clock: 56 bits at 100MHz, resolution 10ns, wraps every 4398046511100ns [ 0.008452] Console: colour dummy device 80x25 [ 0.012484] Calibrating delay loop (skipped), value calculated using timer frequency.. 200.00 BogoMIPS (lpj=400000) [ 0.022839] pid_max: default: 32768 minimum: 301 [ 0.027641] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.034786] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.043615] rcu: Hierarchical SRCU implementation. [ 0.047524] EFI services will not be available. [ 0.051959] smp: Bringing up secondary CPUs ... [ 0.056702] Detected VIPT I-cache on CPU1 [ 0.056742] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.057135] Detected VIPT I-cache on CPU2 [ 0.057159] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] [ 0.057542] Detected VIPT I-cache on CPU3 [ 0.057565] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] [ 0.057609] smp: Brought up 1 node, 4 CPUs [ 0.091778] SMP: Total of 4 processors activated. [ 0.096450] CPU features: detected: 32-bit EL0 Support [ 0.101554] CPU features: detected: CRC32 instructions [ 0.106695] CPU: All CPU(s) started at EL2 [ 0.110736] alternatives: patching kernel code [ 0.116061] devtmpfs: initialized [ 0.123539] Registered cp15_barrier emulation handler [ 0.123590] Registered setend emulation handler [ 0.128044] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.137637] futex hash table entries: 1024 (order: 4, 65536 bytes, linear) [ 0.150172] pinctrl core: initialized pinctrl subsystem [ 0.150917] NET: Registered PF_NETLINK/PF_ROUTE protocol family [ 0.156660] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations [ 0.162749] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.170498] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.178265] audit: initializing netlink subsys (disabled) [ 0.183665] audit: type=2000 audit(0.116:1): state=initialized audit_enabled=0 res=1 [ 0.184002] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.198091] ASID allocator initialised with 65536 entries [ 0.225897] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages [ 0.226959] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages [ 0.233628] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.240289] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages [ 1.331024] DRBG: Continuing without Jitter RNG [ 1.431803] raid6: neonx8 gen() 2132 MB/s [ 1.499864] raid6: neonx8 xor() 1583 MB/s [ 1.567927] raid6: neonx4 gen() 2177 MB/s [ 1.635985] raid6: neonx4 xor() 1556 MB/s [ 1.704056] raid6: neonx2 gen() 2069 MB/s [ 1.772112] raid6: neonx2 xor() 1423 MB/s [ 1.840182] raid6: neonx1 gen() 1766 MB/s [ 1.908240] raid6: neonx1 xor() 1213 MB/s [ 1.976312] raid6: int64x8 gen() 1366 MB/s [ 2.044373] raid6: int64x8 xor() 773 MB/s [ 2.112440] raid6: int64x4 gen() 1599 MB/s [ 2.180496] raid6: int64x4 xor() 848 MB/s [ 2.248579] raid6: int64x2 gen() 1393 MB/s [ 2.316637] raid6: int64x2 xor() 750 MB/s [ 2.384708] raid6: int64x1 gen() 1036 MB/s [ 2.452762] raid6: int64x1 xor() 517 MB/s [ 2.452802] raid6: using algorithm neonx4 gen() 2177 MB/s [ 2.456753] raid6: .... xor() 1556 MB/s, rmw enabled [ 2.461689] raid6: using neon recovery algorithm [ 2.466762] iommu: Default domain type: Translated [ 2.471119] iommu: DMA domain TLB invalidation policy: strict mode [ 2.477543] SCSI subsystem initialized [ 2.481215] usbcore: registered new interface driver usbfs [ 2.486555] usbcore: registered new interface driver hub [ 2.491814] usbcore: registered new device driver usb [ 2.496951] mc: Linux media interface: v0.10 [ 2.501064] videodev: Linux video capture interface: v2.00 [ 2.506552] pps_core: LinuxPPS API ver. 1 registered [ 2.511427] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 2.520517] PTP clock support registered [ 2.524420] EDAC MC: Ver: 3.0.0 [ 2.527789] zynqmp-ipi-mbox mailbox@ff990400: Registered ZynqMP IPI mbox with TX/RX channels. [ 2.536207] zynqmp-ipi-mbox mailbox@ff990600: Registered ZynqMP IPI mbox with TX/RX channels. [ 2.544767] jesd204: created con: id=0, topo=0, link=0, /axi/spi@ff040000/ad9528-1@0 <-> /fpga-axi@0/axi-adxcvr-tx@84a80000 [ 2.555548] jesd204: created con: id=1, topo=0, link=2, /axi/spi@ff040000/ad9528-1@0 <-> /fpga-axi@0/axi-adxcvr-rx-os@84a50000 [ 2.566880] jesd204: created con: id=2, topo=0, link=1, /axi/spi@ff040000/ad9528-1@0 <-> /fpga-axi@0/axi-adxcvr-rx@84a60000 [ 2.577949] jesd204: created con: id=3, topo=0, link=2, /fpga-axi@0/axi-adxcvr-rx-os@84a50000 <-> /fpga-axi@0/axi-jesd204-rx-os@84ab0000 [ 2.590146] jesd204: created con: id=4, topo=0, link=0, /fpga-axi@0/axi-adxcvr-tx@84a80000 <-> /fpga-axi@0/axi-jesd204-tx@84a90000 [ 2.601823] jesd204: created con: id=5, topo=0, link=1, /fpga-axi@0/axi-adxcvr-rx@84a60000 <-> /fpga-axi@0/axi-jesd204-rx@84aa0000 [ 2.613500] jesd204: created con: id=6, topo=0, link=0, /fpga-axi@0/axi-jesd204-tx@84a90000 <-> /fpga-axi@0/axi-ad9371-tx-hpc@84a04000 [ 2.625532] jesd204: created con: id=7, topo=0, link=1, /fpga-axi@0/axi-jesd204-rx@84aa0000 <-> /axi/spi@ff040000/ad9371-phy@1 [ 2.636857] jesd204: created con: id=8, topo=0, link=2, /fpga-axi@0/axi-jesd204-rx-os@84ab0000 <-> /axi/spi@ff040000/ad9371-phy@1 [ 2.648448] jesd204: created con: id=9, topo=0, link=0, /fpga-axi@0/axi-ad9371-tx-hpc@84a04000 <-> /axi/spi@ff040000/ad9371-phy@1 [ 2.660045] jesd204: /axi/spi@ff040000/ad9371-phy@1: JESD204[0:0] transition uninitialized -> initialized [ 2.669548] jesd204: /axi/spi@ff040000/ad9371-phy@1: JESD204[0:1] transition uninitialized -> initialized [ 2.679063] jesd204: /axi/spi@ff040000/ad9371-phy@1: JESD204[0:2] transition uninitialized -> initialized [ 2.688578] jesd204: found 9 devices and 1 topologies [ 2.693626] FPGA manager framework [ 2.697099] Advanced Linux Sound Architecture Driver Initialized. [ 2.703435] Bluetooth: Core ver 2.22 [ 2.706581] NET: Registered PF_BLUETOOTH protocol family [ 2.711848] Bluetooth: HCI device and connection manager initialized [ 2.718165] Bluetooth: HCI socket layer initialized [ 2.723007] Bluetooth: L2CAP socket layer initialized [ 2.728031] Bluetooth: SCO socket layer initialized [ 2.733283] clocksource: Switched to clocksource arch_sys_counter [ 2.739062] VFS: Disk quotas dquot_6.6.0 [ 2.742859] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 2.754102] NET: Registered PF_INET protocol family [ 2.754606] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear) [ 2.763419] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear) [ 2.770362] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear) [ 2.778396] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear) [ 2.785837] TCP: Hash tables configured (established 32768 bind 32768) [ 2.792013] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear) [ 2.798677] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear) [ 2.805832] NET: Registered PF_UNIX/PF_LOCAL protocol family [ 2.811631] RPC: Registered named UNIX socket transport module. [ 2.817212] RPC: Registered udp transport module. [ 2.821878] RPC: Registered tcp transport module. [ 2.826548] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 2.833556] PCI: CLS 0 bytes, default 64 [ 2.836986] Trying to unpack rootfs image as initramfs... [ 2.842932] armv8-pmu pmu: hw perfevents: no interrupt-affinity property, guessing. [ 2.850282] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available [ 2.858528] Initialise system trusted keyrings [ 2.862066] workingset: timestamp_bits=46 max_order=20 bucket_order=0 [ 2.869813] NFS: Registering the id_resolver key type [ 2.873360] Key type id_resolver registered [ 2.877500] Key type id_legacy registered [ 2.881502] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 2.888143] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 2.895515] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. [ 2.902823] fuse: init (API version 7.34) [ 2.942318] NET: Registered PF_ALG protocol family [ 2.942387] xor: measuring software checksum speed [ 2.950415] 8regs : 2363 MB/sec [ 2.954082] 32regs : 2799 MB/sec [ 2.959155] arm64_neon : 2308 MB/sec [ 2.959215] xor: using function: 32regs (2799 MB/sec) [ 2.964248] Key type asymmetric registered [ 2.968304] Asymmetric key parser 'x509' registered [ 2.973225] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246) [ 2.980502] io scheduler mq-deadline registered [ 2.984997] io scheduler kyber registered [ 3.017529] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled [ 3.020595] cacheinfo: Unable to detect cache hierarchy for CPU 0 [ 3.028663] brd: module loaded [ 3.032239] loop: module loaded [ 3.032664] Registered mathworks_ip class [ 3.037750] tun: Universal TUN/TAP device driver, 1.6 [ 3.039531] CAN device driver interface [ 3.044182] SPI driver wl1271_spi has no spi_device_id for ti,wl1271 [ 3.049574] SPI driver wl1271_spi has no spi_device_id for ti,wl1273 [ 3.055879] SPI driver wl1271_spi has no spi_device_id for ti,wl1281 [ 3.062191] SPI driver wl1271_spi has no spi_device_id for ti,wl1283 [ 3.068505] SPI driver wl1271_spi has no spi_device_id for ti,wl1285 [ 3.074821] SPI driver wl1271_spi has no spi_device_id for ti,wl1801 [ 3.081134] SPI driver wl1271_spi has no spi_device_id for ti,wl1805 [ 3.087448] SPI driver wl1271_spi has no spi_device_id for ti,wl1807 [ 3.093763] SPI driver wl1271_spi has no spi_device_id for ti,wl1831 [ 3.100078] SPI driver wl1271_spi has no spi_device_id for ti,wl1835 [ 3.106392] SPI driver wl1271_spi has no spi_device_id for ti,wl1837 [ 3.112915] usbcore: registered new interface driver asix [ 3.118117] usbcore: registered new interface driver ax88179_178a [ 3.124163] usbcore: registered new interface driver cdc_ether [ 3.129955] usbcore: registered new interface driver net1080 [ 3.135578] usbcore: registered new interface driver cdc_subset [ 3.141456] usbcore: registered new interface driver zaurus [ 3.147014] usbcore: registered new interface driver cdc_ncm [ 3.153465] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 3.159073] ehci-pci: EHCI PCI platform driver [ 3.164057] usbcore: registered new interface driver uas [ 3.168803] usbcore: registered new interface driver usb-storage [ 3.174790] usbcore: registered new interface driver usbserial_generic [ 3.181229] usbserial: USB Serial support registered for generic [ 3.187212] usbcore: registered new interface driver ftdi_sio [ 3.192905] usbserial: USB Serial support registered for FTDI USB Serial Device [ 3.200195] usbcore: registered new interface driver upd78f0730 [ 3.206058] usbserial: USB Serial support registered for upd78f0730 [ 3.213548] SPI driver ads7846 has no spi_device_id for ti,tsc2046 [ 3.218415] SPI driver ads7846 has no spi_device_id for ti,ads7843 [ 3.224550] SPI driver ads7846 has no spi_device_id for ti,ads7845 [ 3.230692] SPI driver ads7846 has no spi_device_id for ti,ads7873 [ 3.237547] rtc_zynqmp ffa60000.rtc: registered as rtc0 [ 3.242044] rtc_zynqmp ffa60000.rtc: setting system clock to 1970-01-12T03:28:34 UTC (962914) [ 3.250673] i2c_dev: i2c /dev entries driver [ 3.256892] usbcore: registered new interface driver uvcvideo [ 3.261556] Bluetooth: HCI UART driver ver 2.3 [ 3.264856] Bluetooth: HCI UART protocol H4 registered [ 3.269982] Bluetooth: HCI UART protocol BCSP registered [ 3.275278] Bluetooth: HCI UART protocol LL registered [ 3.280344] Bluetooth: HCI UART protocol ATH3K registered [ 3.285732] Bluetooth: HCI UART protocol Three-wire (H5) registered [ 3.292067] Bluetooth: HCI UART protocol Intel registered [ 3.297316] Bluetooth: HCI UART protocol QCA registered [ 3.302523] usbcore: registered new interface driver bcm203x [ 3.308151] usbcore: registered new interface driver bpa10x [ 3.313690] usbcore: registered new interface driver bfusb [ 3.319135] usbcore: registered new interface driver btusb [ 3.324593] usbcore: registered new interface driver ath3k [ 3.330188] EDAC MC: ECC not enabled [ 3.333868] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT) [ 3.346313] sdhci: Secure Digital Host Controller Interface driver [ 3.351801] sdhci: Copyright(c) Pierre Ossman [ 3.356118] sdhci-pltfm: SDHCI platform and OF driver helper [ 3.362728] ledtrig-cpu: registered to indicate activity on CPUs [ 3.367888] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 3.374215] zynqmp_firmware_probe Platform Management API v1.1 [ 3.379910] zynqmp_firmware_probe Trustzone version v1.0 [ 3.414375] zynqmp-aes firmware:zynqmp-firmware:zynqmp-aes: will run requests pump with realtime priority [ 6.437542] Freeing initrd memory: 74472K [ 6.454038] zynqmp-keccak-384 firmware:zynqmp-firmware:sha384: The zynqmp-sha-deprecated driver shall be deprecated in 2022.2 and removed in 2023.1 release [ 6.462360] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384) [ 6.468653] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa) [ 6.474109] usbcore: registered new interface driver usbhid [ 6.479494] usbhid: USB HID core driver [ 6.483495] SPI driver fb_seps525 has no spi_device_id for syncoam,seps525 [ 6.490829] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7988-5 [ 6.497314] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7988-1 [ 6.504492] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7984 [ 6.511498] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7983 [ 6.518504] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7982 [ 6.525510] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7980 [ 6.532517] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7949 [ 6.539523] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7946 [ 6.546530] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7942 [ 6.553536] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7699 [ 6.560543] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7693 [ 6.567549] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7691 [ 6.574556] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7690 [ 6.581562] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7689 [ 6.588569] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7688 [ 6.595575] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7687 [ 6.602589] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7686 [ 6.609589] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7685 [ 6.616595] SPI driver pulsar_adc has no spi_device_id for adi,pulsar,ad7682 [ 6.623719] SPI driver ad7124 has no spi_device_id for adi,ad7124-4 [ 6.629831] SPI driver ad7124 has no spi_device_id for adi,ad7124-8 [ 6.636072] SPI driver ad7192 has no spi_device_id for adi,ad7190 [ 6.642113] SPI driver ad7192 has no spi_device_id for adi,ad7193 [ 6.648167] SPI driver ad7192 has no spi_device_id for adi,ad7195 [ 6.655048] SPI driver ad9467 has no spi_device_id for adi,ad9643 [ 6.660279] SPI driver ad9467 has no spi_device_id for adi,ad9250 [ 6.666332] SPI driver ad9467 has no spi_device_id for adi,ad9250_2 [ 6.672560] SPI driver ad9467 has no spi_device_id for adi,ad9265 [ 6.678615] SPI driver ad9467 has no spi_device_id for adi,ad9683 [ 6.684670] SPI driver ad9467 has no spi_device_id for adi,ad9434 [ 6.690725] SPI driver ad9467 has no spi_device_id for adi,ad9625 [ 6.696780] SPI driver ad9467 has no spi_device_id for adi,ad9652 [ 6.702835] SPI driver ad9467 has no spi_device_id for adi,ad9649 [ 6.711736] SPI driver adar3000 has no spi_device_id for adi,adar3001 [ 6.715299] SPI driver adar3000 has no spi_device_id for adi,adar3002 [ 6.722949] SPI driver ad9783 has no spi_device_id for adi,ad9780 [ 6.727753] SPI driver ad9783 has no spi_device_id for adi,ad9781 [ 6.733996] SPI driver adis16475 has no spi_device_id for adi,adis16470 [ 6.740378] SPI driver adis16475 has no spi_device_id for adi,adis16475-1 [ 6.747123] SPI driver adis16475 has no spi_device_id for adi,adis16475-2 [ 6.753870] SPI driver adis16475 has no spi_device_id for adi,adis16475-3 [ 6.760617] SPI driver adis16475 has no spi_device_id for adi,adis16477-1 [ 6.767364] SPI driver adis16475 has no spi_device_id for adi,adis16477-2 [ 6.774111] SPI driver adis16475 has no spi_device_id for adi,adis16477-3 [ 6.780858] SPI driver adis16475 has no spi_device_id for adi,adis16465-1 [ 6.787605] SPI driver adis16475 has no spi_device_id for adi,adis16465-2 [ 6.794352] SPI driver adis16475 has no spi_device_id for adi,adis16465-3 [ 6.801099] SPI driver adis16475 has no spi_device_id for adi,adis16467-1 [ 6.807846] SPI driver adis16475 has no spi_device_id for adi,adis16467-2 [ 6.814596] SPI driver adis16475 has no spi_device_id for adi,adis16467-3 [ 6.821340] SPI driver adis16475 has no spi_device_id for adi,adis16500 [ 6.827914] SPI driver adis16475 has no spi_device_id for adi,adis16505-1 [ 6.834661] SPI driver adis16475 has no spi_device_id for adi,adis16505-2 [ 6.841408] SPI driver adis16475 has no spi_device_id for adi,adis16505-3 [ 6.848155] SPI driver adis16475 has no spi_device_id for adi,adis16507-1 [ 6.854906] SPI driver adis16475 has no spi_device_id for adi,adis16507-2 [ 6.861649] SPI driver adis16475 has no spi_device_id for adi,adis16507-3 [ 6.869543] axi_sysid 85000000.axi-sysid-0: AXI System ID core version (1.01.a) found [ 6.876366] axi_sysid 85000000.axi-sysid-0: [adrv9371x] on [zcu102] git branch <hdl_2022_r2> git <7ea497b6c24172ee293d6e0a9a387a16973da5ce> clean [2023-11-16 07:59:12] UTC [ 6.891994] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered [ 6.898306] usbcore: registered new interface driver snd-usb-audio [ 6.905883] pktgen: Packet Generator for packet performance testing. Version: 2.75 [ 6.912210] Initializing XFRM netlink socket [ 6.915790] NET: Registered PF_INET6 protocol family [ 6.921095] Segment Routing with IPv6 [ 6.924307] In-situ OAM (IOAM) with IPv6 [ 6.928237] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 6.934387] NET: Registered PF_PACKET protocol family [ 6.939080] NET: Registered PF_KEY protocol family [ 6.943900] can: controller area network core [ 6.948181] NET: Registered PF_CAN protocol family [ 6.952911] can: raw protocol [ 6.955850] can: broadcast manager protocol [ 6.960005] can: netlink gateway - max_hops=1 [ 6.964397] Bluetooth: RFCOMM TTY layer initialized [ 6.969178] Bluetooth: RFCOMM socket layer initialized [ 6.974293] Bluetooth: RFCOMM ver 1.11 [ 6.978002] Bluetooth: BNEP (Ethernet Emulation) ver 1.3 [ 6.983271] Bluetooth: BNEP filters: protocol multicast [ 6.988463] Bluetooth: BNEP socket layer initialized [ 6.993391] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 [ 6.999275] Bluetooth: HIDP socket layer initialized [ 7.004344] 9pnet: Installing 9P2000 support [ 7.008471] NET: Registered PF_IEEE802154 protocol family [ 7.013825] Key type dns_resolver registered [ 7.018242] registered taskstats version 1 [ 7.022114] Loading compiled-in X.509 certificates [ 7.027395] Btrfs loaded, crc32c=crc32c-generic, zoned=no, fsverity=no [ 7.042173] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 69, base_baud = 6249999) is a xuartps [ 7.051203] printk: console [ttyPS0] enabled [ 7.051203] printk: console [ttyPS0] enabled [ 7.055507] printk: bootconsole [cdns0] disabled [ 7.055507] printk: bootconsole [cdns0] disabled [ 7.064712] of-fpga-region fpga-full: FPGA Region probed [ 7.074802] nwl-pcie fd0e0000.pcie: host bridge /axi/pcie@fd0e0000 ranges: [ 7.081708] nwl-pcie fd0e0000.pcie: MEM 0x00e0000000..0x00efffffff -> 0x00e0000000 [ 7.089715] nwl-pcie fd0e0000.pcie: MEM 0x0600000000..0x07ffffffff -> 0x0600000000 [ 7.097792] nwl-pcie fd0e0000.pcie: Link is DOWN [ 7.102554] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00 [ 7.108737] pci_bus 0000:00: root bus resource [bus 00-ff] [ 7.114220] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff] [ 7.121098] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref] [ 7.128603] pci 0000:00:00.0: [10ee:d021] type 01 class 0x060400 [ 7.134669] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot [ 7.143417] pci 0000:00:00.0: PCI bridge to [bus 01-0c] [ 7.149600] xilinx-zynqmp-dma fd500000.dma-controller: ZynqMP DMA driver Probe success [ 7.157687] xilinx-zynqmp-dma fd510000.dma-controller: ZynqMP DMA driver Probe success [ 7.165772] xilinx-zynqmp-dma fd520000.dma-controller: ZynqMP DMA driver Probe success [ 7.173855] xilinx-zynqmp-dma fd530000.dma-controller: ZynqMP DMA driver Probe success [ 7.181938] xilinx-zynqmp-dma fd540000.dma-controller: ZynqMP DMA driver Probe success [ 7.190017] xilinx-zynqmp-dma fd550000.dma-controller: ZynqMP DMA driver Probe success [ 7.198100] xilinx-zynqmp-dma fd560000.dma-controller: ZynqMP DMA driver Probe success [ 7.206187] xilinx-zynqmp-dma fd570000.dma-controller: ZynqMP DMA driver Probe success [ 7.214340] xilinx-zynqmp-dma ffa80000.dma-controller: ZynqMP DMA driver Probe success [ 7.222421] xilinx-zynqmp-dma ffa90000.dma-controller: ZynqMP DMA driver Probe success [ 7.230501] xilinx-zynqmp-dma ffaa0000.dma-controller: ZynqMP DMA driver Probe success [ 7.238587] xilinx-zynqmp-dma ffab0000.dma-controller: ZynqMP DMA driver Probe success [ 7.246674] xilinx-zynqmp-dma ffac0000.dma-controller: ZynqMP DMA driver Probe success [ 7.254753] xilinx-zynqmp-dma ffad0000.dma-controller: ZynqMP DMA driver Probe success [ 7.262839] xilinx-zynqmp-dma ffae0000.dma-controller: ZynqMP DMA driver Probe success [ 7.270925] xilinx-zynqmp-dma ffaf0000.dma-controller: ZynqMP DMA driver Probe success [ 7.279242] xilinx-zynqmp-dpdma fd4c0000.dma-controller: Xilinx DPDMA engine is probed [ 7.288173] zynqmp-display fd4a0000.display: vtc bridge property not present [ 7.297442] zynqmp_clk_divider_set_rate() set divider failed for spi1_ref_div1, ret = -13 [ 7.306139] xilinx-dp-snd-codec fd4a0000.display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed [ 7.316240] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed [ 7.324319] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed [ 7.333165] xilinx-dp-snd-card fd4a0000.display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed [ 7.342740] OF: graph: no port node found in /axi/display@fd4a0000 [ 7.349285] xlnx-drm xlnx-drm.0: bound fd4a0000.display (ops 0xffffffc009196640) [ 8.433309] zynqmp-display fd4a0000.display: [drm] Cannot find any crtc or sizes [ 8.440969] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.display on minor 0 [ 8.448478] zynqmp-display fd4a0000.display: ZynqMP DisplayPort Subsystem driver probed [ 8.456728] ahci-ceva fd0c0000.ahci: supply ahci not found, using dummy regulator [ 8.464277] ahci-ceva fd0c0000.ahci: supply phy not found, using dummy regulator [ 8.471702] ahci-ceva fd0c0000.ahci: supply target not found, using dummy regulator [ 8.479450] ahci-ceva fd0c0000.ahci: ceva,p0-cominit-params property not defined [ 8.486879] ahci-ceva: probe of fd0c0000.ahci failed with error -22 [ 8.494683] ad9528 spi1.0: supply vcc not found, using dummy regulator [ 8.522811] jesd204: /axi/spi@ff040000/ad9528-1@0,jesd204:0,parent=spi1.0: Using as SYSREF provider [ 8.533816] xilinx_can ff070000.can can0: TDC Offset value not in range [ 8.540822] macb ff0e0000.ethernet: Not enabling partial store and forward [ 8.550928] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 38 (da:e2:3c:67:5e:8a) [ 8.561148] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM [ 8.567681] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM [ 8.574176] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM [ 8.580670] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM [ 8.608662] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 40 [ 8.615133] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 41 [ 8.621437] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer with timeout 60s [ 8.628897] cdns-wdt ff150000.watchdog: Xilinx Watchdog Timer with timeout 10s [ 8.639974] axi_adxcvr 84a60000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.05.a) using CPLL on GTH4 at 0x84A60000. Number of lanes: 2. [ 8.653066] axi_adxcvr 84a50000.axi-adxcvr-rx-os: AXI-ADXCVR-RX (17.05.a) using CPLL on GTH4 at 0x84A50000. Number of lanes: 2. [ 8.665477] axi_adxcvr 84a80000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.05.a) using QPLL on GTH4 at 0x84A80000. Number of lanes: 4. [ 8.670055] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit [ 8.679345] axi-jesd204-rx 84aa0000.axi-jesd204-rx: AXI-JESD204-RX (1.07.a) at 0x84AA0000. Encoder 8b10b, width 4/4, lanes 2, jesd204-fsm. [ 8.697177] axi-jesd204-rx 84ab0000.axi-jesd204-rx-os: AXI-JESD204-RX (1.07.a) at 0x84AB0000. Encoder 8b10b, width 4/4, lanes 2, jesd204-fsm. [ 8.710212] axi-jesd204-tx 84a90000.axi-jesd204-tx: AXI-JESD204-TX (1.06.a) at 0x84A90000. Encoder 8b10b, width 4/4, lanes 4, jesd204-fsm. [ 8.722811] ad9371 spi1.1: ad9371_probe : enter [ 8.752740] cf_axi_adc 84a00000.axi-ad9371-rx-hpc: ADI AIM (10.03.) at 0x84A00000 mapped to 0x(____ptrval____) probed ADC AD9371 as MASTER [ 8.785848] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition initialized -> probed [ 8.796909] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition initialized -> probed [ 8.807962] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition initialized -> probed [ 8.819020] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition probed -> idle [ 8.829467] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition probed -> idle [ 8.839913] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition probed -> idle [ 8.850360] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition idle -> device_init [ 8.861234] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition idle -> device_init [ 8.872102] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition idle -> device_init [ 8.882980] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition device_init -> link_init [ 8.894289] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition device_init -> link_init [ 8.905598] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition device_init -> link_init [ 8.916915] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_init -> link_supported [ 8.928481] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_init -> link_supported [ 8.940049] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_init -> link_supported [ 8.951808] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_supported -> link_pre_setup [ 8.963812] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_supported -> link_pre_setup [ 8.975815] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_supported -> link_pre_setup [ 8.987941] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_pre_setup -> clk_sync_stage1 [ 9.000035] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_pre_setup -> clk_sync_stage1 [ 9.012119] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_pre_setup -> clk_sync_stage1 [ 9.024214] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage1 -> clk_sync_stage2 [ 9.036390] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage1 -> clk_sync_stage2 [ 9.048570] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage1 -> clk_sync_stage2 [ 9.060753] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage2 -> clk_sync_stage3 [ 9.072942] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage2 -> clk_sync_stage3 [ 9.085118] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage2 -> clk_sync_stage3 [ 9.132352] axi_adxcvr 84a80000.axi-adxcvr-tx: adxcvr_clk_enable: QPLL TX buffer underflow error, status: 0x61 [ 9.142338] axi_adxcvr 84a80000.axi-adxcvr-tx: adxcvr_clk_enable: QPLL TX buffer overflow error, status: 0x61 [ 9.152253] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage3 -> link_setup [ 9.163995] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage3 -> link_setup [ 9.175741] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage3 -> link_setup [ 9.190269] mmc0: new high speed SDHC card at address 59b4 [ 9.196155] mmcblk0: mmc0:59b4 USD 14.7 GiB [ 9.202255] mmcblk0: p1 p2 p3 [ 9.725311] zynqmp-display fd4a0000.display: [drm] Cannot find any crtc or sizes [ 9.930028] random: fast init done [ 9.935866] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_setup -> opt_setup_stage1 [ 9.947695] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_setup -> opt_setup_stage1 [ 9.959524] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_setup -> opt_setup_stage1 [ 10.017318] ad9371 spi1.1: MCS failed (0x8) [ 10.021499] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] In opt_setup_stage2 got error from cb: -14 [ 10.033424] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: Rolling back from 'opt_setup_stage1', got error -14 [ 10.044991] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition opt_setup_stage1 -> opt_setup_stage2 [ 10.057338] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition opt_setup_stage1 -> opt_setup_stage2 [ 10.069682] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition opt_setup_stage1 -> opt_setup_stage2 [ 10.082037] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition opt_setup_stage2 -> opt_setup_stage1 [ 10.094385] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition opt_setup_stage2 -> opt_setup_stage1 [ 10.106735] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition opt_setup_stage2 -> opt_setup_stage1 [ 10.119089] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition opt_setup_stage1 -> link_setup [ 10.130919] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition opt_setup_stage1 -> link_setup [ 10.142754] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition opt_setup_stage1 -> link_setup [ 10.154585] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_setup -> clk_sync_stage3 [ 10.166325] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_setup -> clk_sync_stage3 [ 10.178068] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_setup -> clk_sync_stage3 [ 10.189807] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage3 -> clk_sync_stage2 [ 10.201982] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage3 -> clk_sync_stage2 [ 10.214151] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage3 -> clk_sync_stage2 [ 10.226323] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage2 -> clk_sync_stage1 [ 10.238499] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage2 -> clk_sync_stage1 [ 10.250677] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage2 -> clk_sync_stage1 [ 10.262851] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage1 -> link_pre_setup [ 10.274941] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage1 -> link_pre_setup [ 10.287029] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage1 -> link_pre_setup [ 10.299125] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_pre_setup -> link_supported [ 10.311124] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_pre_setup -> link_supported [ 10.323120] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_pre_setup -> link_supported [ 10.335120] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_supported -> link_init [ 10.346685] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_supported -> link_init [ 10.358248] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_supported -> link_init [ 10.369813] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_init -> device_init [ 10.381120] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_init -> device_init [ 10.392421] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_init -> device_init [ 10.403730] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition device_init -> idle [ 10.414599] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition device_init -> idle [ 10.425474] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition device_init -> idle [ 10.436346] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition idle -> idle [ 10.446611] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition idle -> idle [ 10.456870] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition idle -> idle [ 10.467133] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition idle -> device_init [ 10.478013] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition idle -> device_init [ 10.488882] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition idle -> device_init [ 10.499763] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition device_init -> link_init [ 10.511068] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition device_init -> link_init [ 10.522368] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition device_init -> link_init [ 10.533684] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_init -> link_supported [ 10.545251] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_init -> link_supported [ 10.556819] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_init -> link_supported [ 10.568559] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_supported -> link_pre_setup [ 10.580563] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_supported -> link_pre_setup [ 10.592564] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_supported -> link_pre_setup [ 10.613319] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_pre_setup -> clk_sync_stage1 [ 10.625410] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_pre_setup -> clk_sync_stage1 [ 10.637501] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_pre_setup -> clk_sync_stage1 [ 10.649592] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage1 -> clk_sync_stage2 [ 10.661762] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage1 -> clk_sync_stage2 [ 10.673940] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage1 -> clk_sync_stage2 [ 10.686112] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage2 -> clk_sync_stage3 [ 10.698287] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage2 -> clk_sync_stage3 [ 10.710456] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage2 -> clk_sync_stage3 [ 10.757679] axi_adxcvr 84a80000.axi-adxcvr-tx: adxcvr_clk_enable: QPLL TX buffer underflow error, status: 0x61 [ 10.767668] axi_adxcvr 84a80000.axi-adxcvr-tx: adxcvr_clk_enable: QPLL TX buffer overflow error, status: 0x61 [ 10.777586] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage3 -> link_setup [ 10.789324] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage3 -> link_setup [ 10.801067] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage3 -> link_setup [ 11.531787] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_setup -> opt_setup_stage1 [ 11.543622] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_setup -> opt_setup_stage1 [ 11.555446] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_setup -> opt_setup_stage1 [ 11.613313] ad9371 spi1.1: MCS failed (0x8) [ 11.617491] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] In opt_setup_stage2 got error from cb: -14 [ 11.629409] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: Rolling back from 'opt_setup_stage1', got error -14 [ 11.640981] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition opt_setup_stage1 -> opt_setup_stage2 [ 11.653332] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition opt_setup_stage1 -> opt_setup_stage2 [ 11.665680] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition opt_setup_stage1 -> opt_setup_stage2 [ 11.678032] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition opt_setup_stage2 -> opt_setup_stage1 [ 11.690377] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition opt_setup_stage2 -> opt_setup_stage1 [ 11.702728] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition opt_setup_stage2 -> opt_setup_stage1 [ 11.715077] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition opt_setup_stage1 -> link_setup [ 11.726902] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition opt_setup_stage1 -> link_setup [ 11.738736] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition opt_setup_stage1 -> link_setup [ 11.750568] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_setup -> clk_sync_stage3 [ 11.762310] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_setup -> clk_sync_stage3 [ 11.774052] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_setup -> clk_sync_stage3 [ 11.785790] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage3 -> clk_sync_stage2 [ 11.797965] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage3 -> clk_sync_stage2 [ 11.810134] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage3 -> clk_sync_stage2 [ 11.822307] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage2 -> clk_sync_stage1 [ 11.834482] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage2 -> clk_sync_stage1 [ 11.846651] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage2 -> clk_sync_stage1 [ 11.858824] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage1 -> link_pre_setup [ 11.870918] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage1 -> link_pre_setup [ 11.883003] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage1 -> link_pre_setup [ 11.895098] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_pre_setup -> link_supported [ 11.907097] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_pre_setup -> link_supported [ 11.919093] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_pre_setup -> link_supported [ 11.931094] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_supported -> link_init [ 11.942661] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_supported -> link_init [ 11.954222] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_supported -> link_init [ 11.965787] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_init -> device_init [ 11.977096] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_init -> device_init [ 11.988404] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_init -> device_init [ 11.999713] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition device_init -> idle [ 12.010581] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition device_init -> idle [ 12.021447] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition device_init -> idle [ 12.032321] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition idle -> idle [ 12.042584] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition idle -> idle [ 12.052844] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition idle -> idle [ 12.063108] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition idle -> device_init [ 12.073986] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition idle -> device_init [ 12.084857] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition idle -> device_init [ 12.095737] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition device_init -> link_init [ 12.107042] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition device_init -> link_init [ 12.118344] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition device_init -> link_init [ 12.129656] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_init -> link_supported [ 12.141225] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_init -> link_supported [ 12.152794] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_init -> link_supported [ 12.164548] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_supported -> link_pre_setup [ 12.176555] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_supported -> link_pre_setup [ 12.188557] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_supported -> link_pre_setup [ 12.200680] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_pre_setup -> clk_sync_stage1 [ 12.212766] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_pre_setup -> clk_sync_stage1 [ 12.224856] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_pre_setup -> clk_sync_stage1 [ 12.236942] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage1 -> clk_sync_stage2 [ 12.249116] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage1 -> clk_sync_stage2 [ 12.261289] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage1 -> clk_sync_stage2 [ 12.273471] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage2 -> clk_sync_stage3 [ 12.285643] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage2 -> clk_sync_stage3 [ 12.297822] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage2 -> clk_sync_stage3 [ 12.345050] axi_adxcvr 84a80000.axi-adxcvr-tx: adxcvr_clk_enable: QPLL TX buffer underflow error, status: 0x61 [ 12.355041] axi_adxcvr 84a80000.axi-adxcvr-tx: adxcvr_clk_enable: QPLL TX buffer overflow error, status: 0x61 [ 12.364953] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage3 -> link_setup [ 12.376695] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage3 -> link_setup [ 12.388434] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage3 -> link_setup [ 13.131795] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_setup -> opt_setup_stage1 [ 13.143628] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_setup -> opt_setup_stage1 [ 13.155455] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_setup -> opt_setup_stage1 [ 13.213313] ad9371 spi1.1: MCS failed (0x8) [ 13.217493] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] In opt_setup_stage2 got error from cb: -14 [ 13.229416] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: Rolling back from 'opt_setup_stage1', got error -14 [ 13.240984] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition opt_setup_stage1 -> opt_setup_stage2 [ 13.253332] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition opt_setup_stage1 -> opt_setup_stage2 [ 13.265683] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition opt_setup_stage1 -> opt_setup_stage2 [ 13.278030] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition opt_setup_stage2 -> opt_setup_stage1 [ 13.290378] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition opt_setup_stage2 -> opt_setup_stage1 [ 13.302721] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition opt_setup_stage2 -> opt_setup_stage1 [ 13.315070] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition opt_setup_stage1 -> link_setup [ 13.326895] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition opt_setup_stage1 -> link_setup [ 13.338731] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition opt_setup_stage1 -> link_setup [ 13.350561] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_setup -> clk_sync_stage3 [ 13.362300] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_setup -> clk_sync_stage3 [ 13.374034] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_setup -> clk_sync_stage3 [ 13.385775] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage3 -> clk_sync_stage2 [ 13.397949] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage3 -> clk_sync_stage2 [ 13.410118] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage3 -> clk_sync_stage2 [ 13.422291] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage2 -> clk_sync_stage1 [ 13.434465] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage2 -> clk_sync_stage1 [ 13.446637] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage2 -> clk_sync_stage1 [ 13.458817] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage1 -> link_pre_setup [ 13.470909] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage1 -> link_pre_setup [ 13.482996] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage1 -> link_pre_setup [ 13.495083] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_pre_setup -> link_supported [ 13.507083] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_pre_setup -> link_supported [ 13.519078] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_pre_setup -> link_supported [ 13.531078] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_supported -> link_init [ 13.542645] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_supported -> link_init [ 13.554208] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_supported -> link_init [ 13.565780] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_init -> device_init [ 13.577087] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_init -> device_init [ 13.588388] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_init -> device_init [ 13.599697] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition device_init -> idle [ 13.610566] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition device_init -> idle [ 13.621442] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition device_init -> idle [ 13.632314] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition idle -> idle [ 13.642577] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition idle -> idle [ 13.652837] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition idle -> idle [ 13.663103] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition idle -> device_init [ 13.673972] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition idle -> device_init [ 13.684840] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition idle -> device_init [ 13.695712] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition device_init -> link_init [ 13.707017] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition device_init -> link_init [ 13.718319] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition device_init -> link_init [ 13.729632] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_init -> link_supported [ 13.741201] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_init -> link_supported [ 13.752770] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_init -> link_supported [ 13.764522] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_supported -> link_pre_setup [ 13.776532] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_supported -> link_pre_setup [ 13.788532] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_supported -> link_pre_setup [ 13.800647] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_pre_setup -> clk_sync_stage1 [ 13.812734] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_pre_setup -> clk_sync_stage1 [ 13.824822] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_pre_setup -> clk_sync_stage1 [ 13.836909] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage1 -> clk_sync_stage2 [ 13.849083] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage1 -> clk_sync_stage2 [ 13.861256] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage1 -> clk_sync_stage2 [ 13.873438] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage2 -> clk_sync_stage3 [ 13.885612] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage2 -> clk_sync_stage3 [ 13.897787] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage2 -> clk_sync_stage3 [ 13.945008] axi_adxcvr 84a80000.axi-adxcvr-tx: adxcvr_clk_enable: QPLL TX buffer underflow error, status: 0x61 [ 13.954999] axi_adxcvr 84a80000.axi-adxcvr-tx: adxcvr_clk_enable: QPLL TX buffer overflow error, status: 0x61 [ 13.964911] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage3 -> link_setup [ 13.976654] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage3 -> link_setup [ 13.988391] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage3 -> link_setup [ 14.732371] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_setup -> opt_setup_stage1 [ 14.744203] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_setup -> opt_setup_stage1 [ 14.756031] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_setup -> opt_setup_stage1 [ 14.813317] ad9371 spi1.1: MCS failed (0x8) [ 14.817493] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] In opt_setup_stage2 got error from cb: -14 [ 14.829414] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: Rolling back from 'opt_setup_stage1', got error -14 [ 14.840985] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition opt_setup_stage1 -> opt_setup_stage2 [ 14.853334] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition opt_setup_stage1 -> opt_setup_stage2 [ 14.865685] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition opt_setup_stage1 -> opt_setup_stage2 [ 14.878032] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition opt_setup_stage2 -> opt_setup_stage1 [ 14.890379] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition opt_setup_stage2 -> opt_setup_stage1 [ 14.902722] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition opt_setup_stage2 -> opt_setup_stage1 [ 14.915072] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition opt_setup_stage1 -> link_setup [ 14.926897] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition opt_setup_stage1 -> link_setup [ 14.938731] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition opt_setup_stage1 -> link_setup [ 14.950562] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_setup -> clk_sync_stage3 [ 14.962302] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_setup -> clk_sync_stage3 [ 14.974037] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_setup -> clk_sync_stage3 [ 14.985776] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage3 -> clk_sync_stage2 [ 14.997951] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage3 -> clk_sync_stage2 [ 15.010120] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage3 -> clk_sync_stage2 [ 15.022293] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage2 -> clk_sync_stage1 [ 15.034468] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage2 -> clk_sync_stage1 [ 15.046637] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage2 -> clk_sync_stage1 [ 15.058810] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition clk_sync_stage1 -> link_pre_setup [ 15.070901] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition clk_sync_stage1 -> link_pre_setup [ 15.082988] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition clk_sync_stage1 -> link_pre_setup [ 15.095076] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_pre_setup -> link_supported [ 15.107076] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_pre_setup -> link_supported [ 15.119080] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_pre_setup -> link_supported [ 15.131078] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_supported -> link_init [ 15.142645] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_supported -> link_init [ 15.154208] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_supported -> link_init [ 15.165773] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition link_init -> device_init [ 15.177080] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition link_init -> device_init [ 15.188381] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition link_init -> device_init [ 15.199690] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:2] transition device_init -> idle [ 15.210559] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:1] transition device_init -> idle [ 15.221426] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: JESD204[0:0] transition device_init -> idle [ 15.232294] jesd204: /axi/spi@ff040000/ad9371-phy@1,jesd204:1,parent=spi1.1: FSM completed with error -14 [ 15.241864] cf_axi_dds 84a04000.axi-ad9371-tx-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x84A04000 mapped to 0x(____ptrval____), probed DDS AD9371 [ 15.258637] of_cfs_init [ 15.261092] of_cfs_init: OK [ 15.264047] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 15.404761] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 15.411300] clk: Not disabling unused clocks [ 15.415861] ALSA device list: [ 15.418818] #0: DisplayPort monitor [ 15.422784] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 [ 15.423403] Freeing unused kernel memory: 2624K [ 15.431398] cfg80211: failed to load regulatory.db [ 15.453344] Run /init as init process [ 15.466672] systemd[1]: System time before build time, advancing clock. [ 15.476919] systemd[1]: systemd 249.7+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid) [ 15.507224] systemd[1]: Detected architecture arm64.
Question:
Is there something I have to change in the configuration of the AD9371 HDL block, specifically relating to the QPLL parameters, to make the firmware work with a 100MHz reference clock? Do you know if the 100MHz reference clock puts the QPLL outside of it's desired operating range when using the default configuration (which is intended for a 122.88MHz reference clock)?
Thank you.