Post Go back to editing

Usage of SYSREF in ADRV9009 reference designs

Thread Summary

The user inquired about the necessity of multiple SYSREF signals for multiple ADRV9009 devices in a design. The final answer confirmed that a single SYSREF is sufficient for synchronizing RX, TX, and ORX JESD modules, with the use of multiple SYSREFs providing flexibility for independent configurations. The issue was resolved and can be closed.
AI Generated Content
Category: Software

Hello,
I've been looking at the ADRV9009 reference designs featuring multiple ADRV9009s, and have a question regarding their usage of SYSREF:
Generally, in the system block diagrams,  three independant sysref ports are connected to RX , ORX and TX JESD modules... and on the top level, ORX and TX share the same SYSREF , associated with one device, while the RX module gets a SYSREF associated to another device.

On a design where multiple ADRV9009s are all locked to the same reference, is there any benefit/requirement of getting multiple SYSREF to the FPGA ? 

My understanding is that we should only require 1 reference clock and 1 sysref going to the FPGA, in order to synchronize multiple ADRV9009s, and thus use that single SYSREF on RX,TX and ORX JESD modules. Is that correct ?


Thank you.
Best regards,
Romain

Parents
  • Hi Romain,

    In the reference designs that you mentioned, we use the two SYSREF just to match the same rates to the same SYSREF . So that's why the ORX and TX share the same SYSREF and the RX uses another one.

    Either way, this is not necessary and it is enough for only one SYSREF to go into the FPGA.

    The main reason for having two SYSREF is flexibility. For example, someone might want to use each chip independently with different configurations.

    Best regards,

    Andrei

Reply
  • Hi Romain,

    In the reference designs that you mentioned, we use the two SYSREF just to match the same rates to the same SYSREF . So that's why the ORX and TX share the same SYSREF and the RX uses another one.

    Either way, this is not necessary and it is enough for only one SYSREF to go into the FPGA.

    The main reason for having two SYSREF is flexibility. For example, someone might want to use each chip independently with different configurations.

    Best regards,

    Andrei

Children
No Data