Post Go back to editing

Enclustra ST1/XU8 and AD-FMCOMMS3-EBZ

Thread Summary

The user successfully connected the AD-FMCOMMS3-EBZ to the Enclustra Mercury ST1/XU8 despite 7 missing connections on the HPC FMC connector. A simple patch was applied, and the user shared the open-source GitHub repository with the solution. The Analog Devices support engineer acknowledged the solution and thanked the user for sharing it.
AI Generated Content
Category: Hardware

I got AD-FMCOMMS3-EBZ in my hands. I also own Enclustra Mercury ST1/XU8.

There are 7 missing connections between ST1/XU8 and FMCOMMS3 HPC FMC connector.

With relatively simple patch I managed to make it works.

I would like to share what I did, so here is link to open source git hub xu8_fmcomms3 and image

image