Post Go back to editing

can not update iio with zc706+adrv9371

Category: Software
Product Number: ad9371, zc706

Hi team,

I try to configure SD card for adrv9371-w/pcbz and zc706 platform. The problem is no IIO GUI showed on the monitor.

I followed the steps from wiki to configure sd-cardhttps://wiki.analog.com/resources/tools-software/linux-software/kuiper-linux.

After I wrote the image file to sd-card, I copied three documents below to BOOT partition.

  1. Zynq-zc706-adv7511-adrv937x/BOOT.BIN
  2. Zynq-zc706-adv7511-adrv937x/devicetree/dtb
  3. Zynq-common/ulmage

Then I setup the physical system. The hdmi monitor could not show IIO gui.

How do I solve this problem?

Parents
  • I just tried with a clean 2021_R2 Kuiper image card and those files as you mentioned, and for me it opens the GUI and also catches signals in the capture window.

    There is a situation when it doesn't capture, and it is the following: if I open IIO Oscilloscope on my computer and connect to the board through IP, and then open it in Kuiper, then indeed the capture is shown only on my computer since is the first one opened. But this is not the case for you.

    Anyway, it opens the IIO Oscilloscope GUI in both situations.

    Did you try opening a terminal in Kuiper and writing sudo osc to open IIO Oscilloscope? The password for the user <analog> is again <analog>.

    Best regards,
    Iulia

  • Hi Lulia,

    Thanks for your reply.

    In the meantime, could you please tell me what Kuiper image you used? Is it the 2021_r2 one, the latest?

    Yes, I used the lasted image document.

    Actually I tried to open an serial terminal on PC after setting up the physical system, but nothing printed on the terminal. Maybe I installed the wrong UART driver on PC? Could you tell me which version of UART driver you used?

Reply
  • Hi Lulia,

    Thanks for your reply.

    In the meantime, could you please tell me what Kuiper image you used? Is it the 2021_r2 one, the latest?

    Yes, I used the lasted image document.

    Actually I tried to open an serial terminal on PC after setting up the physical system, but nothing printed on the terminal. Maybe I installed the wrong UART driver on PC? Could you tell me which version of UART driver you used?

Children
No Data