Hi,
I am trying to calibrate AD9361 on a custom board with A10 FPGA.
For initial setup, In RX mode AD9361 is tuning for 25MHz and 40MHz but not for 61.44MHz
TX is not at all tuning
What might be the reason for this error.
Thanks
Prince
AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiver™ designed for use in 3G and
4G base station applications. Its...
Datasheet
AD9361 on Analog.com
AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiver™ designed for use in 3G and
4G base station applications. Its...
Datasheet
AD9361 on Analog.com
Hi,
I am trying to calibrate AD9361 on a custom board with A10 FPGA.
For initial setup, In RX mode AD9361 is tuning for 25MHz and 40MHz but not for 61.44MHz
TX is not at all tuning
What might be the reason for this error.
Thanks
Prince
let me know if more clarification is required
Are you using CMOS or LVDS interface?
Also, are you using the latest no-OS drivers? If not using latest, then please upgrade to the latest and then try initializing with the default sequence:
https://github.com/analogdevicesinc/no-OS/tree/master/projects/ad9361
https://github.com/analogdevicesinc/no-OS/tree/master/drivers/rf-transceiver/ad9361
https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/software/baremetal#downloads
Hi srimoyi
I am using LVDS interface
As for the hdl, I am using hdl_2019R1, for its compatibility with Quartus 18.1 std.
Does executing intel_serdes in non-dpa mode, affects the digital tuning of ad9361?
Also which is the best suitable hdl repository for A10+AD9361
Does executing intel_serdes in non-dpa mode, affects the digital tuning of ad9361?
Also which is the best suitable hdl repository for A10+AD9361
Moving to FPGA reference designs for comments.
Hi,
there is one more observation in the design, if we try to calibrate it at LO > 3 GHz, it throws error ”Failed to restore ensm state”
Hi,
Sorry for the delay.
Does executing intel_serdes in non-dpa mode, affects the digital tuning of ad9361?
Active DPA helps. Ideally you wil control the PLL feeding the DPA at run time. If you create the proper constraints regarding the delays between data lines and clock, you should be fine.
Also which is the best suitable hdl repository for A10+AD9361
We always recommend the latest release or master branch, because we have the tools installed and have a good knowledge of the features/fixes/limitations/bugs.
But in this case, we do not have an active design supported on a10 with AD9361, and the last functional changes done on axi_ad9361 for a10 were included in hdl_2019_r2 branch.
You decide what version is better suited for you. The support we ca offer is limited in this case.
Andrei
there is one more observation in the design, if we try to calibrate it at LO > 3 GHz, it throws error ”Failed to restore ensm state”
Can you open a new thread regarding this on the no-OS/Linux forum?
Andrei
Hi Andrei,
As of now, while calibrating AD9361, it gets tuned at 25MHz, but not at 40MHz and 61.44 MHz (In 2r2t mode)
Where as, it gets tuned at 25MHz and 40Mhz but not at 61.44 MHz (In 1r1t mode)
I would also like to add that this is the case with RX.
In case of TX, Tuning Fails for all three rates i.e. 25Mhz, 40Mhz and 61.44MHz.
Should I add some kind of delay in tx_frame or tx_data_out?
Hi,
Ideally the delay for data and frame in regards to the tx clock should be close to none. The tuning algorithm should set the right delays at the ad9361 level.
Can you add a signal tap and look at the signals? Is there something strange on the tx side.
I would suggest to double check the hardware connections as much as possible on the tx.
- are data/frame pins connected correctly?
- do you have test points on the FMC doughtier card or an extender/expansion card that word allow you access to the clock/frame/data lines for debug?
Andrei
Hi,
I added a few clk_buffers at rx_clk, after that ad9361 is tuning at 25 MHz for both RX and TX but failing for both 40MHz and 61.44MHz.
I just want to point out that this is the case with a10 and ad9361. So Altera serdes IP is used and that too in non-dpa mode.
Maybe individual serdes elements (one for each tx_data_out[0..5]) are adding variable delays, due to which ad9361 is not tuning at higher data rates?
Would request your comments on this issue.
Regards
Prince
Hi,
I will have to think/consult with colleagues about this, mostly in regards with the a10 SERDES, haven't played with it in a while. From the top of my head, this should not be the case on tx, but maybe I'm missing something.
Andrei
Hi,
Some hardware things that can cause this behavior:
1. trace length mismatch
2. cross talk between clock and data/frame lines.
My suggestion is to check the above and play a bit with the drive strength of the tx pins.
Andrei