Post Go back to editing

EVAL-TPG-ZYNQ3 for AD9680

Thread Summary

The user inquires about replacing the ZC706 with the EVAL-TPG-ZYNQ3 for a system using the AD9680 EVM (DAQ3). The final answer confirms that the ZYNQ3 should work with the ZC706 collateral, noting potential hardware differences. The EVAL-TPG-ZYNQ3 does not offer a Vivado license for the Zynq device, and the user should use the ZC706 Vivado board license. The user is directed to the ADRV9008-1/ADRV9008-2/ADRV9009 forum for more details on the ZYNQ3 product.
AI Generated Content
Category: Hardware
Product Number: EVAL-TPG-ZYNQ3

Hi,

I was using Zc706 + AD9680 EVM (DAQ3). Due to some sourcing issue we are unable to procure ZC706. I have developed some Proof of concept system using Zc706.

1. In this case , we can i replace ZC706 with EVAL-TPG-ZYNQ3. 

2. In case these is no software support for AD9680 (DAQ3) avb in  EVAL-TPG-ZYNQ3.Can I port the FPGA reference design in Zc706 to EVAL-TPG-ZYNQ3 and re-build?

3. Similar case for Linux system

4. Does EVAL-TPG-ZYNQ3 offer Vivado license for Zynq Device or can i use Zc706 Vivado board license to access SoC in EVAL-TPG-ZYNQ3?