Post Go back to editing

Gen waveform with No-OS design with FMCOMMS4 and Zynq7000

Software Version: 2019_r2

Hi,

AD-FMCOMMS4-EBZ + ZEDBOARD

I would like to use No-OS in Zedboard and FMCOMMS4 to generate some signals like (sinewave, sawtooth, fmcw ...)

How can I do it in PS or may be PL? Searching for some examples in this problems but could not found. 

Is there someone have done this with No-Os + Zynq + FMCOMMS2/3/4 ?

Any answer would be appreciated!

Thanks

Top Replies

    •  Analog Employees 
    Mar 23, 2023 in reply to VPHAM589 +1 verified

    According to your answer, just only sine-waves could be used with this board (FMCOMMS4)!?

    Are you sure? Because I have seen the references design (in the SD card) booting with the SD Card.

    A…

Parents Reply Children