Post Go back to editing

External booting from ADRV9361-Z7035

Category: Hardware
Product Number: ADRV9361-Z7035

We have a problem with external booting the ADRV9361-Z7035 , We cannot boot. We follow the Switch setting for external boot but it didn't help.
Is there a recommendation on what type of micro SD to use? Are there other recommendations?
We use a SAN DISK micro SD card, type "EXTREME PRO-SDSQXCY-064G-GN6MA" and as mentioned, can boot only when it is inserted in the SOM SD card socket.

Top Replies

    •  Analog Employees 
    Mar 22, 2023 in reply to D_S +1 verified

    Hi,

    The report from the serial port is that Uboot is OK while the RAM boot fails.

    Have you probed de VCC on the SD card ?

    Our suggestions, if possible, are:

    1. Test your SD card with the reference…