Post Go back to editing

ADRV9364-z7020 in ADRV1CRR-FMC

Category: Hardware
Product Number: ADRV-9364-z7020
Software Version: Vivado 2021.2

Hey guys,

I wanted to reach out because I am planning to do a temporary development step of using the ADRV1CRR-FMC carrier to power/connect to my newly acquired z7020. My current FPGA image/kuiper software stack ran well on this carrier with the z7035, but I wanted to check for the latest information on installing the "smaller" FPGA card onto this carrier. It would seem that there would be no IO conflicts/bus contention risks in any of the documentation, but I want to be sure.

My plan is the implement a custom version of the BOB, which is in the works, but to continue the software porting work I need to use the ADRV1CRR-FMC.

I know you guys have said it can work, but has there been any change to this? I assume I would just use the same Vivado project as the BOB to do this, since it shares a common header set.

Am I on the right track? Should I reconsider? I will be scrutinizing both schematics to see if there is anything sus, but I also wanted to reach out.

Thank you,

Luke

Parents Reply Children
  • Hi,

    So, I would need to edit the .xdc files for the pins I want to change?

    Yes.

    Is there no example project of someone doing this?

    I'm not aware of any.

    Andrei

  • Andrei, I spent a good part of yesterday trying to edit the .xdc files to get a working image. I also went into the BD in Vivado and removed a bunch of the IP, like HDMI, that I won't be using. Is there no way to just add ethernet support to the example BOB project for the z7020? They have a common pinning for the ethernet PHY. It just would seem to be much cleaner since I only need linux running a shell over ethernet.

    Luke

  • Is there no way to just add ethernet support to the example BOB project for the z7020? They have a common pinning for the ethernet PHY. It just would seem to be much cleaner since I only need linux running a shell over ethernet.

    The ADI designs for adrv9361z7035 and adrv9364z7020 both have ethernet connections in our reference design. The eth phy is directly connected to the zynq mio's.
    That is all. no separate license needed for ethernet. 

    Andrei

  • Hi Andrei,

    I am trying to work from ../hdl/projects/adrv9364z7020 (or z7035) and using vivado. When I scrutinize the XDC for the z7020 I do not see any ethernet parameters or pins called out. I want to use the PHY on the card. Is this just a constraint that Vivado knows to apply for this device? I really would like some clear instructions on how to build the z7020 image ensuring ethernet is included. Right now, in Vivado, I see no indication that ethernet is being included in the design. Am I missing something?

    Thank you,

    Luke

  • Andrei,

    I believe I have figured this out. The key is Vivado (and more specifically the Zynq IP) configures the "fixed" IO from its own knowledge of each device. When I look at the output of the z7020 example that can be built I see my ethernet pins are completely routed to MIO "fixed IO" pins and are consistent with my schematic for the PHY interface. These are then consistent with the IP configuration tool in Vivado for the Zynq. I appreciate all of your help, but this seems very clear now.

    Luke