KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
Datasheet
AD9361 on Analog.com
Hello everyone,
I'm working on a design with AD9361 and Zedboard. I was able to run the SAMPLE project designed in Ad9361 in the name_HDL. I work for no-os. I have a few questions about AD9361 IP;
1- What I want to do in my design is actually to print the signs of different frequencies I produce in numerical design. All I need is the 16bit input pin that I will enter the I and Q channels on IP. But it seems to have your own DDS on the IP. Although I do DDS_DISABLE 1, I see that sign on what I just entered into the tx_lo_en value at the txout. What do you think I should do?
2- I want to be able to take the signs produced in different tones and process those signs in different tones using the AD9361's download. But now I can't see ADC Raw Data with ILA. How can I correct this situation?
As you can see for the DAC, I produce signs at 2 different frequency and enter the dac_datai and q pins of the AD9361 IP. I want to do the signs of 3 and 5mhz with tx_lo and see it in TXout.
For example tx_lo = 2400MHz
Two tone = 3mhz and 5 MHz
tx_out = 2403MHz and 2405mhz or 2397mhz and 2395mhz

Sincelery
Closed due to inactivity