Hello,
I want to use AD9517 to generate the internal clock. I have populated C304, C305, C306, and C307 with 0.1 µF capacitors and have removed C209 and C210 to disconnect the default clock path inputs as mentioned on (wiki.analog.com/.../ad9467). The Jumper P200 is in OFF position using a jumper.
I have tried to set the clock frequency to 150 MHz using Zedboard via SPI. However, the actual clock frequency read is random (varies between 100MHz to 200MHz). How can I resolve this issue ?