Hi,
We are trying to bring up(initialize) the ad axi xcvr, In the IP documentation, as per the software guidelines it is mentioned to control "LPM_DFE_N, RATE, SYSCLK_SEL, OUTCLK_SEL register bits and then set RESETN bit to 0x1",which we are taking care off in software, however xvr_clk_enable() is failing, and there is some issue with the vco frequency selection too. We are using HMC7044 as clock generator to generate required reference clock which is working fine.
Is there any sequence to bring up the FPGA JESD IPs(xcvr) because after setting the RESETN bit(reg 0x0010), we are not getting anything in the status register(reg 0x0014), i.e (It is always 0x00).So is there anything else that we are missing and that has to be taken care off. Is there something to do with the ref clock frequency or the JESD parameters for xcvr (however we are taking that too into consideration).
We are using AD9208.
Needed some solution/suggestion on this asap.
Regards,
Sourav