Category: Hardware
Product Number: ADRV9361-Z7035
I am running HDL reference design on ADRV9361-Z7035 + ADRV1CRR-BOB using Kuiper Linux OS and want to add a couple more UART ports. I think I need to add UART IP blocks to the PL part and customize the kernel as well.
Is there any tutorial on how to add user logic to the HDL reference design and write a driver or configure the kernel image?
If it is already possible to control any unused I/O pins as GPIO using IIO library, I can try to write a “bit-banging” software UART code.
Kind regards.