Post Go back to editing

clock domain crossing in ADI HDL projects

Category: Hardware

Hello,

We'd like to design an FPGA interface and control logic for AD9648 ADC. As I can see there is no reference design for this chip, but are for many others similar. Regarding the structure of these design, it seems common that the applied AXI interconnect clock/aresetn signals between the master CPU and slave peripherals are the same and the clock domain crossing and data transfer is implemented in the peripherals (hdl/up_xfer_cntrl.v at master · analogdevicesinc/hdl · GitHub).

Is there any specific reason that your designs prefer this method excusively instead of suppling AXI interconnect with different clocks and reset signals?

In other words, why don't we leave the interconnect to synchronize the different clock domains?

It would be great to have some explanation for this. 

Thanks

  • Hello Molnar,

    For AXI Interconnect you had to connect a clock and reset for every port, and as you noticed they were usually the same clocks and resets that were used in the entire system. If two different clocks are needed, it forces the interconnect to infer an async clock crossing. The clock domain is usually inferred from the AXI Interface connections you make.

    Also, you may have noticed that  in some cases, instead of AXI Interconnect we use AXI SmartConnect, which is the successor of AXI Interconnect. And in this case only a clock an reset are required. Of course, the number of individual input clocks can be increased if needed. 

    Hope this information will give you a better understading upon the AXI Interconnect clocking.

    Kind Regards,

    Stanca