Thanks in Advance
Goli Ganesh
AD9231
Production
The AD9231 is a monolithic, dual-channel, 1.8 V supply, 12-bit, 20 MSPS / 40 MSPS / 65 MSPS/80 MSPS analog-to-digital converter (ADC). It features a high...
Datasheet
AD9231 on Analog.com
Thanks in Advance
Goli Ganesh
Hello,
The AD9213 evaluation board doesn't have clocking onboard so there is no path to clock the trasceivers clocking input. How did you got around this ?
Regards,
Adrian
Hi AdrianC ,
Hello,
I don't have access to that FMC board schematic. Is it something you can share ?
Regards,
Adrian
Hi AdrianC ,
Here I am attaching the HTG AD9213 FMC board Schematic.
https://drive.google.com/drive/folders/1gjMeuWKi18H41zhVwqu5rQ1X3AdprupG?usp=sharing
Thanks in Advance
Goli Ganesh
Hi AdrianC ,
I am using the below clock configurations for HTG_AD9213_VCU118. Can you please verify whether I am configuring it correctly or not.
L = 16, M =1 (real ADC) , N = NP = 16 , fout = 10Gsps , F = 2 , S = 16, HD = 0, JESD Subclass = 1.
HMC7044 clkin freq = 122.88MHz , PLL2 frequency = 2457600000.
FMC_REFCLK0 = 307.2MHz, FMC_REFCLK1 = 307.2MHz
Lane rate = 12288.00MHz
Lane rate /40 = 307.200MHz
LMFC rate = 19.200MHz
Sysref Divider Value = 512
ADF4371 RF16 frequency = 9830400000
AD9213 PLL is Locked
SYSREF captured : Yes
SYSREF alignment error : No
Link status : CGS
Thanks in Advance
Goli Ganesh
Hello Goli Ganesh,
The configuration looks ok.
Are you using No-OS to configure the transceivers on the FPGA side ?
When you say you started from AD9208 design, you mean this one: AD9208-DUAL-EBZ HDL reference design [Analog Devices Wiki] ?
If you're using no-os, can you post the output of the run ?
Regards,
Adrian
Hi AdrianC ,
Hi AdrianC
Hi AdrianC
Hi AdrianC
Hello Goli Ganesh,
Sorry I haven't replied in a while. We were trying to get the new version of the AD9213 Eval Board working on the VCU118 so we have something to experiment on our side. Although we have an HDL design, we haven't yet managed to update the software with the additional drivers required for the EVB. Until we have things working on our side, it's unlikely we can help debug designs with hardware we cannot test on.
Regards,
Adrian