Post Go back to editing

JESD204B arbitrary lane selection

Category: Software
Product Number: AD9154-FMC-EBZ
Software Version: DAC-FMC-EBZ

Hello,

I am trying to port the example DAC-FMC-EBZ hdl project (built for the AD9154 and ZCU102) from the ZCU102 to ZCU104. The main issue with the ZCU104 is that it has an LPC connector so only lane 7 is connected. According to https://wiki.analog.com/resources/eval/user-guides/ad-dac-fmc-ebz the AD9154 supports JESD mode 10 with a single converter using a single lane.

My question is - how can I specify lane 7 when configuring the AD9154 to mode 10? We are using the SPI PRO GUI tool and it is not clear how to configure it to use this lane only. Is this possible?

Thanks,

svv9

Parents Reply Children
No Data