Hello,
After checking, I saw there had been similar questions in the past regarding the error " rx_clkgen: MMCM-PLL NOT locked (245760000 Hz)
error: rx_clkgen: axi_clkgen_set_rate() failed" but I couldn't find a suitable answer to this error.
After building successfully the no-OS project (HDL and no-OS project driver : 2019_R2 branch) for ADRV9009, I tried to run the "headless.c" which contains the main function, and I get the above mentionned error.
As far as I can understand, this error is related to clock issue. I didn't change anything in the design neither in the no-OS SDK project (the ref clock for ad9528 is vcxo).
I'm using one of the profiles provided. I tried the other profiles and got exactly the same error.
Is there a change that must be made in the clock generator files ?
Thanks
MMCM
[edited by: Me_ at 1:14 PM (GMT -4) on 13 May 2022]