Post Go back to editing

Frequency Hopping Example Design with ADRV9361-z7035 and ADRV1CRR-BOB

I am using ADRV9361-z7035 and ADRV1CRR-BOB reference design HDL 2019_r2 . I want to add Frequency hopping example in the HDL reference . Is it possible to add frequency hopping IP in reference design targeting ADRV1CRR-BOB as I went through the literature and I found that this IP is working only ADRV1CRR-FMC.

Best Regards

Parents Reply
  • I selected LOs frequencies as I did for adrv1crr-fmc reference design ( that is RF Bandwidth 50 MHz , Profile 1 2425MHz, Profile 2 2475MHz , dwell sample value 15000).

    The above settings work correctly with Adrv9361-z7035+adrv1crr-fmc but not working with Adrv9361-z7035+adrv1crr-bob .

    let me share how I am testing with  Adrv9361-z7035+adrv1crr-fmc

    1- Input frequency span 2400-2500MHz , profile 1 2425MHz, profile 2 2475MHz ,dwell sample 15000

    2- I injected RF_in from Signal generator any frequency within above span

    3- I got output (DAC-Spectrum Analyser) same injected frequency   

    but  i am not gettting same result with Adrv9361-z7035+adrv1crr-bob

    BR

Children