Post Go back to editing

Weird behaviour / noise in 4-channel Quad MxFE design

Thread Summary

The user is experiencing unexpected noise and signal behavior in a design with the Quad MxFE using a single Tx and Rx channel per MxFE. The final answer suggests that the issue is likely due to incorrect timing constraints in the HDL design, specifically the rx_device_clk and tx_device_clk clocks being constrained to 250 MHz instead of 375 MHz. The solution is to manually update the timing constraint file to reflect the correct lane rate and re-run the build.
AI Generated Content

Hi there,

I'm currently working on developing a design that works with the Quad MxFE with a single Tx and Rx channel operating per MxFE.

My setup and JESD parameters are as follows:

1Txs / 1Rxs per MxFE
DAC_CLK = 12GSPS
ADC_CLK = 3GSPS
Tx I/Q Rate: 3 GSPS (Interpolation of 4x1)
Rx I/Q Rate: 1.5 GSPS (Decimation of 2x1)
DAC JESD204C: Mode 12, L=4, M=2, N=N'=16
ADC JESD204C: Mode 7, L=2, M=2, N=N'=16
DAC-Side JESD204C Lane Rate: 24.75Gbps
ADC-Side JESD204C Lane Rate: 24.75Gbps

I have compiled a new FPGA bitfile for this setup, with the following compilation parameters:

JESD_MODE=64B66B
RX_RATE=24.75
TX_RATE=24.75
RX_PLL_SEL=1
TX_PLL_SEL=1
REF_CLK_RATE=250
RX_JESD_L=2
RX_JESD_M=2
RX_JESD_S=1
RX_JESD_NP=16
TX_JESD_L=4
TX_JESD_M=2
TX_JESD_S=1
TX_JESD_NP=16
RX_KS_PER_CHANNEL=16
TX_KS_PER_CHANNEL=16

Synthesis and implementation of the design went without trouble, and I created a new device tree to set things up correctly:

// SPDX-License-Identifier: GPL-2.0
/*
 * Analog Devices Quad-MxFE
 * https://wiki.analog.com/resources/eval/user-guides/quadmxfe
 * https://wiki.analog.com/resources/tools-software/linux-drivers/iio-mxfe/ad9081
 * https://wiki.analog.com/resources/eval/user-guides/ad_quadmxfe1_ebz/ad_quadmxfe1_ebz_hdl
 *
 * hdl_project: <ad_quadmxfe1_ebz/vcu118>
 * board_revision: <>
 *
 * Copyright (C) 2019-2020 Analog Devices Inc.
 *
 * Adapted by Dr. Kari Clark for 4x ADC and 4x DAC operation in February 2022
 */

#include <dt-bindings/iio/frequency/hmc7044.h>
#include <dt-bindings/iio/adc/adi,ad9081.h>
#include <dt-bindings/gpio/gpio.h>

#include "vcu118_quad_ad9081.dtsi"

// This setup assumes 500MHz clock into J41 (0 dBm)
// ad9081_204c_4dac_12gsps_4adc_6gsps_iq:
//     * 1Txs / 1Rxs per MxFE
//     * DAC_CLK = 12GSPS
//     * ADC_CLK = 3GSPS
//     * Tx I/Q Rate: 3 GSPS (Interpolation of 4x1)
//     * Rx I/Q Rate: 1.5 GSPS (Decimation of 2x1)
//     * DAC JESD204C: Mode 12, L=4, M=2, N=N'=16
//     * ADC JESD204C: Mode  7, L=2, M=2, N=N'=16
//     * DAC-Side JESD204C Lane Rate: 24.75Gbps
//     * ADC-Side JESD204C Lane Rate: 24.75Gbps

// HDL Synthesis Parameters:
// JESD_MODE=64B66B
// RX_RATE=24.75
// TX_RATE=24.75
// REF_CLK_RATE=250
// RX_JESD_M=2
// RX_JESD_L=2
// RX_JESD_S=1
// RX_JESD_NP=16
// TX_JESD_M=2
// TX_JESD_L=4
// TX_JESD_S=1
// TX_JESD_NP=16
// RX_PLL_SEL=1
// TX_PLL_SEL=1
// RX_KS_PER_CHANNEL=2 (maybe 4?)
// TX_KS_PER_CHANNEL=32

#define ADRF4360_RF16_FREQUENCY_HZ		12000000000

#define HMC7043_FPGA_XCVR_CLKDIV		2
#define HMC7043_FPGA_LINK_CLKDIV_TX		2
#define HMC7043_FPGA_LINK_CLKDIV_RX		2
#define HMC7043_SYSREF_CLKDIV			1024

#define AD9081_DAC_FREQUENCY			ADRF4360_RF16_FREQUENCY_HZ
#define AD9081_ADC_FREQUENCY			3000000000

 /* TX path */
#define AD9081_TX_LANERATE_KHZ			24750000
#define AD9081_TX_LINK_CLK				375000000

#define AD9081_TX_MAIN_INTERPOLATION		4
#define AD9081_TX_CHAN_INTERPOLATION		1

#ifndef AD9081_TX_MAIN_NCO_SHIFT
#define AD9081_TX_MAIN_NCO_SHIFT		3000000000
#endif
#ifndef AD9081_TX_CHAN_NCO_SHIFT
#define AD9081_TX_CHAN_NCO_SHIFT		0
#endif

#define AD9081_GAIN					1024

#define AD9081_TX_JESD_MODE			12
#define AD9081_TX_JESD_SUBCLASS			1
#define AD9081_TX_JESD_VERSION			2
#define AD9081_TX_JESD_M			2
#define AD9081_TX_JESD_F			1
#define AD9081_TX_JESD_K			256
#define AD9081_TX_JESD_N			16
#define AD9081_TX_JESD_NP			16
#define AD9081_TX_JESD_CS			0
#define AD9081_TX_JESD_L			4
#define AD9081_TX_JESD_S			1
#define AD9081_TX_JESD_HD			1

#define AD9081_JRX_TPL_PHASE_ADJUST		16

/* RX path */
#define AD9081_RX_LANERATE_KHZ			24750000
#define AD9081_RX_LINK_CLK				375000000
#define AD9081_RX_MAIN_DECIMATION		2
#define AD9081_RX_CHAN_DECIMATION		1

#ifndef AD9081_RX_MAIN_NCO_SHIFT
#define AD9081_RX_MAIN_NCO_SHIFT		1000000000
#endif
#ifndef AD9081_RX_CHAN_NCO_SHIFT
#define AD9081_RX_CHAN_NCO_SHIFT		0
#endif

#ifndef AD9081_ADC_NYQUIST_ZONE
#define AD9081_ADC_NYQUIST_ZONE		AD9081_ADC_NYQUIST_ZONE_EVEN
#endif

#define AD9081_RX_JESD_MODE			7
#define AD9081_RX_JESD_SUBCLASS			1
#define AD9081_RX_JESD_VERSION			2
#define AD9081_RX_JESD_M			2
#define AD9081_RX_JESD_F			2
#define AD9081_RX_JESD_K			128
#define AD9081_RX_JESD_N			16
#define AD9081_RX_JESD_NP			16
#define AD9081_RX_JESD_CS			0
#define AD9081_RX_JESD_L			2
#define AD9081_RX_JESD_S			1
#define AD9081_RX_JESD_HD			0


/ {
	model = "Analog Devices AD-QUADMXFE1-EBZ Rev.C";
};

&gpio_hmc425a {
	compatible = "adi,hmc540s";
	ctrl-gpios = <&axi_gpio 38 GPIO_ACTIVE_HIGH>,
		<&axi_gpio 37 GPIO_ACTIVE_HIGH>,
		<&axi_gpio 36 GPIO_ACTIVE_HIGH>,
		<&axi_gpio 35 GPIO_ACTIVE_HIGH>;
};

&fmc_i2c {
	current_limiter@58 {
		compatible = "adi,adm1177-iio";
		reg = <0x58>;
		adi,r-sense-mohm = <10>; /* 10 mOhm */
		adi,shutdown-threshold-ma = <10000>; /* 10 A */
		adi,vrange-high-enable;
	};
};

/ {
	rx_fixed_linerate: clock@2 {
		#clock-cells = <0>;
		compatible = "fixed-clock";
		clock-frequency = <AD9081_RX_LANERATE_KHZ>;
		clock-output-names = "rx_lane_clk";
	};

	tx_fixed_linerate: clock@3 {
		#clock-cells = <0>;
		compatible = "fixed-clock";
		clock-frequency = <AD9081_TX_LANERATE_KHZ>;
		clock-output-names = "tx_lane_clk";
	};

	rx_fixed_link_clk: clock@4 {
		#clock-cells = <0>;
		compatible = "fixed-clock";
		clock-frequency = <AD9081_RX_LINK_CLK>;
		clock-output-names = "rx_link_clk";
	};

	tx_fixed_link_clk: clock@5 {
		#clock-cells = <0>;
		compatible = "fixed-clock";
		clock-frequency = <AD9081_TX_LINK_CLK>;
		clock-output-names = "tx_link_clk";
	};
};

/delete-node/ &axi_ad9081_adxcvr_rx;
/delete-node/ &axi_ad9081_adxcvr_tx;

&axi_ad9081_rx_jesd {
	clock-names = "s_axi_aclk", "device_clk", "link_clk", "lane_clk";
	clocks = <&clk_bus_0>, <&hmc7043 2>, <&rx_fixed_link_clk>, <&rx_fixed_linerate>;
	jesd204-inputs = <&hmc7043 0 FRAMER_LINK0_RX>; /* omit axi_ad9081_adxcvr_rx */
};

&axi_ad9081_tx_jesd {
	clock-names = "s_axi_aclk", "device_clk", "link_clk", "lane_clk";
	clocks = <&clk_bus_0>, <&hmc7043 4>, <&tx_fixed_link_clk>, <&tx_fixed_linerate>;
	jesd204-inputs = <&hmc7043 0 DEFRAMER_LINK0_TX>; /* omit axi_ad9081_adxcvr_tx */
};

&rx_dma {
	/delete-node/ adi,channels; /* This comes from the synthesis paramtes */
};

&tx_dma {
	/delete-node/ adi,channels; /* This comes from the synthesis paramtes */
};

&adf4371_clk0 {
	channel@2 {
		reg = <2>;
		adi,power-up-frequency = /bits/ 64 <ADRF4360_RF16_FREQUENCY_HZ>;
	};
};

&adf4371_clk1 {
	channel@2 {
		reg = <2>;
		adi,power-up-frequency = /bits/ 64 <ADRF4360_RF16_FREQUENCY_HZ>;
	};
};

&adf4371_clk2 {
	channel@2 {
		reg = <2>;
		adi,power-up-frequency = /bits/ 64 <ADRF4360_RF16_FREQUENCY_HZ>;
	};
};

&adf4371_clk3 {
	channel@2 {
		reg = <2>;
		adi,power-up-frequency = /bits/ 64 <ADRF4360_RF16_FREQUENCY_HZ>;
	};
};

&hmc7043 {
	hmc7043_c0: channel@0 {
		reg = <0>;
		adi,extended-name = "FPGA_REFCLK";
		adi,divider = <HMC7043_FPGA_XCVR_CLKDIV>;
		adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
	};

	hmc7043_c1: channel@1 {
		reg = <1>;
		adi,extended-name = "SYSREF_FPGA";
		adi,divider = <HMC7043_SYSREF_CLKDIV>;
		adi,driver-mode = <HMC7044_DRIVER_MODE_LVPECL>;
		adi,coarse-digital-delay = <0>;
		adi,fine-analog-delay = <0>;
		adi,output-mux-mode = <0>;
		adi,jesd204-sysref-chan;
	};

	hmc7043_c2: channel@2 {
		reg = <2>;
		adi,extended-name = "RX_CORE_LINK_CLK";
		adi,divider = <HMC7043_FPGA_LINK_CLKDIV_RX>;
		adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
	};

	/delete-node/ hmc7043_c3;

	hmc7043_c4: channel@4 {
		reg = <4>;
		adi,extended-name = "TX_CORE_LINK_CLK";
		adi,divider = <HMC7043_FPGA_LINK_CLKDIV_TX>;
		adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
	};

	/delete-node/ hmc7043_c5;
	/delete-node/ hmc7043_c6;

	hmc7043_c7: channel@7 {
		reg = <7>;
		adi,extended-name = "SYSREF_MXFE0";
		adi,divider = <HMC7043_SYSREF_CLKDIV>;
		adi,driver-mode = <HMC7044_DRIVER_MODE_LVPECL>;
		adi,coarse-digital-delay = <0>;
		adi,fine-analog-delay = <0>;
		adi,output-mux-mode = <0>;
		adi,jesd204-sysref-chan;
	};

	/delete-node/ hmc7043_c8;

	hmc7043_c9: channel@9 {
		reg = <9>;
		adi,extended-name = "SYSREF_MXFE1";
		adi,divider = <HMC7043_SYSREF_CLKDIV>;
		adi,driver-mode = <HMC7044_DRIVER_MODE_LVPECL>;
		adi,coarse-digital-delay = <0>;
		adi,fine-analog-delay = <0>;
		adi,output-mux-mode = <0>;
		adi,jesd204-sysref-chan;
	};

	/delete-node/ hmc7043_c10;

	hmc7043_c11: channel@11 {
		reg = <11>;
		adi,extended-name = "SYSREF_MXFE2";
		adi,divider = <HMC7043_SYSREF_CLKDIV>;
		adi,driver-mode = <HMC7044_DRIVER_MODE_LVPECL>;
		adi,coarse-digital-delay = <0>;
		adi,fine-analog-delay = <0>;
		adi,output-mux-mode = <0>;
		adi,jesd204-sysref-chan;
	};

	/delete-node/ hmc7043_c12;

	hmc7043_c13: channel@13 {
		reg = <13>;
		adi,extended-name = "SYSREF_MXFE3";
		adi,divider = <HMC7043_SYSREF_CLKDIV>;
		adi,driver-mode = <HMC7044_DRIVER_MODE_LVPECL>;
		adi,coarse-digital-delay = <0>;
		adi,fine-analog-delay = <0>;
		adi,output-mux-mode = <0>;
		adi,jesd204-sysref-chan;
	};
};

&trx0_ad9081 {
	/delete-property/ adi,jesd-sync-pins-01-swap-enable;
	adi,jesd-sync-pin-0a-cmos-enable;

	adi,tx-dacs {
		#size-cells = <0>;
		#address-cells = <1>;
		adi,dac-frequency-hz = /bits/ 64 <AD9081_DAC_FREQUENCY>;
		adi,main-data-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			adi,interpolation = <AD9081_TX_MAIN_INTERPOLATION>;
			trx0_ad9081_dac0: dac@0 {
			    reg = <0>;
			    adi,crossbar-select = <&trx0_ad9081_tx_fddc_chan0>;
			    adi,nco-frequency-shift-hz = /bits/ 64 <AD9081_TX_MAIN_NCO_SHIFT>;
			};
		};
		adi,channelizer-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			adi,interpolation = <AD9081_TX_CHAN_INTERPOLATION>;
			trx0_ad9081_tx_fddc_chan0: channel@0 {
			    reg = <0>;
			    adi,gain = <AD9081_GAIN>; /* gain_dB = 20*log_10(value/2048) */
			    adi,nco-frequency-shift-hz =  /bits/ 64 <AD9081_TX_CHAN_NCO_SHIFT>;
			};
		};
		adi,jesd-links {
			#size-cells = <0>;
			#address-cells = <1>;
			trx0_ad9081_tx_jesd_l0: link@0 {
				#address-cells = <1>;
				#size-cells = <0>;
				reg = <0>;
				adi,tpl-phase-adjust = <AD9081_JRX_TPL_PHASE_ADJUST>;
				adi,logical-lane-mapping = /bits/ 8 <0 1 2 3 4 5 6 7>;
				adi,link-mode = <AD9081_TX_JESD_MODE>;			/* JESD Quick Configuration Mode */
				adi,subclass = <AD9081_TX_JESD_SUBCLASS>;			/* JESD SUBCLASS 0,1,2 */
				adi,version = <AD9081_TX_JESD_VERSION>;			/* JESD VERSION 0=204A,1=204B,2=204C */
				adi,dual-link = <0>;			/* JESD Dual Link Mode */
				adi,converters-per-device = <AD9081_TX_JESD_M>;	/* JESD M */
				adi,octets-per-frame = <AD9081_TX_JESD_F>;		/* JESD F */
				adi,frames-per-multiframe = <AD9081_TX_JESD_K>;	/* JESD K */
				adi,converter-resolution = <AD9081_TX_JESD_N>;	/* JESD N */
				adi,bits-per-sample = <AD9081_TX_JESD_N>;		/* JESD NP' */
				adi,control-bits-per-sample = <AD9081_TX_JESD_CS>;	/* JESD CS */
				adi,lanes-per-device = <AD9081_TX_JESD_L>;		/* JESD L */
				adi,samples-per-converter-per-frame = <AD9081_TX_JESD_S>; /* JESD S */
				adi,high-density = <AD9081_TX_JESD_HD>;			/* JESD HD */
			};
		};
	};

	adi,rx-adcs {
		#size-cells = <0>;
		#address-cells = <1>;
		adi,adc-frequency-hz = /bits/ 64 <AD9081_ADC_FREQUENCY>;
		adi,nyquist-zone = <AD9081_ADC_NYQUIST_ZONE>;
		adi,main-data-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			trx0_ad9081_adc2: adc@2 {
				reg = <2>;
				adi,decimation = <AD9081_RX_MAIN_DECIMATION>;
				adi,nco-frequency-shift-hz =  /bits/ 64 <AD9081_RX_MAIN_NCO_SHIFT>;
				adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
			};
		};
		adi,channelizer-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			trx0_ad9081_rx_fddc_chan4: channel@4 {
				reg = <4>;
				adi,decimation = <AD9081_RX_CHAN_DECIMATION>;
				adi,gain = <AD9081_GAIN>; /* gain_dB = 20*log_10(value/2048) */
				adi,nco-frequency-shift-hz =  /bits/ 64 <AD9081_RX_CHAN_NCO_SHIFT>;
			};
		};
		adi,jesd-links {
			#size-cells = <0>;
			#address-cells = <1>;
			trx0_ad9081_rx_jesd_l0: link@0 {
				reg = <0>;
				adi,converter-select =
					<&trx0_ad9081_rx_fddc_chan4 FDDC_I>, <&trx0_ad9081_rx_fddc_chan4 FDDC_Q>;
				adi,logical-lane-mapping = /bits/ 8 <0 1 2 3 4 5 6 7>;
				adi,link-mode = <AD9081_RX_JESD_MODE>;			/* JESD Quick Configuration Mode */
				adi,subclass = <AD9081_RX_JESD_SUBCLASS>;			/* JESD SUBCLASS 0,1,2 */
				adi,version = <AD9081_RX_JESD_VERSION>;			/* JESD VERSION 0=204A,1=204B,2=204C */
				adi,dual-link = <0>;			/* JESD Dual Link Mode */
				adi,device-id = <3>;
				adi,converters-per-device = <AD9081_RX_JESD_M>;	/* JESD M */
				adi,octets-per-frame = <AD9081_RX_JESD_F>;		/* JESD F */
				adi,frames-per-multiframe = <AD9081_RX_JESD_K>;	/* JESD K */
				adi,converter-resolution = <AD9081_RX_JESD_N>;	/* JESD N */
				adi,bits-per-sample = <AD9081_RX_JESD_NP>;		/* JESD NP' */
				adi,control-bits-per-sample = <AD9081_RX_JESD_CS>;	/* JESD CS */
				adi,lanes-per-device = <AD9081_RX_JESD_L>;		/* JESD L */
				adi,samples-per-converter-per-frame = <AD9081_RX_JESD_S>; /* JESD S */
				adi,high-density = <AD9081_RX_JESD_HD>;			/* JESD HD */
			};
		};
	};
};

&trx1_ad9081 {
	/delete-property/ adi,jesd-sync-pins-01-swap-enable;
	adi,jesd-sync-pin-0a-cmos-enable;

	adi,tx-dacs {
		#size-cells = <0>;
		#address-cells = <1>;
		adi,dac-frequency-hz = /bits/ 64 <AD9081_DAC_FREQUENCY>;
		adi,main-data-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			adi,interpolation = <AD9081_TX_MAIN_INTERPOLATION>;
			trx1_ad9081_dac0: dac@0 {
			    reg = <0>;
			    adi,crossbar-select = <&trx1_ad9081_tx_fddc_chan0>;
			    adi,nco-frequency-shift-hz = /bits/ 64 <AD9081_TX_MAIN_NCO_SHIFT>;
			};
		};
		adi,channelizer-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			adi,interpolation = <AD9081_TX_CHAN_INTERPOLATION>;
			trx1_ad9081_tx_fddc_chan0: channel@0 {
			    reg = <0>;
			    adi,gain = <AD9081_GAIN>; /* gain_dB = 20*log_10(value/2048) */
			    adi,nco-frequency-shift-hz =  /bits/ 64 <AD9081_TX_CHAN_NCO_SHIFT>;
			};
		};
		adi,jesd-links {
			#size-cells = <0>;
			#address-cells = <1>;
			trx1_ad9081_tx_jesd_l0: link@0 {
				#address-cells = <1>;
				#size-cells = <0>;
				reg = <0>;
				adi,tpl-phase-adjust = <AD9081_JRX_TPL_PHASE_ADJUST>;
				adi,logical-lane-mapping = /bits/ 8 <0 1 2 3 4 5 6 7>;
				adi,link-mode = <AD9081_TX_JESD_MODE>;			/* JESD Quick Configuration Mode */
				adi,subclass = <AD9081_TX_JESD_SUBCLASS>;			/* JESD SUBCLASS 0,1,2 */
				adi,version = <AD9081_TX_JESD_VERSION>;			/* JESD VERSION 0=204A,1=204B,2=204C */
				adi,dual-link = <0>;			/* JESD Dual Link Mode */
				adi,converters-per-device = <AD9081_TX_JESD_M>;	/* JESD M */
				adi,octets-per-frame = <AD9081_TX_JESD_F>;		/* JESD F */
				adi,frames-per-multiframe = <AD9081_TX_JESD_K>;	/* JESD K */
				adi,converter-resolution = <AD9081_TX_JESD_N>;	/* JESD N */
				adi,bits-per-sample = <AD9081_TX_JESD_N>;		/* JESD NP' */
				adi,control-bits-per-sample = <AD9081_TX_JESD_CS>;	/* JESD CS */
				adi,lanes-per-device = <AD9081_TX_JESD_L>;		/* JESD L */
				adi,samples-per-converter-per-frame = <AD9081_TX_JESD_S>; /* JESD S */
				adi,high-density = <AD9081_TX_JESD_HD>;			/* JESD HD */
			};
		};
	};

	adi,rx-adcs {
		#size-cells = <0>;
		#address-cells = <1>;
		adi,adc-frequency-hz = /bits/ 64 <AD9081_ADC_FREQUENCY>;
		adi,nyquist-zone = <AD9081_ADC_NYQUIST_ZONE>;
		adi,main-data-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			trx1_ad9081_adc2: adc@2 {
				reg = <2>;
				adi,decimation = <AD9081_RX_MAIN_DECIMATION>;
				adi,nco-frequency-shift-hz =  /bits/ 64 <AD9081_RX_MAIN_NCO_SHIFT>;
				adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
			};
		};
		adi,channelizer-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			trx1_ad9081_rx_fddc_chan4: channel@4 {
				reg = <4>;
				adi,decimation = <AD9081_RX_CHAN_DECIMATION>;
				adi,gain = <AD9081_GAIN>; /* gain_dB = 20*log_10(value/2048) */
				adi,nco-frequency-shift-hz =  /bits/ 64 <AD9081_RX_CHAN_NCO_SHIFT>;
			};
		};
		adi,jesd-links {
			#size-cells = <0>;
			#address-cells = <1>;
			trx1_ad9081_rx_jesd_l0: link@0 {
				reg = <0>;
				adi,converter-select =
					<&trx1_ad9081_rx_fddc_chan4 FDDC_I>, <&trx1_ad9081_rx_fddc_chan4 FDDC_Q>;
				adi,logical-lane-mapping = /bits/ 8 <0 1 2 3 4 5 6 7>;
				adi,link-mode = <AD9081_RX_JESD_MODE>;			/* JESD Quick Configuration Mode */
				adi,subclass = <AD9081_RX_JESD_SUBCLASS>;			/* JESD SUBCLASS 0,1,2 */
				adi,version = <AD9081_RX_JESD_VERSION>;			/* JESD VERSION 0=204A,1=204B,2=204C */
				adi,dual-link = <0>;			/* JESD Dual Link Mode */
				adi,device-id = <3>;
				adi,converters-per-device = <AD9081_RX_JESD_M>;	/* JESD M */
				adi,octets-per-frame = <AD9081_RX_JESD_F>;		/* JESD F */
				adi,frames-per-multiframe = <AD9081_RX_JESD_K>;	/* JESD K */
				adi,converter-resolution = <AD9081_RX_JESD_N>;	/* JESD N */
				adi,bits-per-sample = <AD9081_RX_JESD_NP>;		/* JESD NP' */
				adi,control-bits-per-sample = <AD9081_RX_JESD_CS>;	/* JESD CS */
				adi,lanes-per-device = <AD9081_RX_JESD_L>;		/* JESD L */
				adi,samples-per-converter-per-frame = <AD9081_RX_JESD_S>; /* JESD S */
				adi,high-density = <AD9081_RX_JESD_HD>;			/* JESD HD */
			};
		};
	};
};

&trx2_ad9081 {
	/delete-property/ adi,jesd-sync-pins-01-swap-enable;
	adi,jesd-sync-pin-0a-cmos-enable;

	adi,tx-dacs {
		#size-cells = <0>;
		#address-cells = <1>;
		adi,dac-frequency-hz = /bits/ 64 <AD9081_DAC_FREQUENCY>;
		adi,main-data-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			adi,interpolation = <AD9081_TX_MAIN_INTERPOLATION>;
			trx2_ad9081_dac0: dac@0 {
			    reg = <0>;
			    adi,crossbar-select = <&trx2_ad9081_tx_fddc_chan0>;
			    adi,nco-frequency-shift-hz = /bits/ 64 <AD9081_TX_MAIN_NCO_SHIFT>;
			};
		};
		adi,channelizer-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			adi,interpolation = <AD9081_TX_CHAN_INTERPOLATION>;
			trx2_ad9081_tx_fddc_chan0: channel@0 {
			    reg = <0>;
			    adi,gain = <AD9081_GAIN>; /* gain_dB = 20*log_10(value/2048) */
			    adi,nco-frequency-shift-hz =  /bits/ 64 <AD9081_TX_CHAN_NCO_SHIFT>;
			};
		};
		adi,jesd-links {
			#size-cells = <0>;
			#address-cells = <1>;
			trx2_ad9081_tx_jesd_l0: link@0 {
				#address-cells = <1>;
				#size-cells = <0>;
				reg = <0>;
				adi,tpl-phase-adjust = <AD9081_JRX_TPL_PHASE_ADJUST>;
				adi,logical-lane-mapping = /bits/ 8 <0 1 2 3 4 5 6 7>;
				adi,link-mode = <AD9081_TX_JESD_MODE>;			/* JESD Quick Configuration Mode */
				adi,subclass = <AD9081_TX_JESD_SUBCLASS>;			/* JESD SUBCLASS 0,1,2 */
				adi,version = <AD9081_TX_JESD_VERSION>;			/* JESD VERSION 0=204A,1=204B,2=204C */
				adi,dual-link = <0>;			/* JESD Dual Link Mode */
				adi,converters-per-device = <AD9081_TX_JESD_M>;	/* JESD M */
				adi,octets-per-frame = <AD9081_TX_JESD_F>;		/* JESD F */
				adi,frames-per-multiframe = <AD9081_TX_JESD_K>;	/* JESD K */
				adi,converter-resolution = <AD9081_TX_JESD_N>;	/* JESD N */
				adi,bits-per-sample = <AD9081_TX_JESD_N>;		/* JESD NP' */
				adi,control-bits-per-sample = <AD9081_TX_JESD_CS>;	/* JESD CS */
				adi,lanes-per-device = <AD9081_TX_JESD_L>;		/* JESD L */
				adi,samples-per-converter-per-frame = <AD9081_TX_JESD_S>; /* JESD S */
				adi,high-density = <AD9081_TX_JESD_HD>;			/* JESD HD */
			};
		};
	};

	adi,rx-adcs {
		#size-cells = <0>;
		#address-cells = <1>;
		adi,adc-frequency-hz = /bits/ 64 <AD9081_ADC_FREQUENCY>;
		adi,nyquist-zone = <AD9081_ADC_NYQUIST_ZONE>;
		adi,main-data-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			trx2_ad9081_adc2: adc@2 {
				reg = <2>;
				adi,decimation = <AD9081_RX_MAIN_DECIMATION>;
				adi,nco-frequency-shift-hz =  /bits/ 64 <AD9081_RX_MAIN_NCO_SHIFT>;
				adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
			};
		};
		adi,channelizer-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			trx2_ad9081_rx_fddc_chan4: channel@4 {
				reg = <4>;
				adi,decimation = <AD9081_RX_CHAN_DECIMATION>;
				adi,gain = <AD9081_GAIN>; /* gain_dB = 20*log_10(value/2048) */
				adi,nco-frequency-shift-hz =  /bits/ 64 <AD9081_RX_CHAN_NCO_SHIFT>;
			};
		};
		adi,jesd-links {
			#size-cells = <0>;
			#address-cells = <1>;
			trx2_ad9081_rx_jesd_l0: link@0 {
				reg = <0>;
				adi,converter-select =
					<&trx2_ad9081_rx_fddc_chan4 FDDC_I>, <&trx2_ad9081_rx_fddc_chan4 FDDC_Q>;
				adi,logical-lane-mapping = /bits/ 8 <0 1 2 3 4 5 6 7>;
				adi,link-mode = <AD9081_RX_JESD_MODE>;			/* JESD Quick Configuration Mode */
				adi,subclass = <AD9081_RX_JESD_SUBCLASS>;			/* JESD SUBCLASS 0,1,2 */
				adi,version = <AD9081_RX_JESD_VERSION>;			/* JESD VERSION 0=204A,1=204B,2=204C */
				adi,dual-link = <0>;			/* JESD Dual Link Mode */
				adi,device-id = <3>;
				adi,converters-per-device = <AD9081_RX_JESD_M>;	/* JESD M */
				adi,octets-per-frame = <AD9081_RX_JESD_F>;		/* JESD F */
				adi,frames-per-multiframe = <AD9081_RX_JESD_K>;	/* JESD K */
				adi,converter-resolution = <AD9081_RX_JESD_N>;	/* JESD N */
				adi,bits-per-sample = <AD9081_RX_JESD_NP>;		/* JESD NP' */
				adi,control-bits-per-sample = <AD9081_RX_JESD_CS>;	/* JESD CS */
				adi,lanes-per-device = <AD9081_RX_JESD_L>;		/* JESD L */
				adi,samples-per-converter-per-frame = <AD9081_RX_JESD_S>; /* JESD S */
				adi,high-density = <AD9081_RX_JESD_HD>;			/* JESD HD */
			};
		};
	};
};

&trx3_ad9081 {
	/delete-property/ adi,jesd-sync-pins-01-swap-enable;
	adi,jesd-sync-pin-0a-cmos-enable;

	adi,tx-dacs {
		#size-cells = <0>;
		#address-cells = <1>;
		adi,dac-frequency-hz = /bits/ 64 <AD9081_DAC_FREQUENCY>;
		adi,main-data-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			adi,interpolation = <AD9081_TX_MAIN_INTERPOLATION>;
			trx3_ad9081_dac0: dac@0 {
			    reg = <0>;
			    adi,crossbar-select = <&trx3_ad9081_tx_fddc_chan0>;
			    adi,nco-frequency-shift-hz = /bits/ 64 <AD9081_TX_MAIN_NCO_SHIFT>;
			};
		};
		adi,channelizer-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			adi,interpolation = <AD9081_TX_CHAN_INTERPOLATION>;
			trx3_ad9081_tx_fddc_chan0: channel@0 {
			    reg = <0>;
			    adi,gain = <AD9081_GAIN>; /* gain_dB = 20*log_10(value/2048) */
			    adi,nco-frequency-shift-hz =  /bits/ 64 <AD9081_TX_CHAN_NCO_SHIFT>;
			};
		};
		adi,jesd-links {
			#size-cells = <0>;
			#address-cells = <1>;
			trx3_ad9081_tx_jesd_l0: link@0 {
				#address-cells = <1>;
				#size-cells = <0>;
				reg = <0>;
				adi,tpl-phase-adjust = <AD9081_JRX_TPL_PHASE_ADJUST>;
				adi,logical-lane-mapping = /bits/ 8 <0 1 2 3 4 5 6 7>;
				adi,link-mode = <AD9081_TX_JESD_MODE>;			/* JESD Quick Configuration Mode */
				adi,subclass = <AD9081_TX_JESD_SUBCLASS>;			/* JESD SUBCLASS 0,1,2 */
				adi,version = <AD9081_TX_JESD_VERSION>;			/* JESD VERSION 0=204A,1=204B,2=204C */
				adi,dual-link = <0>;			/* JESD Dual Link Mode */
				adi,converters-per-device = <AD9081_TX_JESD_M>;	/* JESD M */
				adi,octets-per-frame = <AD9081_TX_JESD_F>;		/* JESD F */
				adi,frames-per-multiframe = <AD9081_TX_JESD_K>;	/* JESD K */
				adi,converter-resolution = <AD9081_TX_JESD_N>;	/* JESD N */
				adi,bits-per-sample = <AD9081_TX_JESD_N>;		/* JESD NP' */
				adi,control-bits-per-sample = <AD9081_TX_JESD_CS>;	/* JESD CS */
				adi,lanes-per-device = <AD9081_TX_JESD_L>;		/* JESD L */
				adi,samples-per-converter-per-frame = <AD9081_TX_JESD_S>; /* JESD S */
				adi,high-density = <AD9081_TX_JESD_HD>;			/* JESD HD */
			};
		};
	};

	adi,rx-adcs {
		#size-cells = <0>;
		#address-cells = <1>;
		adi,adc-frequency-hz = /bits/ 64 <AD9081_ADC_FREQUENCY>;
		adi,nyquist-zone = <AD9081_ADC_NYQUIST_ZONE>;
		adi,main-data-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			trx3_ad9081_adc2: adc@2 {
				reg = <2>;
				adi,decimation = <AD9081_RX_MAIN_DECIMATION>;
				adi,nco-frequency-shift-hz =  /bits/ 64 <AD9081_RX_MAIN_NCO_SHIFT>;
				adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
			};
		};
		adi,channelizer-paths {
			#address-cells = <1>;
			#size-cells = <0>;
			trx3_ad9081_rx_fddc_chan4: channel@4 {
				reg = <4>;
				adi,decimation = <AD9081_RX_CHAN_DECIMATION>;
				adi,gain = <AD9081_GAIN>; /* gain_dB = 20*log_10(value/2048) */
				adi,nco-frequency-shift-hz =  /bits/ 64 <AD9081_RX_CHAN_NCO_SHIFT>;
			};
		};
		adi,jesd-links {
			#size-cells = <0>;
			#address-cells = <1>;
			trx3_ad9081_rx_jesd_l0: link@0 {
				reg = <0>;
				adi,converter-select =
					<&trx3_ad9081_rx_fddc_chan4 FDDC_I>, <&trx3_ad9081_rx_fddc_chan4 FDDC_Q>;
				adi,logical-lane-mapping = /bits/ 8 <0 1 2 3 4 5 6 7>;
				adi,link-mode = <AD9081_RX_JESD_MODE>;			/* JESD Quick Configuration Mode */
				adi,subclass = <AD9081_RX_JESD_SUBCLASS>;			/* JESD SUBCLASS 0,1,2 */
				adi,version = <AD9081_RX_JESD_VERSION>;			/* JESD VERSION 0=204A,1=204B,2=204C */
				adi,dual-link = <0>;			/* JESD Dual Link Mode */
				adi,device-id = <3>;
				adi,converters-per-device = <AD9081_RX_JESD_M>;	/* JESD M */
				adi,octets-per-frame = <AD9081_RX_JESD_F>;		/* JESD F */
				adi,frames-per-multiframe = <AD9081_RX_JESD_K>;	/* JESD K */
				adi,converter-resolution = <AD9081_RX_JESD_N>;	/* JESD N */
				adi,bits-per-sample = <AD9081_RX_JESD_NP>;		/* JESD NP' */
				adi,control-bits-per-sample = <AD9081_RX_JESD_CS>;	/* JESD CS */
				adi,lanes-per-device = <AD9081_RX_JESD_L>;		/* JESD L */
				adi,samples-per-converter-per-frame = <AD9081_RX_JESD_S>; /* JESD S */
				adi,high-density = <AD9081_RX_JESD_HD>;			/* JESD HD */
			};
		};
	};
};

However, when I actually run the design, I'm getting a tonne of unexpected noise / weird behaviour that I'm unable to explain - see MATLAB FFT output below:

Digging more deeply and playing about with the various test modes for the Rx, I'm seeing some very strange behaviour. When I run neg_fullscale and post_fullscale tests, I get a deterministic fall/rise to 0 of the signal (which may partly explain the above noise).

None of my other designs are showing this behaviour - they all work fine. Any idea what might be going on here, and what steps should I try to fix this?

Thanks,
Kari

Edit Notes

Minor clarification
[edited by: Salisen at 5:05 PM (GMT -4) on 12 Apr 2022]