Post Go back to editing

Use external clock in FPGA Design, assure AD3963 passes the reference clock (PLUTO SDR)

Hi,

I would like to use the clock of the XO inside of my fpga design.

I found out this clock is passed trough the RF-chip XTALN--> CLK_OUT (https://www.analog.com/media/en/technical-documentation/data-sheets/ad9363.pdf)

1) How do I assure the CLK_OUT of the RF-chip is the DCXO? Found this in the datasheet of the AD9363

Output Clock. This pin can be configured to output either a buffered version of the
external input clock (the digital controlled crystal oscillator (DCXO)) or a divided-
down version of the internal ADC sample clock (ADC_CLK)

2) I found that the CLK_OUT is connected to P8 of the zynq 7010. But how do I include this port in the block design in Vivado? The port is already declared in the constrain file.

Can I just add a port and call it CLK_OUT? Or are there any others steps I should take?

3) Is the clock always passed? Or is it only passed when the RF-chip is in use? (transmitting and receiving).

Kind regards,

Dieter Verbruggen
 

Top Replies

Parents Reply
  • 1) I found a workaround!

    I made a script and added it to the buildroot: ref
    Inside this script I added:

    echo 1  >  /sys/kernel/debug/iio/iio\:device0/adi,clk-output-mode-select
    echo 1  >  /sys/kernel/debug/iio/iio\:device0/initialize
    

    This allows me to enable the clk_out as the right clock.

    2) Just adding this in hdl/projects/pluto/system_constr.xdc made the error go away.

    set_property CLOCK_DEDICATED_ROUTE FALSE [get_nets clk_out_IBUF]

Children
No Data