Post Go back to editing

How can I change "ADC Sample Rate" of AD9680 on FMCDAQ2

Hello.

I'm using the AD-FMCDAQ2-EBZ module for utilizing the ADC (AD9680).

The sample rate of ADC was set 1000 MSPS automatically.

I want to change the ADC sample rate to 998MSPS or 997MSPS.

But I don't know whether it is possible or not.

Please let me know how to change the ADC sample rate.

Thanks.

Parents
  • Hi Riache,

    The clock generator on AD-FMCDAQ2-EBZ is AD9523-1 and you can obtain the initialization parameters using the Evaluation software from EVAL-AD9523-1 page.  In this case the closest value I found is 995 MHz (as seen in the picture below). Because the value you want is close to 1000MSPS you only need to change the values for N DIVIDER, R DIVIDER and VCO DIVIDER 1 and the lane rate and ref rate should remain as in the case of 1000MSPS.  Here you can find details on how to calculate all the clock generator parameters.

    Thanks,

    Paul

  • Hi, Paul.

    Thanks a lot for reply.

     

    I tried to change ADC sample rate (1GSPS to 995MSPS) by using your suggestion.

    So, I edited some registers which you mentioned (R,N Divider) by IIO Oscilloscope tool as shown : 

     

    But, ADC capture result was still 1000 samples as shown : 

    (I counted 1000 samples by using .csv data)

    (If it is applied rightly, it must be 995 samples because time period is set 1 us.)

     

    In another way,

    I tried to change frequency in IIO Device Attributes of Debug Tab.

    However, It can't be changed too, as shown : 

    (I edited the value 1000000000 → 995000000, and then I clicked write button. But the value was returned 1000000000.)

      

    Is there a problem with the method I tried?

    Please help me.

     

    Thanks.

  • Hi Paul,

    Thanks for explanation detail.

     

    Before I do the method you told me, I just have one question.

    Is there any way to use Vitis (no-OS) by any chance?

    When I followed the "no-OS" method and then I checked the fmcdaq2.c code on Vitis,

    there was an option to change "R,N Divider" as shown : 

      

    Is it posiible to change sample rate on Vitis?

    Thanks.

  • Hi Riache,

    Yes, it is possible to change the parameters from the fmcdaq2.c file.
    In this case, if you change the parameters you highlighted and choose the profile in which the sample rate for the ADC and DAC is 1GSPS you should see in the IIO Oscilloscope a 995 MHz sampling frequency.


    I modified the parameters highlighted below and obtained using the .csv data method 995 samples for 1 μs and the sampling frequency as in the picture below.


    Thanks, 

    Paul

  • Hi, Paul.

    Thanks for your help.

     

    As your explanation,

    I edited all "adi-daq2.dtsi" files in "linux" sub folders whch paths are : 

    ./arch/microblaze/boot/dts/adi-daq2.dtsi

    ./arch/arm/boot/dts/adi-daq2.dtsi

    ./arch/arm64/boot/dts/xilinx/adi-daq2.dtsi

     

    I edited only 3 parameters shown as : 

     

     

    And then, I did "make" for exporting a "simpleImage.kcu105_fmcdaq2.strip" file as following wiki process : 

    https://wiki.analog.com/resources/eval/user-guides/ad-fmcdaq2-ebz/software/linux/microblaze

     

    After that,

    I uploaded a "bit file" and "simpleImage file", and connected to IIO Oscilloscope.

    However the "Sample Rate" was still 1000MSPS as shown that : 

     

    Did I miss something in the process I did?

    Help me a little more, please...

    Thanks.

  • I got the 995MSPS sample rate finally.

    I edited the value of "adi,pll2-m1-freq" in ".dtsi" file additionally.

     

    So, I got correct 995MSPS and I could see the sample rate in IIO Oscilloscope as shown that : 

    Then, I got the captured data of 995 samples during 1us time period.

     

    I could success due to your detail help.

    Thank you very much, Paul.

    Have a good Christmas day~!

  • Hi Riache, 

    I'm glad that I was able to help you. You too! 

         

  • Hi, 

       In this case you only need to modify a single adi-daq2.dtsi file depending on the architecture of the carrier board( arm / arm64 / microblaze). 

    Thanks,

    Paul

        

  • Hello Paul and Riache,

    Thank you very much for your interesting discussions!

    First of all, I had followed your discussion and the instructions given, since I wanted to change the sample rate of my DAC board. Actually, my DAC board is integrated in EVAL-FMCDAQ3-EBZ card and attached in the Xilinx Zynq ZC706 as the carrier board.

    I wanted to change the sample rate of my DAC device because as I have explored the DDS mode can only handle the external (table) file with maximum of 1000000 samples. Meanwhile, since my DAC runs on 1.233 Gsps of sample rate and I want to generate 1 millisecond chirp signal, my file has the sample size of 1233000, which is larger than the maximum sample size DDS mode could handle. 

    One of the solutions I had been thinking was to reduce the sample rate of DAC, therefore with the same signal's specification my table file will reduced respectively.

    I changed the sample rate of my device as your instruction above. Here is the documentation.

    After I changed the sample rate, I restart the IIO Oscilloscope application and found that the DAC sample rate were changed.

    However, after I changed the sample rate of my DAC, I couldn't saw any signal generated by my DAC, though I put the DDS mode to "One CW Tone". But, if I reverted back the sample rate to the default value, the oscilloscope shown a sinusoid signal.

    Therefore, with this reply, I would like to discuss with you about this problem. If you ever had any experience like this, would you mind sharing it here? That will be very helpful information. Looking forward to hearing from you.

    Thank you very much. Have a nice day!

  • Hello,

    I am trying to reproduce your setup and will get back with an answer as soon as possible.

    Thanks,

    Paul

  • Hello, 

    What is the new sample rate you will need for the DAC? Also, will it be ok if you open a new thread for this question so it will be much easier to follow?

    Thanks,

    Paul

  • Hello PaulPG,

    Thank you for your reply. I do really appreciate it.

    Actually, I tried to change the sample rate below 1 Gsps. Let say, 150 Msps.

    My main goal is to reduce the sample size of the signal file; therefore, the sample rate should be reduced as well.

Reply Children