Using HDL workflow advisor in Matlab/Simulink with the ADRV9364-Z7020

Hello, I am using the ADRV9364-Z7020 with the ADRV1CRR-BOB. I am trying to use HDL workflow advisor to target my board, but I am getting an error on section "4.1: Create Project". I am using the hdlcoder_led_blinking example so I can just see if I can successfully target my board before actually starting my own code. Also, I am using Xlinix Vivado version 2018.3 and Matlab version 2021. My first question is: Is the hdlcoder_led_blinking example compatible with my devices? If not, Is there another example I can use just to test if it is properly targeting my device? My next question is: Is any of the devices or software that I am using a reason why it cant create the project?