Post Go back to editing

Switch in ADRV9364-Z7020

Hello

I am trying to run a simple example on the FPGA of the adrv9364-z7020 + bob board

where the switches S1 and S2 of the bob board work as inputs and the led gpio0 as output.

I find that the switch on the bob board is related to one of the JX connectors on the adrv9364-z7020 board but it is not related to the FPGA.

Is it possible to relate them or does this board not give me the possibility?

I am programming my board from the JTAG regardless of the OS.

Thank you,

Nicole.

Parents
  • Hi Nicole,

    from what I see the S1 and S2 do not have a connection to the adrv9364-z7020 som.

    The bob was designed to work with multiple som's, but some of these have only partial support due fewer pins on the FPGA. 

    The ADRV9364-Z7020 supports a subset of features because the Zynq Z7020 has fewer available user I/Os

    Laszlo

Reply
  • Hi Nicole,

    from what I see the S1 and S2 do not have a connection to the adrv9364-z7020 som.

    The bob was designed to work with multiple som's, but some of these have only partial support due fewer pins on the FPGA. 

    The ADRV9364-Z7020 supports a subset of features because the Zynq Z7020 has fewer available user I/Os

    Laszlo

Children