AD9467
Recommended for New Designs
The AD9467 is a 16-bit, monolithic, IF sampling analog-to-digital converter (ADC). It is optimized for high performance over wide bandwidths and ease of...
Datasheet
AD9467 on Analog.com
Hi,
I am new to this forum and I just purchased AD9467 FMC card and connect to my Xilinx Zed Board.
I'm trying to build an application and I follow these links:
1- wiki.analog.com/.../build.
2- To run the no-OS application need to:
I had cloned the no-OS repository: github.com/.../no-OS
in addition, I had followed the steps from wiki.analog.com/.../software_setup and add the no-OS project's sources located in no-OS/projects/ad9467/src in the SDK Application Project under the src folder as shown here: wiki.analog.com/.../empty_project.png either by drag and drop or by import sources.
After the system worked as shown in the figure below, I had modified it to capture 12500 simple :
1- To capture the signal by AD9467 FMC card and SoC Board, We used signal generator 1v, 25khz signal
2- I modify the c code from SDK software to capture 12500 simple and send to PC to display.
/* Set the simpling capture per time */
axi_dmac_transfer(ad9467_dmac, (BASE1 + 12500 * 2 * i), 12500 * 2);
3- sampling rate of the ADC is 250MSPS.
/* Set the channel 3 frequency to 250Mhz */
ad9517_frequency(ad9517_device, 3, 250000000);
However, I’m capturing the sine wave signal under the same condition using an oscilloscope and AD9467 FMC card. where the capturing signal was two waveforms in the (oscilloscope figure2_b) and one waveform signal by using AD9467 FMC card.
Please could you help me with capturing the signal under 250MSPS by using AD9467 FMC card and zedboard?
Hi,
I can't see the images/figures you mentioned.
Have you provided the external clock( or sampling clock) https://wiki.analog.com/resources/fpga/xilinx/fmc/ad9467?
Andrei
Hi Dear, I had uploaded all the details and pictures to this document. yes, I used a 250MSPS clock from AWG to the ADC. However, the capturing was different on the oscilloscope as shown in the document.
Thanks Andrei for the reply.
I'm not sure which memory you're referring to.
In the reference design, the ADC block connects to AXI bus and then moved to main memory with DMA.
Say that we have 4 samples, each of them are 16-bit and the DMA target base address is 0x80_0000, what we think the memory arrangement is:
0x80_0000: sample1(16-bit)
0x80_0002: sample2(16-bit)
0x80_0004: sample3(16-bit)
0x80_0006: sample4(16-bit)
From your "the memory is 32-bit aligned, are you saying the arrangement is below?
0x80_0000: 0x0000 & sample1(16-bit)
0x80_0004: 0x0000 & sample2(16-bit)
0x80_0008: 0x0000 & sample3(16-bit)
0x80_000C: 0x0000 & sample4(16-bit)
iwan
Hi,
Your setup is ok, I presumed the dma driver accepts number of samples instead of bytes. Sorry about that.
The arrangement is like you described it. This is how I look at it:
0x80_0000: {sample2(16-bit), sample1(16-bit)}
0x80_0004: {sample4(16-bit), sample3(16-bit)}
0x80_0008: ...
Same thing.
I made a setup(as you described), to determine if there is a bug, I did not found one.
Attached you can find the data I captured. capture_ch1.txt
In my UART console I get "ad9467_core: Successfully initialized (250000000 Hz)" do you get half?
What release are you using and have you made other changes?
I would suggest, testing with linux also. Use IIO-Oscilloscope to capture data, set it to FFT and use markers.
Andrei
Hi Andrei,
Thanks for your reply. We actually only get "ad9467_core: Successfully initialized (125013732 Hz)".
So we have problem here. We supply 250MHz to the input clock connector and we expect that the ADC will use that clock. It seems that there's an internal divider(?) or the clock source completely from something else?
Best regards,
Iwan
Hi Iwan,
Can you check the schematic and the components on your board.
You want to check that the external clock path is connected to the ADC device, as expected, or it is routed through AD9517(see the description on wiki)
Are C209 and C210 populated on your board?
Andrei
Hi Andrei,
We found the issue is in our local setup. We have made some basic mistake in our signal generator and measurements.
Really thank you for your response. They're really helpful.
Hello brother, can you inform me about your Vivado and the release version you used for this process...?
By the way, I use Vivado /SDK 2019.1 and release version No-OS (2019_R2).
Hi Dear. Abbas
yes, I used Vivado /SDK 2019.1. it working with no issues.
Abdulwahhab
Hi Abdulwahhab ,
Thank you brother, now it works fine with me in Vivado/ Vitis 2021.2.
Abbas Ali
FPGA Engineer
Hi Dear. Brother Abbas Ali
That's great and sorry for the late replay.
Abdulwahhab Essa
FPGA Engineer
Hi Dear. Brother Abbas Ali
That's great and sorry for the late replay.
Abdulwahhab Essa
FPGA Engineer