Post Go back to editing

Enable DDC in FMCDAQ2 + kc705

Hi,

I am using KC705 & FMCDAQ2 combo. I would finally move to ZC706 + FMCDAQ2

I would like enable DDC in AD9680. My preferred configuration is given in ""Table 23. DDC Example Configurations"" Chip decimation ratio is 16 ie no of virtual converters 8.
I have referred to below link.

ez.analog.com/.../412002

In case of HDL design, ""you could modify the design to M=8 ""

Does that mean I need to edit projects\daq2\common\daq2_bd.tcl? What are the other parameters to change?

""
ad_ip_instance util_cpack2 axi_ad9680_cpack { \
NUM_OF_CHANNELS 2 \
SAMPLES_PER_CHANNEL 4 \
SAMPLE_DATA_WIDTH 16 \
}
""

to

""
ad_ip_instance util_cpack2 axi_ad9680_cpack { \
NUM_OF_CHANNELS 8 \
SAMPLES_PER_CHANNEL 1 \
SAMPLE_DATA_WIDTH 16 \
}
""


our requirement is similar to ""Example 2: ADC with DDC Option (Two ADCs Plus Four DDCs)"" in AD9680 data sheet.

As i understand, we may have to reduce no of lanes to 2 from given default 4 lanes in example design to maintain minimum lane rate of >3.125Gbps.

Is there any guidelines to reduce the lane nos in HDL design? Do I need to just edit daq2_bd.tcl?

Parents
  • Hello,

    You just need to edit the daq2_bd.tcl file in the common directory. Since the architecture construction is parameterized you just need to modify the variables defined in the beginning of the file: set RX_NUM_OF_LANES 2 ; # L
                                                                                 set RX_NUM_OF_CONVERTERS 8 ; # M
                                                                                 set RX_SAMPLES_PER_FRAME 1 ; # S
                                                                                 set RX_SAMPLE_WIDTH 16 ; # N/NP

    Best Regards,

    Dan Hotoleanu

  • Hello Dan,

    In the original version (hdl_2019_r1 ) of daq2_bd.tcl I could for find the fields you mentioned so edited after referring to 

    https://github.com/hotoleanudan/hdl/tree/daq2_without_ad9144_proj/projects/daq2/kc705 

    Here line 

    ""set RX_SAMPLES_PER_CHANNEL [expr $RX_NUM_OF_LANES * 32 / ($RX_NUM_OF_CONVERTERS * $RX_SAMPLE_WIDTH)""

    in daq2_bd.tcl  results in some errors. I guess this line results in synthesis error util_cpack2.v . As per calculation this formula will result in a value of 0.5 for RX_SAMPLES_PER_CHANNEL.

    So I just changed it to 

    set RX_SAMPLES_PER_CHANNEL [expr $RX_NUM_OF_LANES * 64 / ($RX_NUM_OF_CONVERTERS * $RX_SAMPLE_WIDTH) 

    I do not have any rational for this with this.

    editing system_top.v to remove rx_data_p path I guess I am able to build the project.

Reply
  • Hello Dan,

    In the original version (hdl_2019_r1 ) of daq2_bd.tcl I could for find the fields you mentioned so edited after referring to 

    https://github.com/hotoleanudan/hdl/tree/daq2_without_ad9144_proj/projects/daq2/kc705 

    Here line 

    ""set RX_SAMPLES_PER_CHANNEL [expr $RX_NUM_OF_LANES * 32 / ($RX_NUM_OF_CONVERTERS * $RX_SAMPLE_WIDTH)""

    in daq2_bd.tcl  results in some errors. I guess this line results in synthesis error util_cpack2.v . As per calculation this formula will result in a value of 0.5 for RX_SAMPLES_PER_CHANNEL.

    So I just changed it to 

    set RX_SAMPLES_PER_CHANNEL [expr $RX_NUM_OF_LANES * 64 / ($RX_NUM_OF_CONVERTERS * $RX_SAMPLE_WIDTH) 

    I do not have any rational for this with this.

    editing system_top.v to remove rx_data_p path I guess I am able to build the project.

Children